SRP#
This module includes functions that control SRP client behavior.
This module includes functions of the Service Registration Protocol.
This module includes functions for SRP client buffers and service pool.
Functions in this module are only available when feature OPENTHREAD_CONFIG_SRP_CLIENT_BUFFERS_ENABLE is enabled.
Modules#
otSrpClientBuffersServiceEntry
Enumerations#
Specifies an SRP client item (service or host info) state.
Represents the state of the SRP server.
Represents the address mode used by the SRP server.
Typedefs#
Represents an SRP client host info.
Represents an SRP client service.
Pointer type defines the callback used by SRP client to notify user of changes/events/errors.
Pointer type defines the callback used by SRP client to notify user when it is auto-started or stopped.
Represents a SRP client service pool entry.
This opaque type represents a SRP service host.
This opaque type represents a SRP service.
The ID of a SRP service update transaction on the SRP Server.
Represents the address mode used by the SRP server.
Includes SRP server TTL configurations.
Includes SRP server LEASE and KEY-LEASE configurations.
Includes SRP server lease information of a host/service.
Includes the statistics of SRP server responses.
Handles SRP service updates.
Functions#
Starts the SRP client operation.
Stops the SRP client operation.
Indicates whether the SRP client is running or not.
Gets the socket address (IPv6 address and port number) of the SRP server which is being used by SRP client.
Sets the callback to notify caller of events/changes from SRP client.
Enables the auto-start mode.
Disables the auto-start mode.
Indicates the current state of auto-start mode (enabled or disabled).
Gets the TTL value in every record included in SRP update requests.
Sets the TTL value in every record included in SRP update requests.
Gets the default lease interval used in SRP update requests.
Sets the default lease interval used in SRP update requests.
Gets the default key lease interval used in SRP update requests.
Sets the default key lease interval used in SRP update requests.
Gets the host info.
Sets the host name label.
Enables auto host address mode.
Sets/updates the list of host IPv6 address.
Adds a service to be registered with server.
Requests a service to be unregistered with server.
Clears a service, immediately removing it from the client service list.
Gets the list of services being managed by client.
Starts the remove process of the host info and all services.
Clears all host info and all the services.
Gets the domain name being used by SRP client.
Sets the domain name to be used by SRP client.
Converts a otSrpClientItemState
to a string.
Enables/disables "service key record inclusion" mode.
Indicates whether the "service key record inclusion" mode is enabled or disabled.
Gets the string buffer to use for SRP client host name.
Gets the array of IPv6 address entries to use as SRP client host address list.
Allocates a new service entry from the pool.
Frees a previously allocated service entry.
Frees all previously allocated service entries.
Gets the string buffer for service name from a service entry.
Gets the string buffer for service instance name from a service entry.
Gets the buffer for TXT record from a service entry.
Gets the array for service subtype labels from the service entry.
Returns the domain authorized to the SRP server.
Sets the domain on the SRP server.
Returns the state of the SRP server.
Returns the port the SRP server is listening to.
Returns the address mode being used by the SRP server.
Sets the address mode to be used by the SRP server.
Returns the sequence number used with anycast address mode.
Sets the sequence number used with anycast address mode.
Enables/disables the SRP server.
Enables/disables the auto-enable mode on SRP server.
Indicates whether the auto-enable mode is enabled or disabled.
Returns SRP server TTL configuration.
Sets SRP server TTL configuration.
Returns SRP server LEASE and KEY-LEASE configurations.
Sets SRP server LEASE and KEY-LEASE configurations.
Sets the SRP service updates handler on SRP server.
Reports the result of processing a SRP update to the SRP server.
Returns the next registered host on the SRP server.
Returns the response counters of the SRP server.
Tells if the SRP service host has been deleted.
Returns the full name of the host.
Indicates whether the host matches a given host name.
Returns the addresses of given host.
Returns the LEASE and KEY-LEASE information of a given host.
Returns the next service of given host.
Indicates whether or not the SRP service has been deleted.
Returns the full service instance name of the service.
Indicates whether this service matches a given service instance name.
Returns the service instance label (first label in instance name) of the service.
Returns the full service name of the service.
Indicates whether this service matches a given service name.
Gets the number of sub-types of the service.
Gets the sub-type service name (full name) of the service at a given index.
Indicates whether or not the service has a given sub-type.
Parses a sub-type service name (full name) and extracts the sub-type label.
Returns the port of the service instance.
Returns the weight of the service instance.
Returns the priority of the service instance.
Returns the TTL of the service instance.
Returns the TXT record data of the service instance.
Returns the host which the service instance reside on.
Returns the LEASE and KEY-LEASE information of a given service.
Enumeration Documentation#
otSrpClientItemState#
otSrpClientItemState
Specifies an SRP client item (service or host info) state.
Enumerator | |
---|---|
OT_SRP_CLIENT_ITEM_STATE_TO_ADD | Item to be added/registered. |
OT_SRP_CLIENT_ITEM_STATE_ADDING | Item is being added/registered. |
OT_SRP_CLIENT_ITEM_STATE_TO_REFRESH | Item to be refreshed (re-register to renew lease). |
OT_SRP_CLIENT_ITEM_STATE_REFRESHING | Item is being refreshed. |
OT_SRP_CLIENT_ITEM_STATE_TO_REMOVE | Item to be removed. |
OT_SRP_CLIENT_ITEM_STATE_REMOVING | Item is being removed. |
OT_SRP_CLIENT_ITEM_STATE_REGISTERED | Item is registered with server. |
OT_SRP_CLIENT_ITEM_STATE_REMOVED | Item is removed. |
57
of file include/openthread/srp_client.h
otSrpServerState#
otSrpServerState
Represents the state of the SRP server.
Enumerator | |
---|---|
OT_SRP_SERVER_STATE_DISABLED | The SRP server is disabled. |
OT_SRP_SERVER_STATE_RUNNING | The SRP server is enabled and running. |
OT_SRP_SERVER_STATE_STOPPED | The SRP server is enabled but stopped. |
75
of file include/openthread/srp_server.h
otSrpServerAddressMode#
otSrpServerAddressMode
Represents the address mode used by the SRP server.
Address mode specifies how the address and port number are determined by the SRP server and how this info is published in the Thread Network Data.
Enumerator | |
---|---|
OT_SRP_SERVER_ADDRESS_MODE_UNICAST | Unicast address mode. |
OT_SRP_SERVER_ADDRESS_MODE_ANYCAST | Anycast address mode. |
88
of file include/openthread/srp_server.h
Typedef Documentation#
otSrpClientHostInfo#
typedef struct otSrpClientHostInfo otSrpClientHostInfo
Represents an SRP client host info.
79
of file include/openthread/srp_client.h
otSrpClientService#
typedef struct otSrpClientService otSrpClientService
Represents an SRP client service.
The values in this structure, including the string buffers for the names and the TXT record entries, MUST persist and stay constant after an instance of this structure is passed to OpenThread from otSrpClientAddService()
or otSrpClientRemoveService()
.
The mState
, mData
, mNext
fields are used/managed by OT core only. Their value is ignored when an instance of otSrpClientService
is passed in otSrpClientAddService()
or otSrpClientRemoveService()
or other functions. The caller does not need to set these fields.
The mLease
and mKeyLease
fields specify the desired lease and key lease intervals for this service. Zero value indicates that the interval is unspecified and then the default lease or key lease intervals from otSrpClientGetLeaseInterval()
and otSrpClientGetKeyLeaseInterval()
are used for this service. If the key lease interval (whether set explicitly or determined from the default) is shorter than the lease interval for a service, SRP client will re-use the lease interval value for key lease interval as well. For example, if in service mLease
is explicitly set to 2 days and mKeyLease
is set to zero and default key lease is set to 1 day, then when registering this service, the requested key lease for this service is also set to 2 days.
115
of file include/openthread/srp_client.h
otSrpClientCallback#
typedef void(* otSrpClientCallback) (otError aError, const otSrpClientHostInfo *aHostInfo, const otSrpClientService *aServices, const otSrpClientService *aRemovedServices, void *aContext) )(otError aError, const otSrpClientHostInfo *aHostInfo, const otSrpClientService *aServices, const otSrpClientService *aRemovedServices, void *aContext)
Pointer type defines the callback used by SRP client to notify user of changes/events/errors.
[in] | aError | The error (see above). |
[in] | aHostInfo | A pointer to host info. |
[in] | aServices | The head of linked-list containing all services (excluding the ones removed). NULL if the list is empty. |
[in] | aRemovedServices | The head of linked-list containing all removed services. NULL if the list is empty. |
[in] | aContext | A pointer to an arbitrary context (provided when callback was registered). |
This callback is invoked on a successful registration of an update (i.e., add/remove of host-info and/or some service(s)) with the SRP server, or if there is a failure or error (e.g., server rejects a update request or client times out waiting for response, etc).
In case of a successful reregistration of an update, aError
parameter would be OT_ERROR_NONE
and the host info and the full list of services is provided as input parameters to the callback. Note that host info and services each track its own state in the corresponding mState
member variable of the related data structure (the state indicating whether the host-info/service is registered or removed or still being added/removed, etc).
The list of removed services is passed as its own linked-list aRemovedServices
in the callback. Note that when the callback is invoked, the SRP client (OpenThread implementation) is done with the removed service instances listed in aRemovedServices
and no longer tracks/stores them (i.e., if from the callback we call otSrpClientGetServices()
the removed services will not be present in the returned list). Providing a separate list of removed services in the callback helps indicate to user which items are now removed and allow user to re-claim/reuse the instances.
If the server rejects an SRP update request, the DNS response code (RFC 2136) is mapped to the following errors:
(0) NOERROR Success (no error condition) -> OT_ERROR_NONE
(1) FORMERR Server unable to interpret due to format error -> OT_ERROR_PARSE
(2) SERVFAIL Server encountered an internal failure -> OT_ERROR_FAILED
(3) NXDOMAIN Name that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
(4) NOTIMP Server does not support the query type (OpCode) -> OT_ERROR_NOT_IMPLEMENTED
(5) REFUSED Server refused for policy/security reasons -> OT_ERROR_SECURITY
(6) YXDOMAIN Some name that ought not to exist, does exist -> OT_ERROR_DUPLICATED
(7) YXRRSET Some RRset that ought not to exist, does exist -> OT_ERROR_DUPLICATED
(8) NXRRSET Some RRset that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
(9) NOTAUTH Service is not authoritative for zone -> OT_ERROR_SECURITY
(10) NOTZONE A name is not in the zone -> OT_ERROR_PARSE
(20) BADNAME Bad name -> OT_ERROR_PARSE
(21) BADALG Bad algorithm -> OT_ERROR_SECURITY
(22) BADTRUN Bad truncation -> OT_ERROR_PARSE
Other response codes -> OT_ERROR_FAILED
The following errors are also possible:
OT_ERROR_RESPONSE_TIMEOUT : Timed out waiting for response from server (client would continue to retry).
OT_ERROR_INVALID_ARGS : The provided service structure is invalid (e.g., bad service name or
otDnsTxtEntry
).OT_ERROR_NO_BUFS : Insufficient buffer to prepare or send the update message.
Note that in case of any failure, the client continues the operation, i.e. it prepares and (re)transmits the SRP update message to the server, after some wait interval. The retry wait interval starts from the minimum value and is increased by the growth factor every failure up to the max value (please see configuration parameter OPENTHREAD_CONFIG_SRP_CLIENT_MIN_RETRY_WAIT_INTERVAL
and the related ones for more details).
171
of file include/openthread/srp_client.h
otSrpClientAutoStartCallback#
typedef void(* otSrpClientAutoStartCallback) (const otSockAddr *aServerSockAddr, void *aContext) )(const otSockAddr *aServerSockAddr, void *aContext)
Pointer type defines the callback used by SRP client to notify user when it is auto-started or stopped.
[in] | aServerSockAddr | A non-NULL pointer indicates SRP server was started and pointer will give the selected server socket address. A NULL pointer indicates SRP server was stopped. |
[in] | aContext | A pointer to an arbitrary context (provided when callback was registered). |
This is only used when auto-start feature OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
This callback is invoked when auto-start mode is enabled and the SRP client is either automatically started or stopped.
189
of file include/openthread/srp_client.h
otSrpClientBuffersServiceEntry#
typedef struct otSrpClientBuffersServiceEntry otSrpClientBuffersServiceEntry
Represents a SRP client service pool entry.
63
of file include/openthread/srp_client_buffers.h
otSrpServerHost#
typedef struct otSrpServerHost otSrpServerHost
This opaque type represents a SRP service host.
60
of file include/openthread/srp_server.h
otSrpServerService#
typedef struct otSrpServerService otSrpServerService
This opaque type represents a SRP service.
65
of file include/openthread/srp_server.h
otSrpServerServiceUpdateId#
typedef uint32_t otSrpServerServiceUpdateId
The ID of a SRP service update transaction on the SRP Server.
70
of file include/openthread/srp_server.h
otSrpServerAddressMode#
typedef enum otSrpServerAddressMode otSrpServerAddressMode
Represents the address mode used by the SRP server.
Address mode specifies how the address and port number are determined by the SRP server and how this info is published in the Thread Network Data.
92
of file include/openthread/srp_server.h
otSrpServerTtlConfig#
typedef struct otSrpServerTtlConfig otSrpServerTtlConfig
Includes SRP server TTL configurations.
101
of file include/openthread/srp_server.h
otSrpServerLeaseConfig#
typedef struct otSrpServerLeaseConfig otSrpServerLeaseConfig
Includes SRP server LEASE and KEY-LEASE configurations.
112
of file include/openthread/srp_server.h
otSrpServerLeaseInfo#
typedef struct otSrpServerLeaseInfo otSrpServerLeaseInfo
Includes SRP server lease information of a host/service.
123
of file include/openthread/srp_server.h
otSrpServerResponseCounters#
typedef struct otSrpServerResponseCounters otSrpServerResponseCounters
Includes the statistics of SRP server responses.
136
of file include/openthread/srp_server.h
otSrpServerServiceUpdateHandler#
typedef void(* otSrpServerServiceUpdateHandler) (otSrpServerServiceUpdateId aId, const otSrpServerHost *aHost, uint32_t aTimeout, void *aContext) )(otSrpServerServiceUpdateId aId, const otSrpServerHost *aHost, uint32_t aTimeout, void *aContext)
Handles SRP service updates.
[in] | aId | The service update transaction ID. This ID must be passed back with |
[in] | aHost | A pointer to the otSrpServerHost object which contains the SRP updates. The handler should publish/un-publish the host and each service points to this host with below rules:
|
[in] | aTimeout | The maximum time in milliseconds for the handler to process the service event. |
[in] | aContext | A pointer to application-specific context. |
Is called by the SRP server to notify that a SRP host and possibly SRP services are being updated. It is important that the SRP updates are not committed until the handler returns the result by calling otSrpServerHandleServiceUpdateResult or times out after aTimeout
.
A SRP service observer should always call otSrpServerHandleServiceUpdateResult with error code OT_ERROR_NONE immediately after receiving the update events.
A more generic handler may perform validations on the SRP host/services and rejects the SRP updates if any validation fails. For example, an Advertising Proxy should advertise (or remove) the host and services on a multicast-capable link and returns specific error code if any failure occurs.
See Also
347
of file include/openthread/srp_server.h
Function Documentation#
otSrpClientStart#
otError otSrpClientStart (otInstance * aInstance, const otSockAddr * aServerSockAddr)
Starts the SRP client operation.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aServerSockAddr | The socket address (IPv6 address and port number) of the SRP server. |
SRP client will prepare and send "SRP Update" message to the SRP server once all the following conditions are met:
The SRP client is started -
otSrpClientStart()
is called.Host name is set -
otSrpClientSetHostName()
is called.At least one host IPv6 address is set -
otSrpClientSetHostAddresses()
is called.At least one service is added -
otSrpClientAddService()
is called.
It does not matter in which order these functions are called. When all conditions are met, the SRP client will wait for a short delay before preparing an "SRP Update" message and sending it to server. This delay allows for user to add multiple services and/or IPv6 addresses before the first SRP Update message is sent (ensuring a single SRP Update is sent containing all the info). The config OPENTHREAD_CONFIG_SRP_CLIENT_UPDATE_TX_DELAY
specifies the delay interval.
215
of file include/openthread/srp_client.h
otSrpClientStop#
void otSrpClientStop (otInstance * aInstance)
Stops the SRP client operation.
[in] | aInstance | A pointer to the OpenThread instance. |
Stops any further interactions with the SRP server. Note that it does not remove or clear host info and/or list of services. It marks all services to be added/removed again once the client is (re)started.
225
of file include/openthread/srp_client.h
otSrpClientIsRunning#
bool otSrpClientIsRunning (otInstance * aInstance)
Indicates whether the SRP client is running or not.
[in] | aInstance | A pointer to the OpenThread instance. |
Returns
TRUE if the SRP client is running, FALSE otherwise.
234
of file include/openthread/srp_client.h
otSrpClientGetServerAddress#
const otSockAddr * otSrpClientGetServerAddress (otInstance * aInstance)
Gets the socket address (IPv6 address and port number) of the SRP server which is being used by SRP client.
[in] | aInstance | A pointer to the OpenThread instance. |
If the client is not running, the address is unspecified (all zero) with zero port number.
Returns
A pointer to the SRP server's socket address (is always non-NULL).
246
of file include/openthread/srp_client.h
otSrpClientSetCallback#
void otSrpClientSetCallback (otInstance * aInstance, otSrpClientCallback aCallback, void * aContext)
Sets the callback to notify caller of events/changes from SRP client.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aCallback | The callback to notify of events and changes. Can be NULL if not needed. |
[in] | aContext | An arbitrary context used with |
The SRP client allows a single callback to be registered. So consecutive calls to this function will overwrite any previously set callback functions.
258
of file include/openthread/srp_client.h
otSrpClientEnableAutoStartMode#
void otSrpClientEnableAutoStartMode (otInstance * aInstance, otSrpClientAutoStartCallback aCallback, void * aContext)
Enables the auto-start mode.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aCallback | A callback to notify when client is auto-started/stopped. Can be NULL if not needed. |
[in] | aContext | A context to be passed when invoking |
This is only available when auto-start feature OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
Config option OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_DEFAULT_MODE
specifies the default auto-start mode (whether it is enabled or disabled at the start of OT stack).
When auto-start is enabled, the SRP client will monitor the Thread Network Data to discover SRP servers and select the preferred server and automatically start and stop the client when an SRP server is detected.
There are three categories of Network Data entries indicating presence of SRP sever. They are preferred in the following order:
1) Preferred unicast entries where server address is included in the service data. If there are multiple options, the one with numerically lowest IPv6 address is preferred.
2) Anycast entries each having a seq number. A larger sequence number in the sense specified by Serial Number Arithmetic logic in RFC-1982 is considered more recent and therefore preferred. The largest seq number using serial number arithmetic is preferred if it is well-defined (i.e., the seq number is larger than all other seq numbers). If it is not well-defined, then the numerically largest seq number is preferred.
3) Unicast entries where the server address info is included in server data. If there are multiple options, the one with numerically lowest IPv6 address is preferred.
When there is a change in the Network Data entries, client will check that the currently selected server is still present in the Network Data and is still the preferred one. Otherwise the client will switch to the new preferred server or stop if there is none.
When the SRP client is explicitly started through a successful call to otSrpClientStart()
, the given SRP server address in otSrpClientStart()
will continue to be used regardless of the state of auto-start mode and whether the same SRP server address is discovered or not in the Thread Network Data. In this case, only an explicit otSrpClientStop()
call will stop the client.
298
of file include/openthread/srp_client.h
otSrpClientDisableAutoStartMode#
void otSrpClientDisableAutoStartMode (otInstance * aInstance)
Disables the auto-start mode.
[in] | aInstance | A pointer to the OpenThread instance. |
This is only available when auto-start feature OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
Disabling the auto-start mode will not stop the client if it is already running but the client stops monitoring the Thread Network Data to verify that the selected SRP server is still present in it.
Note that a call to otSrpClientStop()
will also disable the auto-start mode.
312
of file include/openthread/srp_client.h
otSrpClientIsAutoStartModeEnabled#
bool otSrpClientIsAutoStartModeEnabled (otInstance * aInstance)
Indicates the current state of auto-start mode (enabled or disabled).
[in] | aInstance | A pointer to the OpenThread instance. |
This is only available when auto-start feature OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
Returns
TRUE if the auto-start mode is enabled, FALSE otherwise.
323
of file include/openthread/srp_client.h
otSrpClientGetTtl#
uint32_t otSrpClientGetTtl (otInstance * aInstance)
Gets the TTL value in every record included in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
Note that this is the TTL requested by the SRP client. The server may choose to accept a different TTL.
By default, the TTL will equal the lease interval. Passing 0 or a value larger than the lease interval via otSrpClientSetTtl()
will also cause the TTL to equal the lease interval.
Returns
The TTL (in seconds).
337
of file include/openthread/srp_client.h
otSrpClientSetTtl#
void otSrpClientSetTtl (otInstance * aInstance, uint32_t aTtl)
Sets the TTL value in every record included in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aTtl | The TTL (in seconds). If value is zero or greater than lease interval, the TTL is set to the lease interval. |
Changing the TTL does not impact the TTL of already registered services/host-info. It only affects future SRP update messages (i.e., adding new services and/or refreshes of the existing services).
349
of file include/openthread/srp_client.h
otSrpClientGetLeaseInterval#
uint32_t otSrpClientGetLeaseInterval (otInstance * aInstance)
Gets the default lease interval used in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
The default interval is used only for otSrpClientService
instances with mLease
set to zero.
Note that this is the lease duration requested by the SRP client. The server may choose to accept a different lease interval.
Returns
The lease interval (in seconds).
363
of file include/openthread/srp_client.h
otSrpClientSetLeaseInterval#
void otSrpClientSetLeaseInterval (otInstance * aInstance, uint32_t aInterval)
Sets the default lease interval used in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aInterval | The lease interval (in seconds). If zero, the default value specified by |
The default interval is used only for otSrpClientService
instances with mLease
set to zero.
Changing the lease interval does not impact the accepted lease interval of already registered services/host-info. It only affects any future SRP update messages (i.e., adding new services and/or refreshes of the existing services).
377
of file include/openthread/srp_client.h
otSrpClientGetKeyLeaseInterval#
uint32_t otSrpClientGetKeyLeaseInterval (otInstance * aInstance)
Gets the default key lease interval used in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
The default interval is used only for otSrpClientService
instances with mKeyLease
set to zero.
Note that this is the lease duration requested by the SRP client. The server may choose to accept a different lease interval.
Returns
The key lease interval (in seconds).
391
of file include/openthread/srp_client.h
otSrpClientSetKeyLeaseInterval#
void otSrpClientSetKeyLeaseInterval (otInstance * aInstance, uint32_t aInterval)
Sets the default key lease interval used in SRP update requests.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aInterval | The key lease interval (in seconds). If zero, the default value specified by |
The default interval is used only for otSrpClientService
instances with mKeyLease
set to zero.
Changing the lease interval does not impact the accepted lease interval of already registered services/host-info. It only affects any future SRP update messages (i.e., adding new services and/or refreshes of existing services).
405
of file include/openthread/srp_client.h
otSrpClientGetHostInfo#
const otSrpClientHostInfo * otSrpClientGetHostInfo (otInstance * aInstance)
Gets the host info.
[in] | aInstance | A pointer to the OpenThread instance. |
Returns
A pointer to host info structure.
414
of file include/openthread/srp_client.h
otSrpClientSetHostName#
otError otSrpClientSetHostName (otInstance * aInstance, const char * aName)
Sets the host name label.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aName | A pointer to host name label string (MUST NOT be NULL). Pointer to the string buffer MUST persist and remain valid and constant after return from this function. |
After a successful call to this function, otSrpClientCallback
will be called to report the status of host info registration with SRP server.
The name string buffer pointed to by aName
MUST persist and stay unchanged after returning from this function. OpenThread will keep the pointer to the string.
The host name can be set before client is started or after start but before host info is registered with server (host info should be in either STATE_TO_ADD
or STATE_REMOVED
).
436
of file include/openthread/srp_client.h
otSrpClientEnableAutoHostAddress#
otError otSrpClientEnableAutoHostAddress (otInstance * aInstance)
Enables auto host address mode.
N/A | aInstance |
When enabled host IPv6 addresses are automatically set by SRP client using all the preferred unicast addresses on Thread netif excluding all link-local and mesh-local addresses. If there is no preferred address, then Mesh Local EID address is added. The SRP client will automatically re-register when/if addresses on Thread netif are updated (new addresses are added or existing addresses are removed or marked as non-preferred).
The auto host address mode can be enabled before start or during operation of SRP client except when the host info is being removed (client is busy handling a remove request from an call to otSrpClientRemoveHostAndServices()
and host info still being in either STATE_TO_REMOVE
or STATE_REMOVING
states).
After auto host address mode is enabled, it can be disabled by a call to otSrpClientSetHostAddresses()
which then explicitly sets the host addresses.
456
of file include/openthread/srp_client.h
otSrpClientSetHostAddresses#
otError otSrpClientSetHostAddresses (otInstance * aInstance, const otIp6Address * aIp6Addresses, uint8_t aNumAddresses)
Sets/updates the list of host IPv6 address.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aIp6Addresses | A pointer to the an array containing the host IPv6 addresses. |
[in] | aNumAddresses | The number of addresses in the |
Host IPv6 addresses can be set/changed before start or during operation of SRP client (e.g. to add/remove or change a previously registered host address), except when the host info is being removed (client is busy handling a remove request from an earlier call to otSrpClientRemoveHostAndServices()
and host info still being in either STATE_TO_REMOVE
or STATE_REMOVING
states).
The host IPv6 address array pointed to by aIp6Addresses
MUST persist and remain unchanged after returning from this function (with OT_ERROR_NONE
). OpenThread will save the pointer to the array.
After a successful call to this function, otSrpClientCallback
will be called to report the status of the address registration with SRP server.
Calling this function disables auto host address mode if it was previously enabled from a successful call to otSrpClientEnableAutoHostAddress()
.
484
of file include/openthread/srp_client.h
otSrpClientAddService#
otError otSrpClientAddService (otInstance * aInstance, otSrpClientService * aService)
Adds a service to be registered with server.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aService | A pointer to a |
After a successful call to this function, otSrpClientCallback
will be called to report the status of the service addition/registration with SRP server.
The otSrpClientService
instance being pointed to by aService
MUST persist and remain unchanged after returning from this function (with OT_ERROR_NONE
). OpenThread will save the pointer to the service instance.
The otSrpClientService
instance is not longer tracked by OpenThread and can be reclaimed only when
It is removed explicitly by a call to
otSrpClientRemoveService()
or removed along with other services by a call tootSrpClientRemoveHostAndServices() and only after the
otSrpClientCallback` is called indicating the service was removed. Or,A call to
otSrpClientClearHostAndServices()
which removes the host and all related services immediately.
510
of file include/openthread/srp_client.h
otSrpClientRemoveService#
otError otSrpClientRemoveService (otInstance * aInstance, otSrpClientService * aService)
Requests a service to be unregistered with server.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aService | A pointer to a |
After a successful call to this function, otSrpClientCallback
will be called to report the status of remove request with SRP server.
The otSrpClientService
instance being pointed to by aService
MUST persist and remain unchanged after returning from this function (with OT_ERROR_NONE
). OpenThread will keep the service instance during the remove process. Only after the otSrpClientCallback
is called indicating the service instance is removed from SRP client service list and can be be freed/reused.
530
of file include/openthread/srp_client.h
otSrpClientClearService#
otError otSrpClientClearService (otInstance * aInstance, otSrpClientService * aService)
Clears a service, immediately removing it from the client service list.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aService | A pointer to a |
Unlike otSrpClientRemoveService()
which sends an update message to the server to remove the service, this function clears the service from the client's service list without any interaction with the server. On a successful call to this function, the otSrpClientCallback
will NOT be called and the aService
entry can be reclaimed and re-used by the caller immediately.
Can be used along with a subsequent call to otSrpClientAddService()
(potentially reusing the same aService
entry with the same service and instance names) to update some of the parameters in an existing service.
549
of file include/openthread/srp_client.h
otSrpClientGetServices#
const otSrpClientService * otSrpClientGetServices (otInstance * aInstance)
Gets the list of services being managed by client.
[in] | aInstance | A pointer to the OpenThread instance. |
Returns
A pointer to the head of linked-list of all services or NULL if the list is empty.
558
of file include/openthread/srp_client.h
otSrpClientRemoveHostAndServices#
otError otSrpClientRemoveHostAndServices (otInstance * aInstance, bool aRemoveKeyLease, bool aSendUnregToServer)
Starts the remove process of the host info and all services.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aRemoveKeyLease | A boolean indicating whether or not the host key lease should also be removed. |
[in] | aSendUnregToServer | A boolean indicating whether to send update to server when host info is not registered. |
After returning from this function, otSrpClientCallback
will be called to report the status of remove request with SRP server.
If the host info is to be permanently removed from server, aRemoveKeyLease
should be set to true
which removes the key lease associated with host on server. Otherwise, the key lease record is kept as before, which ensures that the server holds the host name in reserve for when the client is once again able to provide and register its service(s).
The aSendUnregToServer
determines the behavior when the host info is not yet registered with the server. If aSendUnregToServer
is set to false
(which is the default/expected value) then the SRP client will immediately remove the host info and services without sending an update message to server (no need to update the server if nothing is yet registered with it). If aSendUnregToServer
is set to true
then the SRP client will send an update message to the server. Note that if the host info is registered then the value of aSendUnregToServer
does not matter and the SRP client will always send an update message to server requesting removal of all info.
One situation where aSendUnregToServer
can be useful is on a device reset/reboot, caller may want to remove any previously registered services with the server. In this case, caller can otSrpClientSetHostName()
and then request otSrpClientRemoveHostAndServices()
with aSendUnregToServer
as true
.
590
of file include/openthread/srp_client.h
otSrpClientClearHostAndServices#
void otSrpClientClearHostAndServices (otInstance * aInstance)
Clears all host info and all the services.
[in] | aInstance | A pointer to the OpenThread instance. |
Unlike otSrpClientRemoveHostAndServices()
which sends an update message to the server to remove all the info, this function clears all the info immediately without any interaction with the server.
600
of file include/openthread/srp_client.h
otSrpClientGetDomainName#
const char * otSrpClientGetDomainName (otInstance * aInstance)
Gets the domain name being used by SRP client.
[in] | aInstance | A pointer to the OpenThread instance. |
Requires OPENTHREAD_CONFIG_SRP_CLIENT_DOMAIN_NAME_API_ENABLE
to be enabled.
If domain name is not set, "default.service.arpa" will be used.
Returns
The domain name string.
613
of file include/openthread/srp_client.h
otSrpClientSetDomainName#
otError otSrpClientSetDomainName (otInstance * aInstance, const char * aName)
Sets the domain name to be used by SRP client.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aName | A pointer to the domain name string. If NULL sets it to default "default.service.arpa". |
Requires OPENTHREAD_CONFIG_SRP_CLIENT_DOMAIN_NAME_API_ENABLE
to be enabled.
If not set "default.service.arpa" will be used.
The name string buffer pointed to by aName
MUST persist and stay unchanged after returning from this function. OpenThread will keep the pointer to the string.
The domain name can be set before client is started or after start but before host info is registered with server (host info should be in either STATE_TO_ADD
or STATE_TO_REMOVE
).
634
of file include/openthread/srp_client.h
otSrpClientItemStateToString#
const char * otSrpClientItemStateToString (otSrpClientItemState aItemState)
Converts a otSrpClientItemState
to a string.
[in] | aItemState | An item state. |
Returns
A string representation of
aItemState
.
643
of file include/openthread/srp_client.h
otSrpClientSetServiceKeyRecordEnabled#
void otSrpClientSetServiceKeyRecordEnabled (otInstance * aInstance, bool aEnabled)
Enables/disables "service key record inclusion" mode.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aEnabled | TRUE to enable, FALSE to disable the "service key record inclusion" mode. |
When enabled, SRP client will include KEY record in Service Description Instructions in the SRP update messages that it sends.
Is available when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
configuration is enabled.
Note
KEY record is optional in Service Description Instruction (it is required and always included in the Host Description Instruction). The default behavior of SRP client is to not include it. This function is intended to override the default behavior for testing only.
660
of file include/openthread/srp_client.h
otSrpClientIsServiceKeyRecordEnabled#
bool otSrpClientIsServiceKeyRecordEnabled (otInstance * aInstance)
Indicates whether the "service key record inclusion" mode is enabled or disabled.
[in] | aInstance | A pointer to the OpenThread instance. |
Is available when OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
configuration is enabled.
Returns
TRUE if "service key record inclusion" mode is enabled, FALSE otherwise.
671
of file include/openthread/srp_client.h
otSrpClientBuffersGetHostNameString#
char * otSrpClientBuffersGetHostNameString (otInstance * aInstance, uint16_t * aSize)
Gets the string buffer to use for SRP client host name.
[in] | aInstance | A pointer to the OpenThread instance. |
[out] | aSize | Pointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL). |
Returns
A pointer to char buffer to use for SRP client host name.
74
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersGetHostAddressesArray#
otIp6Address * otSrpClientBuffersGetHostAddressesArray (otInstance * aInstance, uint8_t * aArrayLength)
Gets the array of IPv6 address entries to use as SRP client host address list.
[in] | aInstance | A pointer to the OpenThread instance. |
[out] | aArrayLength | Pointer to a variable to return the array length i.e., number of IPv6 address entries in the array (MUST NOT be NULL). |
Returns
A pointer to an array of
otIp6Address
entries (number of entries is returned inaArrayLength
).
85
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersAllocateService#
otSrpClientBuffersServiceEntry * otSrpClientBuffersAllocateService (otInstance * aInstance)
Allocates a new service entry from the pool.
[in] | aInstance | A pointer to the OpenThread instance. |
The returned service entry instance will be initialized as follows:
mService.mName
will point to an allocated string buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryServiceNameString()
.mService.mInstanceName
will point to an allocated string buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryInstanceNameString()
.mService.mSubTypeLabels
points to an array that is returned fromotSrpClientBuffersGetSubTypeLabelsArray()
.mService.mTxtEntries
will point tomTxtEntry
.mService.mNumTxtEntries
will be set to one.Other
mService
fields (port, priority, weight) are set to zero.mTxtEntry.mKey
is set to NULL (value is treated as already encoded).mTxtEntry.mValue
will point to an allocated buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryTxtBuffer()
.mTxtEntry.mValueLength
is set to zero.All related data/string buffers and arrays are cleared to all zero.
Returns
A pointer to the newly allocated service entry or NULL if not more entry available in the pool.
110
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersFreeService#
void otSrpClientBuffersFreeService (otInstance * aInstance, otSrpClientBuffersServiceEntry * aService)
Frees a previously allocated service entry.
[in] | aInstance | A pointer to the OpenThread instance. |
[in] | aService | A pointer to the service entry to free (MUST NOT be NULL). |
The aService
MUST be previously allocated using otSrpClientBuffersAllocateService()
and not yet freed. Otherwise the behavior of this function is undefined.
121
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersFreeAllServices#
void otSrpClientBuffersFreeAllServices (otInstance * aInstance)
Frees all previously allocated service entries.
[in] | aInstance | A pointer to the OpenThread instance. |
128
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersGetServiceEntryServiceNameString#
char * otSrpClientBuffersGetServiceEntryServiceNameString (otSrpClientBuffersServiceEntry * aEntry, uint16_t * aSize)
Gets the string buffer for service name from a service entry.
[in] | aEntry | A pointer to a previously allocated service entry (MUST NOT be NULL). |
[out] | aSize | A pointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL). |
Returns
A pointer to the string buffer.
139
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersGetServiceEntryInstanceNameString#
char * otSrpClientBuffersGetServiceEntryInstanceNameString (otSrpClientBuffersServiceEntry * aEntry, uint16_t * aSize)
Gets the string buffer for service instance name from a service entry.
[in] | aEntry | A pointer to a previously allocated service entry (MUST NOT be NULL). |
[out] | aSize | A pointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL). |
Returns
A pointer to the string buffer.
150
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersGetServiceEntryTxtBuffer#
uint8_t * otSrpClientBuffersGetServiceEntryTxtBuffer (otSrpClientBuffersServiceEntry * aEntry, uint16_t * aSize)
Gets the buffer for TXT record from a service entry.
[in] | aEntry | A pointer to a previously allocated service entry (MUST NOT be NULL). |
[out] | aSize | A pointer to a variable to return the size (number of bytes) of the buffer (MUST NOT be NULL). |
Returns
A pointer to the buffer.
160
of file include/openthread/srp_client_buffers.h
otSrpClientBuffersGetSubTypeLabelsArray#
const char ** otSrpClientBuffersGetSubTypeLabelsArray (otSrpClientBuffersServiceEntry * aEntry, uint16_t * aArrayLength)
Gets the array for service subtype labels from the service entry.
[in] | aEntry | A pointer to a previously allocated service entry (MUST NOT be NULL). |
[out] | aArrayLength | A pointer to a variable to return the array length (MUST NOT be NULL). |
Returns
A pointer to the array.
170
of file include/openthread/srp_client_buffers.h
otSrpServerGetDomain#
const char * otSrpServerGetDomain (otInstance * aInstance)
Returns the domain authorized to the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
If the domain if not set by SetDomain, "default.service.arpa." will be returned. A trailing dot is always appended even if the domain is set without it.
Returns
A pointer to the dot-joined domain string.
148
of file include/openthread/srp_server.h
otSrpServerSetDomain#
otError otSrpServerSetDomain (otInstance * aInstance, const char * aDomain)
Sets the domain on the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aDomain | The domain to be set. MUST NOT be NULL. |
A trailing dot will be appended to aDomain
if it is not already there. Should only be called before the SRP server is enabled.
164
of file include/openthread/srp_server.h
otSrpServerGetState#
otSrpServerState otSrpServerGetState (otInstance * aInstance)
Returns the state of the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The current state of the SRP server.
173
of file include/openthread/srp_server.h
otSrpServerGetPort#
uint16_t otSrpServerGetPort (otInstance * aInstance)
Returns the port the SRP server is listening to.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The port of the SRP server. It returns 0 if the server is not running.
182
of file include/openthread/srp_server.h
otSrpServerGetAddressMode#
otSrpServerAddressMode otSrpServerGetAddressMode (otInstance * aInstance)
Returns the address mode being used by the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The SRP server's address mode.
191
of file include/openthread/srp_server.h
otSrpServerSetAddressMode#
otError otSrpServerSetAddressMode (otInstance * aInstance, otSrpServerAddressMode aMode)
Sets the address mode to be used by the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aMode | The address mode to use. |
202
of file include/openthread/srp_server.h
otSrpServerGetAnycastModeSequenceNumber#
uint8_t otSrpServerGetAnycastModeSequenceNumber (otInstance * aInstance)
Returns the sequence number used with anycast address mode.
[in] | aInstance | A pointer to an OpenThread instance. |
The sequence number is included in "DNS/SRP Service Anycast Address" entry published in the Network Data.
Returns
The anycast sequence number.
213
of file include/openthread/srp_server.h
otSrpServerSetAnycastModeSequenceNumber#
otError otSrpServerSetAnycastModeSequenceNumber (otInstance * aInstance, uint8_t aSequenceNumber)
Sets the sequence number used with anycast address mode.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aSequenceNumber | The sequence number to use. |
224
of file include/openthread/srp_server.h
otSrpServerSetEnabled#
void otSrpServerSetEnabled (otInstance * aInstance, bool aEnabled)
Enables/disables the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aEnabled | A boolean to enable/disable the SRP server. |
On a Border Router, it is recommended to use otSrpServerSetAutoEnableMode()
instead.
234
of file include/openthread/srp_server.h
otSrpServerSetAutoEnableMode#
void otSrpServerSetAutoEnableMode (otInstance * aInstance, bool aEnabled)
Enables/disables the auto-enable mode on SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aEnabled | A boolean to enable/disable the auto-enable mode. |
Requires OPENTHREAD_CONFIG_BORDER_ROUTING_ENABLE
feature.
When this mode is enabled, the Border Routing Manager controls if/when to enable or disable the SRP server. SRP sever is auto-enabled if/when Border Routing is started and it is done with the initial prefix and route configurations (when the OMR and on-link prefixes are determined, advertised in emitted Router Advertisement message on infrastructure side and published in the Thread Network Data). The SRP server is auto-disabled if/when BR is stopped (e.g., if the infrastructure network interface is brought down or if BR gets detached).
This mode can be disabled by a otSrpServerSetAutoEnableMode()
call with aEnabled
set to false
or if the SRP server is explicitly enabled or disabled by a call to otSrpServerSetEnabled()
function. Disabling auto-enable mode using otSrpServerSetAutoEnableMode(false)
will not change the current state of SRP sever (e.g., if it is enabled it stays enabled).
255
of file include/openthread/srp_server.h
otSrpServerIsAutoEnableMode#
bool otSrpServerIsAutoEnableMode (otInstance * aInstance)
Indicates whether the auto-enable mode is enabled or disabled.
[in] | aInstance | A pointer to an OpenThread instance. |
Requires OPENTHREAD_CONFIG_BORDER_ROUTING_ENABLE
feature.
267
of file include/openthread/srp_server.h
otSrpServerGetTtlConfig#
void otSrpServerGetTtlConfig (otInstance * aInstance, otSrpServerTtlConfig * aTtlConfig)
Returns SRP server TTL configuration.
[in] | aInstance | A pointer to an OpenThread instance. |
[out] | aTtlConfig | A pointer to an |
275
of file include/openthread/srp_server.h
otSrpServerSetTtlConfig#
otError otSrpServerSetTtlConfig (otInstance * aInstance, const otSrpServerTtlConfig * aTtlConfig)
Sets SRP server TTL configuration.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aTtlConfig | A pointer to an |
The granted TTL will always be no greater than the max lease interval configured via otSrpServerSetLeaseConfig()
, regardless of the minimum and maximum TTL configuration.
289
of file include/openthread/srp_server.h
otSrpServerGetLeaseConfig#
void otSrpServerGetLeaseConfig (otInstance * aInstance, otSrpServerLeaseConfig * aLeaseConfig)
Returns SRP server LEASE and KEY-LEASE configurations.
[in] | aInstance | A pointer to an OpenThread instance. |
[out] | aLeaseConfig | A pointer to an |
297
of file include/openthread/srp_server.h
otSrpServerSetLeaseConfig#
otError otSrpServerSetLeaseConfig (otInstance * aInstance, const otSrpServerLeaseConfig * aLeaseConfig)
Sets SRP server LEASE and KEY-LEASE configurations.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aLeaseConfig | A pointer to an |
When a non-zero LEASE time is requested from a client, the granted value will be limited in range [aMinLease, aMaxLease]; and a non-zero KEY-LEASE will be granted in range [aMinKeyLease, aMaxKeyLease]. For zero LEASE or KEY-LEASE time, zero will be granted.
313
of file include/openthread/srp_server.h
otSrpServerSetServiceUpdateHandler#
void otSrpServerSetServiceUpdateHandler (otInstance * aInstance, otSrpServerServiceUpdateHandler aServiceHandler, void * aContext)
Sets the SRP service updates handler on SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aServiceHandler | A pointer to a service handler. Use NULL to remove the handler. |
[in] | aContext | A pointer to arbitrary context information. May be NULL if not used. |
360
of file include/openthread/srp_server.h
otSrpServerHandleServiceUpdateResult#
void otSrpServerHandleServiceUpdateResult (otInstance * aInstance, otSrpServerServiceUpdateId aId, otError aError)
Reports the result of processing a SRP update to the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aId | The service update transaction ID. This should be the same ID provided via |
[in] | aError | An error to be returned to the SRP server. Use OT_ERROR_DUPLICATED to represent DNS name conflicts. |
The Service Update Handler should call this function to return the result of its processing of a SRP update.
376
of file include/openthread/srp_server.h
otSrpServerGetNextHost#
const otSrpServerHost * otSrpServerGetNextHost (otInstance * aInstance, const otSrpServerHost * aHost)
Returns the next registered host on the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aHost | A pointer to current host; use NULL to get the first host. |
Returns
A pointer to the registered host. NULL, if no more hosts can be found.
386
of file include/openthread/srp_server.h
otSrpServerGetResponseCounters#
const otSrpServerResponseCounters * otSrpServerGetResponseCounters (otInstance * aInstance)
Returns the response counters of the SRP server.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
A pointer to the response counters of the SRP server.
395
of file include/openthread/srp_server.h
otSrpServerHostIsDeleted#
bool otSrpServerHostIsDeleted (const otSrpServerHost * aHost)
Tells if the SRP service host has been deleted.
[in] | aHost | A pointer to the SRP service host. |
A SRP service host can be deleted but retains its name for future uses. In this case, the host instance is not removed from the SRP server/registry.
Returns
TRUE if the host has been deleted, FALSE if not.
407
of file include/openthread/srp_server.h
otSrpServerHostGetFullName#
const char * otSrpServerHostGetFullName (const otSrpServerHost * aHost)
Returns the full name of the host.
[in] | aHost | A pointer to the SRP service host. |
Returns
A pointer to the null-terminated host name string.
416
of file include/openthread/srp_server.h
otSrpServerHostMatchesFullName#
bool otSrpServerHostMatchesFullName (const otSrpServerHost * aHost, const char * aFullName)
Indicates whether the host matches a given host name.
[in] | aHost | A pointer to the SRP service host. |
[in] | aFullName | A full host name. |
DNS name matches are performed using a case-insensitive string comparison (i.e., "Abc" and "aBc" are considered to be the same).
430
of file include/openthread/srp_server.h
otSrpServerHostGetAddresses#
const otIp6Address * otSrpServerHostGetAddresses (const otSrpServerHost * aHost, uint8_t * aAddressesNum)
Returns the addresses of given host.
[in] | aHost | A pointer to the SRP service host. |
[out] | aAddressesNum | A pointer to where we should output the number of the addresses to. |
Returns
A pointer to the array of IPv6 Address.
440
of file include/openthread/srp_server.h
otSrpServerHostGetLeaseInfo#
void otSrpServerHostGetLeaseInfo (const otSrpServerHost * aHost, otSrpServerLeaseInfo * aLeaseInfo)
Returns the LEASE and KEY-LEASE information of a given host.
[in] | aHost | A pointer to the SRP server host. |
[out] | aLeaseInfo | A pointer to where to output the LEASE and KEY-LEASE information. |
448
of file include/openthread/srp_server.h
otSrpServerHostGetNextService#
const otSrpServerService * otSrpServerHostGetNextService (const otSrpServerHost * aHost, const otSrpServerService * aService)
Returns the next service of given host.
[in] | aHost | A pointer to the SRP service host. |
[in] | aService | A pointer to current SRP service instance; use NULL to get the first service. |
Returns
A pointer to the next service or NULL if there is no more services.
458
of file include/openthread/srp_server.h
otSrpServerServiceIsDeleted#
bool otSrpServerServiceIsDeleted (const otSrpServerService * aService)
Indicates whether or not the SRP service has been deleted.
[in] | aService | A pointer to the SRP service. |
A SRP service can be deleted but retains its name for future uses. In this case, the service instance is not removed from the SRP server/registry. It is guaranteed that all services are deleted if the host is deleted.
Returns
TRUE if the service has been deleted, FALSE if not.
472
of file include/openthread/srp_server.h
otSrpServerServiceGetInstanceName#
const char * otSrpServerServiceGetInstanceName (const otSrpServerService * aService)
Returns the full service instance name of the service.
[in] | aService | A pointer to the SRP service. |
Returns
A pointer to the null-terminated service instance name string.
481
of file include/openthread/srp_server.h
otSrpServerServiceMatchesInstanceName#
bool otSrpServerServiceMatchesInstanceName (const otSrpServerService * aService, const char * aInstanceName)
Indicates whether this service matches a given service instance name.
[in] | aService | A pointer to the SRP service. |
[in] | aInstanceName | The service instance name. |
DNS name matches are performed using a case-insensitive string comparison (i.e., "Abc" and "aBc" are considered to be the same).
495
of file include/openthread/srp_server.h
otSrpServerServiceGetInstanceLabel#
const char * otSrpServerServiceGetInstanceLabel (const otSrpServerService * aService)
Returns the service instance label (first label in instance name) of the service.
[in] | aService | A pointer to the SRP service. |
Returns
A pointer to the null-terminated service instance label string..
504
of file include/openthread/srp_server.h
otSrpServerServiceGetServiceName#
const char * otSrpServerServiceGetServiceName (const otSrpServerService * aService)
Returns the full service name of the service.
[in] | aService | A pointer to the SRP service. |
Returns
A pointer to the null-terminated service name string.
513
of file include/openthread/srp_server.h
otSrpServerServiceMatchesServiceName#
bool otSrpServerServiceMatchesServiceName (const otSrpServerService * aService, const char * aServiceName)
Indicates whether this service matches a given service name.
[in] | aService | A pointer to the SRP service. |
[in] | aServiceName | The service name. |
DNS name matches are performed using a case-insensitive string comparison (i.e., "Abc" and "aBc" are considered to be the same).
527
of file include/openthread/srp_server.h
otSrpServerServiceGetNumberOfSubTypes#
uint16_t otSrpServerServiceGetNumberOfSubTypes (const otSrpServerService * aService)
Gets the number of sub-types of the service.
[in] | aService | A pointer to the SRP service. |
Returns
The number of sub-types of
aService
.
536
of file include/openthread/srp_server.h
otSrpServerServiceGetSubTypeServiceNameAt#
const char * otSrpServerServiceGetSubTypeServiceNameAt (const otSrpServerService * aService, uint16_t aIndex)
Gets the sub-type service name (full name) of the service at a given index.
[in] | aService | A pointer to the SRP service. |
[in] | aIndex | The index to get. |
The full service name for a sub-type service follows "<sub-label>._sub.<service-labels>.<domain>.".
Returns
A pointer to sub-type service name at
aIndex
, orNULL
if no sub-type at this index.
548
of file include/openthread/srp_server.h
otSrpServerServiceHasSubTypeServiceName#
bool otSrpServerServiceHasSubTypeServiceName (const otSrpServerService * aService, const char * aSubTypeServiceName)
Indicates whether or not the service has a given sub-type.
[in] | aService | A pointer to the SRP service. |
[in] | aSubTypeServiceName | The sub-type service name (full name) to check. |
DNS name matches are performed using a case-insensitive string comparison (i.e., "Abc" and "aBc" are considered to be the same).
562
of file include/openthread/srp_server.h
otSrpServerParseSubTypeServiceName#
otError otSrpServerParseSubTypeServiceName (const char * aSubTypeServiceName, char * aLabel, uint8_t aLabelSize)
Parses a sub-type service name (full name) and extracts the sub-type label.
[in] | aSubTypeServiceName | A sub-type service name (full name). |
[out] | aLabel | A pointer to a buffer to copy the extracted sub-type label. |
[in] | aLabelSize | Maximum size of |
The full service name for a sub-type service follows "<sub-label>._sub.<service-labels>.<domain>.".
578
of file include/openthread/srp_server.h
otSrpServerServiceGetPort#
uint16_t otSrpServerServiceGetPort (const otSrpServerService * aService)
Returns the port of the service instance.
[in] | aService | A pointer to the SRP service. |
Returns
The port of the service.
587
of file include/openthread/srp_server.h
otSrpServerServiceGetWeight#
uint16_t otSrpServerServiceGetWeight (const otSrpServerService * aService)
Returns the weight of the service instance.
[in] | aService | A pointer to the SRP service. |
Returns
The weight of the service.
596
of file include/openthread/srp_server.h
otSrpServerServiceGetPriority#
uint16_t otSrpServerServiceGetPriority (const otSrpServerService * aService)
Returns the priority of the service instance.
[in] | aService | A pointer to the SRP service. |
Returns
The priority of the service.
605
of file include/openthread/srp_server.h
otSrpServerServiceGetTtl#
uint32_t otSrpServerServiceGetTtl (const otSrpServerService * aService)
Returns the TTL of the service instance.
[in] | aService | A pointer to the SRP service. |
Returns
The TTL of the service instance..
614
of file include/openthread/srp_server.h
otSrpServerServiceGetTxtData#
const uint8_t * otSrpServerServiceGetTxtData (const otSrpServerService * aService, uint16_t * aDataLength)
Returns the TXT record data of the service instance.
[in] | aService | A pointer to the SRP service. |
[out] | aDataLength | A pointer to return the TXT record data length. MUST NOT be NULL. |
Returns
A pointer to the buffer containing the TXT record data (the TXT data length is returned in
aDataLength
).
624
of file include/openthread/srp_server.h
otSrpServerServiceGetHost#
const otSrpServerHost * otSrpServerServiceGetHost (const otSrpServerService * aService)
Returns the host which the service instance reside on.
[in] | aService | A pointer to the SRP service. |
Returns
A pointer to the host instance.
633
of file include/openthread/srp_server.h
otSrpServerServiceGetLeaseInfo#
void otSrpServerServiceGetLeaseInfo (const otSrpServerService * aService, otSrpServerLeaseInfo * aLeaseInfo)
Returns the LEASE and KEY-LEASE information of a given service.
[in] | aService | A pointer to the SRP server service. |
[out] | aLeaseInfo | A pointer to where to output the LEASE and KEY-LEASE information. |
641
of file include/openthread/srp_server.h