Represents the count of queries, responses, failures handled by upstream DNS server.

Requires OPENTHREAD_CONFIG_DNS_UPSTREAM_QUERY_ENABLE.

Public Attributes#

uint32_t

The number of queries forwarded.

uint32_t

The number of responses forwarded.

uint32_t

The number of upstream DNS failures.

Public Attribute Documentation#

mQueries#

uint32_t otUpstreamDnsCounters::mQueries

The number of queries forwarded.


Definition at line 150 of file include/openthread/dnssd_server.h

mResponses#

uint32_t otUpstreamDnsCounters::mResponses

The number of responses forwarded.


Definition at line 151 of file include/openthread/dnssd_server.h

mFailures#

uint32_t otUpstreamDnsCounters::mFailures

The number of upstream DNS failures.


Definition at line 152 of file include/openthread/dnssd_server.h