Instance#
This module includes functions that control the OpenThread Instance.
Typedefs#
Represents the OpenThread instance structure.
Represents a bit-field indicating specific state/configuration that has changed.
Pointer is called to notify certain configuration or state changes within OpenThread.
Functions#
Initializes the OpenThread library.
Initializes the static single instance of the OpenThread library.
Initializes the OpenThread instance.
Gets the instance identifier.
Indicates whether or not the instance is valid/initialized.
Disables the OpenThread library.
Returns the current instance uptime (in msec).
Returns the current instance uptime as a human-readable string.
Registers a callback to indicate when certain configuration or state changes within OpenThread.
Removes a callback to indicate when certain configuration or state changes within OpenThread.
Triggers a platform reset.
Triggers a platform reset to bootloader mode, if supported.
Deletes all the settings stored on non-volatile memory, and then triggers a platform reset.
Resets the internal states of the OpenThread radio stack.
Erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
Gets the OpenThread version string.
Gets the OpenThread radio version string.
Macros#
Recommended size for string representation of uptime.
IPv6 address was added.
IPv6 address was removed.
Role (disabled, detached, child, router, leader) changed.
The link-local address changed.
The mesh-local address changed.
RLOC was added.
RLOC was removed.
Partition ID changed.
Thread Key Sequence changed.
Thread Network Data changed.
Child was added.
Child was removed.
Subscribed to a IPv6 multicast address.
Unsubscribed from a IPv6 multicast address.
Thread network channel changed.
Thread network PAN Id changed.
Thread network name changed.
Thread network extended PAN ID changed.
Network key changed.
PSKc changed.
Security Policy changed.
Channel Manager new pending Thread channel changed.
Supported channel mask changed.
Commissioner state changed.
Thread network interface state changed.
Backbone Router state changed.
Local Backbone Router configuration changed.
Joiner state changed.
Active Operational Dataset changed.
Pending Operational Dataset changed.
The state of NAT64 translator changed.
Parent link quality changed.
Typedef Documentation#
otChangedFlags#
typedef uint32_t otChangedFlags
Represents a bit-field indicating specific state/configuration that has changed.
See OT_CHANGED_* definitions.
otStateChangedCallback#
typedef void(* otStateChangedCallback) (otChangedFlags aFlags, void *aContext) )(otChangedFlags aFlags, void *aContext)
Pointer is called to notify certain configuration or state changes within OpenThread.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| [in] | aFlags | A bit-field indicating specific state that has changed. See | |
| [in] | aContext | A pointer to application-specific context. |
Function Documentation#
otInstanceInit#
otInstance * otInstanceInit (void * aInstanceBuffer, size_t * aInstanceBufferSize)
Initializes the OpenThread library.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void * | [in] | aInstanceBuffer | The buffer for OpenThread to use for allocating the otInstance structure. |
| size_t * | [inout] | aInstanceBufferSize | On input, the size of aInstanceBuffer. On output, if not enough space for otInstance, the number of bytes required for otInstance. |
Initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.
Is available and can only be used when support for multiple OpenThread instances is enabled.
Returns
A pointer to the new OpenThread instance.
See Also
otInstanceInitSingle#
otInstance * otInstanceInitSingle (void )
Initializes the static single instance of the OpenThread library.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.
Is available and can only be used when support for multiple OpenThread instances is disabled.
Returns
A pointer to the single OpenThread instance.
otInstanceInitMultiple#
otInstance * otInstanceInitMultiple (uint8_t aIdx)
Initializes the OpenThread instance.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| uint8_t | [in] | aIdx | The index of the OpenThread instance to initialize. |
This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread. This method utilizes static buffer to initialize the OpenThread instance.
This function is available and can only be used when support for multiple OpenThread static instances is enabled (OPENTHREAD_CONFIG_MULTIPLE_STATIC_INSTANCE_ENABLE)
Returns
A pointer to the new OpenThread instance.
otInstanceGetId#
uint32_t otInstanceGetId (otInstance * aInstance)
Gets the instance identifier.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | N/A | aInstance |
The instance identifier is set to a random value when the instance is constructed, and then its value will not change after initialization.
Returns
The instance identifier.
otInstanceIsInitialized#
bool otInstanceIsInitialized (otInstance * aInstance)
Indicates whether or not the instance is valid/initialized.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
The instance is considered valid if it is acquired and initialized using either otInstanceInitSingle() (in single instance case) or otInstanceInit() (in multi instance case). A subsequent call to otInstanceFinalize() causes the instance to be considered as uninitialized.
Returns
TRUE if the given instance is valid/initialized, FALSE otherwise.
otInstanceFinalize#
void otInstanceFinalize (otInstance * aInstance)
Disables the OpenThread library.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Call this function when OpenThread is no longer in use.
otInstanceGetUptime#
uint64_t otInstanceGetUptime (otInstance * aInstance)
Returns the current instance uptime (in msec).
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Requires OPENTHREAD_CONFIG_UPTIME_ENABLE to be enabled.
The uptime is given as number of milliseconds since OpenThread instance was initialized.
Returns
The uptime (number of milliseconds).
otInstanceGetUptimeAsString#
void otInstanceGetUptimeAsString (otInstance * aInstance, char * aBuffer, uint16_t aSize)
Returns the current instance uptime as a human-readable string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| char * | [out] | aBuffer | A pointer to a char array to output the string. |
| uint16_t | [in] | aSize | The size of |
Requires OPENTHREAD_CONFIG_UPTIME_ENABLE to be enabled.
The string follows the format "<hh>:<mm>:<ss>.<mmmm>" for hours, minutes, seconds and millisecond (if uptime is shorter than one day) or "<dd>d.<hh>:<mm>:<ss>.<mmmm>" (if longer than a day).
If the resulting string does not fit in aBuffer (within its aSize characters), the string will be truncated but the outputted string is always null-terminated.
otSetStateChangedCallback#
otError otSetStateChangedCallback (otInstance * aInstance, otStateChangedCallback aCallback, void * aContext)
Registers a callback to indicate when certain configuration or state changes within OpenThread.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otStateChangedCallback | [in] | aCallback | A pointer to a function that is called with certain configuration or state changes. |
| void * | [in] | aContext | A pointer to application-specific context. |
otRemoveStateChangeCallback#
void otRemoveStateChangeCallback (otInstance * aInstance, otStateChangedCallback aCallback, void * aContext)
Removes a callback to indicate when certain configuration or state changes within OpenThread.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
| otStateChangedCallback | [in] | aCallback | A pointer to a function that is called with certain configuration or state changes. |
| void * | [in] | aContext | A pointer to application-specific context. |
otInstanceReset#
void otInstanceReset (otInstance * aInstance)
Triggers a platform reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
The reset process ensures that all the OpenThread state/info (stored in volatile memory) is erased. Note that the otPlatformReset does not erase any persistent state/info saved in non-volatile memory.
otInstanceResetToBootloader#
otError otInstanceResetToBootloader (otInstance * aInstance)
Triggers a platform reset to bootloader mode, if supported.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Requires OPENTHREAD_CONFIG_PLATFORM_BOOTLOADER_MODE_ENABLE.
otInstanceFactoryReset#
void otInstanceFactoryReset (otInstance * aInstance)
Deletes all the settings stored on non-volatile memory, and then triggers a platform reset.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
otInstanceResetRadioStack#
void otInstanceResetRadioStack (otInstance * aInstance)
Resets the internal states of the OpenThread radio stack.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Callbacks and configurations are preserved.
This API is only available under radio builds (OPENTHREAD_RADIO = 1).
otInstanceErasePersistentInfo#
otError otInstanceErasePersistentInfo (otInstance * aInstance)
Erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Erase is successful only if the device is in disabled state/role.
otGetVersionString#
const char * otGetVersionString (void )
Gets the OpenThread version string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| void | N/A |
Returns
A pointer to the OpenThread version.
otGetRadioVersionString#
const char * otGetRadioVersionString (otInstance * aInstance)
Gets the OpenThread radio version string.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| otInstance * | [in] | aInstance | A pointer to an OpenThread instance. |
Returns
A pointer to the OpenThread radio version.