Represents the counters of packets forwarded via Border Routing.

Public Attributes#

The counters for inbound unicast.

The counters for inbound multicast.

The counters for outbound unicast.

The counters for outbound multicast.

The counters for inbound Internet when DHCPv6 PD enabled.

The counters for outbound Internet when DHCPv6 PD enabled.

uint32_t

The number of received RA packets.

uint32_t

The number of RA packets successfully transmitted.

uint32_t

The number of RA packets failed to transmit.

uint32_t

The number of received RS packets.

uint32_t

The number of RS packets successfully transmitted.

uint32_t

The number of RS packets failed to transmit.

Public Attribute Documentation#

mInboundUnicast#

otPacketsAndBytes otBorderRoutingCounters::mInboundUnicast

The counters for inbound unicast.


Definition at line 907 of file include/openthread/ip6.h

mInboundMulticast#

otPacketsAndBytes otBorderRoutingCounters::mInboundMulticast

The counters for inbound multicast.


Definition at line 908 of file include/openthread/ip6.h

mOutboundUnicast#

otPacketsAndBytes otBorderRoutingCounters::mOutboundUnicast

The counters for outbound unicast.


Definition at line 909 of file include/openthread/ip6.h

mOutboundMulticast#

otPacketsAndBytes otBorderRoutingCounters::mOutboundMulticast

The counters for outbound multicast.


Definition at line 910 of file include/openthread/ip6.h

mInboundInternet#

otPacketsAndBytes otBorderRoutingCounters::mInboundInternet

The counters for inbound Internet when DHCPv6 PD enabled.


Definition at line 911 of file include/openthread/ip6.h

mOutboundInternet#

otPacketsAndBytes otBorderRoutingCounters::mOutboundInternet

The counters for outbound Internet when DHCPv6 PD enabled.


Definition at line 912 of file include/openthread/ip6.h

mRaRx#

uint32_t otBorderRoutingCounters::mRaRx

The number of received RA packets.


Definition at line 913 of file include/openthread/ip6.h

mRaTxSuccess#

uint32_t otBorderRoutingCounters::mRaTxSuccess

The number of RA packets successfully transmitted.


Definition at line 914 of file include/openthread/ip6.h

mRaTxFailure#

uint32_t otBorderRoutingCounters::mRaTxFailure

The number of RA packets failed to transmit.


Definition at line 915 of file include/openthread/ip6.h

mRsRx#

uint32_t otBorderRoutingCounters::mRsRx

The number of received RS packets.


Definition at line 916 of file include/openthread/ip6.h

mRsTxSuccess#

uint32_t otBorderRoutingCounters::mRsTxSuccess

The number of RS packets successfully transmitted.


Definition at line 917 of file include/openthread/ip6.h

mRsTxFailure#

uint32_t otBorderRoutingCounters::mRsTxFailure

The number of RS packets failed to transmit.


Definition at line 918 of file include/openthread/ip6.h