Represents a Joiner Discerner.
Public Attributes#
uint64_t
Discerner value (the lowest mLength
bits specify the discerner).
uint8_t
Length (number of bits) - must be non-zero and at most OT_JOINER_MAX_DISCERNER_LENGTH
.
Public Attribute Documentation#
mValue#
uint64_t otJoinerDiscerner::mValue
Discerner value (the lowest mLength
bits specify the discerner).
Definition at line
80
of file include/openthread/joiner.h
mLength#
uint8_t otJoinerDiscerner::mLength
Length (number of bits) - must be non-zero and at most OT_JOINER_MAX_DISCERNER_LENGTH
.
Definition at line
81
of file include/openthread/joiner.h