Commissioner#
This module includes functions for the Thread Commissioner role.
Modules#
Enumerations#
Defines the Commissioner State.
Defines a Joiner Event on the Commissioner.
Defines a Joiner Info Type.
Typedefs#
Defines the Commissioner State.
Defines a Joiner Event on the Commissioner.
Represents the steering data.
Represents a Commissioning Dataset.
Represents a Joiner PSKd.
Defines a Joiner Info Type.
Represents a Joiner Info.
Pointer is called whenever the commissioner state changes.
Pointer is called whenever the joiner state changes.
Pointer is called when the Commissioner receives an Energy Report.
Pointer is called when the Commissioner receives a PAN ID Conflict message.
Functions#
Enables the Thread Commissioner role.
Disables the Thread Commissioner role.
Returns the Commissioner Id.
Sets the Commissioner Id.
Adds a Joiner entry.
Adds a Joiner entry with a given Joiner Discerner value.
Get joiner info at aIterator position.
Removes a Joiner entry.
Removes a Joiner entry.
Gets the Provisioning URL.
Sets the Provisioning URL.
Sends an Announce Begin message.
Sends an Energy Scan Query message.
Sends a PAN ID Query message.
Sends MGMT_COMMISSIONER_GET.
Sends MGMT_COMMISSIONER_SET.
Returns the Commissioner Session ID.
Returns the Commissioner State.
Macros#
Minimum size of the Commissioning Passphrase.
Maximum size of the Commissioning Passphrase.
Max size (number of chars) in Provisioning URL string (excludes null char).
Max steering data length (bytes)
Maximum string length of a Joiner PSKd (does not include null char).
Enumeration Documentation#
otCommissionerState#
otCommissionerState
Defines the Commissioner State.
Enumerator | |
---|---|
OT_COMMISSIONER_STATE_DISABLED | Commissioner role is disabled. |
OT_COMMISSIONER_STATE_PETITION | Currently petitioning to become a Commissioner. |
OT_COMMISSIONER_STATE_ACTIVE | Commissioner role is active. |
62
of file include/openthread/commissioner.h
otCommissionerJoinerEvent#
otCommissionerJoinerEvent
Defines a Joiner Event on the Commissioner.
Enumerator | |
---|---|
OT_COMMISSIONER_JOINER_START | |
OT_COMMISSIONER_JOINER_CONNECTED | |
OT_COMMISSIONER_JOINER_FINALIZE | |
OT_COMMISSIONER_JOINER_END | |
OT_COMMISSIONER_JOINER_REMOVED |
73
of file include/openthread/commissioner.h
otJoinerInfoType#
otJoinerInfoType
Defines a Joiner Info Type.
Enumerator | |
---|---|
OT_JOINER_INFO_TYPE_ANY | Accept any Joiner (no EUI64 or Discerner is specified). |
OT_JOINER_INFO_TYPE_EUI64 | Joiner EUI-64 is specified ( |
OT_JOINER_INFO_TYPE_DISCERNER | Joiner Discerner is specified ( |
132
of file include/openthread/commissioner.h
Typedef Documentation#
otCommissionerState#
typedef enum otCommissionerState otCommissionerState
Defines the Commissioner State.
67
of file include/openthread/commissioner.h
otCommissionerJoinerEvent#
typedef enum otCommissionerJoinerEvent otCommissionerJoinerEvent
Defines a Joiner Event on the Commissioner.
80
of file include/openthread/commissioner.h
otSteeringData#
typedef struct otSteeringData otSteeringData
Represents the steering data.
97
of file include/openthread/commissioner.h
otCommissioningDataset#
typedef struct otCommissioningDataset otCommissioningDataset
Represents a Commissioning Dataset.
115
of file include/openthread/commissioner.h
otJoinerPskd#
typedef struct otJoinerPskd otJoinerPskd
Represents a Joiner PSKd.
126
of file include/openthread/commissioner.h
otJoinerInfoType#
typedef enum otJoinerInfoType otJoinerInfoType
Defines a Joiner Info Type.
137
of file include/openthread/commissioner.h
otJoinerInfo#
typedef struct otJoinerInfo otJoinerInfo
Represents a Joiner Info.
153
of file include/openthread/commissioner.h
otCommissionerStateCallback#
typedef void(* otCommissionerStateCallback) (otCommissionerState aState, void *aContext) )(otCommissionerState aState, void *aContext)
Pointer is called whenever the commissioner state changes.
[in] | aState | The Commissioner state. |
[in] | aContext | A pointer to application-specific context. |
162
of file include/openthread/commissioner.h
otCommissionerJoinerCallback#
typedef void(* otCommissionerJoinerCallback) (otCommissionerJoinerEvent aEvent, const otJoinerInfo *aJoinerInfo, const otExtAddress *aJoinerId, void *aContext) )(otCommissionerJoinerEvent aEvent, const otJoinerInfo *aJoinerInfo, const otExtAddress *aJoinerId, void *aContext)
Pointer is called whenever the joiner state changes.
[in] | aEvent | The joiner event type. |
[in] | aJoinerInfo | A pointer to the Joiner Info. |
[in] | aJoinerId | A pointer to the Joiner ID (if not known, it will be NULL). |
[in] | aContext | A pointer to application-specific context. |
173
of file include/openthread/commissioner.h
otCommissionerEnergyReportCallback#
typedef void(* otCommissionerEnergyReportCallback) (uint32_t aChannelMask, const uint8_t *aEnergyList, uint8_t aEnergyListLength, void *aContext) )(uint32_t aChannelMask, const uint8_t *aEnergyList, uint8_t aEnergyListLength, void *aContext)
Pointer is called when the Commissioner receives an Energy Report.
[in] | aChannelMask | The channel mask value. |
[in] | aEnergyList | A pointer to the energy measurement list. |
[in] | aEnergyListLength | Number of entries in |
[in] | aContext | A pointer to application-specific context. |
370
of file include/openthread/commissioner.h
otCommissionerPanIdConflictCallback#
typedef void(* otCommissionerPanIdConflictCallback) (uint16_t aPanId, uint32_t aChannelMask, void *aContext) )(uint16_t aPanId, uint32_t aChannelMask, void *aContext)
Pointer is called when the Commissioner receives a PAN ID Conflict message.
[in] | aPanId | The PAN ID value. |
[in] | aChannelMask | The channel mask value. |
[in] | aContext | A pointer to application-specific context. |
411
of file include/openthread/commissioner.h
Function Documentation#
otCommissionerStart#
otError otCommissionerStart (otInstance * aInstance, otCommissionerStateCallback aStateCallback, otCommissionerJoinerCallback aJoinerCallback, void * aCallbackContext)
Enables the Thread Commissioner role.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aStateCallback | A pointer to a function that is called when the commissioner state changes. |
[in] | aJoinerCallback | A pointer to a function that is called with a joiner event occurs. |
[in] | aCallbackContext | A pointer to application-specific context. |
191
of file include/openthread/commissioner.h
otCommissionerStop#
otError otCommissionerStop (otInstance * aInstance)
Disables the Thread Commissioner role.
[in] | aInstance | A pointer to an OpenThread instance. |
205
of file include/openthread/commissioner.h
otCommissionerGetId#
const char * otCommissionerGetId (otInstance * aInstance)
Returns the Commissioner Id.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The Commissioner Id.
215
of file include/openthread/commissioner.h
otCommissionerSetId#
otError otCommissionerSetId (otInstance * aInstance, const char * aId)
Sets the Commissioner Id.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aId | A pointer to a string character array. Must be null terminated. |
228
of file include/openthread/commissioner.h
otCommissionerAddJoiner#
otError otCommissionerAddJoiner (otInstance * aInstance, const otExtAddress * aEui64, const char * aPskd, uint32_t aTimeout)
Adds a Joiner entry.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aEui64 | A pointer to the Joiner's IEEE EUI-64 or NULL for any Joiner. |
[in] | aPskd | A pointer to the PSKd. |
[in] | aTimeout | A time after which a Joiner is automatically removed, in seconds. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
246
of file include/openthread/commissioner.h
otCommissionerAddJoinerWithDiscerner#
otError otCommissionerAddJoinerWithDiscerner (otInstance * aInstance, const otJoinerDiscerner * aDiscerner, const char * aPskd, uint32_t aTimeout)
Adds a Joiner entry with a given Joiner Discerner value.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aDiscerner | A pointer to the Joiner Discerner. |
[in] | aPskd | A pointer to the PSKd. |
[in] | aTimeout | A time after which a Joiner is automatically removed, in seconds. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
267
of file include/openthread/commissioner.h
otCommissionerGetNextJoinerInfo#
otError otCommissionerGetNextJoinerInfo (otInstance * aInstance, uint16_t * aIterator, otJoinerInfo * aJoiner)
Get joiner info at aIterator position.
[in] | aInstance | A pointer to instance. |
[inout] | aIterator | A pointer to the Joiner Info iterator context. |
[out] | aJoiner | A reference to Joiner info. |
283
of file include/openthread/commissioner.h
otCommissionerRemoveJoiner#
otError otCommissionerRemoveJoiner (otInstance * aInstance, const otExtAddress * aEui64)
Removes a Joiner entry.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aEui64 | A pointer to the Joiner's IEEE EUI-64 or NULL for any Joiner. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
299
of file include/openthread/commissioner.h
otCommissionerRemoveJoinerWithDiscerner#
otError otCommissionerRemoveJoinerWithDiscerner (otInstance * aInstance, const otJoinerDiscerner * aDiscerner)
Removes a Joiner entry.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aDiscerner | A pointer to the Joiner Discerner. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
315
of file include/openthread/commissioner.h
otCommissionerGetProvisioningUrl#
const char * otCommissionerGetProvisioningUrl (otInstance * aInstance)
Gets the Provisioning URL.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
A pointer to the URL string.
325
of file include/openthread/commissioner.h
otCommissionerSetProvisioningUrl#
otError otCommissionerSetProvisioningUrl (otInstance * aInstance, const char * aProvisioningUrl)
Sets the Provisioning URL.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aProvisioningUrl | A pointer to the Provisioning URL (may be NULL to set as empty string). |
337
of file include/openthread/commissioner.h
otCommissionerAnnounceBegin#
otError otCommissionerAnnounceBegin (otInstance * aInstance, uint32_t aChannelMask, uint8_t aCount, uint16_t aPeriod, const otIp6Address * aAddress)
Sends an Announce Begin message.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aChannelMask | The channel mask value. |
[in] | aCount | The number of Announcement messages per channel. |
[in] | aPeriod | The time between two successive MLE Announce transmissions (in milliseconds). |
[in] | aAddress | A pointer to the IPv6 destination. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
355
of file include/openthread/commissioner.h
otCommissionerEnergyScan#
otError otCommissionerEnergyScan (otInstance * aInstance, uint32_t aChannelMask, uint8_t aCount, uint16_t aPeriod, uint16_t aScanDuration, const otIp6Address * aAddress, otCommissionerEnergyReportCallback aCallback, void * aContext)
Sends an Energy Scan Query message.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aChannelMask | The channel mask value. |
[in] | aCount | The number of energy measurements per channel. |
[in] | aPeriod | The time between energy measurements (milliseconds). |
[in] | aScanDuration | The scan duration for each energy measurement (milliseconds). |
[in] | aAddress | A pointer to the IPv6 destination. |
[in] | aCallback | A pointer to a function called on receiving an Energy Report message. |
[in] | aContext | A pointer to application-specific context. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
394
of file include/openthread/commissioner.h
otCommissionerPanIdQuery#
otError otCommissionerPanIdQuery (otInstance * aInstance, uint16_t aPanId, uint32_t aChannelMask, const otIp6Address * aAddress, otCommissionerPanIdConflictCallback aCallback, void * aContext)
Sends a PAN ID Query message.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aPanId | The PAN ID to query. |
[in] | aChannelMask | The channel mask value. |
[in] | aAddress | A pointer to the IPv6 destination. |
[in] | aCallback | A pointer to a function called on receiving a PAN ID Conflict message. |
[in] | aContext | A pointer to application-specific context. |
Note
Only use this after successfully starting the Commissioner role with otCommissionerStart().
430
of file include/openthread/commissioner.h
otCommissionerSendMgmtGet#
otError otCommissionerSendMgmtGet (otInstance * aInstance, const uint8_t * aTlvs, uint8_t aLength)
Sends MGMT_COMMISSIONER_GET.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aTlvs | A pointer to TLVs. |
[in] | aLength | The length of TLVs. |
449
of file include/openthread/commissioner.h
otCommissionerSendMgmtSet#
otError otCommissionerSendMgmtSet (otInstance * aInstance, const otCommissioningDataset * aDataset, const uint8_t * aTlvs, uint8_t aLength)
Sends MGMT_COMMISSIONER_SET.
[in] | aInstance | A pointer to an OpenThread instance. |
[in] | aDataset | A pointer to commissioning dataset. |
[in] | aTlvs | A pointer to TLVs. |
[in] | aLength | The length of TLVs. |
464
of file include/openthread/commissioner.h
otCommissionerGetSessionId#
uint16_t otCommissionerGetSessionId (otInstance * aInstance)
Returns the Commissioner Session ID.
[in] | aInstance | A pointer to an OpenThread instance. |
Returns
The current commissioner session id.
477
of file include/openthread/commissioner.h
otCommissionerGetState#
otCommissionerState otCommissionerGetState (otInstance * aInstance)
Returns the Commissioner State.
[in] | aInstance | A pointer to an OpenThread instance. |
489
of file include/openthread/commissioner.h
Macro Definition Documentation#
OT_COMMISSIONING_PASSPHRASE_MIN_SIZE#
#define OT_COMMISSIONING_PASSPHRASE_MIN_SIZEValue:
6
Minimum size of the Commissioning Passphrase.
82
of file include/openthread/commissioner.h
OT_COMMISSIONING_PASSPHRASE_MAX_SIZE#
#define OT_COMMISSIONING_PASSPHRASE_MAX_SIZEValue:
255
Maximum size of the Commissioning Passphrase.
83
of file include/openthread/commissioner.h
OT_PROVISIONING_URL_MAX_SIZE#
#define OT_PROVISIONING_URL_MAX_SIZEValue:
64
Max size (number of chars) in Provisioning URL string (excludes null char).
85
of file include/openthread/commissioner.h
OT_STEERING_DATA_MAX_LENGTH#
#define OT_STEERING_DATA_MAX_LENGTHValue:
16
Max steering data length (bytes)
87
of file include/openthread/commissioner.h
OT_JOINER_MAX_PSKD_LENGTH#
#define OT_JOINER_MAX_PSKD_LENGTHValue:
32
Maximum string length of a Joiner PSKd (does not include null char).
117
of file include/openthread/commissioner.h