Represents a Joiner Info.

Public Attributes#

Joiner EUI64 (when mType is OT_JOINER_INFO_TYPE_EUI64)

Joiner Discerner (when mType is OT_JOINER_INFO_TYPE_DISCERNER)

union otJoinerInfo::@0

Shared fields.

Joiner PSKd.

uint32_t

Joiner expiration time in msec.

Public Attribute Documentation#

mType#

otJoinerInfoType otJoinerInfo::mType

Joiner type.


Definition at line 145 of file include/openthread/commissioner.h

mEui64#

otExtAddress otJoinerInfo::mEui64

Joiner EUI64 (when mType is OT_JOINER_INFO_TYPE_EUI64)


Definition at line 148 of file include/openthread/commissioner.h

mDiscerner#

otJoinerDiscerner otJoinerInfo::mDiscerner

Joiner Discerner (when mType is OT_JOINER_INFO_TYPE_DISCERNER)


Definition at line 149 of file include/openthread/commissioner.h

mSharedId#

union otJoinerInfo::@0 otJoinerInfo::mSharedId

Shared fields.


Definition at line 150 of file include/openthread/commissioner.h

mPskd#

otJoinerPskd otJoinerInfo::mPskd

Joiner PSKd.


Definition at line 151 of file include/openthread/commissioner.h

mExpirationTime#

uint32_t otJoinerInfo::mExpirationTime

Joiner expiration time in msec.


Definition at line 152 of file include/openthread/commissioner.h