Represents a Commissioning Dataset.

Public Attributes#

uint16_t

Border Router RLOC16.

uint16_t

Commissioner Session Id.

uint16_t

Joiner UDP Port.

bool

TRUE if Border Router RLOC16 is set, FALSE otherwise.

bool

TRUE if Commissioner Session Id is set, FALSE otherwise.

bool

TRUE if Steering Data is set, FALSE otherwise.

bool

TRUE if Joiner UDP Port is set, FALSE otherwise.

bool

TRUE if the Dataset contains any extra unknown sub-TLV, FALSE otherwise.

Public Attribute Documentation#

mLocator#

uint16_t otCommissioningDataset::mLocator

Border Router RLOC16.


Definition at line 105 of file include/openthread/commissioner.h

mSessionId#

uint16_t otCommissioningDataset::mSessionId

Commissioner Session Id.


Definition at line 106 of file include/openthread/commissioner.h

mSteeringData#

otSteeringData otCommissioningDataset::mSteeringData

Steering Data.


Definition at line 107 of file include/openthread/commissioner.h

mJoinerUdpPort#

uint16_t otCommissioningDataset::mJoinerUdpPort

Joiner UDP Port.


Definition at line 108 of file include/openthread/commissioner.h

mIsLocatorSet#

bool otCommissioningDataset::mIsLocatorSet

TRUE if Border Router RLOC16 is set, FALSE otherwise.


Definition at line 110 of file include/openthread/commissioner.h

mIsSessionIdSet#

bool otCommissioningDataset::mIsSessionIdSet

TRUE if Commissioner Session Id is set, FALSE otherwise.


Definition at line 111 of file include/openthread/commissioner.h

mIsSteeringDataSet#

bool otCommissioningDataset::mIsSteeringDataSet

TRUE if Steering Data is set, FALSE otherwise.


Definition at line 112 of file include/openthread/commissioner.h

mIsJoinerUdpPortSet#

bool otCommissioningDataset::mIsJoinerUdpPortSet

TRUE if Joiner UDP Port is set, FALSE otherwise.


Definition at line 113 of file include/openthread/commissioner.h

mHasExtraTlv#

bool otCommissioningDataset::mHasExtraTlv

TRUE if the Dataset contains any extra unknown sub-TLV, FALSE otherwise.


Definition at line 114 of file include/openthread/commissioner.h