You are viewing documentation for version:
PDFHolds diagnostic information for a Thread Child.
Public Attributes#
IEEE 802.15.4 Extended Address.
uint32_t
Seconds since last heard.
uint16_t
Frame error rate (0xffff->100%). Requires error tracking feature.
uint16_t
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
uint16_t
Number of queued messages for the child.
uint16_t
Supervision interval (in seconds).
bool
Is child CSL synchronized.
Public Attribute Documentation#
mExtAddress#
otExtAddress otChildInfo::mExtAddress
IEEE 802.15.4 Extended Address.
mTimeout#
uint32_t otChildInfo::mTimeout
Timeout.
mAge#
uint32_t otChildInfo::mAge
Seconds since last heard.
mConnectionTime#
uint64_t otChildInfo::mConnectionTime
Seconds since attach.
mRloc16#
uint16_t otChildInfo::mRloc16
RLOC16.
mChildId#
uint16_t otChildInfo::mChildId
Child ID.
mNetworkDataVersion#
uint8_t otChildInfo::mNetworkDataVersion
Network Data Version.
mLinkQualityIn#
uint8_t otChildInfo::mLinkQualityIn
Link Quality In.
mAverageRssi
int8_t otChildInfo::mAverageRssi
Average RSSI.
mLastRssi
int8_t otChildInfo::mLastRssi
Last observed RSSI.
mFrameErrorRate#
uint16_t otChildInfo::mFrameErrorRate
Frame error rate (0xffff->100%). Requires error tracking feature.
mMessageErrorRate#
uint16_t otChildInfo::mMessageErrorRate
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
mQueuedMessageCnt#
uint16_t otChildInfo::mQueuedMessageCnt
Number of queued messages for the child.
mSupervisionInterval#
uint16_t otChildInfo::mSupervisionInterval
Supervision interval (in seconds).
mVersion#
uint8_t otChildInfo::mVersion
MLE version.
mRxOnWhenIdle#
bool otChildInfo::mRxOnWhenIdle
rx-on-when-idle
mFullThreadDevice#
bool otChildInfo::mFullThreadDevice
Full Thread Device.
mFullNetworkData#
bool otChildInfo::mFullNetworkData
Full Network Data.
mIsStateRestoring#
bool otChildInfo::mIsStateRestoring
Is in restoring state.
mIsCslSynced#
bool otChildInfo::mIsCslSynced
Is child CSL synchronized.