Includes the statistics of SRP server responses.

Public Attributes#

uint32_t

The number of successful responses.

uint32_t

The number of server failure responses.

uint32_t

The number of format error responses.

uint32_t

The number of 'name exists' responses.

uint32_t

The number of refused responses.

uint32_t

The number of other responses.

Public Attribute Documentation#

mSuccess#

uint32_t otSrpServerResponseCounters::mSuccess

The number of successful responses.


Definition at line 140 of file include/openthread/srp_server.h

mServerFailure#

uint32_t otSrpServerResponseCounters::mServerFailure

The number of server failure responses.


Definition at line 141 of file include/openthread/srp_server.h

mFormatError#

uint32_t otSrpServerResponseCounters::mFormatError

The number of format error responses.


Definition at line 142 of file include/openthread/srp_server.h

mNameExists#

uint32_t otSrpServerResponseCounters::mNameExists

The number of 'name exists' responses.


Definition at line 143 of file include/openthread/srp_server.h

mRefused#

uint32_t otSrpServerResponseCounters::mRefused

The number of refused responses.


Definition at line 144 of file include/openthread/srp_server.h

mOther#

uint32_t otSrpServerResponseCounters::mOther

The number of other responses.


Definition at line 145 of file include/openthread/srp_server.h