Represents a TCP endpoint.

A TCP endpoint acts an endpoint of TCP connection. It can be used to initiate TCP connections, and, once a TCP connection is established, send data to and receive data from the connection peer.

The application should not inspect the fields of this structure directly; it should only interact with it via the TCP API functions whose signatures are provided in this file.

Public Attributes#

uint8_t
uint64_t
union otTcpEndpoint::@24
struct otTcpEndpoint *

A pointer to the next TCP endpoint (internal use only)

void *

A pointer to application-specific context.

"Established" callback function

"Send done" callback function

"Forward progress" callback function

"Receive available" callback function

"Disconnected" callback function

uint32_t

Public Attribute Documentation#

mSize#

uint8_t otTcpEndpoint::mSize[OT_TCP_ENDPOINT_TCB_SIZE_BASE+OT_TCP_ENDPOINT_TCB_NUM_PTR *sizeof(void *)]

mAlign#

uint64_t otTcpEndpoint::mAlign

mTcb#

union otTcpEndpoint::@24 otTcpEndpoint::mTcb

mNext#

struct otTcpEndpoint* otTcpEndpoint::mNext

A pointer to the next TCP endpoint (internal use only)


mContext#

void* otTcpEndpoint::mContext

A pointer to application-specific context.


mEstablishedCallback#

otTcpEstablished otTcpEndpoint::mEstablishedCallback

"Established" callback function


mSendDoneCallback#

otTcpSendDone otTcpEndpoint::mSendDoneCallback

"Send done" callback function


mForwardProgressCallback#

otTcpForwardProgress otTcpEndpoint::mForwardProgressCallback

"Forward progress" callback function


mReceiveAvailableCallback#

otTcpReceiveAvailable otTcpEndpoint::mReceiveAvailableCallback

"Receive available" callback function


mDisconnectedCallback#

otTcpDisconnected otTcpEndpoint::mDisconnectedCallback

"Disconnected" callback function


mTimers#

uint32_t otTcpEndpoint::mTimers[4]

mReceiveLinks#

otLinkedBuffer otTcpEndpoint::mReceiveLinks[2]

mSockAddr#

otSockAddr otTcpEndpoint::mSockAddr

mPendingCallbacks#

uint8_t otTcpEndpoint::mPendingCallbacks