Represents a UDP socket.
Public Attributes#
The local IPv6 socket address.
The peer IPv6 socket address.
A function pointer to the application callback.
void *
A pointer to application-specific context.
void *
A handle to platform's UDP.
struct otUdpSocket *
A pointer to the next UDP socket (internal use only).
Public Attribute Documentation#
mSockName#
otSockAddr otUdpSocket::mSockName
The local IPv6 socket address.
Definition at line
126
of file include/openthread/udp.h
mPeerName#
otSockAddr otUdpSocket::mPeerName
The peer IPv6 socket address.
Definition at line
127
of file include/openthread/udp.h
mHandler#
otUdpReceive otUdpSocket::mHandler
A function pointer to the application callback.
Definition at line
128
of file include/openthread/udp.h
mContext#
void* otUdpSocket::mContext
A pointer to application-specific context.
Definition at line
129
of file include/openthread/udp.h
mHandle#
void* otUdpSocket::mHandle
A handle to platform's UDP.
Definition at line
130
of file include/openthread/udp.h
mNext#
struct otUdpSocket* otUdpSocket::mNext
A pointer to the next UDP socket (internal use only).
Definition at line
131
of file include/openthread/udp.h