Events#

APIs related to events.

Enumerations#

enum
RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT = 0
RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT
RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT
RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT
RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT
RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT
RAIL_EVENT_RX_SYNC1_DETECT_SHIFT
RAIL_EVENT_RX_SYNC2_DETECT_SHIFT
RAIL_EVENT_RX_FRAME_ERROR_SHIFT
RAIL_EVENT_RX_FIFO_FULL_SHIFT
RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT
RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT
RAIL_EVENT_RX_TIMEOUT_SHIFT
RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT
RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT
RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT
RAIL_EVENT_RX_PACKET_ABORTED_SHIFT
RAIL_EVENT_RX_FILTER_PASSED_SHIFT
RAIL_EVENT_RX_TIMING_LOST_SHIFT
RAIL_EVENT_RX_TIMING_DETECT_SHIFT
RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT
RAIL_EVENT_ZWAVE_BEAM_SHIFT
RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT
RAIL_EVENT_TX_PACKET_SENT_SHIFT
RAIL_EVENT_TXACK_PACKET_SENT_SHIFT
RAIL_EVENT_TX_ABORTED_SHIFT
RAIL_EVENT_TXACK_ABORTED_SHIFT
RAIL_EVENT_TX_BLOCKED_SHIFT
RAIL_EVENT_TXACK_BLOCKED_SHIFT
RAIL_EVENT_TX_UNDERFLOW_SHIFT
RAIL_EVENT_TXACK_UNDERFLOW_SHIFT
RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT
RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT
RAIL_EVENT_TX_CCA_RETRY_SHIFT
RAIL_EVENT_TX_START_CCA_SHIFT
RAIL_EVENT_TX_STARTED_SHIFT
RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT
RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT
RAIL_EVENT_CONFIG_SCHEDULED_SHIFT
RAIL_EVENT_SCHEDULER_STATUS_SHIFT
RAIL_EVENT_CAL_NEEDED_SHIFT
RAIL_EVENT_RF_SENSED_SHIFT
RAIL_EVENT_PA_PROTECTION_SHIFT
RAIL_EVENT_SIGNAL_DETECTED_SHIFT
RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT
RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT
RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT
RAIL_EVENT_THERMISTOR_DONE_SHIFT
RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT
RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT
RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT
}

RAIL events passed to the event callback.

Functions#

RAIL_ConfigEvents(RAIL_Handle_t railHandle, RAIL_Events_t mask, RAIL_Events_t events)

Configure radio events.

Macros#

#define
RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT

Shift position of RAIL_EVENT_SCHEDULED_TX_STARTED bit.

#define
RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT

Shift position of RAIL_EVENT_RX_DUTY_CYCLE_RX_END bit.

#define
RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT
#define
RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_MFM_TX_BUFFER_DONE bit.

#define

A value representing no events.

#define
RAIL_EVENT_RSSI_AVERAGE_DONE (1ULL << RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT)

Occurs when the hardware-averaged RSSI is done in response to RAIL_StartAverageRssi() to indicate that the hardware has completed averaging.

#define
RAIL_EVENT_RX_ACK_TIMEOUT (1ULL << RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT)

Occurs when the ACK timeout expires while waiting to receive the sync word of an expected ACK.

#define
RAIL_EVENT_RX_FIFO_ALMOST_FULL (1ULL << RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT)

Keeps occurring as long as the number of bytes in the receive FIFO exceeds the configured threshold value.

#define
RAIL_EVENT_RX_PACKET_RECEIVED (1ULL << RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT)

Occurs whenever a packet is received with RAIL_RX_PACKET_READY_SUCCESS or RAIL_RX_PACKET_READY_CRC_ERROR.

#define
RAIL_EVENT_RX_PREAMBLE_LOST (1ULL << RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT)

Occurs when the radio has lost a preamble.

#define
RAIL_EVENT_RX_PREAMBLE_DETECT (1ULL << RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT)

Occurs when the radio has detected a preamble.

#define
RAIL_EVENT_RX_SYNC1_DETECT (1ULL << RAIL_EVENT_RX_SYNC1_DETECT_SHIFT)

Occurs when the first sync word is detected.

#define
RAIL_EVENT_RX_SYNC2_DETECT (1ULL << RAIL_EVENT_RX_SYNC2_DETECT_SHIFT)

Occurs when the second sync word is detected.

#define
RAIL_EVENT_RX_FRAME_ERROR (1ULL << RAIL_EVENT_RX_FRAME_ERROR_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_CRC_ERROR which only happens after any filtering has passed.

#define
RAIL_EVENT_RX_FIFO_FULL (1ULL << RAIL_EVENT_RX_FIFO_FULL_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs coincident to a receive packet completion event in which the receive FIFO or any supplemental packet metadata FIFO (see Data Management) are full and further packet reception is jeopardized.

#define
RAIL_EVENT_RX_FIFO_OVERFLOW (1ULL << RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_OVERFLOW due to overflowing the receive FIFO or any supplemental packet metadata FIFO (see Data Management).

#define
RAIL_EVENT_RX_ADDRESS_FILTERED (1ULL << RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_FILTERED because its address does not match the filtering settings.

#define
RAIL_EVENT_RX_TIMEOUT (1ULL << RAIL_EVENT_RX_TIMEOUT_SHIFT)

Occurs when an RX event times out.

#define
RAIL_EVENT_SCHEDULED_RX_STARTED (1ULL << RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT)

Occurs when a scheduled RX begins turning on the transmitter.

#define
RAIL_EVENT_SCHEDULED_TX_STARTED (1ULL << RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT)

Occurs when a scheduled TX begins turning on the transmitter.

#define
RAIL_EVENT_RX_SCHEDULED_RX_END (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT)

Occurs when the scheduled RX window ends.

#define
RAIL_EVENT_RX_SCHEDULED_RX_MISSED (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT)

Occurs when start of a scheduled receive is missed.

#define
RAIL_EVENT_RX_PACKET_ABORTED (1ULL << RAIL_EVENT_RX_PACKET_ABORTED_SHIFT)

Occurs when a receive is aborted during filtering with RAIL_RX_PACKET_ABORT_FORMAT or after filtering with RAIL_RX_PACKET_ABORT_ABORTED for reasons other than address filtering mismatch (which triggers RAIL_EVENT_RX_ADDRESS_FILTERED instead).

#define
RAIL_EVENT_RX_FILTER_PASSED (1ULL << RAIL_EVENT_RX_FILTER_PASSED_SHIFT)

Occurs when the packet has passed any configured address and frame filtering options.

#define
RAIL_EVENT_RX_TIMING_LOST (1ULL << RAIL_EVENT_RX_TIMING_LOST_SHIFT)

Occurs when the modem timing is lost.

#define
RAIL_EVENT_RX_TIMING_DETECT (1ULL << RAIL_EVENT_RX_TIMING_DETECT_SHIFT)

Occurs when the modem timing is detected.

#define
RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE (1ULL << RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT)

Occurs when RX Channel Hopping is enabled and channel hopping finishes receiving on the last channel in its sequence.

#define
RAIL_EVENT_RX_DUTY_CYCLE_RX_END (1ULL << RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT)

Occurs during RX duty cycle mode when the radio finishes its time in receive mode.

#define
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND (1ULL << RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT)

Indicate a Data Request is received when using IEEE 802.15.4 functionality.

#define
RAIL_EVENT_ZWAVE_BEAM (1ULL << RAIL_EVENT_ZWAVE_BEAM_SHIFT)

Indicate a Z-Wave Beam Request relevant to the node was received.

#define
RAIL_EVENT_MFM_TX_BUFFER_DONE (1ULL << RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT)

Indicate a MFM buffer has completely transmitted.

#define
RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND (1ULL << RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT)

Indicate a request for populating Z-Wave LR ACK packet.

#define

The mask representing all events that determine the end of a received packet.

#define
RAIL_EVENT_TX_FIFO_ALMOST_EMPTY (1ULL << RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT)

Occurs when the number of bytes in the transmit FIFO falls below the configured threshold value.

#define
RAIL_EVENT_TX_PACKET_SENT (1ULL << RAIL_EVENT_TX_PACKET_SENT_SHIFT)

Occurs after a packet has been transmitted.

#define
RAIL_EVENT_TXACK_PACKET_SENT (1ULL << RAIL_EVENT_TXACK_PACKET_SENT_SHIFT)

Occurs after an ACK packet has been transmitted.

#define
RAIL_EVENT_TX_ABORTED (1ULL << RAIL_EVENT_TX_ABORTED_SHIFT)

Occurs when a transmit is aborted by the user.

#define
RAIL_EVENT_TXACK_ABORTED (1ULL << RAIL_EVENT_TXACK_ABORTED_SHIFT)

Occurs when an ACK transmit is aborted by the user.

#define
RAIL_EVENT_TX_BLOCKED (1ULL << RAIL_EVENT_TX_BLOCKED_SHIFT)

Occurs when a transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

#define
RAIL_EVENT_TXACK_BLOCKED (1ULL << RAIL_EVENT_TXACK_BLOCKED_SHIFT)

Occurs when an ACK transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

#define
RAIL_EVENT_TX_UNDERFLOW (1ULL << RAIL_EVENT_TX_UNDERFLOW_SHIFT)

Occurs when the transmit buffer underflows.

#define
RAIL_EVENT_TXACK_UNDERFLOW (1ULL << RAIL_EVENT_TXACK_UNDERFLOW_SHIFT)

Occurs when the ACK transmit buffer underflows.

#define
RAIL_EVENT_TX_CHANNEL_CLEAR (1ULL << RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) succeeds.

#define
RAIL_EVENT_TX_CHANNEL_BUSY (1ULL << RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) fails.

#define
RAIL_EVENT_TX_CCA_RETRY (1ULL << RAIL_EVENT_TX_CCA_RETRY_SHIFT)

Occurs during CSMA or LBT when an individual Clear Channel Assessment (CCA) check fails, but there are more tries needed before the overall operation completes.

#define
RAIL_EVENT_TX_START_CCA (1ULL << RAIL_EVENT_TX_START_CCA_SHIFT)

Occurs when the receiver is activated to perform a Clear Channel Assessment (CCA) check.

#define
RAIL_EVENT_TX_STARTED (1ULL << RAIL_EVENT_TX_STARTED_SHIFT)

Occurs when the radio starts transmitting a normal packet on the air.

#define

A value to pass as RAIL_GetTxTimePreambleStart() totalPacketBytes parameter to retrieve the RAIL_EVENT_TX_STARTED timestamp.

#define
RAIL_EVENT_TX_SCHEDULED_TX_MISSED (1ULL << RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT)

Occurs when the start of a scheduled transmit is missed.

#define

A mask representing all events that determine the end of a transmitted packet.

#define

A mask representing all events that determine the end of a transmitted ACK packet.

#define
RAIL_EVENT_CONFIG_UNSCHEDULED (1ULL << RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT)

Occurs when the scheduler switches away from this configuration.

#define
RAIL_EVENT_CONFIG_SCHEDULED (1ULL << RAIL_EVENT_CONFIG_SCHEDULED_SHIFT)

Occurs when the scheduler switches to this configuration.

#define
RAIL_EVENT_SCHEDULER_STATUS (1ULL << RAIL_EVENT_SCHEDULER_STATUS_SHIFT)

Occurs when the scheduler has a status to report.

#define
RAIL_EVENT_CAL_NEEDED (1ULL << RAIL_EVENT_CAL_NEEDED_SHIFT)

Occurs when the application needs to run a calibration, as determined by the RAIL library.

#define
RAIL_EVENT_RF_SENSED (1ULL << RAIL_EVENT_RF_SENSED_SHIFT)

Occurs when RF energy is sensed from the radio.

#define
RAIL_EVENT_PA_PROTECTION (1ULL << RAIL_EVENT_PA_PROTECTION_SHIFT)

Occurs when PA protection circuit kicks in.

#define
RAIL_EVENT_SIGNAL_DETECTED (1ULL << RAIL_EVENT_SIGNAL_DETECTED_SHIFT)

Occurs after enabling the signal detection using RAIL_BLE_EnableSignalDetection or RAIL_IEEE802154_EnableSignalDetection when a signal is detected.

#define
RAIL_EVENT_IEEE802154_MODESWITCH_START (1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT)

Occurs when a Wi-SUN mode switch packet has been received, after switching to the new PHY.

#define
RAIL_EVENT_IEEE802154_MODESWITCH_END (1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT)

Occurs when switching back to the original base PHY in effect prior to the Wi-SUN mode switch reception.

#define
RAIL_EVENT_DETECT_RSSI_THRESHOLD (1ULL << RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT)

Occurs when the sampled RSSI is above the threshold set by RAIL_SetRssiDetectThreshold().

#define
RAIL_EVENT_THERMISTOR_DONE (1ULL << RAIL_EVENT_THERMISTOR_DONE_SHIFT)

Occurs when the thermistor has finished its measurement in response to RAIL_StartThermistorMeasurement().

#define
RAIL_EVENT_TX_BLOCKED_TOO_HOT (1ULL << RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT)

Occurs when a Tx has been blocked because of temperature exceeding the safety threshold.

#define
RAIL_EVENT_TEMPERATURE_TOO_HOT (1ULL << RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT)

Occurs when die internal temperature exceeds the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

#define
RAIL_EVENT_TEMPERATURE_COOL_DOWN (1ULL << RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT)

Occurs when die internal temperature falls below the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

#define
RAIL_EVENTS_ALL 0xFFFFFFFFFFFFFFFFULL

A value representing all possible events.

Enumeration Documentation#

RAIL_Events_t#

RAIL_Events_t

RAIL events passed to the event callback.

More than one event may be indicated due to interrupt latency.

Enumerator
RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT

Shift position of RAIL_EVENT_RSSI_AVERAGE_DONE bit.

RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT

Shift position of RAIL_EVENT_RX_ACK_TIMEOUT bit.

RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_ALMOST_FULL bit.

RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT

Shift position of RAIL_EVENT_RX_PACKET_RECEIVED bit.

RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT

Shift position of RAIL_EVENT_RX_PREAMBLE_LOST bit.

RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_PREAMBLE_DETECT bit.

RAIL_EVENT_RX_SYNC1_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_SYNC1_DETECT bit.

RAIL_EVENT_RX_SYNC2_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_SYNC2_DETECT bit.

RAIL_EVENT_RX_FRAME_ERROR_SHIFT

Shift position of RAIL_EVENT_RX_FRAME_ERROR bit.

RAIL_EVENT_RX_FIFO_FULL_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_FULL bit.

RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_OVERFLOW bit.

RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT

Shift position of RAIL_EVENT_RX_ADDRESS_FILTERED bit.

RAIL_EVENT_RX_TIMEOUT_SHIFT

Shift position of RAIL_EVENT_RX_TIMEOUT bit.

RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT

Shift position of RAIL_EVENT_SCHEDULED_RX_STARTED bit.

RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT

Shift position of RAIL_EVENT_RX_SCHEDULED_RX_END bit.

RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT

Shift position of RAIL_EVENT_RX_SCHEDULED_RX_MISSED bit.

RAIL_EVENT_RX_PACKET_ABORTED_SHIFT

Shift position of RAIL_EVENT_RX_PACKET_ABORTED bit.

RAIL_EVENT_RX_FILTER_PASSED_SHIFT

Shift position of RAIL_EVENT_RX_FILTER_PASSED bit.

RAIL_EVENT_RX_TIMING_LOST_SHIFT

Shift position of RAIL_EVENT_RX_TIMING_LOST bit.

RAIL_EVENT_RX_TIMING_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_TIMING_DETECT bit.

RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT

Shift position of RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE bit.

RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND bit.

RAIL_EVENT_ZWAVE_BEAM_SHIFT

Shift position of RAIL_EVENT_ZWAVE_BEAM bit.

RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT

Shift position of RAIL_EVENT_TX_FIFO_ALMOST_EMPTY bit.

RAIL_EVENT_TX_PACKET_SENT_SHIFT

Shift position of RAIL_EVENT_TX_PACKET_SENT bit.

RAIL_EVENT_TXACK_PACKET_SENT_SHIFT

Shift position of RAIL_EVENT_TXACK_PACKET_SENT bit.

RAIL_EVENT_TX_ABORTED_SHIFT

Shift position of RAIL_EVENT_TX_ABORTED bit.

RAIL_EVENT_TXACK_ABORTED_SHIFT

Shift position of RAIL_EVENT_TXACK_ABORTED bit.

RAIL_EVENT_TX_BLOCKED_SHIFT

Shift position of RAIL_EVENT_TX_BLOCKED bit.

RAIL_EVENT_TXACK_BLOCKED_SHIFT

Shift position of RAIL_EVENT_TXACK_BLOCKED bit.

RAIL_EVENT_TX_UNDERFLOW_SHIFT

Shift position of RAIL_EVENT_TX_UNDERFLOW bit.

RAIL_EVENT_TXACK_UNDERFLOW_SHIFT

Shift position of RAIL_EVENT_TXACK_UNDERFLOW bit.

RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT

Shift position of RAIL_EVENT_TX_CHANNEL_CLEAR bit.

RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT

Shift position of RAIL_EVENT_TX_CHANNEL_BUSY bit.

RAIL_EVENT_TX_CCA_RETRY_SHIFT

Shift position of RAIL_EVENT_TX_CCA_RETRY bit.

RAIL_EVENT_TX_START_CCA_SHIFT

Shift position of RAIL_EVENT_TX_START_CCA bit.

RAIL_EVENT_TX_STARTED_SHIFT

Shift position of RAIL_EVENT_TX_STARTED bit.

RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT

Shift position of RAIL_EVENT_TX_SCHEDULED_TX_MISSED bit.

RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT

Shift position of RAIL_EVENT_CONFIG_UNSCHEDULED bit.

RAIL_EVENT_CONFIG_SCHEDULED_SHIFT

Shift position of RAIL_EVENT_CONFIG_SCHEDULED bit.

RAIL_EVENT_SCHEDULER_STATUS_SHIFT

Shift position of RAIL_EVENT_SCHEDULER_STATUS bit.

RAIL_EVENT_CAL_NEEDED_SHIFT

Shift position of RAIL_EVENT_CAL_NEEDED bit.

RAIL_EVENT_RF_SENSED_SHIFT

Shift position of RAIL_EVENT_RF_SENSED bit.

RAIL_EVENT_PA_PROTECTION_SHIFT

Shift position of RAIL_EVENT_PA_PROTECTION bit.

RAIL_EVENT_SIGNAL_DETECTED_SHIFT

Shift position of RAIL_EVENT_SIGNAL_DETECTED bit.

RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT

Shift position of RAIL_EVENT_IEEE802154_MODESWITCH_START bit.

RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT

Shift position of RAIL_EVENT_IEEE802154_MODESWITCH_END bit.

RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT

Shift position of RAIL_EVENT_DETECT_RSSI_THRESHOLD bit.

RAIL_EVENT_THERMISTOR_DONE_SHIFT

Shift position of RAIL_EVENT_THERMISTOR_DONE bit.

RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT

Shift position of RAIL_EVENT_TX_BLOCKED_TOO_HOT bit.

RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT

Shift position of RAIL_EVENT_TEMPERATURE_TOO_HOT bit.

RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT

Shift position of RAIL_EVENT_TEMPERATURE_COOL_DOWN bit.


Function Documentation#

RAIL_ConfigEvents#

RAIL_Status_t RAIL_ConfigEvents (RAIL_Handle_t railHandle, RAIL_Events_t mask, RAIL_Events_t events)

Configure radio events.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_Events_t[in]mask

A bitmask of events to configure.

RAIL_Events_t[in]events

A bitmask of events to trigger RAIL_Config_t::eventsCallback For a full list of available callbacks, see RAIL_EVENT_* set of defines.

Returns

  • Status code indicating success of the function call.

Sets up which radio interrupts generate a RAIL event. The full list of options is in RAIL_Events_t.


Macro Definition Documentation#

RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT#

#define RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT
Value:
RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT

Shift position of RAIL_EVENT_SCHEDULED_TX_STARTED bit.


RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT#

#define RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT
Value:
RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT

Shift position of RAIL_EVENT_RX_DUTY_CYCLE_RX_END bit.


RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT#

#define RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT
Value:
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT bit.


RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT#

#define RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT
Value:
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_MFM_TX_BUFFER_DONE bit.


RAIL_EVENTS_NONE#

#define RAIL_EVENTS_NONE
Value:
0ULL

A value representing no events.


RAIL_EVENT_RSSI_AVERAGE_DONE#

#define RAIL_EVENT_RSSI_AVERAGE_DONE
Value:
(1ULL << RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT)

Occurs when the hardware-averaged RSSI is done in response to RAIL_StartAverageRssi() to indicate that the hardware has completed averaging.

Call RAIL_GetAverageRssi() to get the result.


RAIL_EVENT_RX_ACK_TIMEOUT#

#define RAIL_EVENT_RX_ACK_TIMEOUT
Value:
(1ULL << RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT)

Occurs when the ACK timeout expires while waiting to receive the sync word of an expected ACK.

If the timeout occurs within packet reception, this event won't be signaled until after packet completion has determined the packet wasn't the expected ACK. See RAIL_RxPacketDetails_t::isAck for the definition of an expected ACK.

This event only occurs after calling RAIL_ConfigAutoAck() and after transmitting a packet with RAIL_TX_OPTION_WAIT_FOR_ACK set.


RAIL_EVENT_RX_FIFO_ALMOST_FULL#

#define RAIL_EVENT_RX_FIFO_ALMOST_FULL
Value:
(1ULL << RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT)

Keeps occurring as long as the number of bytes in the receive FIFO exceeds the configured threshold value.

Call RAIL_GetRxFifoBytesAvailable() to get the number of bytes available. When using this event, the threshold should be set via RAIL_SetRxFifoThreshold().

How to avoid sticking in the event handler (even in idle state):

  1. Disable the event (via the config events API or the RAIL_FIFO_THRESHOLD_DISABLED parameter)

  2. Increase FIFO threshold

  3. Read the FIFO (that's not an option in RAIL_DataMethod_t::PACKET_MODE) in the event handler


RAIL_EVENT_RX_PACKET_RECEIVED#

#define RAIL_EVENT_RX_PACKET_RECEIVED
Value:
(1ULL << RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT)

Occurs whenever a packet is received with RAIL_RX_PACKET_READY_SUCCESS or RAIL_RX_PACKET_READY_CRC_ERROR.

Call RAIL_GetRxPacketInfo() to get basic information about the packet along with a handle to this packet for subsequent use with RAIL_PeekRxPacket(), RAIL_GetRxPacketDetails(), RAIL_HoldRxPacket(), and RAIL_ReleaseRxPacket() as needed.


RAIL_EVENT_RX_PREAMBLE_LOST#

#define RAIL_EVENT_RX_PREAMBLE_LOST
Value:
(1ULL << RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT)

Occurs when the radio has lost a preamble.

This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_PREAMBLE_DETECT event has already occurred.


RAIL_EVENT_RX_PREAMBLE_DETECT#

#define RAIL_EVENT_RX_PREAMBLE_DETECT
Value:
(1ULL << RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT)

Occurs when the radio has detected a preamble.

This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_TIMING_DETECT event has already occurred.


RAIL_EVENT_RX_SYNC1_DETECT#

#define RAIL_EVENT_RX_SYNC1_DETECT
Value:
(1ULL << RAIL_EVENT_RX_SYNC1_DETECT_SHIFT)

Occurs when the first sync word is detected.

After this event occurs, one of the events in the RAIL_EVENTS_RX_COMPLETION mask will occur.


RAIL_EVENT_RX_SYNC2_DETECT#

#define RAIL_EVENT_RX_SYNC2_DETECT
Value:
(1ULL << RAIL_EVENT_RX_SYNC2_DETECT_SHIFT)

Occurs when the second sync word is detected.

After this event occurs, one of the events in the RAIL_EVENTS_RX_COMPLETION mask will occur.


RAIL_EVENT_RX_FRAME_ERROR#

#define RAIL_EVENT_RX_FRAME_ERROR
Value:
(1ULL << RAIL_EVENT_RX_FRAME_ERROR_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_CRC_ERROR which only happens after any filtering has passed.

For EFR32 parts, this event includes CRC errors, block decoding errors, and illegal frame length – when detected after filtering. (When such errors are detected during filtering, they're signaled as RAIL_EVENT_RX_PACKET_ABORTED instead.)

If RAIL_RX_OPTION_IGNORE_CRC_ERRORS is set, this event will not occur for CRC errors, but could still occur for the other errors.


RAIL_EVENT_RX_FIFO_FULL#

#define RAIL_EVENT_RX_FIFO_FULL
Value:
(1ULL << RAIL_EVENT_RX_FIFO_FULL_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs coincident to a receive packet completion event in which the receive FIFO or any supplemental packet metadata FIFO (see Data Management) are full and further packet reception is jeopardized.

It signals that an overflow is imminent (and may already have occurred) telling the application it should release the oldest packet(s) as soon as possible. This event may may be posted multiple times with subsequent receive completion events if the FIFO(s) remain full, and should also occur coincident with RAIL_EVENT_RX_FIFO_OVERFLOW.

When not using RAIL_RxDataSource_t::RX_PACKET_DATA this event is not tied to packet completion and will occur coincident with RAIL_EVENT_RX_FIFO_OVERFLOW when the receive FIFO has filled and overflowed. The application should consume receive FIFO data via RAIL_ReadRxFifo() as soon as possible to minimize lost raw data.


RAIL_EVENT_RX_FIFO_OVERFLOW#

#define RAIL_EVENT_RX_FIFO_OVERFLOW
Value:
(1ULL << RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_OVERFLOW due to overflowing the receive FIFO or any supplemental packet metadata FIFO (see Data Management).

The radio suspends receiving packets until this event is posted and the receive FIFO(s) have been fully processed (drained and released or reset). It is not guaranteed that a RAIL_EVENT_RX_FIFO_FULL will precede this event, but both events should be coincident.

When not using RAIL_RxDataSource_t::RX_PACKET_DATA this event is not tied to packet completion and will occur coincident with RAIL_EVENT_RX_FIFO_FULL when the receive FIFO has filled and overflowed. The application should consume receive FIFO data via RAIL_ReadRxFifo() as soon as possible to minimize lost raw data.


RAIL_EVENT_RX_ADDRESS_FILTERED#

#define RAIL_EVENT_RX_ADDRESS_FILTERED
Value:
(1ULL << RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_FILTERED because its address does not match the filtering settings.

This event can only occur after calling RAIL_EnableAddressFilter().


RAIL_EVENT_RX_TIMEOUT#

#define RAIL_EVENT_RX_TIMEOUT
Value:
(1ULL << RAIL_EVENT_RX_TIMEOUT_SHIFT)

Occurs when an RX event times out.

This event can only occur if the RAIL_StateTiming_t::rxSearchTimeout passed to RAIL_SetStateTiming() is not zero.


RAIL_EVENT_SCHEDULED_RX_STARTED#

#define RAIL_EVENT_SCHEDULED_RX_STARTED
Value:
(1ULL << RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT)

Occurs when a scheduled RX begins turning on the transmitter.

This event has the same numerical value as RAIL_EVENT_SCHEDULED_TX_STARTED because one cannot schedule both RX and TX simultaneously.


RAIL_EVENT_SCHEDULED_TX_STARTED#

#define RAIL_EVENT_SCHEDULED_TX_STARTED
Value:
(1ULL << RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT)

Occurs when a scheduled TX begins turning on the transmitter.

This event has the same numerical value as RAIL_EVENT_SCHEDULED_RX_STARTED because one cannot schedule both RX and TX simultaneously.


RAIL_EVENT_RX_SCHEDULED_RX_END#

#define RAIL_EVENT_RX_SCHEDULED_RX_END
Value:
(1ULL << RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT)

Occurs when the scheduled RX window ends.

This event only occurs in response to a scheduled receive timeout after calling RAIL_ScheduleRx(). If RAIL_ScheduleRxConfig_t::rxTransitionEndSchedule was passed as false, this event will occur unless the receive is aborted (due to a call to RAIL_Idle() or a scheduler preemption, for instance). If RAIL_ScheduleRxConfig_t::rxTransitionEndSchedule was passed as true, any of the RAIL_EVENTS_RX_COMPLETION events occurring will also cause this event not to occur, since the scheduled receive will end with the transition at the end of the packet. However, if the application has not enabled the specific RAIL_EVENTS_RX_COMPLETION event which implicitly ended the scheduled receive, this event will be posted instead.


RAIL_EVENT_RX_SCHEDULED_RX_MISSED#

#define RAIL_EVENT_RX_SCHEDULED_RX_MISSED
Value:
(1ULL << RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT)

Occurs when start of a scheduled receive is missed.

This can occur if the radio is put to sleep and not woken up with enough time to configure the scheduled receive event.


RAIL_EVENT_RX_PACKET_ABORTED#

#define RAIL_EVENT_RX_PACKET_ABORTED
Value:
(1ULL << RAIL_EVENT_RX_PACKET_ABORTED_SHIFT)

Occurs when a receive is aborted during filtering with RAIL_RX_PACKET_ABORT_FORMAT or after filtering with RAIL_RX_PACKET_ABORT_ABORTED for reasons other than address filtering mismatch (which triggers RAIL_EVENT_RX_ADDRESS_FILTERED instead).

For EFR32 parts, this event includes CRC errors, block decoding errors, illegal frame length, and other RAIL built-in protocol-specific packet content errors – when detected during filtering. (When such errors are detected after filtering, they're signaled as RAIL_EVENT_RX_FRAME_ERROR instead.) It also includes application or multiprotocol scheduler aborting a receive after filtering has passed.


RAIL_EVENT_RX_FILTER_PASSED#

#define RAIL_EVENT_RX_FILTER_PASSED
Value:
(1ULL << RAIL_EVENT_RX_FILTER_PASSED_SHIFT)

Occurs when the packet has passed any configured address and frame filtering options.

This event will only occur between the start of the packet, indicated by RAIL_EVENT_RX_SYNC1_DETECT or RAIL_EVENT_RX_SYNC2_DETECT and one of the events in the RAIL_EVENTS_RX_COMPLETION mask. It will always occur before or concurrently with RAIL_EVENT_RX_PACKET_RECEIVED. If IEEE 802.15.4 frame and address filtering are enabled, this event will occur immediately after destination address filtering.


RAIL_EVENT_RX_TIMING_LOST#

#define RAIL_EVENT_RX_TIMING_LOST
Value:
(1ULL << RAIL_EVENT_RX_TIMING_LOST_SHIFT)

Occurs when the modem timing is lost.

This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes. It can only occur after a RAIL_EVENT_RX_TIMING_DETECT event has already occurred.


RAIL_EVENT_RX_TIMING_DETECT#

#define RAIL_EVENT_RX_TIMING_DETECT
Value:
(1ULL << RAIL_EVENT_RX_TIMING_DETECT_SHIFT)

Occurs when the modem timing is detected.

This event can occur multiple times while searching for a packet and is generally used for diagnostic purposes.


RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE#

#define RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE
Value:
(1ULL << RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT)

Occurs when RX Channel Hopping is enabled and channel hopping finishes receiving on the last channel in its sequence.

The intent behind this event is to allow the user to keep the radio on for as short a time as possible. That is, once the channel sequence is complete, the application will receive this event and can trigger a sleep/idle until it is necessary to cycle through the channels again. If this event is left on indefinitely and not handled it will likely be a fairly noisy event, as it continues to fire each time the hopping algorithm cycles through the channel sequence.


RAIL_EVENT_RX_DUTY_CYCLE_RX_END#

#define RAIL_EVENT_RX_DUTY_CYCLE_RX_END
Value:
(1ULL << RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT)

Occurs during RX duty cycle mode when the radio finishes its time in receive mode.

The application can then trigger a sleep/idle until it needs to listen again.


RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND#

#define RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND
Value:
(1ULL << RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT)

Indicate a Data Request is received when using IEEE 802.15.4 functionality.

It occurs when the command byte of an incoming ACK-requesting MAC Control frame is for a data request. This callback is called before the packet is fully received to allow the node to have more time to decide whether to indicate a frame is pending in the outgoing ACK. This event only occurs if the RAIL IEEE 802.15.4 functionality is enabled, but will never occur if promiscuous mode is enabled via RAIL_IEEE802154_SetPromiscuousMode().

Call RAIL_IEEE802154_GetAddress() to get the source address of the packet.


RAIL_EVENT_ZWAVE_BEAM#

#define RAIL_EVENT_ZWAVE_BEAM
Value:
(1ULL << RAIL_EVENT_ZWAVE_BEAM_SHIFT)

Indicate a Z-Wave Beam Request relevant to the node was received.

This event only occurs if the RAIL Z-Wave functionality is enabled and its RAIL_ZWAVE_OPTION_DETECT_BEAM_FRAMES is enabled. This event is used in lieu of RAIL_EVENT_RX_PACKET_RECEIVED, which is reserved for Z-Wave packets other than Beams.

Call RAIL_ZWAVE_GetBeamNodeId() to get the NodeId to which the Beam was targeted, which would be either the broadcast id 0xFF or the node's own single-cast id.

Note


RAIL_EVENT_MFM_TX_BUFFER_DONE#

#define RAIL_EVENT_MFM_TX_BUFFER_DONE
Value:
(1ULL << RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT)

Indicate a MFM buffer has completely transmitted.

This event only occurs if the RAIL MFM functionality is enabled and a MFM buffer has completely transmitted.

Following this event, the application can update the MFM buffer that has transmitted to be used for the next transmission.


RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND#

#define RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND
Value:
(1ULL << RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT)

Indicate a request for populating Z-Wave LR ACK packet.

This event only occurs if the RAIL Z-Wave functionality is enabled.

Following this event, the application must call RAIL_ZWAVE_SetLrAckData() to populate noise floor, TX power and receive RSSI fields of the Z-Wave Long Range ACK packet.


RAIL_EVENTS_RX_COMPLETION#

#define RAIL_EVENTS_RX_COMPLETION
Value:
(RAIL_EVENT_RX_PACKET_RECEIVED \
| RAIL_EVENT_RX_PACKET_ABORTED \
| RAIL_EVENT_RX_FRAME_ERROR \
| RAIL_EVENT_RX_FIFO_OVERFLOW \
| RAIL_EVENT_RX_ADDRESS_FILTERED \
| RAIL_EVENT_RX_SCHEDULED_RX_MISSED)

The mask representing all events that determine the end of a received packet.

After a RAIL_EVENT_RX_SYNC1_DETECT or a RAIL_EVENT_RX_SYNC2_DETECT, exactly one of the following events will occur. When one of these events occurs, a state transition will take place based on the parameter passed to RAIL_SetRxTransitions(). The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_RX_PACKET_RECEIVED event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.


RAIL_EVENT_TX_FIFO_ALMOST_EMPTY#

#define RAIL_EVENT_TX_FIFO_ALMOST_EMPTY
Value:
(1ULL << RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT)

Occurs when the number of bytes in the transmit FIFO falls below the configured threshold value.

This event does not occur on initialization or after resetting the transmit FIFO with RAIL_ResetFifo().

Call RAIL_GetTxFifoSpaceAvailable() to get the number of bytes available in the transmit FIFO at the time of the callback dispatch. When using this event, the threshold should be set via RAIL_SetTxFifoThreshold().


RAIL_EVENT_TX_PACKET_SENT#

#define RAIL_EVENT_TX_PACKET_SENT
Value:
(1ULL << RAIL_EVENT_TX_PACKET_SENT_SHIFT)

Occurs after a packet has been transmitted.

Call RAIL_GetTxPacketDetails() to get information about the packet that was transmitted. Note


RAIL_EVENT_TXACK_PACKET_SENT#

#define RAIL_EVENT_TXACK_PACKET_SENT
Value:
(1ULL << RAIL_EVENT_TXACK_PACKET_SENT_SHIFT)

Occurs after an ACK packet has been transmitted.

Call RAIL_GetTxPacketDetails() to get information about the packet that was transmitted. This event can only occur after calling RAIL_ConfigAutoAck(). Note


RAIL_EVENT_TX_ABORTED#

#define RAIL_EVENT_TX_ABORTED
Value:
(1ULL << RAIL_EVENT_TX_ABORTED_SHIFT)

Occurs when a transmit is aborted by the user.

This can happen due to calling RAIL_Idle() or due to a scheduler preemption.

Note

  • The Transmit FIFO is left in an indeterminate state and should be reset prior to reuse for sending a new packet. Contrast this with RAIL_EVENT_TX_BLOCKED.


RAIL_EVENT_TXACK_ABORTED#

#define RAIL_EVENT_TXACK_ABORTED
Value:
(1ULL << RAIL_EVENT_TXACK_ABORTED_SHIFT)

Occurs when an ACK transmit is aborted by the user.

This event can only occur after calling RAIL_ConfigAutoAck(), which can happen due to calling RAIL_Idle() or due to a scheduler preemption.


RAIL_EVENT_TX_BLOCKED#

#define RAIL_EVENT_TX_BLOCKED
Value:
(1ULL << RAIL_EVENT_TX_BLOCKED_SHIFT)

Occurs when a transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

Note

  • Since the transmit never started, the Transmit FIFO remains intact after this event – no packet data was consumed from it. Contrast this with RAIL_EVENT_TX_ABORTED.


RAIL_EVENT_TXACK_BLOCKED#

#define RAIL_EVENT_TXACK_BLOCKED
Value:
(1ULL << RAIL_EVENT_TXACK_BLOCKED_SHIFT)

Occurs when an ACK transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

This event can only occur after calling RAIL_ConfigAutoAck().


RAIL_EVENT_TX_UNDERFLOW#

#define RAIL_EVENT_TX_UNDERFLOW
Value:
(1ULL << RAIL_EVENT_TX_UNDERFLOW_SHIFT)

Occurs when the transmit buffer underflows.

This can happen due to the transmitted packet specifying an unintended length based on the current radio configuration or due to RAIL_WriteTxFifo() calls not keeping up with the transmit rate if the entire packet isn't loaded at once.

Note

  • The Transmit FIFO is left in an indeterminate state and should be reset prior to reuse for sending a new packet. Contrast this with RAIL_EVENT_TX_BLOCKED.


RAIL_EVENT_TXACK_UNDERFLOW#

#define RAIL_EVENT_TXACK_UNDERFLOW
Value:
(1ULL << RAIL_EVENT_TXACK_UNDERFLOW_SHIFT)

Occurs when the ACK transmit buffer underflows.

This can happen due to the transmitted packet specifying an unintended length based on the current radio configuration or due to RAIL_WriteAutoAckFifo() not being called at all before an ACK transmit.

This event can only occur after calling RAIL_ConfigAutoAck().


RAIL_EVENT_TX_CHANNEL_CLEAR#

#define RAIL_EVENT_TX_CHANNEL_CLEAR
Value:
(1ULL << RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) succeeds.

This event can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx().


RAIL_EVENT_TX_CHANNEL_BUSY#

#define RAIL_EVENT_TX_CHANNEL_BUSY
Value:
(1ULL << RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) fails.

This event can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx().

Note

  • Since the transmit never started, the Transmit FIFO remains intact after this event – no packet data was consumed from it.


RAIL_EVENT_TX_CCA_RETRY#

#define RAIL_EVENT_TX_CCA_RETRY
Value:
(1ULL << RAIL_EVENT_TX_CCA_RETRY_SHIFT)

Occurs during CSMA or LBT when an individual Clear Channel Assessment (CCA) check fails, but there are more tries needed before the overall operation completes.

This event can occur multiple times based on the configuration of the ongoing CSMA or LBT transmission. It can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx().


RAIL_EVENT_TX_START_CCA#

#define RAIL_EVENT_TX_START_CCA
Value:
(1ULL << RAIL_EVENT_TX_START_CCA_SHIFT)

Occurs when the receiver is activated to perform a Clear Channel Assessment (CCA) check.

This event generally precedes the actual start of a CCA check by roughly the RAIL_StateTiming_t::idleToRx time (subject to RAIL_MINIMUM_TRANSITION_US). It can occur multiple times based on the configuration of the ongoing CSMA or LBT transmission. It can only happen after calling RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx().


RAIL_EVENT_TX_STARTED#

#define RAIL_EVENT_TX_STARTED
Value:
(1ULL << RAIL_EVENT_TX_STARTED_SHIFT)

Occurs when the radio starts transmitting a normal packet on the air.

A start-of-transmit timestamp is captured for this event. It can be retrieved by calling RAIL_GetTxTimePreambleStart() passing RAIL_TX_STARTED_BYTES for its totalPacketBytes parameter.

Note

  • This event does not apply to ACK transmits. Currently there is no equivalent event or timestamp captured for the start of an ACK transmit.


RAIL_TX_STARTED_BYTES#

#define RAIL_TX_STARTED_BYTES
Value:
0U

A value to pass as RAIL_GetTxTimePreambleStart() totalPacketBytes parameter to retrieve the RAIL_EVENT_TX_STARTED timestamp.


RAIL_EVENT_TX_SCHEDULED_TX_MISSED#

#define RAIL_EVENT_TX_SCHEDULED_TX_MISSED
Value:
(1ULL << RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT)

Occurs when the start of a scheduled transmit is missed.

This can occur if the radio is put to sleep and not woken up with enough time to configure the scheduled transmit event.

Note

  • Since the transmit never started, the Transmit FIFO remains intact after this event – no packet data was consumed from it.


RAIL_EVENTS_TX_COMPLETION#

#define RAIL_EVENTS_TX_COMPLETION
Value:
(RAIL_EVENT_TX_PACKET_SENT \
| RAIL_EVENT_TX_ABORTED \
| RAIL_EVENT_TX_BLOCKED \
| RAIL_EVENT_TX_UNDERFLOW \
| RAIL_EVENT_TX_CHANNEL_BUSY \
| RAIL_EVENT_TX_SCHEDULED_TX_MISSED)

A mask representing all events that determine the end of a transmitted packet.

After a RAIL_STATUS_NO_ERROR return value from one of the transmit functions, exactly one of the following events will occur. When one of these events occurs, a state transition takes place based on the parameter passed to RAIL_SetTxTransitions(). The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_TX_PACKET_SENT event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.


RAIL_EVENTS_TXACK_COMPLETION#

#define RAIL_EVENTS_TXACK_COMPLETION
Value:
(RAIL_EVENT_TXACK_PACKET_SENT \
| RAIL_EVENT_TXACK_ABORTED \
| RAIL_EVENT_TXACK_BLOCKED \
| RAIL_EVENT_TXACK_UNDERFLOW)

A mask representing all events that determine the end of a transmitted ACK packet.

After an ACK-requesting receive, exactly one of the following events will occur. When one of these events occurs, a state transition takes place based on the RAIL_AutoAckConfig_t::rxTransitions passed to RAIL_ConfigAutoAck(). The receive transitions are used because the transmitted ACK packet is considered a part of the ACK-requesting received packet. The RAIL_StateTransitions_t::success transition will be followed only if the RAIL_EVENT_TXACK_PACKET_SENT event occurs. Any of the other events will trigger the RAIL_StateTransitions_t::error transition.


RAIL_EVENT_CONFIG_UNSCHEDULED#

#define RAIL_EVENT_CONFIG_UNSCHEDULED
Value:
(1ULL << RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT)

Occurs when the scheduler switches away from this configuration.

This event will occur in dynamic multiprotocol scenarios each time a protocol is shutting down. When it does occur, it will be the only event passed to RAIL_Config_t::eventsCallback. Therefore, to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.

Note

  • : To minimize protocol switch time, Silicon Labs recommends this event event being turned off unless it is used.


RAIL_EVENT_CONFIG_SCHEDULED#

#define RAIL_EVENT_CONFIG_SCHEDULED
Value:
(1ULL << RAIL_EVENT_CONFIG_SCHEDULED_SHIFT)

Occurs when the scheduler switches to this configuration.

This event will occur in dynamic multiprotocol scenarios each time a protocol is starting up. When it does occur, it will be the only event passed to RAIL_Config_t::eventsCallback. Therefore, in order to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.

Note

  • : To minimize protocol switch time, Silicon Labs recommends this event event being turned off unless it is used.


RAIL_EVENT_SCHEDULER_STATUS#

#define RAIL_EVENT_SCHEDULER_STATUS
Value:
(1ULL << RAIL_EVENT_SCHEDULER_STATUS_SHIFT)

Occurs when the scheduler has a status to report.

The exact status can be found with RAIL_GetSchedulerStatus(). See RAIL_SchedulerStatus_t for more details. When this event does occur, it will be the only event passed to RAIL_Config_t::eventsCallback. Therefore, to optimize protocol switch time, this event should be handled among the first in that callback, and then the application can return immediately.

Note


RAIL_EVENT_CAL_NEEDED#

#define RAIL_EVENT_CAL_NEEDED
Value:
(1ULL << RAIL_EVENT_CAL_NEEDED_SHIFT)

Occurs when the application needs to run a calibration, as determined by the RAIL library.

The application determines the opportune time to call RAIL_Calibrate().


RAIL_EVENT_RF_SENSED#

#define RAIL_EVENT_RF_SENSED
Value:
(1ULL << RAIL_EVENT_RF_SENSED_SHIFT)

Occurs when RF energy is sensed from the radio.

This event can be used as an alternative to the callback passed as RAIL_RfSense_CallbackPtr_t.

Alternatively, the application can poll using RAIL_IsRfSensed().

Note

  • This event will not occur when waking up from EM4. Prefer RAIL_IsRfSensed() when waking from EM4.


RAIL_EVENT_PA_PROTECTION#

#define RAIL_EVENT_PA_PROTECTION
Value:
(1ULL << RAIL_EVENT_PA_PROTECTION_SHIFT)

Occurs when PA protection circuit kicks in.


RAIL_EVENT_SIGNAL_DETECTED#

#define RAIL_EVENT_SIGNAL_DETECTED
Value:
(1ULL << RAIL_EVENT_SIGNAL_DETECTED_SHIFT)

Occurs after enabling the signal detection using RAIL_BLE_EnableSignalDetection or RAIL_IEEE802154_EnableSignalDetection when a signal is detected.

This is only used on platforms that support signal identifier, where RAIL_BLE_SUPPORTS_SIGNAL_IDENTIFIER or RAIL_IEEE802154_SUPPORTS_SIGNAL_IDENTIFIER is true.


RAIL_EVENT_IEEE802154_MODESWITCH_START#

#define RAIL_EVENT_IEEE802154_MODESWITCH_START
Value:
(1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT)

Occurs when a Wi-SUN mode switch packet has been received, after switching to the new PHY.

It doesn't occur when a mode switch packet is transmitted.

IEEE 802.15.4 option RAIL_IEEE802154_G_OPTION_WISUN_MODESWITCH must be enabled for this event to occur.

Only available on platforms where RAIL_IEEE802154_SUPPORTS_G_MODESWITCH is true.


RAIL_EVENT_IEEE802154_MODESWITCH_END#

#define RAIL_EVENT_IEEE802154_MODESWITCH_END
Value:
(1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT)

Occurs when switching back to the original base PHY in effect prior to the Wi-SUN mode switch reception.

This typically occurs if no packet is seen within some timeframe after the mode switch packet was received or if the first packet received in the new PHY is aborted, filtered, or fails CRC.

IEEE 802.15.4 option RAIL_IEEE802154_G_OPTION_WISUN_MODESWITCH must be enabled for this event to occur.

Only available on platforms where RAIL_IEEE802154_SUPPORTS_G_MODESWITCH is true.


RAIL_EVENT_DETECT_RSSI_THRESHOLD#

#define RAIL_EVENT_DETECT_RSSI_THRESHOLD
Value:
(1ULL << RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT)

Occurs when the sampled RSSI is above the threshold set by RAIL_SetRssiDetectThreshold().


RAIL_EVENT_THERMISTOR_DONE#

#define RAIL_EVENT_THERMISTOR_DONE
Value:
(1ULL << RAIL_EVENT_THERMISTOR_DONE_SHIFT)

Occurs when the thermistor has finished its measurement in response to RAIL_StartThermistorMeasurement().


RAIL_EVENT_TX_BLOCKED_TOO_HOT#

#define RAIL_EVENT_TX_BLOCKED_TOO_HOT
Value:
(1ULL << RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT)

Occurs when a Tx has been blocked because of temperature exceeding the safety threshold.

Only occurs on platforms where RAIL_SUPPORTS_EFF is true, and only when also reporting RAIL_EVENT_TX_BLOCKED.


RAIL_EVENT_TEMPERATURE_TOO_HOT#

#define RAIL_EVENT_TEMPERATURE_TOO_HOT
Value:
(1ULL << RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT)

Occurs when die internal temperature exceeds the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

Transmits are blocked until temperature has cooled enough, indicated by RAIL_EVENT_TEMPERATURE_COOL_DOWN.

Only occurs on platforms where RAIL_SUPPORTS_THERMAL_PROTECTION is true.


RAIL_EVENT_TEMPERATURE_COOL_DOWN#

#define RAIL_EVENT_TEMPERATURE_COOL_DOWN
Value:
(1ULL << RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT)

Occurs when die internal temperature falls below the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

Transmits are no longer blocked by temperature limitation, indicated by RAIL_EVENT_TEMPERATURE_TOO_HOT.

Only occurs on platforms where RAIL_SUPPORTS_THERMAL_PROTECTION is true.


RAIL_EVENTS_ALL#

#define RAIL_EVENTS_ALL
Value:
0xFFFFFFFFFFFFFFFFULL

A value representing all possible events.