General#

Basic APIs to set up and interact with the RAIL library.

Modules#

RAIL_Version_t

EFR32xG1

Enumerations#

enum
RAIL_STATUS_NO_ERROR
RAIL_STATUS_INVALID_PARAMETER
RAIL_STATUS_INVALID_STATE
RAIL_STATUS_INVALID_CALL
RAIL_STATUS_SUSPENDED
RAIL_STATUS_SCHED_ERROR
}

A status returned by many RAIL API calls indicating their success or failure.

Typedefs#

typedef void *

A generic handle to a particular radio (e.g.

typedef void(*
RAIL_InitCompleteCallbackPtr_t)(RAIL_Handle_t railHandle)

A pointer to init complete callback function.

Functions#

void
RAIL_GetVersion(RAIL_Version_t *version, bool verbose)

Get the version information for the compiled RAIL library.

RAIL_AddStateBuffer3(RAIL_Handle_t genericRailHandle)

Add a 3rd multiprotocol internal state buffer for use by RAIL_Init().

RAIL_AddStateBuffer4(RAIL_Handle_t genericRailHandle)

Add a 4th multiprotocol internal state buffer for use by RAIL_Init().

RAIL_UseDma(uint8_t channel)

Allocate a DMA channel for RAIL to work with.

RAIL_Init(RAIL_Config_t *railCfg, RAIL_InitCompleteCallbackPtr_t cb)

Initialize RAIL.

bool

Get RAIL initialization status.

uint16_t
RAIL_GetRadioEntropy(RAIL_Handle_t railHandle, uint8_t *buffer, uint16_t bytes)

Collect entropy from the radio if available.

Macros#

#define

A value to signal that RAIL should not use DMA.

Enumeration Documentation#

RAIL_Status_t#

RAIL_Status_t

A status returned by many RAIL API calls indicating their success or failure.

Enumerator
RAIL_STATUS_NO_ERROR

RAIL function reports no error.

RAIL_STATUS_INVALID_PARAMETER

Call to RAIL function threw an error because of an invalid parameter.

RAIL_STATUS_INVALID_STATE

Call to RAIL function threw an error because it was called during an invalid radio state.

RAIL_STATUS_INVALID_CALL

RAIL function is called in an invalid order.

RAIL_STATUS_SUSPENDED

RAIL function did not finish in the allotted time.

RAIL_STATUS_SCHED_ERROR

RAIL function could not be scheduled by the Radio scheduler.


Typedef Documentation#

RAIL_Handle_t#

RAIL_Handle_t

A generic handle to a particular radio (e.g.

RAIL_EFR32_HANDLE), or a real handle of a RAIL instance, as returned from RAIL_Init().

Generic handles should be used for certain RAIL APIs that are called prior to RAIL initialization. However, once RAIL has been initialized, the real handle returned by RAIL_Init() should be used instead.


RAIL_InitCompleteCallbackPtr_t#

typedef void(* RAIL_InitCompleteCallbackPtr_t) (RAIL_Handle_t railHandle) )(RAIL_Handle_t railHandle)

A pointer to init complete callback function.

Parameters
TypeDirectionArgument NameDescription
[in]railHandle

The initialized RAIL instance handle.


Function Documentation#

RAIL_GetVersion#

void RAIL_GetVersion (RAIL_Version_t * version, bool verbose)

Get the version information for the compiled RAIL library.

Parameters
TypeDirectionArgument NameDescription
RAIL_Version_t *[out]version

A pointer to RAIL_Version_t structure to populate with version information.

bool[in]verbose

Populate RAIL_Version_t struct with verbose information.

The version information contains a major version number, a minor version number, and a rev (revision) number.


RAIL_AddStateBuffer3#

RAIL_Status_t RAIL_AddStateBuffer3 (RAIL_Handle_t genericRailHandle)

Add a 3rd multiprotocol internal state buffer for use by RAIL_Init().

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]genericRailHandle

A generic RAIL instance handle.

Returns

  • Status code indicating success of the function call. An error is returned if the 3rd state buffer was previously added or this isn't the RAIL multiprotocol library.


RAIL_AddStateBuffer4#

RAIL_Status_t RAIL_AddStateBuffer4 (RAIL_Handle_t genericRailHandle)

Add a 4th multiprotocol internal state buffer for use by RAIL_Init().

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]genericRailHandle

A generic RAIL instance handle.

Returns

  • Status code indicating success of the function call. An error is returned if the 4th state buffer was previously added. or this isn't the RAIL multiprotocol library.


RAIL_UseDma#

RAIL_Status_t RAIL_UseDma (uint8_t channel)

Allocate a DMA channel for RAIL to work with.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel

The DMA channel to use when copying memory. If a value of RAIL_DMA_INVALID is passed, RAIL will stop using any DMA channel.

Returns

  • Status code indicating success of the function call.

To use this API, the application must initialize the DMA engine on the chip and allocate a DMA channel. This channel will be used periodically to copy memory more efficiently. Call this function before RAIL_Init to have the most benefit. If the application needs to take back control of the DMA channel that RAIL is using, this API may be called with a channel of RAIL_DMA_INVALID to tell RAIL to stop using DMA.


RAIL_Init#

RAIL_Handle_t RAIL_Init (RAIL_Config_t * railCfg, RAIL_InitCompleteCallbackPtr_t cb)

Initialize RAIL.

Parameters
TypeDirectionArgument NameDescription
RAIL_Config_t *[inout]railCfg

The configuration and state structure for setting up the library, which contains memory and other options that RAIL needs. This structure must be allocated in application global read-write memory. RAIL may modify fields within or referenced by this structure during its operation.

RAIL_InitCompleteCallbackPtr_t[in]cb

A callback that notifies the application when the radio is finished initializing and is ready for further configuration. This callback is useful for potential transceiver products that require a power up sequence before further configuration is available. After the callback fires, the radio is ready for additional configuration before transmit and receive operations.

Returns

  • Handle for initialized rail instance or NULL if an invalid value was passed in the railCfg.

Note

  • Call this function only once per protocol. If called again, it will do nothing and return NULL.


RAIL_IsInitialized#

bool RAIL_IsInitialized (void )

Get RAIL initialization status.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • True if the radio has finished initializing and false otherwise.

RAIL APIs, e.g., RAIL_GetTime(), which work only if RAIL_Init() has been called, can use RAIL_IsInitialized() to determine whether RAIL has been initialized or not.


RAIL_GetRadioEntropy#

uint16_t RAIL_GetRadioEntropy (RAIL_Handle_t railHandle, uint8_t * buffer, uint16_t bytes)

Collect entropy from the radio if available.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[out]buffer

The buffer to write the collected entropy.

uint16_t[in]bytes

The number of bytes to fill in the input buffer.

Returns

  • Returns the number of bytes of entropy collected. For chips that don't support entropy collection, the function returns 0. Values less than the requested amount may also be returned on platforms that use entropy pools to collect random data periodically.

Attempts to fill the provided buffer with the requested number of bytes of entropy. If the requested number of bytes can't be provided, as many bytes as possible will be filled and returned. For chips that do not support this function, 0 bytes are always returned. For information about the specific mechanism for gathering entropy, see documentation for the chip family.


Macro Definition Documentation#

RAIL_DMA_INVALID#

#define RAIL_DMA_INVALID
Value:
(0xFFU)

A value to signal that RAIL should not use DMA.