RAIL sync words and length configuration.

Public Attributes#

uint8_t

Sync word length in bits, between 2 and 32, inclusive.

uint32_t

Sync Word1.

uint32_t

Sync Word2.

Public Attribute Documentation#

syncWordBits#

uint8_t RAIL_SyncWordConfig_t::syncWordBits

Sync word length in bits, between 2 and 32, inclusive.


Definition at line 3494 of file common/rail_types.h

syncWord1#

uint32_t RAIL_SyncWordConfig_t::syncWord1

Sync Word1.

Note

  • Only syncWordBits number of LS bits are used, which are sent or received on air LSB first.


Definition at line 3499 of file common/rail_types.h

syncWord2#

uint32_t RAIL_SyncWordConfig_t::syncWord2

Sync Word2.

Note

  • Only syncWordBits number of LS bits are used, which are sent or received on air LSB first.


Definition at line 3504 of file common/rail_types.h