You are viewing documentation for version:
2.16.2 
A state structure for BLE. 
This structure must be allocated in application global read-write memory that persists for the duration of BLE usage. It cannot be allocated in read-only memory or on the call stack. 
Public Attributes#  uint32_t
The value used to initialize the CRC algorithm. 
uint32_t
The access address used for the connection. 
uint16_t
The logical channel used. 
bool
Indicates whether the whitening engine should be off. 
uint16_t
The value used to initialize the whitening algorithm. 
Public Attribute Documentation#  crcInit#  uint32_t RAIL_BLE_State_t::crcInit The value used to initialize the CRC algorithm. 
accessAddress#  uint32_t RAIL_BLE_State_t::accessAddress The access address used for the connection. 
channel#  uint16_t RAIL_BLE_State_t::channel The logical channel used. 
disableWhitening#  bool RAIL_BLE_State_t::disableWhitening Indicates whether the whitening engine should be off. 
whiteInit#  uint16_t RAIL_BLE_State_t::whiteInit The value used to initialize the whitening algorithm.