Enable/disable the auto-ACK algorithm, based on "enable".

The structure provides a default state (the "success" of tx/rxTransitions when ACKing is enabled) for the radio to return to after an ACK operation occurs (transmitting or attempting to receive an ACK), or normal state transitions to return to in the case ACKing is disabled. Regardless whether the ACK operation was successful, the radio returns to the specified success state.

ackTimeout specifies how long to stay in receive and wait for an ACK to start (sync detected) before issuing a RAIL_EVENT_RX_ACK_TIMEOUT event and return to the default state.

Public Attributes#

bool

Indicate whether auto-ACKing should be enabled or disabled.

uint16_t

Define the RX ACK timeout duration in microseconds up to 65535 microseconds maximum.

State transitions to do after receiving a packet.

State transitions to do after transmitting a packet.

Public Attribute Documentation#

enable#

bool RAIL_AutoAckConfig_t::enable

Indicate whether auto-ACKing should be enabled or disabled.


Definition at line 4306 of file common/rail_types.h

ackTimeout#

uint16_t RAIL_AutoAckConfig_t::ackTimeout

Define the RX ACK timeout duration in microseconds up to 65535 microseconds maximum.

Only applied when auto-ACKing is enabled. The ACK timeout timer starts at the completion of a RAIL_TX_OPTION_WAIT_FOR_ACK transmit and expires only while waiting for a packet (prior to SYNC detect), triggering RAIL_EVENT_RX_ACK_TIMEOUT. During packet reception that event is held off until packet completion and suppressed entirely if the received packet is the expected ACK.


Definition at line 4317 of file common/rail_types.h

rxTransitions#

RAIL_StateTransitions_t RAIL_AutoAckConfig_t::rxTransitions

State transitions to do after receiving a packet.

When auto-ACKing is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any ACKing sequence (RAIL_RF_STATE_RX or RAIL_RF_STATE_IDLE). See RAIL_ConfigAutoAck for more details on this.


Definition at line 4325 of file common/rail_types.h

txTransitions#

RAIL_StateTransitions_t RAIL_AutoAckConfig_t::txTransitions

State transitions to do after transmitting a packet.

When auto-ACKing is enabled, the "error" transition is always ignored and the radio will return to the "success" state after any ACKing sequence (RAIL_RF_STATE_RX or RAIL_RF_STATE_IDLE). See RAIL_ConfigAutoAck for more details on this.


Definition at line 4333 of file common/rail_types.h