Data used for thermal protection.

Public Attributes#

uint16_t

Store chip temperature for metrics.

uint16_t

Minimum temperature recorded.

uint16_t

Maximum temperature recorded.

bool

Indicates if data should be reset.

uint8_t

Reserved for future use.

Public Attribute Documentation#

tempK#

uint16_t RAIL_ChipTempMetrics_t::tempK

Store chip temperature for metrics.


Definition at line 5697 of file common/rail_types.h

minTempK#

uint16_t RAIL_ChipTempMetrics_t::minTempK

Minimum temperature recorded.


Definition at line 5698 of file common/rail_types.h

maxTempK#

uint16_t RAIL_ChipTempMetrics_t::maxTempK

Maximum temperature recorded.


Definition at line 5699 of file common/rail_types.h

resetPending#

bool RAIL_ChipTempMetrics_t::resetPending

Indicates if data should be reset.


Definition at line 5700 of file common/rail_types.h

reservedChipTemp#

uint8_t RAIL_ChipTempMetrics_t::reservedChipTemp

Reserved for future use.


Definition at line 5701 of file common/rail_types.h