Angle of Arrival/Departure#
These APIs are to a stack implementing BLE's angle of arrival and angle of departure functionality.
They are designed for use by the Silicon Labs BLE stack only at this time and may cause problems if accessed directly.
Modules#
Enumerations#
Angle of Arrival/Departure options bit fields.
Functions#
Lock/unlock the CTE buffer from the application's perspective.
Determine whether the CTE buffer is currently locked or not.
Get the offset into CTE sample of CTE data.
Get the effective sample rate used by the ADC to capture the CTE samples.
Configure Angle of Arrival/Departure (AoX) functionality.
Perform one time initialization of AoX registers.
Perform initialization of AoX antenna GPIO pins.
Macros#
The maximum number of GPIO pins used for AoX Antenna switching.
DeprecatedObsolete AOX option
DeprecatedObsolete AOX option
DeprecatedObsolete AOX option
DeprecatedPlease use RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK_SHIFT instead.
Disable the AoX feature.
Sets one of the two AoX sampling/switching modes: 1 us or 2 us window.
Enables connectionless AoX Rx packets.
Enables connection based AoX Rx packets.
Disables CTE buffer lock.
Enables connection based or connectionless AoX Rx packets.
Enumeration Documentation#
RAIL_BLE_AoxOptions_t#
RAIL_BLE_AoxOptions_t
Angle of Arrival/Departure options bit fields.
| Enumerator | |
|---|---|
| RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_SAMPLE_MODE bit. |
| RAIL_BLE_AOX_OPTIONS_CONNLESS_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_CONNLESS bit. |
| RAIL_BLE_AOX_OPTIONS_CONN_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_CONN bit. |
| RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK_SHIFT | Shift position of RAIL_BLE_AOX_OPTIONS_DISABLE_BUFFER_LOCK bit. |
Function Documentation#
RAIL_BLE_LockCteBuffer#
bool RAIL_BLE_LockCteBuffer (RAIL_Handle_t railHandle, bool lock)
Lock/unlock the CTE buffer from the application's perspective.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | lock | Lock the CTE buffer if true and unlock it if false. |
The radio will write to the buffer only if the bit is NOT set at the beginning of the sampling period. The radio will set the bit once the sampling period starts to indicate that some CTE data has been collected, which will not be overwritten during the next sampling period, unless the buffer is unlocked by the application.
Returns
True if the CTE buffer is locked after the call, otherwise false.
RAIL_BLE_CteBufferIsLocked#
bool RAIL_BLE_CteBufferIsLocked (RAIL_Handle_t railHandle)
Determine whether the CTE buffer is currently locked or not.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
True if CTE buffer is locked and false otherwise.
RAIL_BLE_GetCteSampleOffset#
uint8_t RAIL_BLE_GetCteSampleOffset (RAIL_Handle_t railHandle)
Get the offset into CTE sample of CTE data.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
The offset of CTE data in a CTE sample in bytes. On unsupported platforms this returns 0.
RAIL_BLE_GetCteSampleRate#
uint32_t RAIL_BLE_GetCteSampleRate (RAIL_Handle_t railHandle)
Get the effective sample rate used by the ADC to capture the CTE samples.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A handle for RAIL instance. |
Returns
The actual sample rate used to capture the CTE in samples per second. On unsupported platforms this returns 0.
RAIL_BLE_ConfigAox#
RAIL_Status_t RAIL_BLE_ConfigAox (RAIL_Handle_t railHandle, const RAIL_BLE_AoxConfig_t * aoxConfig)
Configure Angle of Arrival/Departure (AoX) functionality.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_BLE_AoxConfig_t * | [in] | aoxConfig | Configuration options for AoX |
AoX is a method of radio localization which infers angle of arrival/departure of the signal based on different phases of the raw I/Q signal from different antennas by controlling external RF switch during the continuous tone extension (CTE). Connection based AoX packets are different than normal BLE packets in that they have 3 header bytes instead of 2 and they have CTE appended after the payload's CRC. 3rd byte or CTE info contains CTE length. Connectionless AoX packets have 2 header bytes and CTE info is part of the payload. AoX is supported on EFR32XG12/13/14 only on legacy 1Mbps BLE PHY. Note that calling RAIL_GetRadioEntropy during AoX reception may break receiving packets.
Returns
RAIL_Status_t indicating success or failure of the call.
RAIL_BLE_InitCte#
RAIL_Status_t RAIL_BLE_InitCte (RAIL_Handle_t railHandle)
Perform one time initialization of AoX registers.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
This function must be called before RAIL_BLE_ConfigAox and before configuring the BLE PHY.
Returns
RAIL_Status_t indicating success or failure of the call.
RAIL_BLE_ConfigAoxAntenna#
RAIL_Status_t RAIL_BLE_ConfigAoxAntenna (RAIL_Handle_t railHandle, RAIL_BLE_AoxAntennaConfig_t * antennaConfig)
Perform initialization of AoX antenna GPIO pins.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_BLE_AoxAntennaConfig_t * | [in] | antennaConfig | structure to hold the set of ports and pins to configure Antenna pins for AoX Antenna switching. |
This function must be called before calls to RAIL_BLE_InitCte and RAIL_BLE_ConfigAox, and before configuring the BLE PHY, else a RAIL_STATUS_INVALID_CALL is returned.
If user configures more pins, i.e., antCount in RAIL_BLE_AoxAntennaConfig_t, than allowed RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the API returns RAIL_STATUS_INVALID_PARAMETER.
If user configures lesser than or equal to number of pins allowed by RAIL_BLE_AOX_ANTENNA_PIN_COUNT, then the requested number of pins are configured and RAIL_STATUS_NO_ERROR is returned.
If AoX antenna switching is inactive, non-AoX transmits and receives will occur on the first antenna specified by the antenna pattern or on the default antenna if no antenna pattern is provided.
Returns
RAIL_Status_t indicating success or failure of the call.