Alternate PHY configuration entry structure, which gathers some info on the alternate PHY in the context of concurrent mode.

Public Attributes#

uint32_t

A base frequency in Hz of this channel set.

uint32_t

A channel spacing in Hz of this channel set.

uint16_t

The number of channels (and not the channel number !)

uint16_t

minimum IF for the alternate PHY in kHz.

uint16_t

minimum IF for the base PHY in kHz.

bool

Indicates that OFDM modem is used by this alternate PHY.

uint32_t

rate Info of the alternate PHY.

uint32_t

AGC_CTRL1 configuration for CCA with hw modem.

Public Attribute Documentation#

baseFrequency#

uint32_t RAIL_AlternatePhy_t::baseFrequency

A base frequency in Hz of this channel set.


channelSpacing#

uint32_t RAIL_AlternatePhy_t::channelSpacing

A channel spacing in Hz of this channel set.


numberOfChannels#

uint16_t RAIL_AlternatePhy_t::numberOfChannels

The number of channels (and not the channel number !)


minIf_kHz#

uint16_t RAIL_AlternatePhy_t::minIf_kHz

minimum IF for the alternate PHY in kHz.


minBaseIf_kHz#

uint16_t RAIL_AlternatePhy_t::minBaseIf_kHz

minimum IF for the base PHY in kHz.


isOfdmModem#

bool RAIL_AlternatePhy_t::isOfdmModem

Indicates that OFDM modem is used by this alternate PHY.


rateInfo#

uint32_t RAIL_AlternatePhy_t::rateInfo

rate Info of the alternate PHY.


hwModemAgcCtrl1#

uint32_t RAIL_AlternatePhy_t::hwModemAgcCtrl1

AGC_CTRL1 configuration for CCA with hw modem.

Concurrent phy's AGC CCA-related registers are configured for CCA with OFDM modem. To perform a CCA with hw modem, AGC CTRL1 and CTRL7 need to be reconfigured. CTRL7_SUBPERIOD bit is set to 0 before the CCA and retored to 1 after. CTRL1 is reconfigured using hwModemAgcCtrl1 before the CCA and restore after using pSeqFrcConfig->agcCtrl1 where ofdm MODEM CCA configurations have been stored.