Configuration parameters for thermal protection.
Public Attributes#
bool
Indicates whether the protection is enabled.
uint8_t
Mandatory temperature cool down when the threshold is exceeded, in degrees Kelvin.
uint16_t
Temperature above which transmit is blocked, in degrees Kelvin.
Public Attribute Documentation#
enable#
bool RAIL_ChipTempConfig_t::enable
Indicates whether the protection is enabled.
Definition at line
5716
of file common/rail_types.h
coolDownK#
uint8_t RAIL_ChipTempConfig_t::coolDownK
Mandatory temperature cool down when the threshold is exceeded, in degrees Kelvin.
Definition at line
5718
of file common/rail_types.h
thresholdK#
uint16_t RAIL_ChipTempConfig_t::thresholdK
Temperature above which transmit is blocked, in degrees Kelvin.
Definition at line
5720
of file common/rail_types.h