Allows the user to specify direct mode parameters using RAIL_ConfigDirectMode().
Public Attributes#
Enable synchronous RX DOUT using DCLK vs.
Enable synchronous TX DIN using DCLK vs.
RX Data output (DOUT) GPIO port.
RX Data output (DOUT) GPIO pin.
Data clock (DCLK) GPIO port.
Data clock (DCLK) GPIO pin.
TX Data input (DIN) GPIO port.
TX Data input (DIN) GPIO pin.
Public Attribute Documentation#
syncRx#
bool RAIL_DirectModeConfig_t::syncRx
Enable synchronous RX DOUT using DCLK vs.
asynchronous RX DOUT.
5431
of file common/rail_types.h
syncTx#
bool RAIL_DirectModeConfig_t::syncTx
Enable synchronous TX DIN using DCLK vs.
asynchronous TX DIN.
5433
of file common/rail_types.h
doutPort#
uint8_t RAIL_DirectModeConfig_t::doutPort
RX Data output (DOUT) GPIO port.
5436
of file common/rail_types.h
doutPin#
uint8_t RAIL_DirectModeConfig_t::doutPin
RX Data output (DOUT) GPIO pin.
5438
of file common/rail_types.h
dclkPort#
uint8_t RAIL_DirectModeConfig_t::dclkPort
Data clock (DCLK) GPIO port.
Only used in synchronous mode.
5441
of file common/rail_types.h
dclkPin#
uint8_t RAIL_DirectModeConfig_t::dclkPin
Data clock (DCLK) GPIO pin.
Only used in synchronous mode.
5443
of file common/rail_types.h
dinPort#
uint8_t RAIL_DirectModeConfig_t::dinPort
TX Data input (DIN) GPIO port.
5446
of file common/rail_types.h
dinPin#
uint8_t RAIL_DirectModeConfig_t::dinPin
TX Data input (DIN) GPIO pin.
5448
of file common/rail_types.h
doutLoc#
uint8_t RAIL_DirectModeConfig_t::doutLoc
DeprecatedNo longer used (ignored).
5451
of file common/rail_types.h
dclkLoc#
uint8_t RAIL_DirectModeConfig_t::dclkLoc
DeprecatedNo longer used (ignored).
5453
of file common/rail_types.h
dinLoc#
uint8_t RAIL_DirectModeConfig_t::dinLoc
DeprecatedNo longer used (ignored).
5455
of file common/rail_types.h