Configuration structure for Z-Wave Long Range ACK.

Public Attributes#

int8_t

Radio noise level measured on the channel the frame is transmitted on.

int8_t

Transmit power used to transmit the ongoing Z-Wave Long Range ACK.

int8_t

Signal strength measured while receiving the Z-Wave Long Range frame.

Public Attribute Documentation#

noiseFloorDbm#

int8_t RAIL_ZWAVE_LrAckData_t::noiseFloorDbm

Radio noise level measured on the channel the frame is transmitted on.


Definition at line 405 of file protocol/zwave/rail_zwave.h

txPowerDbm#

int8_t RAIL_ZWAVE_LrAckData_t::txPowerDbm

Transmit power used to transmit the ongoing Z-Wave Long Range ACK.


Definition at line 407 of file protocol/zwave/rail_zwave.h

receiveRssiDbm#

int8_t RAIL_ZWAVE_LrAckData_t::receiveRssiDbm

Signal strength measured while receiving the Z-Wave Long Range frame.


Definition at line 409 of file protocol/zwave/rail_zwave.h