Features#
Overview of support for various features across hardware platforms.
These defines can be used at compile time to determine which features are available on your platform. However, keep in mind that these defines hold true for chip families. Your specific part may have further restrictions (band limitations, power amplifier restrictions, and so on) on top of those listed below, for which runtime RAIL_Supports*() APIs can be used to check availability on a particular chip (after RAIL_Init() has been called). In general, an attempt to call an API that is not supported on your chip family as listed below will result in a RAIL_STATUS_INVALID_CALL.
Functions#
Indicate whether RAIL supports 2.4 GHz band operation on this chip.
Indicate whether RAIL supports SubGHz band operation on this chip.
Indicate whether this chip supports dual 2.4 GHz and SubGHz band operation.
Indicate whether this chip supports bit masked address filtering.
Indicate whether this chip supports address filter mask information for incoming packets in RAIL_RxPacketInfo_t::filterMask and RAIL_IEEE802154_Address_t::filterMask.
Indicate whether this chip supports alternate TX power settings.
Indicate whether this chip supports antenna diversity.
Indicate whether this chip supports internal RF path diversity.
Indicate whether RAIL supports AUXADC measurements on this chip.
Indicate whether RAIL supports channel hopping on this chip.
Indicate whether this chip supports direct mode.
Indicate whether this chip supports dual sync words.
Indicate whether this chip supports start to start TX repeats.
Indicate whether this chip supports VDET.
Indicate whether RAIL supports thermistor measurements on this chip.
Indicate whether RAIL supports HFXO compensation on this chip.
Indicate whether this chip supports MFM protocol.
Indicate whether RAIL supports OFDM band operation on this chip.
Indicate whether this chip supports a high-precision LFRCO.
Indicate whether this chip supports radio entropy.
Indicate whether RAIL supports RFSENSE Energy Detection Mode on this chip.
Indicate whether RAIL supports RFSENSE Selective(OOK) Mode on this chip.
Indicate whether this chip supports configurable RSSI threshold set by RAIL_SetRssiDetectThreshold().
Indicate whether this chip supports RX direct mode data to FIFO.
Indicate whether this chip supports raw RX data sources other than RAIL_RxDataSource_t::RX_PACKET_DATA.
Indicate whether this chip supports SQ-based PHY.
Indicate whether this chip supports a particular power mode (PA).
Indicate whether this chip supports a particular power mode (PA) and provides the maximum and minimum power level for that power mode if supported by the chip.
Indicate whether this chip supports automatic TX to TX transitions.
Indicate whether RAIL supports the BLE protocol on this chip.
Indicate whether this chip supports BLE 1Mbps Non-Viterbi PHY.
Indicate whether this chip supports BLE 1Mbps Viterbi PHY.
Indicate whether this chip supports BLE 1Mbps operation.
Indicate whether this chip supports BLE 2Mbps Non-Viterbi PHY.
Indicate whether this chip supports BLE 2Mbps Viterbi PHY.
Indicate whether this chip supports BLE 2Mbps operation.
Indicate whether this chip supports BLE Antenna Switching needed for Angle-of-Arrival receives or Angle-of-Departure transmits.
Indicate whether this chip supports BLE Coded PHY used for Long-Range.
Indicate whether this chip supports BLE CTE (Constant Tone Extension) needed for Angle-of-Arrival/Departure transmits.
Indicate whether this chip supports BLE IQ Sampling needed for Angle-of-Arrival/Departure receives.
Indicate whether this chip supports BLE PHY switch to RX functionality, which is used to switch BLE PHYs at a specific time to receive auxiliary packets.
Indicate whether this chip supports the Quuppa PHY.
Indicate whether this chip supports BLE signal identifier.
Indicate whether this chip supports BLE Simulscan PHY used for simultaneous BLE 1Mbps and Coded PHY reception.
Indicate whether this chip supports the IEEE 802.15.4 protocol.
Indicate whether this chip supports the IEEE 802.15.4 Wi-Fi Coexistence PHY.
Indicate whether this chip supports the IEEE 802.15.4 2.4 GHz band variant.
Indicate whether this chip supports the thermal protection.
Indicate whether this chip supports the IEEE 802.15.4 2.4 RX channel switching.
Indicate whether this chip supports the IEEE 802.15.4 PHY with custom settings.
Indicate whether this chip supports the IEEE 802.15.4 front end module optimized PHY.
Indicate whether this chip supports canceling the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND when the radio transitions to a state that renders the the reporting of this event moot (i.e., too late for the stack to influence the outgoing ACK).
Indicate whether this chip supports early triggering of the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND just after MAC address fields have been received.
Indicate whether RAIL supports dual PA mode on this chip.
Indicate whether this chip supports IEEE 802.15.4E-2012 Enhanced ACKing.
Indicate whether this chip supports IEEE 802.15.4E-2012 Multipurpose frame reception.
Indicate whether this chip supports the IEEE 802.15.4E-2012 feature subset needed for Zigbee R22 GB868.
Indicate whether this chip supports IEEE 802.15.4G-2012 reception and transmission of frames with 4-byte CRC.
Indicate whether this chip supports IEEE 802.15.4G dynamic FEC.
Indicate whether this chip supports Wi-SUN.
Indicate whether this chip supports Wi-SUN mode switching.
Indicate whether this chip supports IEEE 802.15.4G-2012 feature subset needed for Zigbee R22 GB868.
Indicate whether this chip supports IEEE 802.15.4G-2012 reception of unwhitened frames.
Indicate whether this chip supports IEEE 802.15.4G-2012 transmission of unwhitened frames.
Indicate whether this chip supports WMBUS simultaneous M2O RX of T and C modes.
Indicate whether this chip supports the Z-Wave protocol.
Indicate whether this chip supports the Z-Wave concurrent PHY.
Indicate whether this chip supports the Z-Wave energy detect PHY.
Indicate whether this chip supports Z-Wave Region in PTI.
Indicate whether this chip supports IEEE 802.15.4 signal identifier.
Indicate whether this chip supports fast RX2RX.
Indicate whether this chip supports collision detection.
Indicate whether this chip supports Sidewalk protocol.
Indicate whether this chip supports automatic LNA bypass for external FEM.
Macros#
Boolean to indicate whether the selected chip supports both SubGHz and 2.4 GHz bands.
Backwards-compatible synonym of RAIL_SUPPORTS_DUAL_BAND.
Boolean to indicate whether the selected chip supports the 2.4 GHz band.
Backwards-compatible synonym of RAIL_SUPPORTS_2P4GHZ_BAND.
Boolean to indicate whether the selected chip supports SubGHz bands.
Backwards-compatible synonym of RAIL_SUPPORTS_SUBGHZ_BAND.
Boolean to indicate whether the selected chip supports OFDM PA.
Boolean to indicate whether the selected chip supports bit masked address filtering.
Boolean to indicate whether the selected chip supports address filter mask information for incoming packets in RAIL_RxPacketInfo_t::filterMask and RAIL_IEEE802154_Address_t::filterMask.
Boolean to indicate whether the selected chip supports alternate power settings for the Power Amplifier.
Backwards-compatible synonym of RAIL_SUPPORTS_ALTERNATE_TX_POWER.
Boolean to indicate whether the selected chip supports antenna diversity.
Backwards-compatible synonym of RAIL_SUPPORTS_ANTENNA_DIVERSITY.
Boolean to indicate whether the selected chip supports RF path diversity.
Boolean to indicate whether the selected chip supports channel hopping.
Backwards-compatible synonym of RAIL_SUPPORTS_CHANNEL_HOPPING.
Boolean to indicate whether the selected chip supports dual sync words.
Boolean to indicate whether the selected chip supports automatic transitions from TX to TX.
Boolean to indicate whether the selected chip supports RAIL_TX_REPEAT_OPTION_START_TO_START.
Boolean to indicate whether the selected chip supports thermistor measurements.
Backwards-compatible synonym of RAIL_SUPPORTS_EXTERNAL_THERMISTOR.
Boolean to indicate whether the selected chip supports HFXO compensation.
Boolean to indicate whether the selected chip supports AUXADC measurements.
Boolean to indicate whether the selected chip supports a high-precision LFRCO.
Boolean to indicate whether the selected chip supports radio entropy.
Boolean to indicate whether the selected chip supports RFSENSE Energy Detection Mode.
Boolean to indicate whether the selected chip supports RFSENSE Selective(OOK) Mode.
Backwards-compatible synonym of RAIL_SUPPORTS_RFSENSE_SELECTIVE_OOK.
Boolean to indicate whether the selected chip supports the VDET voltage measurement feature.
Boolean to indicate whether the selected chip supports BLE.
Boolean to indicate whether the selected chip supports BLE 1Mbps Non-Viterbi PHY.
Boolean to indicate whether the selected chip supports BLE 1Mbps Viterbi PHY.
Boolean to indicate whether the selected chip supports BLE 1Mbps operation.
Boolean to indicate whether the selected chip supports BLE 2Mbps Non-Viterbi PHY.
Boolean to indicate whether the selected chip supports BLE 2Mbps Viterbi PHY.
Boolean to indicate whether the selected chip supports BLE 2Mbps operation.
Boolean to indicate whether the selected chip supports BLE Antenna Switching needed for Angle-of-Arrival receives or Angle-of-Departure transmits.
Boolean to indicate whether the selected chip supports the BLE Coded PHY used for Long-Range.
Backwards-compatible synonym of RAIL_BLE_SUPPORTS_CODED_PHY.
Boolean to indicate whether the selected chip supports the BLE Simulscan PHY used for simultaneous BLE 1Mbps and Coded PHY reception.
Boolean to indicate whether the selected chip supports BLE CTE (Constant Tone Extension) needed for Angle-of-Arrival/Departure transmits.
Boolean to indicate whether the selected chip supports the Quuppa PHY.
Boolean to indicate whether the selected chip supports BLE IQ Sampling needed for Angle-of-Arrival/Departure receives.
Boolean to indicate whether the selected chip supports some BLE AOX features.
Backwards-compatible synonym of RAIL_BLE_SUPPORTS_AOX.
Boolean to indicate whether the selected chip supports BLE PHY switch to RX functionality, which is used to switch BLE PHYs at a specific time to receive auxiliary packets.
Backwards-compatible synonym of RAIL_BLE_SUPPORTS_PHY_SWITCH_TO_RX.
Boolean to indicate whether the selected chip supports IEEE 802.15.4.
Boolean to indicate whether the selected chip supports the 802.15.4 Wi-Fi Coexistence PHY.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_COEX_PHY.
Boolean to indicate whether the selected chip supports the IEEE 802.15.4 2.4 GHz band variant.
Boolean to indicate whether the selected chip supports the IEEE 802.15.4 2.4 RX channel switching.
Boolean to indicate whether the selected chip supports a front end module.
Boolean to indicate whether the selected chip supports IEEE 802.15.4E-2012 feature subset needed for Zigbee R22 GB868.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_E_SUBSET_GB868.
Boolean to indicate whether the selected chip supports IEEE 802.15.4E-2012 Enhanced ACKing.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_E_ENHANCED_ACK.
Boolean to indicate whether the selected chip supports receiving IEEE 802.15.4E-2012 Multipurpose frames.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_E_MULTIPURPOSE_FRAMES.
Boolean to indicate whether the selected chip supports IEEE 802.15.4G-2012 feature subset needed for Zigbee R22 GB868.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_G_SUBSET_GB868.
Boolean to indicate whether the selected chip supports dynamic FEC See also runtime refinement RAIL_IEEE802154_SupportsGDynFec().
Boolean to indicate whether the selected chip supports Wi-SUN mode switching See also runtime refinement RAIL_IEEE802154_SupportsGModeSwitch().
Boolean to indicate whether the selected chip supports IEEE 802.15.4G-2012 reception and transmission of frames with 4-byte CRC.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_G_4BYTE_CRC.
Boolean to indicate whether the selected chip supports IEEE 802.15.4G-2012 reception of unwhitened frames.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_G_UNWHITENED_RX.
Boolean to indicate whether the selected chip supports IEEE 802.15.4G-2012 transmission of unwhitened frames.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_G_UNWHITENED_TX.
Boolean to indicate whether the selected chip supports canceling the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND when the radio transitions to a state that renders the the reporting of this event moot (i.e., too late for the stack to influence the outgoing ACK).
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_CANCEL_FRAME_PENDING_LOOKUP.
Boolean to indicate whether the selected chip supports early triggering of the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND just after MAC address fields have been received.
Backwards-compatible synonym of RAIL_IEEE802154_SUPPORTS_EARLY_FRAME_PENDING_LOOKUP.
Boolean to indicate whether the selected chip supports dual PA configs for mode switch or concurrent mode.
Boolean to indicate whether the selected chip supports the pa power setting table.
Boolean to indicate whether the selected chip supports IEEE 802.15.4 PHY with custom settings.
Boolean to indicate whether the selected chip supports Wi-SUN See also runtime refinement RAIL_SupportsProtocolWiSUN().
Boolean to indicate whether the selected chip supports WMBUS simultaneous M2O RX of T and C modes set by RAIL_WMBUS_Config().
Boolean to indicate whether the selected chip supports Z-Wave.
Backwards-compatible synonym of RAIL_SUPPORTS_PROTOCOL_ZWAVE.
Boolean to indicate whether the selected chip supports energy detect PHY.
Boolean to indicate whether the selected chip supports concurrent PHY.
Boolean to indicate whether the selected chip supports SQ-based PHY.
Boolean to indicate whether the code supports Z-Wave region information in PTI and newer RAIL_ZWAVE_RegionConfig_t structure See also runtime refinement RAIL_ZWAVE_SupportsRegionPti().
Backwards-compatible synonym of RAIL_ZWAVE_SUPPORTS_REGION_PTI.
Boolean to indicate whether the selected chip supports raw RX data sources other than RAIL_RxDataSource_t::RX_PACKET_DATA.
Boolean to indicate whether the selected chip supports direct mode.
Boolean to indicate whether the selected chip supports RX direct mode data to FIFO.
Boolean to indicate whether the selected chip supports MFM protocol.
Boolean to indicate whether the selected chip supports 802.15.4 signal detection.
Boolean to indicate whether the selected chip supports BLE signal detection.
Boolean to indicate whether the selected chip supports configurable RSSI threshold set by RAIL_SetRssiDetectThreshold().
Boolean to indicate whether the selected chip supports thermal protection set by RAIL_ConfigThermalProtection().
Boolean to indicate whether the selected chip supports fast RX2RX enabled by RAIL_RX_OPTION_FAST_RX2RX.
Boolean to indicate whether the selected chip supports collision detection enabled by RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION See also runtime refinement RAIL_SupportsCollisionDetection().
Boolean to indicate whether the selected chip supports Sidewalk protocol.
Boolean to indicate whether the selected chip supports automatic LNA bypass for external FEM.
Function Documentation#
RAIL_Supports2p4GHzBand#
bool RAIL_Supports2p4GHzBand (RAIL_Handle_t railHandle)
Indicate whether RAIL supports 2.4 GHz band operation on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the 2.4 GHz band is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_2P4GHZ_BAND.
RAIL_SupportsSubGHzBand#
bool RAIL_SupportsSubGHzBand (RAIL_Handle_t railHandle)
Indicate whether RAIL supports SubGHz band operation on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the SubGHz band is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_SUBGHZ_BAND.
RAIL_SupportsDualBand#
bool RAIL_SupportsDualBand (RAIL_Handle_t railHandle)
Indicate whether this chip supports dual 2.4 GHz and SubGHz band operation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the dual band is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_DUAL_BAND.
RAIL_SupportsAddrFilterAddressBitMask#
bool RAIL_SupportsAddrFilterAddressBitMask (RAIL_Handle_t railHandle)
Indicate whether this chip supports bit masked address filtering.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if bit masked address filtering is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_ADDR_FILTER_ADDRESS_BIT_MASK.
RAIL_SupportsAddrFilterMask#
bool RAIL_SupportsAddrFilterMask (RAIL_Handle_t railHandle)
Indicate whether this chip supports address filter mask information for incoming packets in RAIL_RxPacketInfo_t::filterMask and RAIL_IEEE802154_Address_t::filterMask.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if address filter information is supported; false otherwise (in which case RAIL_RxPacketInfo_t::filterMask value is undefined). 
Runtime refinement of compile-time RAIL_SUPPORTS_ADDR_FILTER_MASK.
RAIL_SupportsAlternateTxPower#
bool RAIL_SupportsAlternateTxPower (RAIL_Handle_t railHandle)
Indicate whether this chip supports alternate TX power settings.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if alternate TX power settings are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_ALTERNATE_TX_POWER.
RAIL_SupportsAntennaDiversity#
bool RAIL_SupportsAntennaDiversity (RAIL_Handle_t railHandle)
Indicate whether this chip supports antenna diversity.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if antenna diversity is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_ANTENNA_DIVERSITY.
Note
- Certain radio configurations may not support this feature even if the chip in general claims to support it. 
RAIL_SupportsPathDiversity#
bool RAIL_SupportsPathDiversity (RAIL_Handle_t railHandle)
Indicate whether this chip supports internal RF path diversity.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if RF path diversity is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PATH_DIVERSITY.
Note
- Certain radio configurations may not support this feature even if the chip in general claims to support it. 
RAIL_SupportsAuxAdc#
bool RAIL_SupportsAuxAdc (RAIL_Handle_t railHandle)
Indicate whether RAIL supports AUXADC measurements on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if AUXADC measurements are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_AUXADC.
RAIL_SupportsChannelHopping#
bool RAIL_SupportsChannelHopping (RAIL_Handle_t railHandle)
Indicate whether RAIL supports channel hopping on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if channel hopping is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_CHANNEL_HOPPING.
RAIL_SupportsDirectMode#
bool RAIL_SupportsDirectMode (RAIL_Handle_t railHandle)
Indicate whether this chip supports direct mode.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if direct mode is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_DIRECT_MODE.
RAIL_SupportsDualSyncWords#
bool RAIL_SupportsDualSyncWords (RAIL_Handle_t railHandle)
Indicate whether this chip supports dual sync words.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if dual sync words are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_DUAL_SYNC_WORDS.
Note
- Certain radio configurations may not support this feature even if the chip in general claims to support it. 
RAIL_SupportsTxRepeatStartToStart#
bool RAIL_SupportsTxRepeatStartToStart (RAIL_Handle_t railHandle)
Indicate whether this chip supports start to start TX repeats.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if start to start TX repeats are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_TX_REPEAT_START_TO_START.
RAIL_SupportsVdet#
bool RAIL_SupportsVdet (RAIL_Handle_t railHandle)
Indicate whether this chip supports VDET.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if VDET is supported; false otherwise. 
RAIL_SupportsExternalThermistor#
bool RAIL_SupportsExternalThermistor (RAIL_Handle_t railHandle)
Indicate whether RAIL supports thermistor measurements on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if thermistor measurements are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_EXTERNAL_THERMISTOR.
RAIL_SupportsHFXOCompensation#
bool RAIL_SupportsHFXOCompensation (RAIL_Handle_t railHandle)
Indicate whether RAIL supports HFXO compensation on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if HFXO compensation is supported and RAIL_ConfigHFXOThermistor() has been successfully called; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_HFXO_COMPENSATION.
RAIL_SupportsMfm#
bool RAIL_SupportsMfm (RAIL_Handle_t railHandle)
Indicate whether this chip supports MFM protocol.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if MFM protocol is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_MFM.
RAIL_SupportsOFDMPA#
bool RAIL_SupportsOFDMPA (RAIL_Handle_t railHandle)
Indicate whether RAIL supports OFDM band operation on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if OFDM operation is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_OFDM_PA.
RAIL_SupportsPrecisionLFRCO#
bool RAIL_SupportsPrecisionLFRCO (RAIL_Handle_t railHandle)
Indicate whether this chip supports a high-precision LFRCO.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if high-precision LFRCO is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PRECISION_LFRCO.
RAIL_SupportsRadioEntropy#
bool RAIL_SupportsRadioEntropy (RAIL_Handle_t railHandle)
Indicate whether this chip supports radio entropy.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if radio entropy is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RADIO_ENTROPY.
RAIL_SupportsRfSenseEnergyDetection#
bool RAIL_SupportsRfSenseEnergyDetection (RAIL_Handle_t railHandle)
Indicate whether RAIL supports RFSENSE Energy Detection Mode on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if RFSENSE Energy Detection Mode is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RFSENSE_ENERGY_DETECTION.
RAIL_SupportsRfSenseSelectiveOok#
bool RAIL_SupportsRfSenseSelectiveOok (RAIL_Handle_t railHandle)
Indicate whether RAIL supports RFSENSE Selective(OOK) Mode on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if RFSENSE Selective(OOK) Mode is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RFSENSE_SELECTIVE_OOK.
RAIL_SupportsRssiDetectThreshold#
bool RAIL_SupportsRssiDetectThreshold (RAIL_Handle_t railHandle)
Indicate whether this chip supports configurable RSSI threshold set by RAIL_SetRssiDetectThreshold().
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if setting configurable RSSI is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RSSI_DETECT_THRESHOLD.
RAIL_SupportsRxDirectModeDataToFifo#
bool RAIL_SupportsRxDirectModeDataToFifo (RAIL_Handle_t railHandle)
Indicate whether this chip supports RX direct mode data to FIFO.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if direct mode data to FIFO is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RX_DIRECT_MODE_DATA_TO_FIFO.
RAIL_SupportsRxRawData#
bool RAIL_SupportsRxRawData (RAIL_Handle_t railHandle)
Indicate whether this chip supports raw RX data sources other than RAIL_RxDataSource_t::RX_PACKET_DATA.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if direct mode is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_RX_RAW_DATA.
RAIL_SupportsSQPhy#
bool RAIL_SupportsSQPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports SQ-based PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the SQ-based PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_SQ_PHY.
RAIL_SupportsTxPowerMode#
bool RAIL_SupportsTxPowerMode (RAIL_Handle_t railHandle, RAIL_TxPowerMode_t powerMode, RAIL_TxPowerLevel_t * pMaxPowerLevel)
Indicate whether this chip supports a particular power mode (PA).
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
| RAIL_TxPowerMode_t | [in] | powerMode | The power mode to check if supported. | 
| RAIL_TxPowerLevel_t * | [out] | pMaxPowerLevel | A pointer to a RAIL_TxPowerLevel_t that if non-NULL will be filled in with the power mode's highest power level allowed if this function returns true. | 
Returns
- true if the powerMode is supported; false otherwise. 
This function has no compile-time equivalent.
Note
- Consider using RAIL_SupportsTxPowerModeAlt to also get the power mode's lowest allowed power level. 
RAIL_SupportsTxPowerModeAlt#
bool RAIL_SupportsTxPowerModeAlt (RAIL_Handle_t railHandle, RAIL_TxPowerMode_t * powerMode, RAIL_TxPowerLevel_t * maxPowerLevel, RAIL_TxPowerLevel_t * minPowerLevel)
Indicate whether this chip supports a particular power mode (PA) and provides the maximum and minimum power level for that power mode if supported by the chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
| RAIL_TxPowerMode_t * | [inout] | powerMode | A pointer to PA power mode to check if supported. For platforms that support RAIL_TX_POWER_MODE_2P4GIG_HIGHEST or RAIL_TX_POWER_MODE_SUBGIG_HIGHEST the powerMode is updated to the highest corresponding PA available on the chip. | 
| RAIL_TxPowerLevel_t * | [out] | maxPowerLevel | A pointer to a RAIL_TxPowerLevel_t that if non-NULL will be filled in with the power mode's highest power level allowed if this function returns true. | 
| RAIL_TxPowerLevel_t * | [out] | minPowerLevel | A pointer to a RAIL_TxPowerLevel_t that if non-NULL will be filled in with the power mode's lowest power level allowed if this function returns true. | 
Returns
- true if powerMode is supported; false otherwise. 
RAIL_SupportsTxToTx#
bool RAIL_SupportsTxToTx (RAIL_Handle_t railHandle)
Indicate whether this chip supports automatic TX to TX transitions.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if TX to TX transitions are supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_TX_TO_TX.
RAIL_SupportsProtocolBLE#
bool RAIL_SupportsProtocolBLE (RAIL_Handle_t railHandle)
Indicate whether RAIL supports the BLE protocol on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PROTOCOL_BLE.
RAIL_BLE_Supports1MbpsNonViterbi#
bool RAIL_BLE_Supports1MbpsNonViterbi (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 1Mbps Non-Viterbi PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 1Mbps Non-Viterbi is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_1MBPS_NON_VITERBI.
RAIL_BLE_Supports1MbpsViterbi#
bool RAIL_BLE_Supports1MbpsViterbi (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 1Mbps Viterbi PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 1Mbps Viterbi is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_1MBPS_VITERBI.
RAIL_BLE_Supports1Mbps#
static bool RAIL_BLE_Supports1Mbps (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 1Mbps operation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 1Mbps operation is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_1MBPS.
RAIL_BLE_Supports2MbpsNonViterbi#
bool RAIL_BLE_Supports2MbpsNonViterbi (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 2Mbps Non-Viterbi PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 2Mbps Non-Viterbi is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_2MBPS_NON_VITERBI.
RAIL_BLE_Supports2MbpsViterbi#
bool RAIL_BLE_Supports2MbpsViterbi (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 2Mbps Viterbi PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 2Mbps Viterbi is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_2MBPS_VITERBI.
RAIL_BLE_Supports2Mbps#
static bool RAIL_BLE_Supports2Mbps (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE 2Mbps operation.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE 2Mbps operation is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_2MBPS.
RAIL_BLE_SupportsAntennaSwitching#
bool RAIL_BLE_SupportsAntennaSwitching (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE Antenna Switching needed for Angle-of-Arrival receives or Angle-of-Departure transmits.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE Antenna Switching is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_ANTENNA_SWITCHING.
RAIL_BLE_SupportsCodedPhy#
bool RAIL_BLE_SupportsCodedPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE Coded PHY used for Long-Range.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE Coded PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_CODED_PHY.
RAIL_BLE_SupportsCte#
bool RAIL_BLE_SupportsCte (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE CTE (Constant Tone Extension) needed for Angle-of-Arrival/Departure transmits.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE CTE is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_CTE.
RAIL_BLE_SupportsIQSampling#
bool RAIL_BLE_SupportsIQSampling (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE IQ Sampling needed for Angle-of-Arrival/Departure receives.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE IQ Sampling is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_IQ_SAMPLING.
RAIL_BLE_SupportsPhySwitchToRx#
bool RAIL_BLE_SupportsPhySwitchToRx (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE PHY switch to RX functionality, which is used to switch BLE PHYs at a specific time to receive auxiliary packets.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE PHY switch to RX is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_PHY_SWITCH_TO_RX.
RAIL_BLE_SupportsQuuppa#
bool RAIL_BLE_SupportsQuuppa (RAIL_Handle_t railHandle)
Indicate whether this chip supports the Quuppa PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the Quuppa is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_QUUPPA.
RAIL_BLE_SupportsSignalIdentifier#
bool RAIL_BLE_SupportsSignalIdentifier (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE signal identifier.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if signal identifier is supported; false otherwise. 
RAIL_BLE_SupportsSimulscanPhy#
bool RAIL_BLE_SupportsSimulscanPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports BLE Simulscan PHY used for simultaneous BLE 1Mbps and Coded PHY reception.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if BLE Simulscan PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_BLE_SUPPORTS_SIMULSCAN_PHY.
RAIL_SupportsProtocolIEEE802154#
bool RAIL_SupportsProtocolIEEE802154 (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 protocol.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the 802.15.4 protocol is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PROTOCOL_IEEE802154.
RAIL_IEEE802154_SupportsCoexPhy#
bool RAIL_IEEE802154_SupportsCoexPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 Wi-Fi Coexistence PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the 802.15.4 COEX PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_COEX_PHY.
RAIL_SupportsIEEE802154Band2P4#
bool RAIL_SupportsIEEE802154Band2P4 (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 2.4 GHz band variant.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if IEEE 802.15.4 2.4 GHz band variant is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_IEEE802154_BAND_2P4.
RAIL_SupportsThermalProtection#
bool RAIL_SupportsThermalProtection (RAIL_Handle_t railHandle)
Indicate whether this chip supports the thermal protection.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if thermal protection is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_THERMAL_PROTECTION.
RAIL_IEEE802154_SupportsRxChannelSwitching#
bool RAIL_IEEE802154_SupportsRxChannelSwitching (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 2.4 RX channel switching.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if IEEE 802.15.4 2.4 GHz RX channel switching is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_RX_CHANNEL_SWITCHING.
RAIL_IEEE802154_SupportsCustom1Phy#
bool RAIL_IEEE802154_SupportsCustom1Phy (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 PHY with custom settings.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the 802.15.4 PHY with custom settings is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_CUSTOM1_PHY.
RAIL_IEEE802154_SupportsFemPhy#
bool RAIL_IEEE802154_SupportsFemPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4 front end module optimized PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if a front end module is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_FEM_PHY.
RAIL_IEEE802154_SupportsCancelFramePendingLookup#
bool RAIL_IEEE802154_SupportsCancelFramePendingLookup (RAIL_Handle_t railHandle)
Indicate whether this chip supports canceling the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND when the radio transitions to a state that renders the the reporting of this event moot (i.e., too late for the stack to influence the outgoing ACK).
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if canceling the lookup event is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_CANCEL_FRAME_PENDING_LOOKUP.
RAIL_IEEE802154_SupportsEarlyFramePendingLookup#
bool RAIL_IEEE802154_SupportsEarlyFramePendingLookup (RAIL_Handle_t railHandle)
Indicate whether this chip supports early triggering of the frame-pending lookup event RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND just after MAC address fields have been received.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if early triggering is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_EARLY_FRAME_PENDING_LOOKUP.
RAIL_IEEE802154_SupportsDualPaConfig#
bool RAIL_IEEE802154_SupportsDualPaConfig (RAIL_Handle_t railHandle)
Indicate whether RAIL supports dual PA mode on this chip.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the dual PA mode is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_DUAL_PA_CONFIG.
RAIL_IEEE802154_SupportsEEnhancedAck#
bool RAIL_IEEE802154_SupportsEEnhancedAck (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4E-2012 Enhanced ACKing.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4E Enhanced ACKing is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_E_ENHANCED_ACK.
RAIL_IEEE802154_SupportsEMultipurposeFrames#
bool RAIL_IEEE802154_SupportsEMultipurposeFrames (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4E-2012 Multipurpose frame reception.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if Multipurpose frame reception is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_E_MULTIPURPOSE_FRAMES.
RAIL_IEEE802154_SupportsESubsetGB868#
bool RAIL_IEEE802154_SupportsESubsetGB868 (RAIL_Handle_t railHandle)
Indicate whether this chip supports the IEEE 802.15.4E-2012 feature subset needed for Zigbee R22 GB868.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4E GB868 subset is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_E_SUBSET_GB868.
RAIL_IEEE802154_SupportsG4ByteCrc#
bool RAIL_IEEE802154_SupportsG4ByteCrc (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4G-2012 reception and transmission of frames with 4-byte CRC.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4G 4-byte CRC is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_4BYTE_CRC.
RAIL_IEEE802154_SupportsGDynFec#
bool RAIL_IEEE802154_SupportsGDynFec (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4G dynamic FEC.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if dynamic FEC is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_DYNFEC.
RAIL_SupportsProtocolWiSUN#
bool RAIL_SupportsProtocolWiSUN (RAIL_Handle_t railHandle)
Indicate whether this chip supports Wi-SUN.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if Wi-SUN is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PROTOCOL_WI_SUN.
RAIL_IEEE802154_SupportsGModeSwitch#
bool RAIL_IEEE802154_SupportsGModeSwitch (RAIL_Handle_t railHandle)
Indicate whether this chip supports Wi-SUN mode switching.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if Wi-SUN mode switching is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_MODESWITCH.
RAIL_IEEE802154_SupportsGSubsetGB868#
bool RAIL_IEEE802154_SupportsGSubsetGB868 (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4G-2012 feature subset needed for Zigbee R22 GB868.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4G GB868 subset is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_SUBSET_GB868.
RAIL_IEEE802154_SupportsGUnwhitenedRx#
bool RAIL_IEEE802154_SupportsGUnwhitenedRx (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4G-2012 reception of unwhitened frames.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4G unwhitened frame reception is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_UNWHITENED_RX.
RAIL_IEEE802154_SupportsGUnwhitenedTx#
bool RAIL_IEEE802154_SupportsGUnwhitenedTx (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4G-2012 transmission of unwhitened frames.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if 802.15.4G unwhitened frame transmit is supported; false otherwise. 
Runtime refinement of compile-time RAIL_IEEE802154_SUPPORTS_G_UNWHITENED_TX.
RAIL_WMBUS_SupportsSimultaneousTCRx#
bool RAIL_WMBUS_SupportsSimultaneousTCRx (RAIL_Handle_t railHandle)
Indicate whether this chip supports WMBUS simultaneous M2O RX of T and C modes.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the WMBUS simultaneous M2O RX of T and C modes is supported; false otherwise. 
Runtime refinement of compile-time RAIL_WMBUS_SUPPORTS_SIMULTANEOUS_T_C_RX.
RAIL_SupportsProtocolZWave#
bool RAIL_SupportsProtocolZWave (RAIL_Handle_t railHandle)
Indicate whether this chip supports the Z-Wave protocol.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the Z-Wave protocol is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PROTOCOL_ZWAVE.
RAIL_ZWAVE_SupportsConcPhy#
bool RAIL_ZWAVE_SupportsConcPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports the Z-Wave concurrent PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the Z-Wave concurrent PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_ZWAVE_SUPPORTS_CONC_PHY.
RAIL_ZWAVE_SupportsEnergyDetectPhy#
bool RAIL_ZWAVE_SupportsEnergyDetectPhy (RAIL_Handle_t railHandle)
Indicate whether this chip supports the Z-Wave energy detect PHY.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if the Z-Wave energy detect PHY is supported; false otherwise. 
Runtime refinement of compile-time RAIL_ZWAVE_SUPPORTS_ED_PHY.
RAIL_ZWAVE_SupportsRegionPti#
bool RAIL_ZWAVE_SupportsRegionPti (RAIL_Handle_t railHandle)
Indicate whether this chip supports Z-Wave Region in PTI.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if ZWAVE Region in PTI is supported; false otherwise. 
Runtime refinement of compile-time RAIL_ZWAVE_SUPPORTS_REGION_PTI.
RAIL_IEEE802154_SupportsSignalIdentifier#
bool RAIL_IEEE802154_SupportsSignalIdentifier (RAIL_Handle_t railHandle)
Indicate whether this chip supports IEEE 802.15.4 signal identifier.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if signal identifier is supported; false otherwise. 
RAIL_SupportsFastRx2Rx#
bool RAIL_SupportsFastRx2Rx (RAIL_Handle_t railHandle)
Indicate whether this chip supports fast RX2RX.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if fast RX2RX is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_FAST_RX2RX.
RAIL_SupportsCollisionDetection#
bool RAIL_SupportsCollisionDetection (RAIL_Handle_t railHandle)
Indicate whether this chip supports collision detection.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if collision detection is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_COLLISION_DETECTION.
RAIL_SupportsProtocolSidewalk#
bool RAIL_SupportsProtocolSidewalk (RAIL_Handle_t railHandle)
Indicate whether this chip supports Sidewalk protocol.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if Sidewalk protocol is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_PROTOCOL_SIDEWALK.
RAIL_SupportsAutoLnaBypass#
bool RAIL_SupportsAutoLnaBypass (RAIL_Handle_t railHandle)
Indicate whether this chip supports automatic LNA bypass for external FEM.
| Type | Direction | Argument Name | Description | 
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A radio-generic or real RAIL instance handle. | 
Returns
- true if automatic LNA bypass is supported; false otherwise. 
Runtime refinement of compile-time RAIL_SUPPORTS_AUTO_LNA_BYPASS.