Events#

APIs related to events.

Enumerations#

enum
RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT = 0
RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT = 1
RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT = 2
RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT = 3
RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT = 4
RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT = 5
RAIL_EVENT_RX_SYNC1_DETECT_SHIFT = 6
RAIL_EVENT_RX_SYNC2_DETECT_SHIFT = 7
RAIL_EVENT_RX_FRAME_ERROR_SHIFT = 8
RAIL_EVENT_RX_FIFO_FULL_SHIFT = 9
RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT = 10
RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT = 11
RAIL_EVENT_RX_TIMEOUT_SHIFT = 12
RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT = 13
RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT = 14
RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT = 15
RAIL_EVENT_RX_PACKET_ABORTED_SHIFT = 16
RAIL_EVENT_RX_FILTER_PASSED_SHIFT = 17
RAIL_EVENT_RX_TIMING_LOST_SHIFT = 18
RAIL_EVENT_RX_TIMING_DETECT_SHIFT = 19
RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT = 20
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT = 21
RAIL_EVENT_ZWAVE_BEAM_SHIFT = 22
RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT = 23
RAIL_EVENT_TX_PACKET_SENT_SHIFT = 24
RAIL_EVENT_TXACK_PACKET_SENT_SHIFT = 25
RAIL_EVENT_TX_ABORTED_SHIFT = 26
RAIL_EVENT_TXACK_ABORTED_SHIFT = 27
RAIL_EVENT_TX_BLOCKED_SHIFT = 28
RAIL_EVENT_TXACK_BLOCKED_SHIFT = 29
RAIL_EVENT_TX_UNDERFLOW_SHIFT = 30
RAIL_EVENT_TXACK_UNDERFLOW_SHIFT = 31
RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT = 32
RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT = 33
RAIL_EVENT_TX_CCA_RETRY_SHIFT = 34
RAIL_EVENT_TX_START_CCA_SHIFT = 35
RAIL_EVENT_TX_STARTED_SHIFT = 36
RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT = 37
RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT = 38
RAIL_EVENT_CONFIG_SCHEDULED_SHIFT = 39
RAIL_EVENT_SCHEDULER_STATUS_SHIFT = 40
RAIL_EVENT_CAL_NEEDED_SHIFT = 41
RAIL_EVENT_RF_SENSED_SHIFT = 42
RAIL_EVENT_PA_PROTECTION_SHIFT = 43
RAIL_EVENT_SIGNAL_DETECTED_SHIFT = 44
RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT = 45
RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT = 46
RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT = 47
RAIL_EVENT_THERMISTOR_DONE_SHIFT = 48
RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT = 49
RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT = 50
RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT = 51
RAIL_EVENT_USER_MBOX_SHIFT = 52
}

RAIL events passed to the event callback.

Functions#

RAIL_ConfigEvents(RAIL_Handle_t railHandle, RAIL_Events_t mask, RAIL_Events_t events)

Configure radio events.

Macros#

#define
RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT

Shift position of RAIL_EVENT_SCHEDULED_TX_STARTED bit.

#define
RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT

Shift position of RAIL_EVENT_RX_DUTY_CYCLE_RX_END bit.

#define
RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT
#define
RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_MFM_TX_BUFFER_DONE bit.

#define
RAIL_EVENTS_NONE 0ULL

A value representing no events.

#define
RAIL_EVENT_RSSI_AVERAGE_DONE (1ULL << RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT)

Occurs when the hardware-averaged RSSI is done in response to RAIL_StartAverageRssi() to indicate that the hardware has completed averaging.

#define
RAIL_EVENT_RX_ACK_TIMEOUT (1ULL << RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT)

Occurs when the ACK timeout expires while waiting to receive the sync word of an expected ACK.

#define
RAIL_EVENT_RX_FIFO_ALMOST_FULL (1ULL << RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT)

Keeps occurring as long as the number of bytes in the receive FIFO exceeds the configured threshold value.

#define
RAIL_EVENT_RX_PACKET_RECEIVED (1ULL << RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT)

Occurs whenever a packet is received with RAIL_RX_PACKET_READY_SUCCESS or RAIL_RX_PACKET_READY_CRC_ERROR.

#define
RAIL_EVENT_RX_PREAMBLE_LOST (1ULL << RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT)

Occurs when the radio has lost a preamble.

#define
RAIL_EVENT_RX_PREAMBLE_DETECT (1ULL << RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT)

Occurs when the radio has detected a preamble.

#define
RAIL_EVENT_RX_SYNC1_DETECT (1ULL << RAIL_EVENT_RX_SYNC1_DETECT_SHIFT)

Occurs when the first sync word is detected.

#define
RAIL_EVENT_RX_SYNC2_DETECT (1ULL << RAIL_EVENT_RX_SYNC2_DETECT_SHIFT)

Occurs when the second sync word is detected.

#define
RAIL_EVENT_RX_FRAME_ERROR (1ULL << RAIL_EVENT_RX_FRAME_ERROR_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_CRC_ERROR which only happens after any filtering has passed.

#define
RAIL_EVENT_RX_FIFO_FULL (1ULL << RAIL_EVENT_RX_FIFO_FULL_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs coincident to a receive packet completion event in which the receive FIFO or any supplemental packet metadata FIFO (see Data Management) are full and further packet reception is jeopardized.

#define
RAIL_EVENT_RX_FIFO_OVERFLOW (1ULL << RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT)

When using RAIL_RxDataSource_t::RX_PACKET_DATA this event occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_OVERFLOW due to overflowing the receive FIFO or any supplemental packet metadata FIFO (see Data Management).

#define
RAIL_EVENT_RX_ADDRESS_FILTERED (1ULL << RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT)

Occurs when a receive is aborted with RAIL_RX_PACKET_ABORT_FILTERED because its address does not match the filtering settings.

#define
RAIL_EVENT_RX_TIMEOUT (1ULL << RAIL_EVENT_RX_TIMEOUT_SHIFT)

Occurs when an RX event times out.

#define
RAIL_EVENT_SCHEDULED_RX_STARTED (1ULL << RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT)

Occurs when a scheduled RX begins turning on the receiver.

#define
RAIL_EVENT_SCHEDULED_TX_STARTED (1ULL << RAIL_EVENT_SCHEDULED_TX_STARTED_SHIFT)

Occurs when a scheduled TX begins turning on the transmitter.

#define
RAIL_EVENT_RX_SCHEDULED_RX_END (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT)

Occurs when the scheduled RX window ends.

#define
RAIL_EVENT_RX_SCHEDULED_RX_MISSED (1ULL << RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT)

Occurs when start of a scheduled receive is missed.

#define
RAIL_EVENT_RX_PACKET_ABORTED (1ULL << RAIL_EVENT_RX_PACKET_ABORTED_SHIFT)

Occurs when a receive is aborted during filtering with RAIL_RX_PACKET_ABORT_FORMAT or after filtering with RAIL_RX_PACKET_ABORT_ABORTED for reasons other than address filtering mismatch (which triggers RAIL_EVENT_RX_ADDRESS_FILTERED instead).

#define
RAIL_EVENT_RX_FILTER_PASSED (1ULL << RAIL_EVENT_RX_FILTER_PASSED_SHIFT)

Occurs when the packet has passed any configured address and frame filtering options.

#define
RAIL_EVENT_RX_TIMING_LOST (1ULL << RAIL_EVENT_RX_TIMING_LOST_SHIFT)

Occurs when the modem timing is lost.

#define
RAIL_EVENT_RX_TIMING_DETECT (1ULL << RAIL_EVENT_RX_TIMING_DETECT_SHIFT)

Occurs when the modem timing is detected.

#define
RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE (1ULL << RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT)

Occurs when RX Channel Hopping is enabled and channel hopping finishes receiving on the last channel in its sequence.

#define
RAIL_EVENT_RX_DUTY_CYCLE_RX_END (1ULL << RAIL_EVENT_RX_DUTY_CYCLE_RX_END_SHIFT)

Occurs during RX duty cycle mode when the radio finishes its time in receive mode.

#define
RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND (1ULL << RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT)

Indicate a Data Request is received when using IEEE 802.15.4 functionality.

#define
RAIL_EVENT_ZWAVE_BEAM (1ULL << RAIL_EVENT_ZWAVE_BEAM_SHIFT)

Indicate a Z-Wave Beam Request relevant to the node was received.

#define
RAIL_EVENT_MFM_TX_BUFFER_DONE (1ULL << RAIL_EVENT_MFM_TX_BUFFER_DONE_SHIFT)

Indicate a MFM buffer has completely transmitted.

#define
RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND (1ULL << RAIL_EVENT_ZWAVE_LR_ACK_REQUEST_COMMAND_SHIFT)

Indicate a request for populating Z-Wave LR ACK packet.

#define
RAIL_EVENTS_RX_COMPLETION undefined

The mask representing all events that determine the end of a received packet.

#define
RAIL_EVENT_TX_FIFO_ALMOST_EMPTY (1ULL << RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT)

Occurs when the number of bytes in the transmit FIFO falls below the configured threshold value.

#define
RAIL_EVENT_TX_PACKET_SENT (1ULL << RAIL_EVENT_TX_PACKET_SENT_SHIFT)

Occurs after a packet has been transmitted.

#define
RAIL_EVENT_TXACK_PACKET_SENT (1ULL << RAIL_EVENT_TXACK_PACKET_SENT_SHIFT)

Occurs after an ACK packet has been transmitted.

#define
RAIL_EVENT_TX_ABORTED (1ULL << RAIL_EVENT_TX_ABORTED_SHIFT)

Occurs when a transmit is aborted by the user.

#define
RAIL_EVENT_TXACK_ABORTED (1ULL << RAIL_EVENT_TXACK_ABORTED_SHIFT)

Occurs when an ACK transmit is aborted by the user.

#define
RAIL_EVENT_TX_BLOCKED (1ULL << RAIL_EVENT_TX_BLOCKED_SHIFT)

Occurs when a transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

#define
RAIL_EVENT_TXACK_BLOCKED (1ULL << RAIL_EVENT_TXACK_BLOCKED_SHIFT)

Occurs when an ACK transmit is blocked from occurring because RAIL_EnableTxHoldOff() was called.

#define
RAIL_EVENT_TX_UNDERFLOW (1ULL << RAIL_EVENT_TX_UNDERFLOW_SHIFT)

Occurs when the transmit buffer underflows.

#define
RAIL_EVENT_TXACK_UNDERFLOW (1ULL << RAIL_EVENT_TXACK_UNDERFLOW_SHIFT)

Occurs when the ACK transmit buffer underflows.

#define
RAIL_EVENT_TX_CHANNEL_CLEAR (1ULL << RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) succeeds.

#define
RAIL_EVENT_TX_CHANNEL_BUSY (1ULL << RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT)

Occurs when Carrier Sense Multiple Access (CSMA) or Listen Before Talk (LBT) fails.

#define
RAIL_EVENT_TX_CCA_RETRY (1ULL << RAIL_EVENT_TX_CCA_RETRY_SHIFT)

Occurs during CSMA or LBT when an individual Clear Channel Assessment (CCA) check fails, but there are more tries needed before the overall operation completes.

#define
RAIL_EVENT_TX_START_CCA (1ULL << RAIL_EVENT_TX_START_CCA_SHIFT)

Occurs when the receiver is activated to perform a Clear Channel Assessment (CCA) check.

#define
RAIL_EVENT_TX_STARTED (1ULL << RAIL_EVENT_TX_STARTED_SHIFT)

Occurs when the radio starts transmitting a normal packet on the air.

#define
RAIL_TX_STARTED_BYTES 0U

A value to pass as RAIL_GetTxTimePreambleStart() totalPacketBytes parameter to retrieve the RAIL_EVENT_TX_STARTED timestamp.

#define
RAIL_EVENT_TX_SCHEDULED_TX_MISSED (1ULL << RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT)

Occurs when the start of a scheduled transmit is missed.

#define
RAIL_EVENTS_TX_COMPLETION undefined

A mask representing all events that determine the end of a transmitted packet.

#define
RAIL_EVENTS_TXACK_COMPLETION undefined

A mask representing all events that determine the end of a transmitted ACK packet.

#define
RAIL_EVENT_CONFIG_UNSCHEDULED (1ULL << RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT)

Occurs when the scheduler switches away from this configuration.

#define
RAIL_EVENT_CONFIG_SCHEDULED (1ULL << RAIL_EVENT_CONFIG_SCHEDULED_SHIFT)

Occurs when the scheduler switches to this configuration.

#define
RAIL_EVENT_SCHEDULER_STATUS (1ULL << RAIL_EVENT_SCHEDULER_STATUS_SHIFT)

Occurs when the scheduler has a status to report.

#define
RAIL_EVENT_CAL_NEEDED (1ULL << RAIL_EVENT_CAL_NEEDED_SHIFT)

Occurs when the application needs to run a calibration, as determined by the RAIL library.

#define
RAIL_EVENT_RF_SENSED (1ULL << RAIL_EVENT_RF_SENSED_SHIFT)

Occurs when RF energy is sensed from the radio.

#define
RAIL_EVENT_PA_PROTECTION (1ULL << RAIL_EVENT_PA_PROTECTION_SHIFT)

Occurs when PA protection circuit kicks in.

#define
RAIL_EVENT_SIGNAL_DETECTED (1ULL << RAIL_EVENT_SIGNAL_DETECTED_SHIFT)

Occurs after enabling the signal detection using RAIL_BLE_EnableSignalDetection or RAIL_IEEE802154_EnableSignalDetection when a signal is detected.

#define
RAIL_EVENT_IEEE802154_MODESWITCH_START (1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT)

Occurs when a Wi-SUN mode switch packet has been received, after switching to the new PHY.

#define
RAIL_EVENT_IEEE802154_MODESWITCH_END (1ULL << RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT)

Occurs when switching back to the original base PHY in effect prior to the Wi-SUN mode switch reception.

#define
RAIL_EVENT_DETECT_RSSI_THRESHOLD (1ULL << RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT)

Occurs when the sampled RSSI is above the threshold set by RAIL_SetRssiDetectThreshold().

#define
RAIL_EVENT_THERMISTOR_DONE (1ULL << RAIL_EVENT_THERMISTOR_DONE_SHIFT)

Occurs when the thermistor has finished its measurement in response to RAIL_StartThermistorMeasurement().

#define
RAIL_EVENT_TX_BLOCKED_TOO_HOT (1ULL << RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT)

Occurs when a Tx has been blocked because of temperature exceeding the safety threshold.

#define
RAIL_EVENT_TEMPERATURE_TOO_HOT (1ULL << RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT)

Occurs when die internal temperature exceeds the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

#define
RAIL_EVENT_TEMPERATURE_COOL_DOWN (1ULL << RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT)

Occurs when die internal temperature falls below the temperature threshold subtracted by the cool down parameter from RAIL_ChipTempConfig_t.

#define
RAIL_EVENT_USER_MBOX (1ULL << RAIL_EVENT_USER_MBOX_SHIFT)

Occurs when the user received a mailbox message.

#define
RAIL_EVENTS_ALL 0xFFFFFFFFFFFFFFFFULL

A value representing all possible events.

Enumeration Documentation#

RAIL_Events_t#

RAIL_Events_t

RAIL events passed to the event callback.

More than one event may be indicated due to interrupt latency.

Enumerator
RAIL_EVENT_RSSI_AVERAGE_DONE_SHIFT

Shift position of RAIL_EVENT_RSSI_AVERAGE_DONE bit.

RAIL_EVENT_RX_ACK_TIMEOUT_SHIFT

Shift position of RAIL_EVENT_RX_ACK_TIMEOUT bit.

RAIL_EVENT_RX_FIFO_ALMOST_FULL_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_ALMOST_FULL bit.

RAIL_EVENT_RX_PACKET_RECEIVED_SHIFT

Shift position of RAIL_EVENT_RX_PACKET_RECEIVED bit.

RAIL_EVENT_RX_PREAMBLE_LOST_SHIFT

Shift position of RAIL_EVENT_RX_PREAMBLE_LOST bit.

RAIL_EVENT_RX_PREAMBLE_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_PREAMBLE_DETECT bit.

RAIL_EVENT_RX_SYNC1_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_SYNC1_DETECT bit.

RAIL_EVENT_RX_SYNC2_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_SYNC2_DETECT bit.

RAIL_EVENT_RX_FRAME_ERROR_SHIFT

Shift position of RAIL_EVENT_RX_FRAME_ERROR bit.

RAIL_EVENT_RX_FIFO_FULL_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_FULL bit.

RAIL_EVENT_RX_FIFO_OVERFLOW_SHIFT

Shift position of RAIL_EVENT_RX_FIFO_OVERFLOW bit.

RAIL_EVENT_RX_ADDRESS_FILTERED_SHIFT

Shift position of RAIL_EVENT_RX_ADDRESS_FILTERED bit.

RAIL_EVENT_RX_TIMEOUT_SHIFT

Shift position of RAIL_EVENT_RX_TIMEOUT bit.

RAIL_EVENT_SCHEDULED_RX_STARTED_SHIFT

Shift position of RAIL_EVENT_SCHEDULED_RX_STARTED bit.

RAIL_EVENT_RX_SCHEDULED_RX_END_SHIFT

Shift position of RAIL_EVENT_RX_SCHEDULED_RX_END bit.

RAIL_EVENT_RX_SCHEDULED_RX_MISSED_SHIFT

Shift position of RAIL_EVENT_RX_SCHEDULED_RX_MISSED bit.

RAIL_EVENT_RX_PACKET_ABORTED_SHIFT

Shift position of RAIL_EVENT_RX_PACKET_ABORTED bit.

RAIL_EVENT_RX_FILTER_PASSED_SHIFT

Shift position of RAIL_EVENT_RX_FILTER_PASSED bit.

RAIL_EVENT_RX_TIMING_LOST_SHIFT

Shift position of RAIL_EVENT_RX_TIMING_LOST bit.

RAIL_EVENT_RX_TIMING_DETECT_SHIFT

Shift position of RAIL_EVENT_RX_TIMING_DETECT bit.

RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE_SHIFT

Shift position of RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE bit.

RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND_SHIFT

Shift position of RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND bit.

RAIL_EVENT_ZWAVE_BEAM_SHIFT

Shift position of RAIL_EVENT_ZWAVE_BEAM bit.

RAIL_EVENT_TX_FIFO_ALMOST_EMPTY_SHIFT

Shift position of RAIL_EVENT_TX_FIFO_ALMOST_EMPTY bit.

RAIL_EVENT_TX_PACKET_SENT_SHIFT

Shift position of RAIL_EVENT_TX_PACKET_SENT bit.

RAIL_EVENT_TXACK_PACKET_SENT_SHIFT

Shift position of RAIL_EVENT_TXACK_PACKET_SENT bit.

RAIL_EVENT_TX_ABORTED_SHIFT

Shift position of RAIL_EVENT_TX_ABORTED bit.

RAIL_EVENT_TXACK_ABORTED_SHIFT

Shift position of RAIL_EVENT_TXACK_ABORTED bit.

RAIL_EVENT_TX_BLOCKED_SHIFT

Shift position of RAIL_EVENT_TX_BLOCKED bit.

RAIL_EVENT_TXACK_BLOCKED_SHIFT

Shift position of RAIL_EVENT_TXACK_BLOCKED bit.

RAIL_EVENT_TX_UNDERFLOW_SHIFT

Shift position of RAIL_EVENT_TX_UNDERFLOW bit.

RAIL_EVENT_TXACK_UNDERFLOW_SHIFT

Shift position of RAIL_EVENT_TXACK_UNDERFLOW bit.

RAIL_EVENT_TX_CHANNEL_CLEAR_SHIFT

Shift position of RAIL_EVENT_TX_CHANNEL_CLEAR bit.

RAIL_EVENT_TX_CHANNEL_BUSY_SHIFT

Shift position of RAIL_EVENT_TX_CHANNEL_BUSY bit.

RAIL_EVENT_TX_CCA_RETRY_SHIFT

Shift position of RAIL_EVENT_TX_CCA_RETRY bit.

RAIL_EVENT_TX_START_CCA_SHIFT

Shift position of RAIL_EVENT_TX_START_CCA bit.

RAIL_EVENT_TX_STARTED_SHIFT

Shift position of RAIL_EVENT_TX_STARTED bit.

RAIL_EVENT_TX_SCHEDULED_TX_MISSED_SHIFT

Shift position of RAIL_EVENT_TX_SCHEDULED_TX_MISSED bit.

RAIL_EVENT_CONFIG_UNSCHEDULED_SHIFT

Shift position of RAIL_EVENT_CONFIG_UNSCHEDULED bit.

RAIL_EVENT_CONFIG_SCHEDULED_SHIFT

Shift position of RAIL_EVENT_CONFIG_SCHEDULED bit.

RAIL_EVENT_SCHEDULER_STATUS_SHIFT

Shift position of RAIL_EVENT_SCHEDULER_STATUS bit.

RAIL_EVENT_CAL_NEEDED_SHIFT

Shift position of RAIL_EVENT_CAL_NEEDED bit.

RAIL_EVENT_RF_SENSED_SHIFT

Shift position of RAIL_EVENT_RF_SENSED bit.

RAIL_EVENT_PA_PROTECTION_SHIFT

Shift position of RAIL_EVENT_PA_PROTECTION bit.

RAIL_EVENT_SIGNAL_DETECTED_SHIFT

Shift position of RAIL_EVENT_SIGNAL_DETECTED bit.

RAIL_EVENT_IEEE802154_MODESWITCH_START_SHIFT

Shift position of RAIL_EVENT_IEEE802154_MODESWITCH_START bit.

RAIL_EVENT_IEEE802154_MODESWITCH_END_SHIFT

Shift position of RAIL_EVENT_IEEE802154_MODESWITCH_END bit.

RAIL_EVENT_DETECT_RSSI_THRESHOLD_SHIFT

Shift position of RAIL_EVENT_DETECT_RSSI_THRESHOLD bit.

RAIL_EVENT_THERMISTOR_DONE_SHIFT

Shift position of RAIL_EVENT_THERMISTOR_DONE bit.

RAIL_EVENT_TX_BLOCKED_TOO_HOT_SHIFT

Shift position of RAIL_EVENT_TX_BLOCKED_TOO_HOT bit.

RAIL_EVENT_TEMPERATURE_TOO_HOT_SHIFT

Shift position of RAIL_EVENT_TEMPERATURE_TOO_HOT bit.

RAIL_EVENT_TEMPERATURE_COOL_DOWN_SHIFT

Shift position of RAIL_EVENT_TEMPERATURE_COOL_DOWN bit.

RAIL_EVENT_USER_MBOX_SHIFT

Shift position of RAIL_EVENT_USER_MBOX bit.


Function Documentation#

RAIL_ConfigEvents#

RAIL_Status_t RAIL_ConfigEvents (RAIL_Handle_t railHandle, RAIL_Events_t mask, RAIL_Events_t events)

Configure radio events.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_Events_t[in]mask

A bitmask of events to configure.

RAIL_Events_t[in]events

A bitmask of events to trigger RAIL_Config_t::eventsCallback For a full list of available callbacks, see RAIL_EVENT_* set of defines.

Returns

  • Status code indicating success of the function call.

Sets up which radio interrupts generate a RAIL event. The full list of options is in RAIL_Events_t.