Retiming#

EFR32-specific retiming capability.

The EFR product families have many digital and analog modules that can run in parallel with a radio. These combinations can cause interference and degradation on the radio RX sensitivity. Retiming can modify the clocking of the digital modules to reduce the interference.

Enumerations#

enum
RAIL_RETIME_OPTION_HFXO_SHIFT = 0
RAIL_RETIME_OPTION_HFRCO_SHIFT = 1
RAIL_RETIME_OPTION_DCDC_SHIFT = 2
RAIL_RETIME_OPTION_LCD_SHIFT = 3
}

Retiming options bit shifts.

Functions#

RAIL_ConfigRetimeOptions(RAIL_Handle_t railHandle, RAIL_RetimeOptions_t mask, RAIL_RetimeOptions_t options)

Configure retiming options.

RAIL_GetRetimeOptions(RAIL_Handle_t railHandle, RAIL_RetimeOptions_t *pOptions)

Get the currently configured retiming option.

Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.

Macros#

#define
RAIL_RETIME_OPTION_HFXO (1U << RAIL_RETIME_OPTION_HFXO_SHIFT)

An option to configure HFXO retiming.

#define
RAIL_RETIME_OPTION_HFRCO (1U << RAIL_RETIME_OPTION_HFRCO_SHIFT)

An option to configure HFRCO retiming.

#define
RAIL_RETIME_OPTION_DCDC (1U << RAIL_RETIME_OPTION_DCDC_SHIFT)

An option to configure DCDC retiming.

#define
RAIL_RETIME_OPTION_LCD (1U << RAIL_RETIME_OPTION_LCD_SHIFT)

An option to configure LCD retiming.

#define
RAIL_RETIME_OPTIONS_NONE 0x0U

A value representing no retiming options.

#define
RAIL_RETIME_OPTIONS_ALL 0xFFU

A value representing all retiming options.

Enumeration Documentation#

RAIL_RetimeOptions_t#

RAIL_RetimeOptions_t

Retiming options bit shifts.

Enumerator
RAIL_RETIME_OPTION_HFXO_SHIFT

Shift position of RAIL_RETIME_OPTION_HFXO bit.

RAIL_RETIME_OPTION_HFRCO_SHIFT

Shift position of RAIL_RETIME_OPTION_HFRCO bit.

RAIL_RETIME_OPTION_DCDC_SHIFT

Shift position of RAIL_RETIME_OPTION_DCDC bit.

RAIL_RETIME_OPTION_LCD_SHIFT

Shift position of RAIL_RETIME_OPTION_LCD bit.


Definition at line 5813 of file common/rail_types.h

Function Documentation#

RAIL_ConfigRetimeOptions#

RAIL_Status_t RAIL_ConfigRetimeOptions (RAIL_Handle_t railHandle, RAIL_RetimeOptions_t mask, RAIL_RetimeOptions_t options)

Configure retiming options.

Parameters
[in]railHandle

A handle of RAIL instance.

[in]mask

A bitmask containing which options should be modified.

[in]options

A bitmask containing desired configuration settings. Bit positions for each option are found in the RAIL_RetimeOptions_t.

Returns

  • Status code indicating success of the function call.


Definition at line 6440 of file common/rail.h

RAIL_GetRetimeOptions#

RAIL_Status_t RAIL_GetRetimeOptions (RAIL_Handle_t railHandle, RAIL_RetimeOptions_t * pOptions)

Get the currently configured retiming option.

Parameters
[in]railHandle

A handle of RAIL instance.

[out]pOptions

A pointer to configured retiming options bitmask indicating which are enabled.

Returns

  • Status code indicating success of the function call.


Definition at line 6452 of file common/rail.h

RAIL_ChangedDcdc#

RAIL_Status_t RAIL_ChangedDcdc (void )

Indicate that the DCDC peripheral bus clock enable has changed allowing RAIL to react accordingly.

Parameters
N/A

Returns

  • Status code indicating success of the function call.

Note

  • This should be called after DCDC has been enabled or disabled.


Definition at line 6463 of file common/rail.h