Transmit#

APIs related to transmitting data packets.

Modules#

RAIL_TxPacketDetails_t

RAIL_ScheduleTxConfig_t

RAIL_CsmaConfig_t

RAIL_LbtConfig_t

RAIL_SyncWordConfig_t

RAIL_TxRepeatConfig_t

Packet Transmit

Power Amplifier (PA)

Enumerations#

enum
RAIL_STOP_MODE_ACTIVE_SHIFT = 0
RAIL_STOP_MODE_PENDING_SHIFT = 1
}

Stop radio operation options bit mask.

enum
RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT = 0
RAIL_TX_OPTION_REMOVE_CRC_SHIFT = 1
RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT = 2
RAIL_TX_OPTION_ANTENNA0_SHIFT = 3
RAIL_TX_OPTION_ANTENNA1_SHIFT = 4
RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT = 5
RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT = 6
RAIL_TX_OPTION_CCA_ONLY_SHIFT = 7
RAIL_TX_OPTION_RESEND_SHIFT = 8
RAIL_TX_OPTION_CONCURRENT_PHY_ID_SHIFT = 9
RAIL_TX_OPTIONS_COUNT
}

Transmit options, in reality a bitmask.

enum
RAIL_SCHEDULED_TX_DURING_RX_POSTPONE_TX = 0
RAIL_SCHEDULED_TX_DURING_RX_ABORT_TX = 1
}

Enumerates the possible outcomes of what will occur if a scheduled TX ends up firing during RX.

enum
RAIL_TX_REPEAT_OPTION_HOP_SHIFT = 0
RAIL_TX_REPEAT_OPTION_START_TO_START_SHIFT = 1
}

Transmit repeat options, in reality a bitmask.

Functions#

RAIL_StopTx(RAIL_Handle_t railHandle, RAIL_StopMode_t mode)

Stop an active or pending transmit.

RAIL_SetCcaThreshold(RAIL_Handle_t railHandle, int8_t ccaThresholdDbm)

Set the CCA threshold in dBm.

RAIL_GetTxPacketDetails(RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails)

Get detailed information about the last packet transmitted.

RAIL_GetTxPacketDetailsAlt(RAIL_Handle_t railHandle, bool isAck, RAIL_Time_t *pPacketTime)

Get detailed information about the last packet transmitted.

RAIL_GetTxPacketDetailsAlt2(RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails)

Get detailed information about the last packet transmitted.

RAIL_GetTxTimePreambleStart(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime)

Adjust a RAIL TX completion timestamp to refer to the start of the preamble.

RAIL_GetTxTimePreambleStartAlt(RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails)

Adjust a RAIL TX completion timestamp to refer to the start of the preamble.

RAIL_GetTxTimeSyncWordEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime)

Adjust a RAIL TX timestamp to refer to the end of the sync word.

RAIL_GetTxTimeSyncWordEndAlt(RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails)

Adjust a RAIL TX timestamp to refer to the end of the sync word.

RAIL_GetTxTimeFrameEnd(RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t *pPacketTime)

Adjust a RAIL TX timestamp to refer to the end of frame.

RAIL_GetTxTimeFrameEndAlt(RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t *pPacketDetails)

Adjust a RAIL TX timestamp to refer to the end of frame.

RAIL_EnableTxHoldOff(RAIL_Handle_t railHandle, bool enable)

Prevent the radio from starting a transmit.

bool
RAIL_IsTxHoldOffEnabled(RAIL_Handle_t railHandle)

Check whether or not TX hold off is enabled.

RAIL_SetTxAltPreambleLength(RAIL_Handle_t railHandle, uint16_t length)

Set an alternate transmitter preamble length.

Macros#

#define
RAIL_STOP_MODES_NONE (0U)

Do not stop any radio operations.

#define
RAIL_STOP_MODE_ACTIVE (1U << RAIL_STOP_MODE_ACTIVE_SHIFT)

Stop active radio operations only.

#define
RAIL_STOP_MODE_PENDING (1U << RAIL_STOP_MODE_PENDING_SHIFT)

Stop pending radio operations.

#define
RAIL_STOP_MODES_ALL (0xFFU)

Stop all radio operations.

#define
RAIL_TX_OPTIONS_NONE 0UL

A value representing no options enabled.

#define
RAIL_TX_OPTIONS_DEFAULT RAIL_TX_OPTIONS_NONE

All options disabled by default.

#define
RAIL_TX_OPTION_WAIT_FOR_ACK (1UL << RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT)

An option when Auto-Ack has been configured, enabled, and not TX paused, to configure whether or not the transmitting node will listen for an Ack response.

#define
RAIL_TX_OPTION_REMOVE_CRC (1UL << RAIL_TX_OPTION_REMOVE_CRC_SHIFT)

An option to remove CRC bytes from TX packets.

#define
RAIL_TX_OPTION_SYNC_WORD_ID (1UL << RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT)

An option to select which sync word is used during the transmission.

#define
RAIL_TX_OPTION_ANTENNA0 (1UL << RAIL_TX_OPTION_ANTENNA0_SHIFT)

An option to select antenna 0 for transmission.

#define
RAIL_TX_OPTION_ANTENNA1 (1UL << RAIL_TX_OPTION_ANTENNA1_SHIFT)

An option to select antenna 1 for transmission.

#define
RAIL_TX_OPTION_ALT_PREAMBLE_LEN (1UL << RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT)

An option to use the alternate preamble length established by RAIL_SetTxAltPreambleLength() for the transmission.

#define
RAIL_TX_OPTION_CCA_PEAK_RSSI (1UL << RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT)

An option to use peak rather than average RSSI energy detected during CSMA's RAIL_CsmaConfig_t::ccaDuration or LBT's RAIL_LbtConfig_t::lbtDuration to determine whether the channel is clear or busy.

#define
RAIL_TX_OPTION_CCA_ONLY (1UL << RAIL_TX_OPTION_CCA_ONLY_SHIFT)

An option to only perform the CCA (CSMA/LBT) operation but not automatically transmit if the channel is clear.

#define
RAIL_TX_OPTION_RESEND (1UL << RAIL_TX_OPTION_RESEND_SHIFT)

An option to resend packet at the beginning of the Transmit FIFO.

#define
RAIL_TX_OPTION_CONCURRENT_PHY_ID (1UL << RAIL_TX_OPTION_CONCURRENT_PHY_ID_SHIFT)

An option to specify which PHY is used to transmit in the case of concurrent mode.

#define
RAIL_TX_OPTIONS_ALL 0xFFFFFFFFUL

A value representing all possible options.

#define
RAIL_MAX_LBT_TRIES (15U)

The maximum number of LBT/CSMA retries supported.

#define
RAIL_MAX_CSMA_EXPONENT (8U)

The maximum power-of-2 exponent for CSMA backoffs.

#define
RAIL_CSMA_CONFIG_802_15_4_2003_2p4_GHz_OQPSK_CSMA undefined

RAIL_CsmaConfig_t initializer configuring CSMA per IEEE 802.15.4-2003 on 2.4 GHz OSPSK, commonly used by Zigbee.

#define
RAIL_CSMA_CONFIG_SINGLE_CCA undefined

RAIL_CsmaConfig_t initializer configuring a single CCA prior to TX.

#define
RAIL_LBT_CONFIG_ETSI_EN_300_220_1_V2_4_1 undefined

RAIL_LbtConfig_t initializer configuring LBT per ETSI 300 220-1 V2.4.1 for a typical Sub-GHz band.

#define
RAIL_LBT_CONFIG_ETSI_EN_300_220_1_V3_1_0 undefined

RAIL_LbtConfig_t initializer configuring LBT per ETSI 300 220-1 V3.1.0 for a typical Sub-GHz band.

#define
RAIL_TX_REPEAT_OPTIONS_NONE 0U

A value representing no repeat options enabled.

#define
RAIL_TX_REPEAT_OPTIONS_DEFAULT RAIL_TX_REPEAT_OPTIONS_NONE

All repeat options disabled by default.

#define
RAIL_TX_REPEAT_OPTION_HOP (1U << RAIL_TX_REPEAT_OPTION_HOP_SHIFT)

An option to configure whether or not to channel-hop before each repeated transmit.

#define
RAIL_TX_REPEAT_OPTION_START_TO_START (1 << RAIL_TX_REPEAT_OPTION_START_TO_START_SHIFT)

An option to configure the delay between transmissions to be from start to start instead of end to start.

#define
RAIL_TX_REPEAT_INFINITE_ITERATIONS (0xFFFFU)

RAIL_TxRepeatConfig_t::iterations initializer configuring infinite repeated transmissions.

Enumeration Documentation#

RAIL_StopMode_t#

RAIL_StopMode_t

Stop radio operation options bit mask.

Enumerator
RAIL_STOP_MODE_ACTIVE_SHIFT

Shift position of RAIL_STOP_MODE_ACTIVE bit.

RAIL_STOP_MODE_PENDING_SHIFT

Shift position of RAIL_STOP_MODE_PENDING bit.


RAIL_TxOptions_t#

RAIL_TxOptions_t

Transmit options, in reality a bitmask.

Enumerator
RAIL_TX_OPTION_WAIT_FOR_ACK_SHIFT

Shift position of RAIL_TX_OPTION_WAIT_FOR_ACK bit.

RAIL_TX_OPTION_REMOVE_CRC_SHIFT

Shift position of RAIL_TX_OPTION_REMOVE_CRC bit.

RAIL_TX_OPTION_SYNC_WORD_ID_SHIFT

Shift position of RAIL_TX_OPTION_SYNC_WORD_ID bit.

RAIL_TX_OPTION_ANTENNA0_SHIFT

Shift position of RAIL_TX_OPTION_ANTENNA0 bit.

RAIL_TX_OPTION_ANTENNA1_SHIFT

Shift position of RAIL_TX_OPTION_ANTENNA1 bit.

RAIL_TX_OPTION_ALT_PREAMBLE_LEN_SHIFT

Shift position of RAIL_TX_OPTION_ALT_PREAMBLE_LEN bit.

RAIL_TX_OPTION_CCA_PEAK_RSSI_SHIFT

Shift position of RAIL_TX_OPTION_CCA_PEAK_RSSI bit.

RAIL_TX_OPTION_CCA_ONLY_SHIFT

Shift position of RAIL_TX_OPTION_CCA_ONLY bit.

RAIL_TX_OPTION_RESEND_SHIFT

Shift position of RAIL_TX_OPTION_RESEND bit.

RAIL_TX_OPTION_CONCURRENT_PHY_ID_SHIFT

Shift position of RAIL_TX_OPTION_CONCURRENT_PHY_ID bit.

RAIL_TX_OPTIONS_COUNT

A count of the choices in this enumeration.


RAIL_ScheduledTxDuringRx_t#

RAIL_ScheduledTxDuringRx_t

Enumerates the possible outcomes of what will occur if a scheduled TX ends up firing during RX.

Because RX and TX can't happen at the same time, it is up to the user how the TX should be handled. This enumeration is passed into RAIL_StartScheduledTx() as part of RAIL_ScheduleTxConfig_t.

Enumerator
RAIL_SCHEDULED_TX_DURING_RX_POSTPONE_TX

The scheduled TX will be postponed until RX completes and then sent.

RAIL_SCHEDULED_TX_DURING_RX_ABORT_TX

The scheduled TX will be aborted and a RAIL_EVENT_TX_BLOCKED event will fire.


RAIL_TxRepeatOptions_t#

RAIL_TxRepeatOptions_t

Transmit repeat options, in reality a bitmask.

Enumerator
RAIL_TX_REPEAT_OPTION_HOP_SHIFT

Shift position of RAIL_TX_REPEAT_OPTION_HOP bit.

RAIL_TX_REPEAT_OPTION_START_TO_START_SHIFT

Shift position of the RAIL_TX_REPEAT_OPTION_START_TO_START bit.


Function Documentation#

RAIL_StopTx#

RAIL_Status_t RAIL_StopTx (RAIL_Handle_t railHandle, RAIL_StopMode_t mode)

Stop an active or pending transmit.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_StopMode_t[in]mode

Specifies the type(s) of transmit to stop.

Returns

Note


RAIL_SetCcaThreshold#

RAIL_Status_t RAIL_SetCcaThreshold (RAIL_Handle_t railHandle, int8_t ccaThresholdDbm)

Set the CCA threshold in dBm.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

int8_t[in]ccaThresholdDbm

The CCA threshold in dBm.

Returns

  • Status code indicating success of the function call.

Unlike RAIL_StartCcaCsmaTx() or RAIL_StartCcaLbtTx(), which can cause a transmit, this function only modifies the CCA threshold. A possible use case for this function involves setting the CCA threshold to invalid RSSI of -128 which blocks transmission by preventing clear channel assessments from succeeding.


RAIL_GetTxPacketDetails#

RAIL_Status_t RAIL_GetTxPacketDetails (RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t * pPacketDetails)

Get detailed information about the last packet transmitted.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_TxPacketDetails_t *[inout]pPacketDetails

An application-provided pointer to store RAIL_TxPacketDetails_t corresponding to the transmit event. The isAck and timeSent fields totalPacketBytes and timePosition must be initialized prior to each call:

  • isAck true to obtain details about the most recent Ack transmit, false to obtain details about the most recent app-initiated transmit.

  • totalPacketBytes with the total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes sent over the air after the Preamble and Sync word(s), including CRC bytes.

  • timePosition with a RAIL_PacketTimePosition_t value specifying the packet position to put in the timeSent field on return. This field will also be updated with the actual position corresponding to the timeSent value filled in.

Returns

Note

This function can only be called from callback context for either RAIL_EVENT_TX_PACKET_SENT or RAIL_EVENT_TXACK_PACKET_SENT events.


RAIL_GetTxPacketDetailsAlt#

RAIL_Status_t RAIL_GetTxPacketDetailsAlt (RAIL_Handle_t railHandle, bool isAck, RAIL_Time_t * pPacketTime)

Get detailed information about the last packet transmitted.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]isAck

true to obtain details about the most recent Ack transmit. false to obtain details about the most recent app-initiated transmit.

RAIL_Time_t *[out]pPacketTime

An application-provided non-NULL pointer to store a RAIL_Time_t corresponding to the transmit event. This will be populated with a timestamp corresponding to an arbitrary location in the packet. Call RAIL_GetTxTimePreambleStart, RAIL_GetTxTimeSyncWordEnd, or RAIL_GetTxTimeFrameEnd to adjust the timestamp for different locations in the packet.

Returns

Note

This function can only be called from callback context for either RAIL_EVENT_TX_PACKET_SENT or RAIL_EVENT_TXACK_PACKET_SENT events.


RAIL_GetTxPacketDetailsAlt2#

RAIL_Status_t RAIL_GetTxPacketDetailsAlt2 (RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t * pPacketDetails)

Get detailed information about the last packet transmitted.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_TxPacketDetails_t *[inout]pPacketDetails

An application-provided pointer to store RAIL_TxPacketDetails_t corresponding to the transmit event. The isAck field must be initialized prior to each call:

Returns

This function can only be called from callback context for either RAIL_EVENT_TX_PACKET_SENT or RAIL_EVENT_TXACK_PACKET_SENT events.


RAIL_GetTxTimePreambleStart#

RAIL_Status_t RAIL_GetTxTimePreambleStart (RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t * pPacketTime)

Adjust a RAIL TX completion timestamp to refer to the start of the preamble.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]totalPacketBytes

The total number of bytes of the transmitted packet for RAIL to use when adjusting the provided timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. Pass RAIL_TX_STARTED_BYTES to retrieve the start-of-normal-TX timestamp (see below).

RAIL_Time_t *[inout]pPacketTime

This points to the RAIL_Time_t returned from a previous call to RAIL_GetTxPacketDetailsAlt() for this same packet. That time will be updated with the time that the preamble for this packet started on air. Must be non-NULL.

Also used to retrieve the RAIL_EVENT_TX_STARTED timestamp.

Returns

  • RAIL_STATUS_NO_ERROR if pPacketTime was successfully determined or an appropriate error code otherwise.

When used for timestamp adjustment, call this function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt() is called.

This function may be called when handling the RAIL_EVENT_TX_STARTED event to retrieve that event's start-of-normal-TX timestamp. (Ack transmits currently have no equivalent event or associated timestamp.) In this case, totalPacketBytes must be RAIL_TX_STARTED_BYTES, and pPacketTime is an output-only parameter filled in with that time (so no need to initialize it beforehand by calling RAIL_GetTxPacketDetailsAlt()).


RAIL_GetTxTimePreambleStartAlt#

RAIL_Status_t RAIL_GetTxTimePreambleStartAlt (RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t * pPacketDetails)

Adjust a RAIL TX completion timestamp to refer to the start of the preamble.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_TxPacketDetails_t *[inout]pPacketDetails

A non-NULL pointer to the details that were returned from a previous call to RAIL_GetTxPacketDetailsAlt2() for this same packet. The application must update the timeSent field totalPacketBytes to be the total number of bytes of the sent packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. Pass RAIL_TX_STARTED_BYTES to retrieve the start-of-normal-TX timestamp (see below). After this function, the timeSent field packetTime will be updated with the time that the preamble for this packet started on air.

Also used to retrieve the RAIL_EVENT_TX_STARTED timestamp.

Returns

  • RAIL_STATUS_NO_ERROR if the packet time was successfully calculated, or an appropriate error code otherwise.

When used for timestamp adjustment, call this function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt2() is called.

This function may be called when handling the RAIL_EVENT_TX_STARTED event to retrieve that event's start-of-normal-TX timestamp. (Ack transmits currently have no equivalent event or associated timestamp.) In this case, the timeSent field totalPacketBytes must be RAIL_TX_STARTED_BYTES, and the timeSent field packetTime is an output-only parameter filled in with that time (so no need to initialize it beforehand by calling RAIL_GetTxPacketDetailsAlt2()).


RAIL_GetTxTimeSyncWordEnd#

RAIL_Status_t RAIL_GetTxTimeSyncWordEnd (RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t * pPacketTime)

Adjust a RAIL TX timestamp to refer to the end of the sync word.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]totalPacketBytes

The total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes.

RAIL_Time_t *[inout]pPacketTime

The time that was returned in a RAIL_Time_t from a previous call to RAIL_GetTxPacketDetailsAlt() for this same packet. After this function, the time at that location will be updated with the time that the sync word for this packet finished on air. Must be non-NULL.

Returns

  • RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.

Call the timestamp adjustment function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt() is called.


RAIL_GetTxTimeSyncWordEndAlt#

RAIL_Status_t RAIL_GetTxTimeSyncWordEndAlt (RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t * pPacketDetails)

Adjust a RAIL TX timestamp to refer to the end of the sync word.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_TxPacketDetails_t *[inout]pPacketDetails

A non-NULL pointer to the details that were returned from a previous call to RAIL_GetTxPacketDetailsAlt2() for this same packet. The application must update the timeSent field totalPacketBytes to be the total number of bytes of the sent packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. After this function, the timeSent field packetTime will be updated with the time that the sync word for this packet finished on air.

Returns

  • RAIL_STATUS_NO_ERROR if the packet time was successfully calculated, or an appropriate error code otherwise.

Call the timestamp adjustment function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt2() is called.


RAIL_GetTxTimeFrameEnd#

RAIL_Status_t RAIL_GetTxTimeFrameEnd (RAIL_Handle_t railHandle, uint16_t totalPacketBytes, RAIL_Time_t * pPacketTime)

Adjust a RAIL TX timestamp to refer to the end of frame.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]totalPacketBytes

The total number of bytes of the transmitted packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes.

RAIL_Time_t *[inout]pPacketTime

The time that was returned in a RAIL_Time_t from a previous call to RAIL_GetTxPacketDetailsAlt() for this same packet. After this function, the time at that location will be updated with the time that this packet finished on air. Must be non-NULL.

Returns

  • RAIL_STATUS_NO_ERROR if pPacketTime was successfully calculated, or an appropriate error code otherwise.

Call the timestamp adjustment function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt() is called.


RAIL_GetTxTimeFrameEndAlt#

RAIL_Status_t RAIL_GetTxTimeFrameEndAlt (RAIL_Handle_t railHandle, RAIL_TxPacketDetails_t * pPacketDetails)

Adjust a RAIL TX timestamp to refer to the end of frame.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_TxPacketDetails_t *[inout]pPacketDetails

A non-NULL pointer to the details that were returned from a previous call to RAIL_GetTxPacketDetailsAlt2() for this same packet. The application must update the timeSent field totalPacketBytes to be the total number of bytes of the sent packet for RAIL to use when calculating the specified timestamp. This should account for all bytes transmitted over the air after the Preamble and Sync word(s), including CRC bytes. After this function, the timeSent field packetTime will be updated with the time that this packet finished on air.

Returns

  • RAIL_STATUS_NO_ERROR if the packet time was successfully calculated, or an appropriate error code otherwise.

Call the timestamp adjustment function in the same transmit-complete event-handling context as RAIL_GetTxPacketDetailsAlt2() is called.


RAIL_EnableTxHoldOff#

RAIL_Status_t RAIL_EnableTxHoldOff (RAIL_Handle_t railHandle, bool enable)

Prevent the radio from starting a transmit.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]enable

Enable/Disable TX hold off.

Returns

  • Status code indicating success of the function call.

Enable TX hold off to prevent the radio from starting any transmits. Disable TX hold off to allow the radio to transmit again. Attempting to transmit with the TX hold off enabled will result in RAIL_EVENT_TX_BLOCKED and/or RAIL_EVENT_TXACK_BLOCKED events.

Note

  • This function does not affect a transmit that has already started. To stop an already-started transmission, use RAIL_Idle() with RAIL_IDLE_ABORT.


RAIL_IsTxHoldOffEnabled#

bool RAIL_IsTxHoldOffEnabled (RAIL_Handle_t railHandle)

Check whether or not TX hold off is enabled.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • true if TX hold off is enabled, false otherwise.

TX hold off can be enabled/disabled using RAIL_EnableTxHoldOff(). Attempting to transmit with the TX hold off enabled will block the transmission and result in RAIL_EVENT_TX_BLOCKED and/or RAIL_EVENT_TXACK_BLOCKED events.


RAIL_SetTxAltPreambleLength#

RAIL_Status_t RAIL_SetTxAltPreambleLength (RAIL_Handle_t railHandle, uint16_t length)

Set an alternate transmitter preamble length.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]length

The desired preamble length, in bits.

Returns

  • Status code indicating success of the function call.

To cause a transmission to use this alternate preamble length, specify RAIL_TX_OPTION_ALT_PREAMBLE_LEN in the txOptions parameter passed to the respective RAIL transmit API.

Note