RAIL sync words and length configuration.

Public Attributes#

uint8_t

Sync word length in bits, between 2 and 32, inclusive.

uint32_t

Sync Word1.

uint32_t

Sync Word2.

Public Attribute Documentation#

syncWordBits#

uint8_t RAIL_SyncWordConfig_t::syncWordBits

Sync word length in bits, between 2 and 32, inclusive.


Definition at line 3573 of file common/rail_types.h

syncWord1#

uint32_t RAIL_SyncWordConfig_t::syncWord1

Sync Word1.

Note

  • Only the least-significant syncWordBits bits are used, which are sent or received on air least-significant-bit first.


Definition at line 3579 of file common/rail_types.h

syncWord2#

uint32_t RAIL_SyncWordConfig_t::syncWord2

Sync Word2.

Note

  • Only the least-significant syncWordBits bits are used, which are sent or received on air least-significant-bit first.


Definition at line 3585 of file common/rail_types.h