Alternate PHY configuration entry structure, which gathers some info on the alternate PHY in the context of concurrent mode.
Public Attributes#
A base frequency in Hz of this channel set.
A channel spacing in Hz of this channel set.
The number of channels (and not the channel number !)
minimum IF for the alternate PHY in kHz.
minimum IF for the base PHY in kHz.
Indicates that OFDM modem is used by this alternate PHY.
Rate info of the alternate PHY.
Used to adjust the AGC for CCA between hard and soft modems.
Public Attribute Documentation#
baseFrequency#
uint32_t RAIL_AlternatePhy_t::baseFrequency
A base frequency in Hz of this channel set.
2065
of file common/rail_types.h
channelSpacing#
uint32_t RAIL_AlternatePhy_t::channelSpacing
A channel spacing in Hz of this channel set.
2067
of file common/rail_types.h
numberOfChannels#
uint16_t RAIL_AlternatePhy_t::numberOfChannels
The number of channels (and not the channel number !)
2069
of file common/rail_types.h
minIf_kHz#
uint16_t RAIL_AlternatePhy_t::minIf_kHz
minimum IF for the alternate PHY in kHz.
2071
of file common/rail_types.h
minBaseIf_kHz#
uint16_t RAIL_AlternatePhy_t::minBaseIf_kHz
minimum IF for the base PHY in kHz.
2073
of file common/rail_types.h
isOfdmModem#
bool RAIL_AlternatePhy_t::isOfdmModem
Indicates that OFDM modem is used by this alternate PHY.
2075
of file common/rail_types.h
rateInfo#
uint32_t RAIL_AlternatePhy_t::rateInfo
Rate info of the alternate PHY.
2077
of file common/rail_types.h
hwModemAgcCtrl1#
uint32_t RAIL_AlternatePhy_t::hwModemAgcCtrl1
Used to adjust the AGC for CCA between hard and soft modems.
2079
of file common/rail_types.h