Long transport layer header.

Public Attributes#

uint8_t

CI (control information) field.

uint8_t

Raw address.

uint32_t

Address, device ID.

uint16_t

Address, manufacturer ID.

uint8_t

Address, version.

uint8_t

Address, device type.

struct sl_rail_sdk_wmbus_ltl_header_t::@5::@6

Detailed address.

union sl_rail_sdk_wmbus_ltl_header_t::@5

Address.

uint8_t

Access number.

uint8_t

Status byte.

Public Attribute Documentation#

ci_field#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::ci_field

CI (control information) field.


Definition at line 244 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

raw#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::raw[8]

Raw address.


Definition at line 246 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

id#

uint32_t sl_rail_sdk_wmbus_ltl_header_t::id

Address, device ID.


Definition at line 248 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

manufacturer#

uint16_t sl_rail_sdk_wmbus_ltl_header_t::manufacturer

Address, manufacturer ID.


Definition at line 249 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

version#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::version

Address, version.


Definition at line 250 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

device_type#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::device_type

Address, device type.


Definition at line 251 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

detailed#

struct sl_rail_sdk_wmbus_ltl_header_t::@5::@6 sl_rail_sdk_wmbus_ltl_header_t::detailed

Detailed address.


Definition at line 252 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

address#

union sl_rail_sdk_wmbus_ltl_header_t::@5 sl_rail_sdk_wmbus_ltl_header_t::address

Address.


Definition at line 253 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

access_number#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::access_number

Access number.


Definition at line 254 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

status#

uint8_t sl_rail_sdk_wmbus_ltl_header_t::status

Status byte.


Definition at line 255 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h

conf_word#

sl_rail_sdk_wmbus_conf_word_t sl_rail_sdk_wmbus_ltl_header_t::conf_word

Config word.


Definition at line 256 of file /mnt/raid/workspaces/ws.usUVI5bCK/overlay/gsdk/app/rail/component/sl_rail_sdk_wmbus_support/sl_rail_sdk_wmbus_support.h