General#

Basic APIs to set up and interact with the RAIL library.

Modules#

RAIL_Version_t

RAILSched_Config_t

RAIL_Config_t

EFR32xG2x

SIxx3xx

Typedefs#

typedef void *

A radio-generic handle (e.g., RAIL_EFR32_HANDLE), or a real RAIL instance handle as returned from RAIL_Init().

typedef sl_status_t

A status returned by many RAIL API calls indicating their success or failure.

typedef void(*
RAIL_InitCompleteCallbackPtr_t)(RAIL_Handle_t railHandle)

A pointer to an initialization complete callback function.

typedef uint8_t

Provided for backwards compatibility.

Functions#

RAIL_GetVersion(RAIL_Version_t *version, bool verbose)

Get the version information for the compiled RAIL library.

RAIL_AddStateBuffer3(RAIL_Handle_t genericRailHandle)

Add a 3rd multiprotocol internal state buffer for use by RAIL_Init().

RAIL_AddStateBuffer4(RAIL_Handle_t genericRailHandle)

Add a 4th multiprotocol internal state buffer for use by RAIL_Init().

RAIL_UseDma(uint8_t channel)

Allocate a DMA channel for RAIL to work with.

RAIL_CopyDeviceInfo(RAIL_Handle_t genericRailHandle)

Reads out device specific data that may be needed by RAIL and populates appropriate data structures in the library.

RAIL_Init(const RAIL_Config_t *railCfg, RAIL_InitCompleteCallbackPtr_t cb)

Initialize RAIL.

bool

Get RAIL initialization status.

uint16_t
RAIL_GetRadioEntropy(RAIL_Handle_t railHandle, uint8_t *buffer, uint16_t bytes)

Collect entropy from the radio if available.

Macros#

#define
RAIL_EFR32_HANDLE ((RAIL_Handle_t)0xFFFFFFFFUL)

A placeholder for a radio-generic RAIL handle.

#define

RAIL function reports no error.

#define
RAIL_STATUS_INVALID_PARAMETER SL_STATUS_INVALID_PARAMETER

Call to RAIL function threw an error because of an invalid parameter.

#define
RAIL_STATUS_INVALID_STATE SL_STATUS_INVALID_STATE

Call to RAIL function threw an error because it was called during an invalid radio state.

#define
RAIL_STATUS_INVALID_CALL SL_STATUS_NOT_AVAILABLE

RAIL function is called in an invalid order.

#define
RAIL_STATUS_SUSPENDED SL_STATUS_IN_PROGRESS

RAIL function did not finish in the allotted time.

#define
RAIL_STATUS_SCHED_ERROR SL_STATUS_ABORT

RAIL function could not be scheduled by the Radio scheduler.

#define

A value to signal that RAIL should not use DMA.

Typedef Documentation#

RAIL_Handle_t#

RAIL_Handle_t

A radio-generic handle (e.g., RAIL_EFR32_HANDLE), or a real RAIL instance handle as returned from RAIL_Init().

Generic handles should be used for certain RAIL APIs that are called prior to RAIL initialization. However, once RAIL has been initialized, the real handle returned by RAIL_Init() should be used instead.


RAIL_Status_t#

RAIL_Status_t

A status returned by many RAIL API calls indicating their success or failure.

It is a subset of sl_status_t.


RAIL_InitCompleteCallbackPtr_t#

typedef void(* RAIL_InitCompleteCallbackPtr_t) (RAIL_Handle_t railHandle) )(RAIL_Handle_t railHandle)

A pointer to an initialization complete callback function.

Parameters
TypeDirectionArgument NameDescription
[in]railHandle

The initialized RAIL instance handle.


RAIL_StateBuffer_t#

RAIL_StateBuffer_t [1]

Provided for backwards compatibility.


Function Documentation#

RAIL_GetVersion#

RAIL_Status_t RAIL_GetVersion (RAIL_Version_t * version, bool verbose)

Get the version information for the compiled RAIL library.

Parameters
TypeDirectionArgument NameDescription
RAIL_Version_t *[out]version

A non-NULL pointer to RAIL_Version_t structure to populate with version information.

bool[in]verbose

Populate RAIL_Version_t struct with verbose information.

Returns

  • Status code indicating success of the function call.

The version information contains a major version number, a minor version number, and a rev (revision) number.


RAIL_AddStateBuffer3#

RAIL_Status_t RAIL_AddStateBuffer3 (RAIL_Handle_t genericRailHandle)

Add a 3rd multiprotocol internal state buffer for use by RAIL_Init().

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]genericRailHandle

A generic RAIL instance handle.

Returns

  • Status code indicating success of the function call. An error is returned if the 3rd state buffer was previously added or this isn't the RAIL multiprotocol library.


RAIL_AddStateBuffer4#

RAIL_Status_t RAIL_AddStateBuffer4 (RAIL_Handle_t genericRailHandle)

Add a 4th multiprotocol internal state buffer for use by RAIL_Init().

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]genericRailHandle

A generic RAIL instance handle.

Returns

  • Status code indicating success of the function call. An error is returned if the 4th state buffer was previously added. or this isn't the RAIL multiprotocol library.


RAIL_UseDma#

RAIL_Status_t RAIL_UseDma (uint8_t channel)

Allocate a DMA channel for RAIL to work with.

Parameters
TypeDirectionArgument NameDescription
uint8_t[in]channel

The DMA channel to use when copying memory. If a value of RAIL_DMA_INVALID is passed, RAIL will stop using any DMA channel.

Returns

  • Status code indicating success of the function call.

To use this API, the application must initialize the DMA engine on the chip and allocate a DMA channel. This channel will be used periodically to copy memory more efficiently. Call this function before RAIL_Init() to have the most benefit. If the application needs to take back control of the DMA channel that RAIL is using, this API may be called with a channel of RAIL_DMA_INVALID to tell RAIL to stop using DMA.

Warnings


RAIL_CopyDeviceInfo#

RAIL_Status_t RAIL_CopyDeviceInfo (RAIL_Handle_t genericRailHandle)

Reads out device specific data that may be needed by RAIL and populates appropriate data structures in the library.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]genericRailHandle

A generic RAIL instance handle.

Returns

  • Status code indicating success of the function call.

Note

  • This function must be called before calling RAIL_Init() on any platforms that require this data and should not be called inside a critical section. This function does nothing on EFR32 Series 2 devices.


RAIL_Init#

RAIL_Handle_t RAIL_Init (const RAIL_Config_t * railCfg, RAIL_InitCompleteCallbackPtr_t cb)

Initialize RAIL.

Parameters
TypeDirectionArgument NameDescription
const RAIL_Config_t *[in]railCfg

The configuration for setting up the protocol.

RAIL_InitCompleteCallbackPtr_t[in]cb

A callback that notifies the application when the radio is finished initializing and is ready for further configuration. This callback is useful for potential transceiver products that require a power up sequence before further configuration is available. After the callback fires, the radio is ready for additional configuration before transmit and receive operations.

Returns

  • Handle for initialized rail instance or NULL if an invalid value was passed in the railCfg.

Note

  • Call this function only once per protocol. If called again, it will do nothing and return NULL. RAIL_CopyDeviceInfo() should be called once before calling this function for Silicon Labs Series 3 devices.

  • The first call to RAIL_Init() implicitly enables PTI, but it won't take effect unless or until RAIL_ConfigPti() has been called with a mode other than the default RAIL_PTI_MODE_DISABLED.


RAIL_IsInitialized#

bool RAIL_IsInitialized (void )

Get RAIL initialization status.

Parameters
TypeDirectionArgument NameDescription
voidN/A

Returns

  • true if the radio has finished initializing and false otherwise.

RAIL APIs, e.g., RAIL_GetTime(), which work only if RAIL_Init() has been called, can use RAIL_IsInitialized() to determine whether RAIL has been initialized or not.


RAIL_GetRadioEntropy#

uint16_t RAIL_GetRadioEntropy (RAIL_Handle_t railHandle, uint8_t * buffer, uint16_t bytes)

Collect entropy from the radio if available.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t *[out]buffer

A non-NULL pointer to the buffer to write the collected entropy.

uint16_t[in]bytes

The number of bytes to fill in the input buffer.

Returns

  • The number of bytes of entropy collected. For radios that don't support entropy collection, the function returns 0. Values less than the requested amount may also be returned on platforms that use entropy pools to collect random data periodically.

Attempts to fill the provided buffer with the requested number of bytes of entropy. If the requested number of bytes can't be provided, as many bytes as possible will be filled and returned. For radios that do not support this function, 0 bytes are always returned. For information about the specific mechanism for gathering entropy, see documentation for the chip family.


Macro Definition Documentation#

RAIL_EFR32_HANDLE#

#define RAIL_EFR32_HANDLE
Value:
((RAIL_Handle_t)0xFFFFFFFFUL)

A placeholder for a radio-generic RAIL handle.

Using NULL as a RAIL handle is not recommended. As a result, another value that can't be de-referenced is used.

This generic handle can and should be used for RAIL APIs that are called prior to RAIL initialization.


RAIL_STATUS_NO_ERROR#

#define RAIL_STATUS_NO_ERROR
Value:
SL_STATUS_OK

RAIL function reports no error.


RAIL_STATUS_INVALID_PARAMETER#

#define RAIL_STATUS_INVALID_PARAMETER
Value:
SL_STATUS_INVALID_PARAMETER

Call to RAIL function threw an error because of an invalid parameter.


RAIL_STATUS_INVALID_STATE#

#define RAIL_STATUS_INVALID_STATE
Value:
SL_STATUS_INVALID_STATE

Call to RAIL function threw an error because it was called during an invalid radio state.


RAIL_STATUS_INVALID_CALL#

#define RAIL_STATUS_INVALID_CALL
Value:
SL_STATUS_NOT_AVAILABLE

RAIL function is called in an invalid order.


RAIL_STATUS_SUSPENDED#

#define RAIL_STATUS_SUSPENDED
Value:
SL_STATUS_IN_PROGRESS

RAIL function did not finish in the allotted time.


RAIL_STATUS_SCHED_ERROR#

#define RAIL_STATUS_SCHED_ERROR
Value:
SL_STATUS_ABORT

RAIL function could not be scheduled by the Radio scheduler.

Only issued when using a Multiprotocol application.


RAIL_DMA_INVALID#

#define RAIL_DMA_INVALID
Value:
(0xFFU)

A value to signal that RAIL should not use DMA.