You are viewing documentation for version:
PDFData used for thermal protection.
Public Attributes#
uint16_t
Store chip temperature for metrics.
uint16_t
Minimum temperature recorded.
uint16_t
Maximum temperature recorded.
bool
Indicates if data should be reset.
Public Attribute Documentation#
tempK#
uint16_t RAIL_ChipTempMetrics_t::tempK
Store chip temperature for metrics.
minTempK#
uint16_t RAIL_ChipTempMetrics_t::minTempK
Minimum temperature recorded.
maxTempK#
uint16_t RAIL_ChipTempMetrics_t::maxTempK
Maximum temperature recorded.
resetPending#
bool RAIL_ChipTempMetrics_t::resetPending
Indicates if data should be reset.
reservedChipTemp#
uint8_t RAIL_ChipTempMetrics_t::reservedChipTemp
Reserved for future use.