RX Channel Hopping#
Hardware accelerated hopping between channels while waiting for a packet in receive.
Channel hopping provides a hardware accelerated method for scanning across multiple channels quickly, as part of a receive protocol. While it is possible to call RAIL_StartRx() on different channels, back to back, and listen on many channels sequentially in that way, the time it takes to switch channels with that method may be too long for some protocols. This API pre-computes necessary channel change operations for a given list of channels, so that the radio can move from channel to channel much faster. Additionally, it leads to more succinct code as channel changes will be done implicitly, without requiring numerous calls to RAIL_StartRx(). Currently, while this feature is enabled, the radio will hop channels in the given sequence each time it enters RX. Note that RX Channel hopping and EFR32xG25's concurrent mode / collision detection are mutually exclusive.
The channel hopping buffer requires RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL number of 32-bit words of overhead per channel, plus 3 words overall plus the twice the size of the RAIL_ChannelConfig_t::phyConfigDeltaSubtract of the whole radio configuration, plus the twice the sum of the sizes of all the RAIL_ChannelConfigEntry_t::phyConfigDeltaAdd in all the channel hopping channels.
The following code gives an example of how to use the RX Channel Hopping API.
#define CHANNEL_HOPPING_NUMBER_OF_CHANNELS 4
#define CHANNEL_HOPPING_BUFFER_SIZE do { \
3 + \
(RAIL_CHANNEL_HOPPING_BUFFER_SIZE_PER_CHANNEL \
* CHANNEL_HOPPING_NUMBER_OF_CHANNELS) + \
2 * (SIZEOF_UINT32_DELTA_SUBTRACT + \
SIZEOF_UINT32_DELTA_ADD_0 + \
SIZEOF_UINT32_DELTA_ADD_1 + \
SIZEOF_UINT32_DELTA_ADD_2 + \
SIZEOF_UINT32_DELTA_ADD_3) \
} while (0)
RAIL_RxChannelHoppingConfigEntry_t channelHoppingEntries[CHANNEL_HOPPING_NUMBER_OF_CHANNELS];
uint32_t channelHoppingBuffer[CHANNEL_HOPPING_BUFFER_SIZE];
RAIL_RxChannelHoppingConfig_t channelHoppingConfig = {
.buffer = channelHoppingBuffer,
.bufferLength = CHANNEL_HOPPING_BUFFER_SIZE,
.numberOfChannels = CHANNEL_HOPPING_NUMBER_OF_CHANNELS,
.entries = channelHoppingEntries
};
channelHoppingEntries[0].channel = 1;
channelHoppingEntries[1].channel = 2;
channelHoppingEntries[2].channel = 3;
RAIL_ConfigRxChannelHopping(railHandle, &channelHoppingConfig);
RAIL_EnableRxChannelHopping(railHandle, true, true)
Channel hopping provides a hardware accelerated method for scanning across multiple channels quickly, as part of a receive protocol. While it is possible to call sl_rail_start_rx() on different channels, back to back, and listen on many channels sequentially in that way, the time it takes to switch channels with that method may be too long for some protocols. This API pre-computes necessary channel change operations for a given list of channels, so that the radio can move from channel to channel much faster. Additionally, it leads to more succinct code as channel changes will be done implicitly, without requiring numerous calls to sl_rail_start_rx(). Currently, while this feature is enabled, the radio will hop channels in the given sequence each time it enters RX. Note that RX Channel hopping and EFR32xG25's concurrent mode / collision detection are mutually exclusive.
The channel hopping buffer requires SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL number of 32-bit words of overhead per channel, plus 3 words overall plus the twice the size of the sl_rail_channel_config_t::phy_config_delta_subtract of the whole radio configuration, plus the twice the sum of the sizes of all the sl_rail_channel_config_entry_t::phy_config_delta_add inall the channel hopping channels.
The following code gives an example of how to use the RX Channel Hopping API.
#define CHANNEL_HOPPING_NUMBER_OF_CHANNELS 4
#define CHANNEL_HOPPING_BUFFER_WORDS do { \
3 + \
(SL_RAIL_CHANNEL_HOPPING_BUFFER_WORDS_PER_CHANNEL \
* CHANNEL_HOPPING_NUMBER_OF_CHANNELS) + \
2 * (SIZEOF_UINT32_DELTA_SUBTRACT + \
SIZEOF_UINT32_DELTA_ADD_0 + \
SIZEOF_UINT32_DELTA_ADD_1 + \
SIZEOF_UINT32_DELTA_ADD_2 + \
SIZEOF_UINT32_DELTA_ADD_3) \
} while (0)
sl_rail_rx_channel_hopping_config_entry_t channel_hopping_entries[CHANNEL_HOPPING_NUMBER_OF_CHANNELS];
uint32_t channel_hopping_buffer[CHANNEL_HOPPING_BUFFER_WORDS];
sl_rail_rx_channel_hopping_config_t channel_hopping_config = {
.buffer = channel_hopping_buffer,
.buffer_words = CHANNEL_HOPPING_BUFFER_WORDS,
.number_of_channels = CHANNEL_HOPPING_NUMBER_OF_CHANNELS,
.entries = channel_hopping_entries,
};
channel_hopping.entries[0].channel = 1;
channel_hopping.entries[1].channel = 2;
channel_hopping_entries[2].channel = 3;
sl_rail_config_rx_channel_hopping(rail_handle, &channel_hopping_config);
sl_rail_enable_rx_channel_hopping(rail_handle, true, true)
Modules#
RAIL_RxChannelHoppingConfigMultiMode_t
RAIL_RxChannelHoppingConfigEntry_t
sl_rail_rx_channel_hopping_config_multi_mode_t
sl_rail_rx_channel_hopping_config_entry_t
sl_rail_rx_channel_hopping_config_t
sl_rail_rx_duty_cycle_config_t
Enumerations#
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
Options that can customize channel hopping behavior on a per-hop basis.
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
Options that can customize channel hopping behavior on a per-hop basis.
Typedefs#
Rx channel hopping on-channel time.
Rx channel hopping on-channel time.
Functions#
Configure RX channel hopping.
Enable RX channel hopping.
Manually trigger an Rx channel hop.
Get RSSI in quarter-dBm of one channel in the channel hopping sequence, during channel hopping.
Configure RX duty cycle mode.
Enable RX duty cycle mode.
Get the default RX duty cycle configuration.
Configure RX channel hopping.
Enable RX channel hopping.
Manually trigger an Rx channel hop.
Get RSSI in quarter-dBm of one channel in the channel hopping sequence, during channel hopping.
Configure RX duty cycle mode.
Enable RX duty cycle mode.
Get the default RX duty cycle configuration.
Macros#
The maximum sense time supported for those RAIL_RxChannelHoppingMode_t modes whose parameter(s) specify a sensing time.
A value representing no options enabled.
All options disabled by default.
DeprecatedPlease use RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT instead. Replaced by SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT.
An option to skip synth calibration while hopping into the channel specified in the current entry.
An option to skip DC calibration while hopping into the channel specified in the current entry.
An option to check RSSI after hopping into the channel specified in the current entry and hop if that RSSI is below the threshold specified in RAIL_RxChannelHoppingConfigEntry_t::rssiThresholdDbm.
An option to stop the hopping sequence at this entry in the hop table, which also idles the radio.
A sentinel value to flag an invalid channel hopping index.
The maximum sense time supported for those sl_rail_rx_channel_hopping_mode_t modes whose parameter(s) specify a sensing time.
A value representing no options enabled.
All options disabled by default.
An option to skip synth calibration while hopping into the channel specified in the current entry.
An option to skip DC calibration while hopping into the channel specified in the current entry.
An option to check RSSI after hopping into the channel specified in the current entry and hop if that RSSI is below the threshold specified in sl_rail_rx_channel_hopping_config_entry_t::rssi_threshold_dbm.
An option to stop the hopping sequence at this entry in the hop table, which also idles the radio.
A sentinel value to flag an invalid channel hopping index.
Enumeration Documentation#
RAIL_RxChannelHoppingMode_t#
RAIL_RxChannelHoppingMode_t
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
DeprecatedRAIL 2.x synonym of sl_rail_rx_channel_hopping_mode_t.
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL | Switch to the next channel each time the radio re-enters RX after packet reception or a transmit based on the corresponding State Transitions. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT | Switch to the next channel after a certain amount of time passes. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE | Listen in receive RX for at least a specified timeout. |
| RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE | Listen in receive RX for at least a specified timeout. |
| RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1 | Placeholder for a reserved hopping mode that is not supported. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE | A mode that combines modes TIMING_SENSE, PREAMBLE_SENSE, and TIMEOUT (sync detect) all running in parallel. |
| RAIL_RX_CHANNEL_HOPPING_MODE_SQ | Switch to the next channel based on the demodulation settings in the PHY config. |
| RAIL_RX_CHANNEL_HOPPING_MODE_CONC | Marks that the channel is concurrent with another channel, and otherwise behaves identically to RAIL_RX_CHANNEL_HOPPING_MODE_SQ. |
| RAIL_RX_CHANNEL_HOPPING_MODE_VT | Indicates that this channel is a virtual channel that is concurrently detected with the channel indicated by the RAIL_RxChannelHoppingConfigEntry_t::parameter. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TX | This is the transmit channel used for Auto-Ack if the regular channel, specified in RAIL_RxChannelHoppingConfigEntry::parameter, is optimized for RX which may degrade some TX performance. |
| RAIL_RX_CHANNEL_HOPPING_MODES_COUNT | A count of the basic choices in this enumeration. |
| RAIL_RX_CHANNEL_HOPPING_MODES_WITH_OPTIONS_BASE | The start of equivalent modes requiring non-default RAIL_RxDutyCycleConfig_t::options, needed for backwards-compatibility with earlier RAIL_RxDutyCycleConfig_t format. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED1 with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_SQ_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_SQ with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_CONC_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_CONC with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_VT_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_VT with options. |
| RAIL_RX_CHANNEL_HOPPING_MODE_TX_WITH_OPTIONS | Variant of RAIL_RX_CHANNEL_HOPPING_MODE_TX with options. |
RAIL_RxChannelHoppingDelayMode_t#
RAIL_RxChannelHoppingDelayMode_t
DeprecatedSet only to RAIL_RX_CHANNEL_DELAY_MODE_STATIC. This enum type has been eliminated in RAIL 3.
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC | Always delay for exactly the amount of time specified in the delay parameter, regardless of how other channel hopping channels were extended via preamble sense or other means. |
RAIL_RxChannelHoppingOptions_t#
RAIL_RxChannelHoppingOptions_t
Options that can customize channel hopping behavior on a per-hop basis.
DeprecatedRAIL 2.x synonym of sl_rail_rx_channel_hopping_options_t.
| Enumerator | |
|---|---|
| RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTION_STOP_SHIFT | Shift position of RAIL_RX_CHANNEL_HOPPING_OPTION_STOP bit. |
| RAIL_RX_CHANNEL_HOPPING_OPTIONS_COUNT | A count of the choices in this enumeration. |
sl_rail_rx_channel_hopping_mode_t#
sl_rail_rx_channel_hopping_mode_t
Modes by which RAIL can determine when to proceed to the next channel during channel hopping.
| Enumerator | |
|---|---|
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL | Switch to the next channel each time the radio re-enters RX after packet reception or a transmit based on the corresponding State Transitions. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT | Switch to the next channel after a certain amount of time passes. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE | Listen in receive RX for at least a specified timeout. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE | Listen in receive RX for at least a specified timeout. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED_4 | Placeholder for a reserved hopping mode that is not supported. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE | A mode that combines modes TIMING_SENSE, PREAMBLE_SENSE, and TIMEOUT (sync detect) all running in parallel. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_SQ | Switch to the next channel based on the demodulation settings in the PHY config. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_CONC | Marks that the channel is concurrent with another channel, and otherwise behaves identically to SL_RAIL_RX_CHANNEL_HOPPING_MODE_SQ. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_VT | Indicates that this channel is a virtual channel that is concurrently detected with the channel indicated by the sl_rail_rx_channel_hopping_config_entry_t::parameter. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TX | This is the transmit channel used for Auto-Ack if the regular channel, specified in sl_rail_rx_channel_hopping_config_entry::parameter, is optimized for RX which may degrade some TX performance. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODES_COUNT | A count of the basic choices in this enumeration. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODES_WITH_OPTIONS_BASE | The start of equivalent modes requiring non-default sl_rail_rx_duty_cycle_config_t::options, needed for backwards-compatibility with earlier sl_rail_rx_duty_cycle_config_t format. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMEOUT with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_TIMING_SENSE with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED_4_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_RESERVED_4 with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_MULTI_SENSE with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_SQ_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_SQ with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_CONC_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_CONC with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_VT_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_VT with options. |
| SL_RAIL_RX_CHANNEL_HOPPING_MODE_TX_WITH_OPTIONS | Variant of SL_RAIL_RX_CHANNEL_HOPPING_MODE_TX with options. |
sl_rail_rx_channel_hopping_options_t#
sl_rail_rx_channel_hopping_options_t
Options that can customize channel hopping behavior on a per-hop basis.
| Enumerator | |
|---|---|
| SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL_SHIFT | Shift position of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL bit. |
| SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL_SHIFT | Shift position of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL bit. |
| SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD_SHIFT | Shift position of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD bit. |
| SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOP_SHIFT | Shift position of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOP bit. |
| SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_COUNT | A count of the choices in this enumeration. |
Typedef Documentation#
RAIL_RxChannelHoppingParameter_t#
RAIL_RxChannelHoppingParameter_t
Rx channel hopping on-channel time.
DeprecatedRAIL 2.x synonym of sl_rail_rx_channel_hopping_parameter_t.
sl_rail_rx_channel_hopping_parameter_t#
sl_rail_rx_channel_hopping_parameter_t
Rx channel hopping on-channel time.
Function Documentation#
RAIL_ConfigRxChannelHopping#
RAIL_Status_t RAIL_ConfigRxChannelHopping (RAIL_Handle_t railHandle, RAIL_RxChannelHoppingConfig_t * config)
Configure RX channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_RxChannelHoppingConfig_t * | [in] | config | A pointer to the configuration parameters for RX Channel Hopping. |
Returns
Status code indicating success of the function call.
Configure channel hopping channels, conditions, and parameters. This API must be called before RAIL_EnableRxChannelHopping(). This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled.
Note
Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_ConfigRxDutyCycle().
DeprecatedRAIL 2.x synonym of sl_rail_config_rx_channel_hopping().
RAIL_EnableRxChannelHopping#
RAIL_Status_t RAIL_EnableRxChannelHopping (RAIL_Handle_t railHandle, bool enable, bool reset)
Enable RX channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Channel Hopping. |
| bool | [in] | reset | Start from the first channel of the channel hopping sequence (true) or from wherever hopping left off last time the code left RX. |
Returns
Status code indicating success of the function call.
Enable or disable Channel Hopping. Additionally, specify whether hopping should be reset to start from the first channel index, or continue from the channel last hopped to. The radio should not be on when this API is called. RAIL_ConfigRxChannelHopping() must be called successfully before this API is called.
Note
Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
RX Channel Hopping may not be enabled while Auto-Acking is enabled.
Calling this function will overwrite any settings configured with RAIL_EnableRxDutyCycle().
DeprecatedRAIL 2.x synonym of sl_rail_enable_rx_channel_hopping().
RAIL_TriggerRxChannelHop#
RAIL_Status_t RAIL_TriggerRxChannelHop (RAIL_Handle_t railHandle)
Manually trigger an Rx channel hop.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
Returns
Status code indicating success of the function call.
This function facilitates a manual hop when using RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL. (It will also trigger a hop in other automatic hop modes as well, so use with caution.)
Note
This function may cause RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE to occur before it returns.
DeprecatedRAIL 2.x synonym of sl_rail_trigger_rx_channel_hop().
RAIL_GetChannelHoppingRssi#
int16_t RAIL_GetChannelHoppingRssi (RAIL_Handle_t railHandle, uint8_t channelIndex)
Get RSSI in quarter-dBm of one channel in the channel hopping sequence, during channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| uint8_t | [in] | channelIndex | Index in the channel hopping sequence of the channel of interest. |
Returns
Latest RSSI in quarter-dBm (dBm * 4) for the channel at the specified index.
Note
Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
In multiprotocol, this function returns RAIL_RSSI_INVALID immediately if railHandle is not the currently active RAIL_Handle_t.
RAIL_ConfigRxChannelHopping() must be called successfully before this API is called.
When the Z-Wave protocol is active, running RAIL_GetChannelHoppingRssi() on the 9.6 kbps PHY returns the RSSI measurement of the 40kpbs PHY. This is because the 9.6 kbps PHY has trouble with RSSI measurements on EFR32xG2x family of chips.
DeprecatedRAIL 2.x synonym of sl_rail_get_channel_hopping_rssi().
RAIL_ConfigRxDutyCycle#
RAIL_Status_t RAIL_ConfigRxDutyCycle (RAIL_Handle_t railHandle, const RAIL_RxDutyCycleConfig_t * config)
Configure RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| const RAIL_RxDutyCycleConfig_t * | [in] | config | A non-NULL pointer to a configuration structure specifying duty cycle parameters. |
Returns
Status code indicating success of the function call.
Configure RX duty cycle mode. With this mode enabled, every time the radio enters RX, it will duty cycle on and off to save power. The duty cycle ratio can be altered dynamically and intelligently by the hardware by staying on longer if a preamble or other packet segments are detected in the air. This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled. For short delays (in the order of microseconds), RAIL_RxDutyCycleConfig_t::delay, this can be used to save receive current while having little impact on the radio performance, for protocols with long preambles. For long delays (in the order of milliseconds or higher) the chip can be put into EM2 energy mode before re-entering RX, to save extra power, with some application hooks as shown below.
#include "rail.h"
extern RAIL_Handle_t railHandle;
RAIL_Time_t periodicWakeupUs;
volatile bool dutyCycleEnd = true;
void RAILCb_Event(RAIL_Handle_t railHandle, RAIL_Events_t events)
{
// Omitting other event handlers
if (events & RAIL_EVENT_RX_DUTY_CYCLE_RX_END) {
dutyCycleEnd = true;
}
}
void main(void)
{
RAIL_Status_t status;
bool shouldSleep = false;
initializeRail(); // Call RAIL_Init() and such
// This function depends on your board/chip but it must enable the LFCLK
// you intend to use for RTCC sync before we configure sleep as that
// function will attempt to auto detect the clock.
BoardSetupLFCLK();
// Initialize Power Manager module
sl_power_manager_init();
// Initialize RAIL Power Manager
RAIL_InitPowerManager();
// Configure sleep for timer synchronization
RAIL_TimerSyncConfig_t timerSyncConfig = RAIL_TIMER_SYNC_DEFAULT;
status = RAIL_ConfigSleep(railHandle, &timerSyncConfig);
assert(status == RAIL_STATUS_NO_ERROR);
// Configure RX duty-cycling
RAIL_RxDutyCycleConfig_t duty_cycle_config = {
.mode = RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE,
.parameter = DUTY_CYCLE_ON_TIME,
.delay_us = DUTY_CYCLE_OFF_TIME,
.delay_mode = RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC,
.options = RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE,
};
status = RAIL_ConfigRxDutyCycle(rail_handle, &duty_cycle_config);
assert(status == RAIL_STATUS_NO_ERROR);
status = RAIL_EnableRxDutyCycle(rail_handle, true);
assert(status == RAIL_STATUS_NO_ERROR);
// Application main loop
while (1) {
if (dutyCycleEnd) {
dutyCycleEnd = false;
// Schedule the next receive.
RAIL_ScheduleRxConfig_t rxConfig = {
.start = periodicWakeupUs,
.startMode = RAIL_TIME_DELAY,
.end = 0U,
.endMode = RAIL_TIME_DISABLED,
.rxTransitionEndSchedule = 0U,
.hardWindowEnd = 0U
};
RAIL_Idle(railHandle, RAIL_IDLE_ABORT, true);
RAIL_StartScheduledRx(railHandle, channel, &rxConfig, NULL);
}
// ... do normal app stuff and set shouldSleep when we want to sleep
if (shouldSleep) {
// Let the CPU go to sleep if the system allows it.
sl_power_manager_sleep();
}
}
}
Note
Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_ConfigRxChannelHopping().
DeprecatedRAIL 2.x synonym of sl_rail_config_rx_duty_cycle().
RAIL_EnableRxDutyCycle#
RAIL_Status_t RAIL_EnableRxDutyCycle (RAIL_Handle_t railHandle, bool enable)
Enable RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Duty Cycling. |
Returns
Status code indicating success of the function call.
Enable or disable RX duty cycle mode. After this is called, the radio will begin duty cycling each time it enters RX, based on the configuration passed to RAIL_ConfigRxDutyCycle(). This API must not be called while the radio is on.
Note
Use the compile time symbol RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call RAIL_SupportsChannelHopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with RAIL_EnableRxChannelHopping().
DeprecatedRAIL 2.x synonym of sl_rail_enable_rx_duty_cycle().
RAIL_GetDefaultRxDutyCycleConfig#
RAIL_Status_t RAIL_GetDefaultRxDutyCycleConfig (RAIL_Handle_t railHandle, RAIL_RxDutyCycleConfig_t * config)
Get the default RX duty cycle configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| RAIL_Handle_t | [in] | railHandle | A RAIL instance handle. |
| RAIL_RxDutyCycleConfig_t * | [out] | config | An application-provided non-NULL pointer to store the default RX duty cycle configuration. |
Returns
Status code indicating success of the function call. Note that RAIL_STATUS_INVALID_PARAMETER will be returned if the current channel's radio configuration does not support the requested information.
To save power during RX, an application may want to go to low power as long as possible by periodically waking up and trying to "sense" if there are any incoming packets. This API returns the recommended RX duty cycle configuration, so the application can enter low power mode periodically without missing packets. To wake up earlier, the application can reduce the delay parameter. Note that these value might be different if any configuration / channel has changed.
DeprecatedRAIL 2.x synonym of sl_rail_get_default_rx_duty_cycle_config().
sl_rail_config_rx_channel_hopping#
sl_rail_status_t sl_rail_config_rx_channel_hopping (sl_rail_handle_t rail_handle, sl_rail_rx_channel_hopping_config_t * p_rx_hopping_config)
Configure RX channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| sl_rail_rx_channel_hopping_config_t * | [in] | p_rx_hopping_config | A pointer to the configuration parameters for RX Channel Hopping. |
Returns
Status code indicating success of the function call.
Configure channel hopping channels, conditions, and parameters. This API must be called before sl_rail_enable_rx_channel_hopping(). This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled.
Note
Use the compile time symbol SL_RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call sl_rail_supports_channel_hopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with sl_rail_config_rx_duty_cycle().
sl_rail_enable_rx_channel_hopping#
sl_rail_status_t sl_rail_enable_rx_channel_hopping (sl_rail_handle_t rail_handle, bool enable, bool reset)
Enable RX channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Channel Hopping. |
| bool | [in] | reset | Start from the first channel of the channel hopping sequence (true) or from wherever hopping left off last time the code left RX. |
Returns
Status code indicating success of the function call.
Enable or disable Channel Hopping. Additionally, specify whether hopping should be reset to start from the first channel index, or continue from the channel last hopped to. The radio should not be on when this API is called. sl_rail_config_rx_channel_hopping() must be called successfully before this API is called.
Note
Use the compile time symbol SL_RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call sl_rail_supports_channel_hopping() to check whether the platform supports this feature.
RX Channel Hopping may not be enabled while Auto-Acking is enabled.
Calling this function will overwrite any settings configured with sl_rail_enable_rx_duty_cycle().
sl_rail_trigger_rx_channel_hop#
sl_rail_status_t sl_rail_trigger_rx_channel_hop (sl_rail_handle_t rail_handle)
Manually trigger an Rx channel hop.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
Returns
Status code indicating success of the function call.
This function facilitates a manual hop when using SL_RAIL_RX_CHANNEL_HOPPING_MODE_MANUAL. (It will also trigger a hop in other automatic hop modes as well, so use with caution.)
Note
This function may cause SL_RAIL_EVENT_RX_CHANNEL_HOPPING_COMPLETE to occur before it returns.
sl_rail_get_channel_hopping_rssi#
int16_t sl_rail_get_channel_hopping_rssi (sl_rail_handle_t rail_handle, uint8_t channel_index)
Get RSSI in quarter-dBm of one channel in the channel hopping sequence, during channel hopping.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| uint8_t | [in] | channel_index | Index in the channel hopping sequence of the channel of interest. |
Returns
Latest RSSI in quarter-dBm (dBm * 4) for the channel at the specified index.
Note
Use the compile time symbol SL_RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call sl_rail_supports_channel_hopping() to check whether the platform supports this feature.
In multiprotocol, this function returns SL_RAIL_RSSI_INVALID immediately if rail_handle is not the currently active sl_rail_handle_t.
sl_rail_config_rx_channel_hopping() must be called successfully before this API is called.
When the Z-Wave protocol is active, running sl_rail_get_channel_hopping_rssi() on the 9.6 kbps PHY returns the RSSI measurement of the 40kpbs PHY. This is because the 9.6 kbps PHY has trouble with RSSI measurements on EFR32xG2x family of chips.
sl_rail_config_rx_duty_cycle#
sl_rail_status_t sl_rail_config_rx_duty_cycle (sl_rail_handle_t rail_handle, const sl_rail_rx_duty_cycle_config_t * p_rx_duty_cycle_config)
Configure RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| const sl_rail_rx_duty_cycle_config_t * | [in] | p_rx_duty_cycle_config | A non-NULL pointer to a configuration structure specifying duty cycle parameters. |
Returns
Status code indicating success of the function call.
Configure RX duty cycle mode. With this mode enabled, every time the radio enters RX, it will duty cycle on and off to save power. The duty cycle ratio can be altered dynamically and intelligently by the hardware by staying on longer if a preamble or other packet segments are detected in the air. This API must never be called while the radio is on with RX Duty Cycle or Channel Hopping enabled. For short delays (in the order of microseconds), sl_rail_rx_duty_cycle_config_t::delay_us, this can be used to save receive current while having little impact on the radio performance, for protocols with long preambles. For long delays (in the order of milliseconds or higher) the chip can be put into EM2 energy mode before re-entering RX, to save extra power, with some application hooks as shown below.
#include "sl_rail.h"
extern sl_rail_handle_t rail_handle;
sl_rail_time_t periodic_wakeup_us;
volatile bool duty_cycle_end = true;
void rail_events_callback(sl_rail_handle_t rail_handle, sl_rail_events_t events)
{
// Omitting other event handlers
if (events & SL_RAIL_EVENT_RX_DUTY_CYCLE_RX_END) {
duty_cycle_end = true;
}
}
void main(void)
{
sl_rail_status_t status;
bool should_sleep = false;
initialize_rail(); // Call sl_rail_init() and such
// This function depends on your board/chip but it must enable the LFCLK
// you intend to use for RTCC sync before we configure sleep as that
// function will attempt to auto detect the clock.
Board_Setup_LFCLK();
// Initialize Power Manager module
sl_power_manager_init();
// Initialize RAIL Power Manager
sl_rail_init_power_manager();
// Configure sleep for timer synchronization
sl_rail_timer_sync_config_t timer_sync_config = SL_RAIL_TIMER_SYNC_DEFAULT;
status = sl_rail_config_sleep(rail_handle, &timer_sync_config);
assert(status == SL_RAIL_STATUS_NO_ERROR);
// Configure RX duty-cycling
sl_rail_rx_duty_cycle_config_t duty_cycle_config = {
.mode = SL_RAIL_RX_CHANNEL_HOPPING_MODE_PREAMBLE_SENSE,
.parameter = DUTY_CYCLE_ON_TIME,
.delay_us = DUTY_CYCLE_OFF_TIME,
.delay_mode = SL_RAIL_RX_CHANNEL_HOPPING_DELAY_MODE_STATIC,
.options = SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE,
};
status = sl_rail_config_rx_duty_cycle(rail_handle, &duty_cycle_config);
assert(status == SL_RAIL_STATUS_NO_ERROR);
status = sl_rail_enable_rx_duty_cycle(rail_handle, true);
assert(status == SL_RAIL_STATUS_NO_ERROR);
// Application main loop
while (1) {
if (duty_cycle_end) {
duty_cycle_end = false;
// Schedule the next receive.
sl_rail_scheduled_rx_config_t rx_config = {
.start = periodic_wakeup_us,
.start_mode = SL_RAIL_TIME_DELAY,
.end = 0U,
.end_mode = SL_RAIL_TIME_DISABLED,
.rx_transition_end_schedule = 0U,
.hard_window_end = 0U,
};
sl_rail_idle(rail_handle, SL_RAIL_IDLE_ABORT, true);
sl_rail_start_scheduled_rx(rail_handle, channel, &rx_config, NULL);
}
// ... do normal app stuff and set should_sleep when we want to sleep
if (should_sleep) {
// Let the CPU go to sleep if the system allows it.
sl_power_manager_sleep();
}
}
}
Note
Use the compile time symbol SL_RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call sl_rail_supports_channel_hopping() to check whether the platform supports this feature.
Calling this function will overwrite any settings configured with sl_rail_config_rx_channel_hopping().
On Series 3 parts, to enable RX duty cycling, use the sl_rail_util_ieee802154_phy_select and sl_rail_util_ieee802154_rx_duty_cycling components instead.
sl_rail_enable_rx_duty_cycle#
sl_rail_status_t sl_rail_enable_rx_duty_cycle (sl_rail_handle_t rail_handle, bool enable)
Enable RX duty cycle mode.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| bool | [in] | enable | Enable (true) or disable (false) RX Duty Cycling. |
Returns
Status code indicating success of the function call.
Enable or disable RX duty cycle mode. After this is called, the radio will begin duty cycling each time it enters RX, based on the configuration passed to sl_rail_config_rx_duty_cycle(). This API must not be called while the radio is on.
Note
Use the compile time symbol SL_RAIL_SUPPORTS_CHANNEL_HOPPING or the runtime call sl_rail_supports_channel_hopping() to check whether the platform supports this feature.
calling this function will overwrite any settings configured with sl_rail_enable_rx_channel_hopping().
On Series 3 parts, to enable RX duty cycling, use the sl_rail_util_ieee802154_phy_select and sl_rail_util_ieee802154_rx_duty_cycling components instead.
sl_rail_get_default_rx_duty_cycle_config#
sl_rail_status_t sl_rail_get_default_rx_duty_cycle_config (sl_rail_handle_t rail_handle, sl_rail_rx_duty_cycle_config_t * p_rx_duty_cycle_config)
Get the default RX duty cycle configuration.
| Type | Direction | Argument Name | Description |
|---|---|---|---|
| sl_rail_handle_t | [in] | rail_handle | A real RAIL instance handle. |
| sl_rail_rx_duty_cycle_config_t * | [out] | p_rx_duty_cycle_config | An application-provided non-NULL pointer to store the default RX duty cycle configuration. |
Returns
Status code indicating success of the function call. Note that SL_RAIL_STATUS_INVALID_PARAMETER will be returned if the current channel's radio configuration does not support the requested information.
To save power during RX, an application may want to go to low power as long as possible by periodically waking up and trying to "sense" if there are any incoming packets. This API returns the recommended RX duty cycle configuration, so the application can enter low power mode periodically without missing packets. To wake up earlier, the application can reduce the delay parameter. Note that these value might be different if any configuration / channel has changed.
Macro Definition Documentation#
RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US#
#define RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_USValue:
0x08000000UL
The maximum sense time supported for those RAIL_RxChannelHoppingMode_t modes whose parameter(s) specify a sensing time.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US.
RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE#
#define RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONEValue:
0U
A value representing no options enabled.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE.
RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT#
#define RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULTValue:
RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE
All options disabled by default.
Channel hopping will behave as described by other parameters as it did in RAIL 2.7 and earlier.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT.
RAIL_RX_CHANNEL_HOPPING_OPTION_DEFAULT#
#define RAIL_RX_CHANNEL_HOPPING_OPTION_DEFAULTValue:
RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT
DeprecatedPlease use RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT instead. Replaced by SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT.
RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL#
#define RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CALValue:
(1U << RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL_SHIFT)
An option to skip synth calibration while hopping into the channel specified in the current entry.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL.
RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL#
#define RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CALValue:
(1U << RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL_SHIFT)
An option to skip DC calibration while hopping into the channel specified in the current entry.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL.
RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD#
#define RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLDValue:
(1U << RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD_SHIFT)
An option to check RSSI after hopping into the channel specified in the current entry and hop if that RSSI is below the threshold specified in RAIL_RxChannelHoppingConfigEntry_t::rssiThresholdDbm.
This check runs in parallel with the RAIL_RxChannelHoppingMode_t specified and may cause a hop sooner than that mode otherwise would.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD.
RAIL_RX_CHANNEL_HOPPING_OPTION_STOP#
#define RAIL_RX_CHANNEL_HOPPING_OPTION_STOPValue:
(1U << RAIL_RX_CHANNEL_HOPPING_OPTION_STOP_SHIFT)
An option to stop the hopping sequence at this entry in the hop table, which also idles the radio.
Intended only for testing purposes and not supported on EFR32xG21.
DeprecatedRAIL 2.x synonym of SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOP.
RAIL_CHANNEL_HOPPING_INVALID_INDEX#
#define RAIL_CHANNEL_HOPPING_INVALID_INDEXValue:
(0xFEU)
A sentinel value to flag an invalid channel hopping index.
DeprecatedRAIL 2.x synonym of SL_RAIL_CHANNEL_HOPPING_INVALID_INDEX.
SL_RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_US#
#define SL_RAIL_RX_CHANNEL_HOPPING_MAX_SENSE_TIME_USValue:
0x08000000UL
The maximum sense time supported for those sl_rail_rx_channel_hopping_mode_t modes whose parameter(s) specify a sensing time.
SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONEValue:
0U
A value representing no options enabled.
SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULT#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_DEFAULTValue:
SL_RAIL_RX_CHANNEL_HOPPING_OPTIONS_NONE
All options disabled by default.
Channel hopping will behave as described by other parameters as it did in RAIL 2.7 and earlier.
SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CALValue:
(1U << SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_SYNTH_CAL_SHIFT)
An option to skip synth calibration while hopping into the channel specified in the current entry.
SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CALValue:
(1U << SL_RAIL_RX_CHANNEL_HOPPING_OPTION_SKIP_DC_CAL_SHIFT)
An option to skip DC calibration while hopping into the channel specified in the current entry.
SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLDValue:
(1U << SL_RAIL_RX_CHANNEL_HOPPING_OPTION_RSSI_THRESHOLD_SHIFT)
An option to check RSSI after hopping into the channel specified in the current entry and hop if that RSSI is below the threshold specified in sl_rail_rx_channel_hopping_config_entry_t::rssi_threshold_dbm.
This check runs in parallel with the sl_rail_rx_channel_hopping_mode_t specified and may cause a hop sooner than that mode otherwise would.
SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOP#
#define SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOPValue:
(1U << SL_RAIL_RX_CHANNEL_HOPPING_OPTION_STOP_SHIFT)
An option to stop the hopping sequence at this entry in the hop table, which also idles the radio.
Intended only for testing purposes and not supported on EFR32xG21.
SL_RAIL_CHANNEL_HOPPING_INVALID_INDEX#
#define SL_RAIL_CHANNEL_HOPPING_INVALID_INDEXValue:
(0xFEU)
A sentinel value to flag an invalid channel hopping index.