Receive#

APIs related to packet receive.

Modules#

RAIL_ScheduleRxConfig_t

RAIL_RxPacketInfo_t

RAIL_RxPacketDetails_t

RAIL_PrsLnaBypassConfig_t

sl_rail_scheduled_rx_config_t

sl_rail_rx_packet_info_t

sl_rail_rx_packet_details_t

sl_rail_prs_lna_bypass_config_t

Address Filtering

Packet Information

Enumerations#

enum
RAIL_RX_OPTION_STORE_CRC_SHIFT = 0
RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT = 1
RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT = 2
RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT = 3
RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT = 4
RAIL_RX_OPTION_ANTENNA0_SHIFT = 5
RAIL_RX_OPTION_ANTENNA1_SHIFT = 6
RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT = 7
RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT = 10
RAIL_RX_OPTION_FAST_RX2RX_SHIFT = 11
RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT = 12
}

Receive options, in reality a bitmask.

enum
RAIL_RX_PACKET_NONE = 0
RAIL_RX_PACKET_ABORT_FORMAT = 1
RAIL_RX_PACKET_ABORT_FILTERED = 2
RAIL_RX_PACKET_ABORT_ABORTED = 3
RAIL_RX_PACKET_ABORT_OVERFLOW = 4
RAIL_RX_PACKET_ABORT_CRC_ERROR = 5
RAIL_RX_PACKET_READY_CRC_ERROR = 6
RAIL_RX_PACKET_READY_SUCCESS = 7
RAIL_RX_PACKET_RECEIVING = 8
}

The packet status code associated with a packet received or currently being received.

enum
SL_RAIL_RX_OPTION_STORE_CRC_SHIFT = 0
SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT = 1
SL_RAIL_RX_OPTION_ENABLE_DUAL_SYNC_SHIFT = 2
SL_RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT = 3
SL_RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT = 4
SL_RAIL_RX_OPTION_ANTENNA_0_SHIFT = 5
SL_RAIL_RX_OPTION_ANTENNA_1_SHIFT = 6
SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT = 7
SL_RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT = 10
SL_RAIL_RX_OPTION_FAST_RX_TO_RX_SHIFT = 11
SL_RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT = 12
}

Receive options, in reality a bitmask.

enum
SL_RAIL_RX_PACKET_NONE = 0u
SL_RAIL_RX_PACKET_ABORT_FORMAT = 1u
SL_RAIL_RX_PACKET_ABORT_FILTERED = 2u
SL_RAIL_RX_PACKET_ABORT_ABORTED = 3u
SL_RAIL_RX_PACKET_ABORT_OVERFLOW = 4u
SL_RAIL_RX_PACKET_ABORT_CRC_ERROR = 5u
SL_RAIL_RX_PACKET_READY_CRC_ERROR = 6u
SL_RAIL_RX_PACKET_READY_SUCCESS = 7u
SL_RAIL_RX_PACKET_RECEIVING = 8u
}

The packet status code associated with a packet received or currently being received.

Typedefs#

typedef const void *

A handle used to reference a packet during reception processing.

typedef uint8_t(*
RAIL_ConvertLqiCallback_t)(uint8_t lqi, int8_t rssi)

A pointer to a function called before LQI is copied into the RAIL_RxPacketDetails_t structure.

typedef const void *

A handle used to reference a packet during reception processing.

typedef uint8_t(*
sl_rail_convert_lqi_callback_t)(uint8_t lqi, int8_t rssi_dbm)

A pointer to a function called before LQI is copied into the sl_rail_rx_packet_details_t structure.

Functions#

RAIL_ConfigRxOptions(RAIL_Handle_t railHandle, RAIL_RxOptions_t mask, RAIL_RxOptions_t options)

Configure receive options.

RAIL_IncludeFrameTypeLength(RAIL_Handle_t railHandle)

Include the code necessary for frame type based length decoding.

void
RAILCb_ConfigFrameTypeLength(RAIL_Handle_t railHandle, const RAIL_FrameType_t *frameType)

Handle frame type length.

RAIL_StartRx(RAIL_Handle_t railHandle, uint16_t channel, const RAIL_SchedulerInfo_t *schedulerInfo)

Start the receiver on a specific channel.

RAIL_ScheduleRx(RAIL_Handle_t railHandle, uint16_t channel, const RAIL_ScheduleRxConfig_t *cfg, const RAIL_SchedulerInfo_t *schedulerInfo)

Schedule a receive window for some future time.

RAIL_EnablePrsLnaBypass(RAIL_Handle_t railHandle, bool enable, const RAIL_PrsLnaBypassConfig_t *pPrsLnaBypassConfig)

Enable automatic PRS LNA bypass for external FEM.

RAIL_HoldRxPacket(RAIL_Handle_t railHandle)

Place a temporary hold on this packet's data in the receive FIFO and internal packet metadata FIFO.

uint16_t
RAIL_PeekRxPacket(RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, uint8_t *pDst, uint16_t len, uint16_t offset)

Copy 'len' bytes of packet data starting from 'offset' from the receive FIFO.

RAIL_ReleaseRxPacket(RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle)

Release RAIL's resources for a packet previously held in the receive FIFO and internal receive metadata FIFO.

int16_t
RAIL_GetRssi(RAIL_Handle_t railHandle, bool wait)

Return the current raw RSSI.

int16_t
RAIL_GetRssiAlt(RAIL_Handle_t railHandle, RAIL_Time_t waitTimeout)

Return the current raw RSSI in quarter-dBm within a definitive time period.

RAIL_StartAverageRssi(RAIL_Handle_t railHandle, uint16_t channel, RAIL_Time_t averagingTimeUs, const RAIL_SchedulerInfo_t *schedulerInfo)

Start the RSSI averaging over a specified time in us.

bool
RAIL_IsAverageRssiReady(RAIL_Handle_t railHandle)

Query whether the RSSI averaging is done.

int16_t
RAIL_GetAverageRssi(RAIL_Handle_t railHandle)

Get the RSSI in quarter-dBm averaged over a specified time in microseconds.

RAIL_SetRssiOffset(RAIL_Handle_t railHandle, int8_t rssiOffset)

Set an RSSI offset.

int8_t
RAIL_GetRssiOffset(RAIL_Handle_t railHandle)

Get the radio or protocol RSSI offset in dB.

RAIL_SetRssiDetectThreshold(RAIL_Handle_t railHandle, int8_t rssiThresholdDbm)

Set the RSSI detection threshold in dBm to trigger RAIL_EVENT_DETECT_RSSI_THRESHOLD.

int8_t
RAIL_GetRssiDetectThreshold(RAIL_Handle_t railHandle)

Get the RSSI detection threshold in dBm.

int8_t
RAIL_GetRxIncomingPacketRssi(RAIL_Handle_t railHandle)

Return the RSSI associated with the incoming packet.

RAIL_ConvertLqi(RAIL_Handle_t railHandle, RAIL_ConvertLqiCallback_t cb)

Set up a callback function capable of converting a RX packet's LQI value before being consumed by application code.

sl_rail_config_rx_options(sl_rail_handle_t rail_handle, sl_rail_rx_options_t rx_options_mask, sl_rail_rx_options_t rx_options)

Configure receive options.

sl_rail_include_frame_type_length(sl_rail_handle_t rail_handle)

Include the code necessary for frame type based length decoding.

sl_rail_start_rx(sl_rail_handle_t rail_handle, uint16_t channel, const sl_rail_scheduler_info_t *p_scheduler_info)

Start the receiver on a specific channel.

sl_rail_start_scheduled_rx(sl_rail_handle_t rail_handle, uint16_t channel, const sl_rail_scheduled_rx_config_t *p_scheduled_rx_config, const sl_rail_scheduler_info_t *p_scheduler_info)

Schedule a receive window for some future time.

sl_rail_enable_prs_lna_bypass(sl_rail_handle_t rail_handle, bool enable, const sl_rail_prs_lna_bypass_config_t *p_prs_lna_bypass_config)

Enable automatic PRS LNA bypass for external FEM.

sl_rail_hold_rx_packet(sl_rail_handle_t rail_handle)

Place a temporary hold on this packet's data and metadata in the receive FIFO and receive Packet Queue.

uint16_t
sl_rail_peek_rx_packet(sl_rail_handle_t rail_handle, sl_rail_rx_packet_handle_t packet_handle, uint8_t *p_dest, uint16_t peek_bytes, uint16_t offset_bytes)

Copy 'len_bytes' of packet data starting from 'byte_offset' from the receive FIFO.

sl_rail_release_rx_packet(sl_rail_handle_t rail_handle, sl_rail_rx_packet_handle_t packet_handle)

Release RAIL's resources for a packet previously held in the receive FIFO and receive Packet Queue.

int16_t
sl_rail_get_rssi(sl_rail_handle_t rail_handle, sl_rail_time_t wait_timeout_us)

Return the current raw RSSI in quarter-dBm within a definitive time period.

sl_rail_start_average_rssi(sl_rail_handle_t rail_handle, uint16_t channel, sl_rail_time_t averaging_time_us, const sl_rail_scheduler_info_t *p_scheduler_info)

Start the RSSI averaging over a specified time in us.

bool
sl_rail_is_average_rssi_ready(sl_rail_handle_t rail_handle)

Query whether the RSSI averaging is done.

int16_t
sl_rail_get_average_rssi(sl_rail_handle_t rail_handle)

Get the RSSI in quarter-dBm averaged over a specified time in microseconds.

sl_rail_set_rssi_offset(sl_rail_handle_t rail_handle, int8_t rssi_offset_db)

Set an RSSI offset.

int8_t
sl_rail_get_rssi_offset(sl_rail_handle_t rail_handle)

Get the radio or protocol RSSI offset in dB.

sl_rail_set_rssi_detect_threshold(sl_rail_handle_t rail_handle, int8_t rssi_threshold_dbm)

Set the RSSI detection threshold in dBm to trigger SL_RAIL_EVENT_DETECT_RSSI_THRESHOLD.

int8_t
sl_rail_get_rssi_detect_threshold(sl_rail_handle_t rail_handle)

Get the RSSI detection threshold in dBm.

int8_t
sl_rail_get_rx_incoming_packet_rssi(sl_rail_handle_t rail_handle)

Return the RSSI associated with the incoming packet.

sl_rail_convert_lqi(sl_rail_handle_t rail_handle, sl_rail_convert_lqi_callback_t lqi_callback)

Set up a callback function capable of converting a RX packet's LQI value before being consumed by application code.

Macros#

#define
RAIL_RX_OPTIONS_NONE 0

A value representing no options enabled.

#define
RAIL_RX_OPTIONS_DEFAULT RAIL_RX_OPTIONS_NONE

All options are disabled by default.

#define
RAIL_RX_OPTION_STORE_CRC (1UL << RAIL_RX_OPTION_STORE_CRC_SHIFT)

An option to configure whether the CRC portion of the packet is included in the packet payload exposed to the app on packet reception.

#define
RAIL_RX_OPTION_IGNORE_CRC_ERRORS (1UL << RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT)

An option to configure whether CRC errors will be ignored.

#define
RAIL_RX_OPTION_ENABLE_DUALSYNC (1UL << RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT)

An option to control which sync words will be accepted.

#define
RAIL_RX_OPTION_TRACK_ABORTED_FRAMES (1UL << RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT)

An option to configure whether frames which are aborted during reception should continue to be tracked.

#define
RAIL_RX_OPTION_REMOVE_APPENDED_INFO (1UL << RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT)

An option to suppress capturing the appended information after received frames.

#define
RAIL_RX_OPTION_ANTENNA0 (1UL << RAIL_RX_OPTION_ANTENNA0_SHIFT)

An option to select the use of antenna 0 during receive (including Auto-Ack receive).

#define
RAIL_RX_OPTION_ANTENNA1 (1UL << RAIL_RX_OPTION_ANTENNA1_SHIFT)

An option to select the use of antenna 1 during receive (including Auto-Ack receive).

#define
RAIL_RX_OPTION_ANTENNA_AUTO (RAIL_RX_OPTION_ANTENNA0 | RAIL_RX_OPTION_ANTENNA1)

An option combination to automatically choose an antenna during receive (including Auto-Ack receive).

#define
RAIL_RX_OPTION_DISABLE_FRAME_DETECTION (1UL << RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT)

An option to disable frame detection.

#define
RAIL_RX_OPTION_CHANNEL_SWITCHING (1U << RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT)

An option to enable IEEE 802.15.4 RX channel switching.

#define
RAIL_RX_OPTION_FAST_RX2RX (1U << RAIL_RX_OPTION_FAST_RX2RX_SHIFT)

An option to enable fast RX2RX state transition.

#define
RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION (1U << RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT)

An option to enable collision detection.

#define
RAIL_RX_OPTIONS_ALL 0xFFFFFFFFUL

A value representing all possible options.

#define
RAIL_RSSI_INVALID_DBM (-128)

The value returned by RAIL for an invalid RSSI, in dBm.

#define
RAIL_RSSI_INVALID ((int16_t)(RAIL_RSSI_INVALID_DBM * 4))

The value returned by RAIL for an invalid RSSI: in quarter dBm.

#define
RAIL_RSSI_LOWEST ((int16_t)(RAIL_RSSI_INVALID + 1))

The lowest RSSI value returned by RAIL: in quarter dBm.

#define
RAIL_RSSI_OFFSET_MAX 35

Maximum absolute value for RSSI offset.

#define
RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT ((RAIL_Time_t)0xFFFFFFFFU)

A sentinel value to indicate waiting for a valid RSSI without a timeout.

#define
RAIL_GET_RSSI_NO_WAIT ((RAIL_Time_t)0U)

A sentinel value to indicate no waiting for a valid RSSI.

#define
RAIL_RX_PACKET_HANDLE_INVALID (NULL)

An invalid RX packet handle value.

#define
RAIL_RX_PACKET_HANDLE_OLDEST ((RAIL_RxPacketHandle_t) 1)

A special RX packet handle to refer to the oldest unreleased packet.

#define
RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE ((RAIL_RxPacketHandle_t) 2)

A special RX packet handle to refer to the oldest unreleased complete packet.

#define
RAIL_RX_PACKET_HANDLE_NEWEST ((RAIL_RxPacketHandle_t) 3)

A special RX packet handle to refer to the newest unreleased packet when in callback context.

#define
SL_RAIL_RX_OPTIONS_NONE 0

A value representing no options enabled.

#define
SL_RAIL_RX_OPTIONS_DEFAULT SL_RAIL_RX_OPTIONS_NONE

All options are disabled by default.

#define
SL_RAIL_RX_OPTION_STORE_CRC (1UL << SL_RAIL_RX_OPTION_STORE_CRC_SHIFT)

An option to configure whether the CRC portion of the packet is included in the packet payload exposed to the app on packet reception.

#define
SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS (1UL << SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT)

An option to configure whether CRC errors will be ignored.

#define
SL_RAIL_RX_OPTION_ENABLE_DUAL_SYNC (1UL << SL_RAIL_RX_OPTION_ENABLE_DUAL_SYNC_SHIFT)

An option to control which sync words will be accepted.

#define
SL_RAIL_RX_OPTION_TRACK_ABORTED_FRAMES (1UL << SL_RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT)

An option to configure whether frames which are aborted during reception should continue to be tracked.

#define
SL_RAIL_RX_OPTION_REMOVE_APPENDED_INFO (1UL << SL_RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT)

An option to suppress capturing the appended information after received frames.

#define
SL_RAIL_RX_OPTION_ANTENNA_0 (1UL << SL_RAIL_RX_OPTION_ANTENNA_0_SHIFT)

An option to select the use of antenna 0 during receive (including Auto-Ack receive).

#define
SL_RAIL_RX_OPTION_ANTENNA_1 (1UL << SL_RAIL_RX_OPTION_ANTENNA_1_SHIFT)

An option to select the use of antenna 1 during receive (including Auto-Ack receive).

#define
SL_RAIL_RX_OPTION_ANTENNA_AUTO (SL_RAIL_RX_OPTION_ANTENNA_0 | SL_RAIL_RX_OPTION_ANTENNA_1)

An option combination to automatically choose an antenna during receive (including Auto-Ack receive).

#define
SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION (1UL << SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT)

An option to disable frame detection.

#define
SL_RAIL_RX_OPTION_CHANNEL_SWITCHING (1U << SL_RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT)

An option to enable IEEE 802.15.4 RX channel switching.

#define
SL_RAIL_RX_OPTION_FAST_RX_TO_RX (1U << SL_RAIL_RX_OPTION_FAST_RX_TO_RX_SHIFT)

An option to enable fast RX-to-RX state transition.

#define
SL_RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION (1U << SL_RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT)

An option to enable collision detection.

#define
SL_RAIL_RX_OPTIONS_ALL 0xFFFFFFFFUL

A value representing all possible options.

#define
SL_RAIL_RSSI_INVALID_DBM (-128)

The value returned by RAIL for an invalid RSSI, in dBm.

#define
SL_RAIL_RSSI_INVALID ((int16_t)(SL_RAIL_RSSI_INVALID_DBM * 4))

The value returned by RAIL for an invalid RSSI: in quarter dBm.

#define
SL_RAIL_RSSI_LOWEST ((int16_t)(SL_RAIL_RSSI_INVALID + 1))

The lowest RSSI value returned by RAIL: in quarter dBm.

#define
SL_RAIL_RSSI_OFFSET_MAX 35

Maximum absolute value for RSSI offset.

#define
SL_RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT ((sl_rail_time_t)0xFFFFFFFFU)

A sentinel value to indicate waiting for a valid RSSI without a timeout.

#define
SL_RAIL_GET_RSSI_NO_WAIT ((sl_rail_time_t)0U)

A sentinel value to indicate no waiting for a valid RSSI.

#define
SL_RAIL_RX_PACKET_HANDLE_INVALID (NULL)

An invalid RX packet handle value.

#define
SL_RAIL_RX_PACKET_HANDLE_OLDEST ((sl_rail_rx_packet_handle_t) 1)

A special RX packet handle to refer to the oldest unreleased packet.

#define
SL_RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE ((sl_rail_rx_packet_handle_t) 2)

A special RX packet handle to refer to the oldest unreleased complete packet.

#define
SL_RAIL_RX_PACKET_HANDLE_NEWEST ((sl_rail_rx_packet_handle_t) 3)

A special RX packet handle to refer to the newest unreleased packet when in callback context.

Enumeration Documentation#

RAIL_RxOptions_t#

RAIL_RxOptions_t

Receive options, in reality a bitmask.

DeprecatedRAIL 2.x synonym of sl_rail_rx_options_t.

Enumerator
RAIL_RX_OPTION_STORE_CRC_SHIFT

Shift position of RAIL_RX_OPTION_STORE_CRC bit.

RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT

Shift position of RAIL_RX_OPTION_IGNORE_CRC_ERRORS bit.

RAIL_RX_OPTION_ENABLE_DUALSYNC_SHIFT

Shift position of RAIL_RX_OPTION_ENABLE_DUALSYNC bit.

RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT

Shift position of RAIL_RX_OPTION_TRACK_ABORTED_FRAMES bit.

RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT

Shift position of RAIL_RX_OPTION_REMOVE_APPENDED_INFO bit.

RAIL_RX_OPTION_ANTENNA0_SHIFT

Shift position of RAIL_RX_OPTION_ANTENNA0 bit.

RAIL_RX_OPTION_ANTENNA1_SHIFT

Shift position of RAIL_RX_OPTION_ANTENNA1 bit.

RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT

Shift position of RAIL_RX_OPTION_DISABLE_FRAME_DETECTION bit.

RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT

Shift position of RAIL_RX_OPTION_CHANNEL_SWITCHING bit.

RAIL_RX_OPTION_FAST_RX2RX_SHIFT

Shift position of RAIL_RX_OPTION_FAST_RX2RX bit.

RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT

Shift position of RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION bit.


RAIL_RxPacketStatus_t#

RAIL_RxPacketStatus_t

The packet status code associated with a packet received or currently being received.

Note

  • RECEIVING implies some packet data may be available, but is untrustworthy (not CRC-verified) and might disappear if the packet is rolled back on error. No packet details are yet available.

  • In RX RAIL_DataMethod_t::FIFO_MODE, ABORT statuses imply some packet data may be available, but it's incomplete and not trustworthy.

DeprecatedRAIL 2.x synonym of sl_rail_rx_packet_status_t.

Enumerator
RAIL_RX_PACKET_NONE

The radio is idle or searching for a packet.

RAIL_RX_PACKET_ABORT_FORMAT

The packet was aborted during filtering because of illegal frame length, CRC or block decoding errors, other RAIL built-in protocol-specific packet content errors, or by the application or multiprotocol scheduler idling the radio with RAIL_IDLE_ABORT or higher.

RAIL_RX_PACKET_ABORT_FILTERED

The packet failed address filtering.

RAIL_RX_PACKET_ABORT_ABORTED

The packet passed any filtering but was aborted by the application or multiprotocol scheduler idling the radio with RAIL_IDLE_ABORT or higher.

RAIL_RX_PACKET_ABORT_OVERFLOW

The packet overflowed the receive buffer.

RAIL_RX_PACKET_ABORT_CRC_ERROR

The packet passed any filtering but subsequently failed CRC check(s) block decoding, or illegal frame length, and was aborted.

RAIL_RX_PACKET_READY_CRC_ERROR

The packet passed any filtering but subsequently failed CRC check(s) with RAIL_RX_OPTION_IGNORE_CRC_ERRORS in effect.

RAIL_RX_PACKET_READY_SUCCESS

The packet was successfully received, passing CRC check(s).

RAIL_RX_PACKET_RECEIVING

A packet is being received and is not yet complete.


sl_rail_rx_options_t#

sl_rail_rx_options_t

Receive options, in reality a bitmask.

Enumerator
SL_RAIL_RX_OPTION_STORE_CRC_SHIFT

Shift position of SL_RAIL_RX_OPTION_STORE_CRC bit.

SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS_SHIFT

Shift position of SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS bit.

SL_RAIL_RX_OPTION_ENABLE_DUAL_SYNC_SHIFT

Shift position of SL_RAIL_RX_OPTION_ENABLE_DUAL_SYNC bit.

SL_RAIL_RX_OPTION_TRACK_ABORTED_FRAMES_SHIFT

Shift position of SL_RAIL_RX_OPTION_TRACK_ABORTED_FRAMES bit.

SL_RAIL_RX_OPTION_REMOVE_APPENDED_INFO_SHIFT

Shift position of SL_RAIL_RX_OPTION_REMOVE_APPENDED_INFO bit.

SL_RAIL_RX_OPTION_ANTENNA_0_SHIFT

Shift position of SL_RAIL_RX_OPTION_ANTENNA_0 bit.

SL_RAIL_RX_OPTION_ANTENNA_1_SHIFT

Shift position of SL_RAIL_RX_OPTION_ANTENNA_1 bit.

SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION_SHIFT

Shift position of SL_RAIL_RX_OPTION_DISABLE_FRAME_DETECTION bit.

SL_RAIL_RX_OPTION_CHANNEL_SWITCHING_SHIFT

Shift position of SL_RAIL_RX_OPTION_CHANNEL_SWITCHING bit.

SL_RAIL_RX_OPTION_FAST_RX_TO_RX_SHIFT

Shift position of SL_RAIL_RX_OPTION_FAST_RX_TO_RX bit.

SL_RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION_SHIFT

Shift position of SL_RAIL_RX_OPTION_ENABLE_COLLISION_DETECTION bit.


sl_rail_rx_packet_status_t#

sl_rail_rx_packet_status_t

The packet status code associated with a packet received or currently being received.

Note

  • RECEIVING implies some packet data may be available, but is untrustworthy (not CRC-verified) and might disappear if the packet is rolled back on error. No packet details are yet available.

  • In RX sl_rail_data_method_t::SL_RAIL_DATA_METHOD_FIFO_MODE, ABORT statuses imply some packet data may be available, but it's incomplete and not trustworthy.

Enumerator
SL_RAIL_RX_PACKET_NONE

The radio is idle or searching for a packet.

SL_RAIL_RX_PACKET_ABORT_FORMAT

The packet was aborted during filtering because of illegal frame length, CRC or block decoding errors, other RAIL built-in protocol-specific packet content errors, or by the application or multiprotocol scheduler idling the radio with SL_RAIL_IDLE_ABORT or higher.

SL_RAIL_RX_PACKET_ABORT_FILTERED

The packet failed address filtering.

SL_RAIL_RX_PACKET_ABORT_ABORTED

The packet passed any filtering but was aborted by the application or multiprotocol scheduler idling the radio with SL_RAIL_IDLE_ABORT or higher.

SL_RAIL_RX_PACKET_ABORT_OVERFLOW

The packet overflowed the receive buffer.

SL_RAIL_RX_PACKET_ABORT_CRC_ERROR

The packet passed any filtering but subsequently failed CRC check(s) block decoding, or illegal frame length, and was aborted.

SL_RAIL_RX_PACKET_READY_CRC_ERROR

The packet passed any filtering but subsequently failed CRC check(s) with SL_RAIL_RX_OPTION_IGNORE_CRC_ERRORS in effect.

SL_RAIL_RX_PACKET_READY_SUCCESS

The packet was successfully received, passing CRC check(s).

SL_RAIL_RX_PACKET_RECEIVING

A packet is being received and is not yet complete.


Typedef Documentation#

RAIL_RxPacketHandle_t#

RAIL_RxPacketHandle_t

A handle used to reference a packet during reception processing.

There are several sentinel handle values that pertain to certain circumstances: RAIL_RX_PACKET_HANDLE_INVALID, RAIL_RX_PACKET_HANDLE_OLDEST, RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE and RAIL_RX_PACKET_HANDLE_NEWEST.

DeprecatedRAIL 2.x synonym of sl_rail_rx_packet_handle_t.


RAIL_ConvertLqiCallback_t#

RAIL_ConvertLqiCallback_t )(uint8_t lqi, int8_t rssi)

A pointer to a function called before LQI is copied into the RAIL_RxPacketDetails_t structure.

Parameters
TypeDirectionArgument NameDescription
[in]lqi

The LQI value obtained by hardware and being readied for application consumption. This LQI value is in integral units ranging from 0 to 255.

[in]rssi

The RSSI value corresponding to the packet from which the hardware LQI value was obtained. This RSSI value is in integral dBm units.

Returns

  • uint8_t The converted LQI value that will be loaded into the RAIL_RxPacketDetails_t structure in preparation for application consumption. This value should likewise be in integral units ranging from 0 to 255.

DeprecatedRAIL 2.x synonym of sl_rail_convert_lqi_callback_t().


sl_rail_rx_packet_handle_t#

sl_rail_rx_packet_handle_t

A handle used to reference a packet during reception processing.

There are several sentinel handle values that pertain to certain circumstances: SL_RAIL_RX_PACKET_HANDLE_INVALID, SL_RAIL_RX_PACKET_HANDLE_OLDEST, SL_RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE and SL_RAIL_RX_PACKET_HANDLE_NEWEST.


sl_rail_convert_lqi_callback_t#

sl_rail_convert_lqi_callback_t )(uint8_t lqi, int8_t rssi_dbm)

A pointer to a function called before LQI is copied into the sl_rail_rx_packet_details_t structure.

Parameters
TypeDirectionArgument NameDescription
[in]lqi

The LQI value obtained by hardware and being readied for application consumption. This LQI value is in integral units ranging from 0 to 255.

[in]rssi_dbm

The RSSI value corresponding to the packet from which the hardware LQI value was obtained. This RSSI value is in integral dBm units.

Returns

  • uint8_t The converted LQI value that will be loaded into the sl_rail_rx_packet_details_t structure in preparation for application consumption. This value should likewise be in integral units ranging from 0 to 255.


Function Documentation#

RAIL_ConfigRxOptions#

RAIL_Status_t RAIL_ConfigRxOptions (RAIL_Handle_t railHandle, RAIL_RxOptions_t mask, RAIL_RxOptions_t options)

Configure receive options.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_RxOptions_t[in]mask

A bitmask containing which options should be modified.

RAIL_RxOptions_t[in]options

A bitmask containing desired configuration settings. Bit positions for each option are found in the RAIL_RxOptions_t.

Returns

  • Status code indicating success of the function call.

Configure the radio receive flow based on the list of available options. Only the options indicated by the mask parameter will be affected. Pass RAIL_RX_OPTIONS_ALL to set all parameters. The previous settings may affect the current frame if a packet is received during this configuration.

DeprecatedRAIL 2.x synonym of sl_rail_config_rx_options().


RAIL_IncludeFrameTypeLength#

RAIL_Status_t RAIL_IncludeFrameTypeLength (RAIL_Handle_t railHandle)

Include the code necessary for frame type based length decoding.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • Status code indicating success of the function call.

This function must be called before RAIL_ConfigChannels() to allow configurations using a frame type based length setup. It is called by default in the RAILCb_ConfigFrameTypeLength() API which can be overridden to save code space.

DeprecatedRAIL 2.x synonym of sl_rail_include_frame_type_length().


RAILCb_ConfigFrameTypeLength#

void RAILCb_ConfigFrameTypeLength (RAIL_Handle_t railHandle, const RAIL_FrameType_t * frameType)

Handle frame type length.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

const RAIL_FrameType_t *[in]frameType

A pointer to a frame type configuration structure.

This function is implemented in the radio configuration. Currently, the frame type passed in only handles packet length decoding. If NULL is passed into this function, it clears any currently configured frame type settings. This will either be implemented as an empty function in the radio configuration if it is not needed, to assist in dead code elimination.

DeprecatedThis RAIL 2.x callback has been eliminated in RAIL 3. Applications needing frame type length decoding must call sl_rail_include_frame_type_length().


RAIL_StartRx#

RAIL_Status_t RAIL_StartRx (RAIL_Handle_t railHandle, uint16_t channel, const RAIL_SchedulerInfo_t * schedulerInfo)

Start the receiver on a specific channel.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]channel

The channel to listen on.

const RAIL_SchedulerInfo_t *[in]schedulerInfo

A pointer to information to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

This is a non-blocking function. Whenever a packet is received, RAIL_Config_t::eventsCallback() will fire with RAIL_EVENT_RX_PACKET_RECEIVED set. If you call this while not idle but with a different channel, any ongoing receive or transmit operation will be aborted.

DeprecatedRAIL 2.x synonym of sl_rail_start_rx().


RAIL_ScheduleRx#

RAIL_Status_t RAIL_ScheduleRx (RAIL_Handle_t railHandle, uint16_t channel, const RAIL_ScheduleRxConfig_t * cfg, const RAIL_SchedulerInfo_t * schedulerInfo)

Schedule a receive window for some future time.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]channel

A channel to listen on.

const RAIL_ScheduleRxConfig_t *[in]cfg

A pointer to a configuration structure to define the receive window.

const RAIL_SchedulerInfo_t *[in]schedulerInfo

A pointer to information to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

This API immediately changes the channel and schedules receive to start at the specified time and end at the given end time. If you do not specify an end time, you may call this API later with an end time as long as you set the start time to disabled. You can also terminate the receive operation immediately using the RAIL_Idle() function. Note that relative end times are always relative to the start unless no start time is specified. If changing channels, the channel is changed immediately and will abort any ongoing packet transmission or reception.

Returns an error if a CSMA or LBT transmit is still in progress.

In multiprotocol, ensure that you properly yield the radio after this call. See Yielding the Radio for more details.

DeprecatedRAIL 2.x synonym of sl_rail_start_scheduled_rx().


RAIL_EnablePrsLnaBypass#

RAIL_Status_t RAIL_EnablePrsLnaBypass (RAIL_Handle_t railHandle, bool enable, const RAIL_PrsLnaBypassConfig_t * pPrsLnaBypassConfig)

Enable automatic PRS LNA bypass for external FEM.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

bool[in]enable

Enable/Disable automatic PRS LNA bypass.

const RAIL_PrsLnaBypassConfig_t *[in]pPrsLnaBypassConfig

A pointer to an automatic PRS LNA bypass configuration structure. It must be non-NULL to enable the feature.

Returns

  • Status code indicating success of the function call.

If automatic PRS LNA bypass is enabled on chip that supports the feature (RAIL_SUPPORTS_PRS_LNA_BYPASS), a level is generated on a PRS channel when the received power exceed a threshold. It is turned off after frame reception or after timeout if no frame has been detected and power is below the threshold.

Warnings

  • Calling this function before RAIL_Init() won't enable the the feature now. It will return RAIL_STATUS_NO_ERROR but the feature will be enabled by RAIL_Init().

  • As this function relies on PRS access and RAIL is meant to run in TrustZone non-secure world, it is not supported if PRS is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.

DeprecatedRAIL 2.x synonym of sl_rail_enable_prs_lna_bypass().


RAIL_HoldRxPacket#

RAIL_RxPacketHandle_t RAIL_HoldRxPacket (RAIL_Handle_t railHandle)

Place a temporary hold on this packet's data in the receive FIFO and internal packet metadata FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

This function can only be called from within RAIL callback context. It can be used in any RX mode.

Normally, when RAIL issues its callback indicating a packet is ready or aborted, it expects the application's callback to retrieve and copy (or discard) the packet's information and data, and will free the packet data and metadata after the callback returns. This function tells RAIL to hold onto those resources in the receive FIFO and internal metadata FIFO after the callback returns in case the application wants to defer processing the packet to a later time, e.g., outside of callback context.

Returns

  • The packet handle for the packet associated with the callback, RAIL_RX_PACKET_HANDLE_INVALID if no such packet yet exists or railHandle is not active.

Note

  • When using multiprotocol the receive FIFO and internal receive metadata FIFO are reset during protocol switches losing any held packets. It is best to avoid using RAIL_HoldRxPacket in DMP or to at least invalidate any held packet handles and related RAIL_RxPacketInfo_t information when the RAIL_EVENT_CONFIG_UNSCHEDULED occurs.

DeprecatedRAIL 2.x synonym of sl_rail_hold_rx_packet().


RAIL_PeekRxPacket#

uint16_t RAIL_PeekRxPacket (RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle, uint8_t * pDst, uint16_t len, uint16_t offset)

Copy 'len' bytes of packet data starting from 'offset' from the receive FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_RxPacketHandle_t[in]packetHandle

A packet handle as returned from a previous RAIL_GetRxPacketInfo() or RAIL_HoldRxPacket() call, or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST, RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE or RAIL_RX_PACKET_HANDLE_NEWEST.

uint8_t *[out]pDst

A pointer to the location where the received bytes will be copied. If NULL, no copying occurs.

uint16_t[in]len

A number of packet data bytes to copy.

uint16_t[in]offset

A byte offset within remaining packet data from which to copy.

Those bytes remain valid for re-peeking.

Returns

  • Number of packet bytes copied.

Note

  • Peek does not permit peeking beyond the requested packet's available packet data (though there is a small chance it might for a RAIL_RX_PACKET_HANDLE_NEWEST packet at the very end of still being received). Nor can one peek into already-consumed data read by RAIL_ReadRxFifo(). len and offset are relative to the remaining data available in the packet, if any was already consumed by RAIL_ReadRxFifo().

DeprecatedRAIL 2.x synonym of sl_rail_peek_rx_packet().


RAIL_ReleaseRxPacket#

RAIL_Status_t RAIL_ReleaseRxPacket (RAIL_Handle_t railHandle, RAIL_RxPacketHandle_t packetHandle)

Release RAIL's resources for a packet previously held in the receive FIFO and internal receive metadata FIFO.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_RxPacketHandle_t[in]packetHandle

A packet handle as returned from a previous RAIL_HoldRxPacket() call, or sentinel values RAIL_RX_PACKET_HANDLE_OLDEST, RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE or RAIL_RX_PACKET_HANDLE_NEWEST. The latter might be used within RAIL callback context to explicitly release the packet associated with the callback early, before it's released automatically by RAIL on callback return (unless explicitly held).

This function must be called for any packet previously held via RAIL_HoldRxPacket(). It may optionally be called within a callback context to release RAIL resources sooner than at callback completion time when not holding the packet. This function can be used in any RX mode.

Returns

DeprecatedRAIL 2.x synonym of sl_rail_release_rx_packet().


RAIL_GetRssi#

int16_t RAIL_GetRssi (RAIL_Handle_t railHandle, bool wait)

Return the current raw RSSI.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]wait

if false returns instant RSSI with no checks.

Returns

  • RAIL_RSSI_INVALID if the receiver is disabled and an RSSI value can't be obtained. Otherwise, return the RSSI in quarter dBm, dbm*4.

Gets the current RSSI value. This value represents the current energy of the channel. It can change rapidly and will be low if no RF energy is in the current channel. The function from the value reported to dBm is an offset dependent on the PHY and the PCB layout. Characterize the RSSI received on your hardware and apply an offset in the application to account for board and PHY parameters. When 'wait' is false, the radio needs to be currently in RX and have been in there for a sufficient amount of time for a fresh RSSI value to be read and returned. Otherwise, the RSSI is considered stale and RAIL_RSSI_INVALID is returned instead. When 'wait' is true, if the radio is transitioning to or already in RX, this function will wait for a valid RSSI to be read and return it. Otherwise, if the radio is in or transitions to IDLE or TX, RAIL_RSSI_INVALID will be returned. On low datarate PHYs, this function can take a significantly longer time when wait is true.

In multiprotocol, this function returns RAIL_RSSI_INVALID immediately if railHandle is not the currently active RAIL_Handle_t. Additionally, 'wait' should never be set 'true' in multiprotocol as the wait time is not consistent, so scheduling a scheduler slot cannot be done accurately. Rather if waiting for a valid RSSI is desired, use RAIL_GetRssiAlt instead to apply a bounded time period.

Note

DeprecatedThis RAIL 2.x function has been replaced in RAIL 3 by sl_rail_get_rssi() with a different parameter.


RAIL_GetRssiAlt#

int16_t RAIL_GetRssiAlt (RAIL_Handle_t railHandle, RAIL_Time_t waitTimeout)

Return the current raw RSSI in quarter-dBm within a definitive time period.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_Time_t[in]waitTimeout

Sets the maximum time in microseconds to wait for a valid RSSI. If equal to RAIL_GET_RSSI_NO_WAIT returns instant RSSI with no checks. If equal to RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT waits for a valid RSSI with no maximum timeout.

Returns

  • RAIL_RSSI_INVALID if the receiver is disabled and an RSSI value can't be obtained. Otherwise, return the RSSI in quarter dBm (dBm*4).

Gets the current RSSI value. This value represents the current energy of the channel. It can change rapidly, and will be low if no RF energy is in the current channel. The function from the value reported to dBm is an offset dependent on the PHY and the PCB layout. Characterize the RSSI received on your hardware and apply an offset in the application to account for board and PHY parameters. If a value of RAIL_GET_RSSI_NO_WAIT is given for waitTimeout, the radio needs to be currently in RX and have been in there for a sufficient amount of time for a fresh RSSI value to be read and returned. Otherwise the RSSI is considered stale and RAIL_RSSI_INVALID is returned instead. For non-zero values of waitTimeout, if the radio is transitioning to or already in RX, this function will wait a maximum time equal to waitTimeout (or indefinitely if waitTimeout is set to RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT) for a valid RSSI to be read and return it. Otherwise, if the waitTimeout is reached, or the radio is in or transitions to IDLE or TX, RAIL_RSSI_INVALID will be returned. On low datarate PHYs, this function can take a significantly longer time when waitTimeout is non-zero.

In multiprotocol, this function returns RAIL_RSSI_INVALID immediately if railHandle is not the currently active RAIL_Handle_t. Additionally, waitTimeout should never be set to a value other than RAIL_GET_RSSI_NO_WAIT in multiprotocol as the integration between this feature and the radio scheduler has not been implemented.

Note

DeprecatedRAIL 2.x synonym of sl_rail_get_rssi().


RAIL_StartAverageRssi#

RAIL_Status_t RAIL_StartAverageRssi (RAIL_Handle_t railHandle, uint16_t channel, RAIL_Time_t averagingTimeUs, const RAIL_SchedulerInfo_t * schedulerInfo)

Start the RSSI averaging over a specified time in us.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint16_t[in]channel

The physical channel to set.

RAIL_Time_t[in]averagingTimeUs

Averaging time in microseconds.

const RAIL_SchedulerInfo_t *[in]schedulerInfo

A pointer to information to allow the radio scheduler to place this operation appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

Starts a non-blocking hardware-based RSSI averaging mechanism. Only a single instance of RSSI averaging can be run at any time and the radio must be idle to start.

In multiprotocol, this is a scheduled event. It will start when railHandle becomes active. railHandle needs to stay active until the averaging completes. If the averaging is interrupted, calls to RAIL_GetAverageRssi() will return RAIL_RSSI_INVALID.

Also in multiprotocol, the user is required to call RAIL_YieldRadio() after this event completes (i.e., when RAIL_EVENT_RSSI_AVERAGE_DONE occurs).

Note

DeprecatedRAIL 2.x synonym of sl_rail_start_average_rssi().


RAIL_IsAverageRssiReady#

bool RAIL_IsAverageRssiReady (RAIL_Handle_t railHandle)

Query whether the RSSI averaging is done.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • true if done and false otherwise.

This function can be used to poll for completion of the RSSI averaging to avoid relying on an interrupt-based callback.

Note

  • If the radio is idled while RSSI averaging is still in effect, this function may never return true.

DeprecatedRAIL 2.x synonym of sl_rail_is_average_rssi_ready().


RAIL_GetAverageRssi#

int16_t RAIL_GetAverageRssi (RAIL_Handle_t railHandle)

Get the RSSI in quarter-dBm averaged over a specified time in microseconds.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • The RSSI in quarter-dBm (dBm * 4), or RAIL_RSSI_INVALID if the receiver is disabled or an an RSSI value couldn't be obtained.

Gets the hardware RSSI average after issuing RAIL_StartAverageRssi(). Use after RAIL_StartAverageRssi().

DeprecatedRAIL 2.x synonym of sl_rail_get_average_rssi().


RAIL_SetRssiOffset#

RAIL_Status_t RAIL_SetRssiOffset (RAIL_Handle_t railHandle, int8_t rssiOffset)

Set an RSSI offset.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

int8_t[in]rssiOffset

desired dB offset to be added to the RSSI measurements.

Returns

Adds an offset to the RSSI in dBm. This offset affects all functionality that depends on RSSI values, such as CCA functions. Do not modify the offset dynamically during packet reception. This function can only be called while the radio is off, or in the case of multiprotocol, on an inactive protocol.

Note

  • : Prior to RAIL being initialized, a radio-wide protocol-independent offset can be established using a radio-generic handle like RAIL_EFR32_HANDLE. The radio RSSI offset can range from -50 to +20 dB.
    After RAIL has been initialized a real RAIL protocol handle must be provided to set a protocol-specific RSSI offset, which is added to any radio offset (plus a per-PHY offset set by the radio calculator). The absolute value of the overall sum of all these offsets cannot exceed RAIL_RSSI_OFFSET_MAX otherwise RSSIs could underflow or overflow.

  • : During RX Channel Hopping this API will not update the RSSI offset immediately if channel hopping has already been configured. A subsequent call to RAIL_ZWAVE_ConfigRxChannelHopping() or RAIL_ConfigRxChannelHopping() is required for the new RSSI offset to take effect.

DeprecatedRAIL 2.x synonym of sl_rail_set_rssi_offset().


RAIL_GetRssiOffset#

int8_t RAIL_GetRssiOffset (RAIL_Handle_t railHandle)

Get the radio or protocol RSSI offset in dB.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

Returns

  • The RSSI offset in dB corresponding to the railHandle.

Note

  • : A radio-generic handle, such as RAIL_EFR32_HANDLE, can be used to get the radio's RSSI offset otherwise this will return the RSSI offset value associated with the RAIL protocol instance handle, exclusive of any radio or PHY-specific RSSI offset correction, if any.

DeprecatedRAIL 2.x synonym of sl_rail_get_rssi_offset().


RAIL_SetRssiDetectThreshold#

RAIL_Status_t RAIL_SetRssiDetectThreshold (RAIL_Handle_t railHandle, int8_t rssiThresholdDbm)

Set the RSSI detection threshold in dBm to trigger RAIL_EVENT_DETECT_RSSI_THRESHOLD.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

int8_t[in]rssiThresholdDbm

desired RSSI threshold in dBm over which the event RAIL_EVENT_DETECT_RSSI_THRESHOLD is triggered.

Returns

When in receive, RSSI is sampled and if it exceeds the threshold, RAIL_EVENT_DETECT_RSSI_THRESHOLD is triggered.

Note

This function is only available on EFR32 Series 2 Sub-GHz parts EFR32xG23 and EFR32xG25.

DeprecatedRAIL 2.x synonym of sl_rail_set_rssi_detect_threshold().


RAIL_GetRssiDetectThreshold#

int8_t RAIL_GetRssiDetectThreshold (RAIL_Handle_t railHandle)

Get the RSSI detection threshold in dBm.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

a RAIL instance handle.

Returns

  • The RSSI threshold in dBm corresponding to the railHandle.

Note

This function is only available on EFR32 Series 2 Sub-GHz parts EFR32xG23 and EFR32xG25.

DeprecatedRAIL 2.x synonym of sl_rail_get_rssi_detect_threshold().


RAIL_GetRxIncomingPacketRssi#

int8_t RAIL_GetRxIncomingPacketRssi (RAIL_Handle_t railHandle)

Return the RSSI associated with the incoming packet.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

This function can only be called from callback context, e.g., when handling RAIL_EVENT_RX_FILTER_PASSED or RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND.

DeprecatedRAIL 2.x synonym of sl_rail_get_rx_incoming_packet_rssi().


RAIL_ConvertLqi#

RAIL_Status_t RAIL_ConvertLqi (RAIL_Handle_t railHandle, RAIL_ConvertLqiCallback_t cb)

Set up a callback function capable of converting a RX packet's LQI value before being consumed by application code.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_ConvertLqiCallback_t[in]cb

A callback of type RAIL_ConvertLqiCallback_t() that is called before the RX packet LQI value is loaded into the RAIL_RxPacketDetails_t structure for application consumption.

Returns

  • Status code indicating success of the function call.

DeprecatedRAIL 2.x synonym of sl_rail_convert_lqi().


sl_rail_config_rx_options#

sl_rail_status_t sl_rail_config_rx_options (sl_rail_handle_t rail_handle, sl_rail_rx_options_t rx_options_mask, sl_rail_rx_options_t rx_options)

Configure receive options.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_rx_options_t[in]rx_options_mask

A bitmask containing which options should be modified.

sl_rail_rx_options_t[in]rx_options

A bitmask containing desired configuration settings. Bit positions for each option are found in the sl_rail_rx_options_t.

Returns

  • Status code indicating success of the function call.

Configure the radio receive flow based on the list of available options. Only the options indicated by the mask parameter will be affected. Pass SL_RAIL_RX_OPTIONS_ALL to set all parameters. The previous settings may affect the current frame if a packet is received during this configuration.


sl_rail_include_frame_type_length#

sl_rail_status_t sl_rail_include_frame_type_length (sl_rail_handle_t rail_handle)

Include the code necessary for frame type based length decoding.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

Returns

  • Status code indicating success of the function call.

This function must be called before sl_rail_config_channels() to allow configurations using a frame type based length setup. It may be called before sl_rail_init() by using a radio-generic handle like SL_RAIL_EFR32_HANDLE.


sl_rail_start_rx#

sl_rail_status_t sl_rail_start_rx (sl_rail_handle_t rail_handle, uint16_t channel, const sl_rail_scheduler_info_t * p_scheduler_info)

Start the receiver on a specific channel.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint16_t[in]channel

The channel to listen on.

const sl_rail_scheduler_info_t *[in]p_scheduler_info

A pointer to information to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

This is a non-blocking function. Whenever a packet is received, sl_rail_config_t::events_callback() will fire with SL_RAIL_EVENT_RX_PACKET_RECEIVED set. If you call this while not idle but with a different channel, any ongoing receive or transmit operation will be aborted.

Returns an error if no receive FIFO or Packet Queue have been configured.


sl_rail_start_scheduled_rx#

sl_rail_status_t sl_rail_start_scheduled_rx (sl_rail_handle_t rail_handle, uint16_t channel, const sl_rail_scheduled_rx_config_t * p_scheduled_rx_config, const sl_rail_scheduler_info_t * p_scheduler_info)

Schedule a receive window for some future time.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint16_t[in]channel

A channel to listen on.

const sl_rail_scheduled_rx_config_t *[in]p_scheduled_rx_config

A pointer to a configuration structure to define the receive window.

const sl_rail_scheduler_info_t *[in]p_scheduler_info

A pointer to information to allow the radio scheduler to place this receive appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

This API immediately changes the channel and schedules receive to start at the specified time and end at the given end time. If you do not specify an end time, you may call this API later with an end time as long as you set the start time to disabled. You can also terminate the receive operation immediately using the sl_rail_idle() function. Note that relative end times are always relative to the start unless no start time is specified. If changing channels, the channel is changed immediately and will abort any ongoing packet transmission or reception.

Returns an error if a CSMA or LBT transmit is still in progress.

Returns an error if no receive FIFO or Packet Queue have been configured.

In multiprotocol, ensure that you properly yield the radio after this call. See Yielding the Radio for more details.

Note


sl_rail_enable_prs_lna_bypass#

sl_rail_status_t sl_rail_enable_prs_lna_bypass (sl_rail_handle_t rail_handle, bool enable, const sl_rail_prs_lna_bypass_config_t * p_prs_lna_bypass_config)

Enable automatic PRS LNA bypass for external FEM.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

bool[in]enable

Enable/Disable automatic PRS LNA bypass.

const sl_rail_prs_lna_bypass_config_t *[in]p_prs_lna_bypass_config

A pointer to an automatic PRS LNA bypass configuration structure. It must be non-NULL to enable the feature.

Returns

  • Status code indicating success of the function call.

If automatic PRS LNA bypass is enabled on chip that supports the feature (SL_RAIL_SUPPORTS_PRS_LNA_BYPASS), a level is generated on a PRS channel when the received power exceed a threshold. It is turned off after frame reception or after timeout if no frame has been detected and power is below the threshold.

Warnings


sl_rail_hold_rx_packet#

sl_rail_rx_packet_handle_t sl_rail_hold_rx_packet (sl_rail_handle_t rail_handle)

Place a temporary hold on this packet's data and metadata in the receive FIFO and receive Packet Queue.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

This function can only be called from within RAIL callback context. It can be used in any RX mode.

Normally, when RAIL issues its callback indicating a packet is ready or aborted, it expects the application's callback to retrieve and copy (or discard) the packet's information and data, and will free the packet data and metadata after the callback returns. This function tells RAIL to hold onto those resources in the receive FIFO and receive Packet Queue after the callback returns in case the application wants to defer processing the packet to a later time, e.g., outside of callback context.

Returns

Note

  • When using multiprotocol and either the receive FIFO or receive Packet Queue are shared with another protocol, both are reset during protocol switches losing any held packets. To avoid this, either give each protocol its own receive FIFO and receive Packet Queue, or make sure to invalidate any held packet handles or related sl_rail_rx_packet_info_t information when the SL_RAIL_EVENT_CONFIG_UNSCHEDULED occurs.


sl_rail_peek_rx_packet#

uint16_t sl_rail_peek_rx_packet (sl_rail_handle_t rail_handle, sl_rail_rx_packet_handle_t packet_handle, uint8_t * p_dest, uint16_t peek_bytes, uint16_t offset_bytes)

Copy 'len_bytes' of packet data starting from 'byte_offset' from the receive FIFO.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_rx_packet_handle_t[in]packet_handle

A packet handle as returned from a previous sl_rail_get_rx_packet_info() or sl_rail_hold_rx_packet() call, or sentinel values SL_RAIL_RX_PACKET_HANDLE_OLDEST, SL_RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE or SL_RAIL_RX_PACKET_HANDLE_NEWEST.

uint8_t *[out]p_dest

A pointer to the location where the received bytes will be copied. If NULL, no copying occurs.

uint16_t[in]peek_bytes

A number of packet data bytes to copy.

uint16_t[in]offset_bytes

A byte offset within remaining packet data from which to copy.

Those bytes remain valid for re-peeking.

Returns

  • Number of packet bytes copied.

Note

  • Peek does not permit peeking beyond the requested packet's available packet data (though there is a small chance it might for a SL_RAIL_RX_PACKET_HANDLE_NEWEST packet at the very end of still being received). Nor can one peek into already-consumed data read by sl_rail_read_rx_fifo(). len and offset are relative to the remaining data available in the packet, if any was already consumed by sl_rail_read_rx_fifo().


sl_rail_release_rx_packet#

sl_rail_status_t sl_rail_release_rx_packet (sl_rail_handle_t rail_handle, sl_rail_rx_packet_handle_t packet_handle)

Release RAIL's resources for a packet previously held in the receive FIFO and receive Packet Queue.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_rx_packet_handle_t[in]packet_handle

A packet handle as returned from a previous sl_rail_hold_rx_packet() call, or sentinel values SL_RAIL_RX_PACKET_HANDLE_OLDEST, SL_RAIL_RX_PACKET_HANDLE_OLDEST_COMPLETE or SL_RAIL_RX_PACKET_HANDLE_NEWEST. The latter might be used within RAIL callback context to explicitly release the packet associated with the callback early, before it's released automatically by RAIL on callback return (unless explicitly held).

This function must be called for any packet previously held via sl_rail_hold_rx_packet(). It may optionally be called within a callback context to release RAIL resources sooner than at callback completion time when not holding the packet. This function can be used in any RX mode.

Returns


sl_rail_get_rssi#

int16_t sl_rail_get_rssi (sl_rail_handle_t rail_handle, sl_rail_time_t wait_timeout_us)

Return the current raw RSSI in quarter-dBm within a definitive time period.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_time_t[in]wait_timeout_us

Sets the maximum time in microseconds to wait for a valid RSSI. If equal to SL_RAIL_GET_RSSI_NO_WAIT returns instant RSSI with no checks. If equal to SL_RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT waits for a valid RSSI with no maximum timeout.

Returns

  • SL_RAIL_RSSI_INVALID if the receiver is disabled and an RSSI value can't be obtained. Otherwise, return the RSSI in quarter dBm (dBm*4).

Gets the current RSSI value. This value represents the current energy of the channel. It can change rapidly, and will be low if no RF energy is in the current channel. The function from the value reported to dBm is an offset dependent on the PHY and the PCB layout. Characterize the RSSI received on your hardware and apply an offset in the application to account for board and PHY parameters. If a value of SL_RAIL_GET_RSSI_NO_WAIT is given for wait_timeout_us, the radio needs to be currently in RX and have been in there for a sufficient amount of time for a fresh RSSI value to be read and returned. Otherwise the RSSI is considered stale and SL_RAIL_RSSI_INVALID is returned instead. For non-zero values of wait_timeout_us, if the radio is transitioning to or already in RX, this function will wait a maximum time equal to wait_timeout_us (or indefinitely if wait_timeout_us is set to SL_RAIL_GET_RSSI_WAIT_WITHOUT_TIMEOUT) for a valid RSSI to be read and return it. Otherwise, if the wait_timeout_us is reached, or the radio is in or transitions to IDLE or TX, SL_RAIL_RSSI_INVALID will be returned. On low datarate PHYs, this function can take a significantly longer time when wait_timeout_us is non-zero.

In multiprotocol, this function returns SL_RAIL_RSSI_INVALID immediately if rail_handle is not the currently active sl_rail_handle_t. Additionally, wait_timeout_us should never be set to a value other than SL_RAIL_GET_RSSI_NO_WAIT in multiprotocol as the integration between this feature and the radio scheduler has not been implemented.

Note


sl_rail_start_average_rssi#

sl_rail_status_t sl_rail_start_average_rssi (sl_rail_handle_t rail_handle, uint16_t channel, sl_rail_time_t averaging_time_us, const sl_rail_scheduler_info_t * p_scheduler_info)

Start the RSSI averaging over a specified time in us.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint16_t[in]channel

The physical channel to set.

sl_rail_time_t[in]averaging_time_us

Averaging time in microseconds.

const sl_rail_scheduler_info_t *[in]p_scheduler_info

A pointer to information to allow the radio scheduler to place this operation appropriately. This is only used in multiprotocol version of RAIL and may be set to NULL in all other versions.

Returns

  • Status code indicating success of the function call.

Starts a non-blocking hardware-based RSSI averaging mechanism. Only a single instance of RSSI averaging can be run at any time and the radio must be idle to start.

In multiprotocol, this is a scheduled event. It will start when rail_handle becomes active. rail_handle needs to stay active until the averaging completes. If the averaging is interrupted, calls to sl_rail_get_average_rssi() will return SL_RAIL_RSSI_INVALID.

Also in multiprotocol, the user is required to call sl_rail_yield_radio() after this event completes (i.e., when SL_RAIL_EVENT_RSSI_AVERAGE_DONE occurs).

Note


sl_rail_is_average_rssi_ready#

bool sl_rail_is_average_rssi_ready (sl_rail_handle_t rail_handle)

Query whether the RSSI averaging is done.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • true if done and false otherwise.

This function can be used to poll for completion of the RSSI averaging to avoid relying on an interrupt-based callback.

Note

  • If the radio is idled while RSSI averaging is still in effect, this function may never return true.


sl_rail_get_average_rssi#

int16_t sl_rail_get_average_rssi (sl_rail_handle_t rail_handle)

Get the RSSI in quarter-dBm averaged over a specified time in microseconds.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • The RSSI in quarter-dBm (dBm * 4), or SL_RAIL_RSSI_INVALID if the receiver is disabled or an an RSSI value couldn't be obtained.

Gets the hardware RSSI average after issuing sl_rail_start_average_rssi(). Use after sl_rail_start_average_rssi().


sl_rail_set_rssi_offset#

sl_rail_status_t sl_rail_set_rssi_offset (sl_rail_handle_t rail_handle, int8_t rssi_offset_db)

Set an RSSI offset.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

a radio-generic or real RAIL instance handle.

int8_t[in]rssi_offset_db

desired dB offset to be added to the RSSI measurements.

Returns

Adds an offset to the RSSI in dBm. This offset affects all functionality that depends on RSSI values, such as CCA functions. Do not modify the offset dynamically during packet reception. This function can only be called while the radio is off, or in the case of multiprotocol, on an inactive protocol.

Note

  • : Prior to RAIL being initialized, a radio-wide protocol-independent offset can be established using a radio-generic handle like SL_RAIL_EFR32_HANDLE. The radio RSSI offset can range from -50 to +20 dB.
    After RAIL has been initialized a real RAIL protocol handle must be provided to set a protocol-specific RSSI offset, which is added to any radio offset (plus a per-PHY offset set by the radio calculator). The absolute value of the overall sum of all these offsets cannot exceed SL_RAIL_RSSI_OFFSET_MAX otherwise RSSIs could underflow or overflow.

  • : During RX Channel Hopping this API will not update the RSSI offset immediately if channel hopping has already been configured. A subsequent call to sl_rail_zwave_config_rx_channel_hopping() or sl_rail_config_rx_channel_hopping() is required for the new RSSI offset to take effect.


sl_rail_get_rssi_offset#

int8_t sl_rail_get_rssi_offset (sl_rail_handle_t rail_handle)

Get the radio or protocol RSSI offset in dB.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

Returns

  • The RSSI offset in dB corresponding to the rail_handle.

Note

  • : A radio-generic handle, such as SL_RAIL_EFR32_HANDLE, can be used to get the radio's RSSI offset otherwise this will return the RSSI offset value associated with the RAIL protocol instance handle, exclusive of any radio or PHY-specific RSSI offset correction, if any.


sl_rail_set_rssi_detect_threshold#

sl_rail_status_t sl_rail_set_rssi_detect_threshold (sl_rail_handle_t rail_handle, int8_t rssi_threshold_dbm)

Set the RSSI detection threshold in dBm to trigger SL_RAIL_EVENT_DETECT_RSSI_THRESHOLD.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

int8_t[in]rssi_threshold_dbm

desired RSSI threshold in dBm over which the event SL_RAIL_EVENT_DETECT_RSSI_THRESHOLD is triggered.

Returns

When in receive, RSSI is sampled and if it exceeds the threshold, SL_RAIL_EVENT_DETECT_RSSI_THRESHOLD is triggered.

Note

This function is only available on EFR32 Series 2 Sub-GHz parts EFR32xG23 and EFR32xG25.


sl_rail_get_rssi_detect_threshold#

int8_t sl_rail_get_rssi_detect_threshold (sl_rail_handle_t rail_handle)

Get the RSSI detection threshold in dBm.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • The RSSI threshold in dBm corresponding to the rail_handle.

Note

This function is only available on EFR32 Series 2 Sub-GHz parts EFR32xG23 and EFR32xG25.


sl_rail_get_rx_incoming_packet_rssi#

int8_t sl_rail_get_rx_incoming_packet_rssi (sl_rail_handle_t rail_handle)

Return the RSSI associated with the incoming packet.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

This function can only be called from callback context, e.g., when handling SL_RAIL_EVENT_RX_FILTER_PASSED or SL_RAIL_EVENT_IEEE802154_DATA_REQUEST_COMMAND.


sl_rail_convert_lqi#

sl_rail_status_t sl_rail_convert_lqi (sl_rail_handle_t rail_handle, sl_rail_convert_lqi_callback_t lqi_callback)

Set up a callback function capable of converting a RX packet's LQI value before being consumed by application code.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_convert_lqi_callback_t[in]lqi_callback

A callback of type sl_rail_convert_lqi_callback_t() that is called before the RX packet LQI value is loaded into the sl_rail_rx_packet_details_t structure for application consumption.

Returns

  • Status code indicating success of the function call.