RAIL configuration structure.
DeprecatedThis RAIL 2.x structure has been replaced in RAIL 3 by sl_rail_config_t.
Public Attributes#
A pointer to a function, which is called whenever a RAIL event occurs.
Provided for backwards compatibility.
Provided for backwards compatibility.
Provided for backwards compatibility.
Public Attribute Documentation#
eventsCallback#
void(* RAIL_Config_t::eventsCallback) (RAIL_Handle_t railHandle, RAIL_Events_t events)
A pointer to a function, which is called whenever a RAIL event occurs.
See the RAIL_Events_t documentation for the list of RAIL events.
DeprecatedRefer to sl_rail_config_t::events_callback().
protocol#
void* RAIL_Config_t::protocol
Provided for backwards compatibility.
Ignored.
DeprecatedRefer to sl_rail_config_t::p_opaque_handle_0.
scheduler#
RAILSched_Config_t* RAIL_Config_t::scheduler
Provided for backwards compatibility.
Ignored.
DeprecatedRefer to sl_rail_config_t::p_opaque_handle_1.
buffer#
RAIL_StateBuffer_t RAIL_Config_t::buffer
Provided for backwards compatibility.
Ignored.
DeprecatedRefer to sl_rail_config_t::opaque_value.