PTI Packet Trace#

Basic APIs to set up and interact with PTI settings.

These enumerations and structures are used with RAIL PTI API.

EFR32 supports SPI and UART PTI and is configurable in terms of baud rates and PTI pin locations.

Modules#

RAIL_PtiConfig_t

sl_rail_pti_config_t

Enumerations#

enum
RAIL_PTI_MODE_DISABLED = 0
RAIL_PTI_MODE_SPI = 1
RAIL_PTI_MODE_UART = 2
RAIL_PTI_MODE_UART_ONEWIRE = 3
}

A channel type enumeration.

enum
RAIL_PTI_PROTOCOL_CUSTOM = 0
RAIL_PTI_PROTOCOL_THREAD = 2
RAIL_PTI_PROTOCOL_BLE = 3
RAIL_PTI_PROTOCOL_CONNECT = 4
RAIL_PTI_PROTOCOL_ZIGBEE = 5
RAIL_PTI_PROTOCOL_ZWAVE = 6
RAIL_PTI_PROTOCOL_WISUN = 7
RAIL_PTI_PROTOCOL_802154 = 8
RAIL_PTI_PROTOCOL_SIDEWALK = 9
RAIL_PTI_PROTOCOL_BTC = 10
}

The protocol that RAIL outputs via the Packet Trace Interface (PTI).

enum
SL_RAIL_PTI_MODE_DISABLED = 0
SL_RAIL_PTI_MODE_SPI = 1
SL_RAIL_PTI_MODE_UART = 2
SL_RAIL_PTI_MODE_UART_ONEWIRE = 3
}

A channel type enumeration.

enum
SL_RAIL_PTI_PROTOCOL_CUSTOM = 0
SL_RAIL_PTI_PROTOCOL_THREAD = 2
SL_RAIL_PTI_PROTOCOL_BLE = 3
SL_RAIL_PTI_PROTOCOL_CONNECT = 4
SL_RAIL_PTI_PROTOCOL_ZIGBEE = 5
SL_RAIL_PTI_PROTOCOL_ZWAVE = 6
SL_RAIL_PTI_PROTOCOL_WI_SUN = 7
SL_RAIL_PTI_PROTOCOL_802154 = 8
SL_RAIL_PTI_PROTOCOL_SIDEWALK = 9
SL_RAIL_PTI_PROTOCOL_BTC = 10
}

The protocol that RAIL outputs via the Packet Trace Interface (PTI).

Functions#

RAIL_ConfigPti(RAIL_Handle_t railHandle, const RAIL_PtiConfig_t *ptiConfig)

Configure PTI pin locations, serial protocols, and baud rates.

RAIL_GetPtiConfig(RAIL_Handle_t railHandle, RAIL_PtiConfig_t *ptiConfig)

Get the currently-active PTI configuration.

RAIL_EnablePti(RAIL_Handle_t railHandle, bool enable)

Enable Packet Trace Interface (PTI) output of packet data.

RAIL_SetPtiProtocol(RAIL_Handle_t railHandle, RAIL_PtiProtocol_t protocol)

Set a protocol that RAIL outputs on PTI.

RAIL_GetPtiProtocol(RAIL_Handle_t railHandle)

Get the protocol that RAIL outputs on PTI.

sl_rail_config_pti(sl_rail_handle_t rail_handle, const sl_rail_pti_config_t *p_pti_config)

Configure PTI pin locations, serial protocols, and baud rates.

sl_rail_get_pti_config(sl_rail_handle_t rail_handle, sl_rail_pti_config_t *p_pti_config)

Get the currently-active PTI configuration.

sl_rail_enable_pti(sl_rail_handle_t rail_handle, bool enable)

Enable Packet Trace Interface (PTI) output of packet data.

sl_rail_set_pti_protocol(sl_rail_handle_t rail_handle, sl_rail_pti_protocol_t protocol)

Set a protocol that RAIL outputs on PTI.

sl_rail_get_pti_protocol(sl_rail_handle_t rail_handle)

Get the protocol that RAIL outputs on PTI.

Enumeration Documentation#

RAIL_PtiMode_t#

RAIL_PtiMode_t

A channel type enumeration.

DeprecatedRAIL 2.x synonym of sl_rail_pti_mode_t.

Enumerator
RAIL_PTI_MODE_DISABLED

Turn PTI off entirely.

RAIL_PTI_MODE_SPI

8-bit SPI mode.

RAIL_PTI_MODE_UART

8-bit UART mode.

RAIL_PTI_MODE_UART_ONEWIRE

9-bit UART mode.


RAIL_PtiProtocol_t#

RAIL_PtiProtocol_t

The protocol that RAIL outputs via the Packet Trace Interface (PTI).

DeprecatedRAIL 2.x synonym of sl_rail_pti_protocol_t.

Enumerator
RAIL_PTI_PROTOCOL_CUSTOM

PTI output for a custom protocol.

RAIL_PTI_PROTOCOL_THREAD

PTI output for the Thread protocol.

RAIL_PTI_PROTOCOL_BLE

PTI output for the Bluetooth Smart protocol.

RAIL_PTI_PROTOCOL_CONNECT

PTI output for the Connect protocol.

RAIL_PTI_PROTOCOL_ZIGBEE

PTI output for the Zigbee protocol.

RAIL_PTI_PROTOCOL_ZWAVE

PTI output for the Z-Wave protocol.

RAIL_PTI_PROTOCOL_WISUN

PTI output for the Wi-SUN protocol.

RAIL_PTI_PROTOCOL_802154

PTI output for a custom protocol using a built-in 802.15.4 radio config.

RAIL_PTI_PROTOCOL_SIDEWALK

PTI output for Sidewalk protocol.

RAIL_PTI_PROTOCOL_BTC

PTI output for the Bluetooth Classic protocol.


sl_rail_pti_mode_t#

sl_rail_pti_mode_t

A channel type enumeration.

Enumerator
SL_RAIL_PTI_MODE_DISABLED

Turn PTI off entirely.

SL_RAIL_PTI_MODE_SPI

8-bit SPI mode.

SL_RAIL_PTI_MODE_UART

8-bit UART mode.

SL_RAIL_PTI_MODE_UART_ONEWIRE

9-bit UART mode.


sl_rail_pti_protocol_t#

sl_rail_pti_protocol_t

The protocol that RAIL outputs via the Packet Trace Interface (PTI).

Enumerator
SL_RAIL_PTI_PROTOCOL_CUSTOM

PTI output for a custom protocol.

SL_RAIL_PTI_PROTOCOL_THREAD

PTI output for the Thread protocol.

SL_RAIL_PTI_PROTOCOL_BLE

PTI output for the Bluetooth Smart protocol.

SL_RAIL_PTI_PROTOCOL_CONNECT

PTI output for the Connect protocol.

SL_RAIL_PTI_PROTOCOL_ZIGBEE

PTI output for the Zigbee protocol.

SL_RAIL_PTI_PROTOCOL_ZWAVE

PTI output for the Z-Wave protocol.

SL_RAIL_PTI_PROTOCOL_WI_SUN

PTI output for the Wi-SUN protocol.

SL_RAIL_PTI_PROTOCOL_802154

PTI output for a custom protocol using a built-in 802.15.4 radio config.

SL_RAIL_PTI_PROTOCOL_SIDEWALK

PTI output for Sidewalk protocol.

SL_RAIL_PTI_PROTOCOL_BTC

PTI output for the Bluetooth Classic protocol.


Function Documentation#

RAIL_ConfigPti#

RAIL_Status_t RAIL_ConfigPti (RAIL_Handle_t railHandle, const RAIL_PtiConfig_t * ptiConfig)

Configure PTI pin locations, serial protocols, and baud rates.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

const RAIL_PtiConfig_t *[in]ptiConfig

A non-NULL pointer to the PTI configuration structure to use.

Returns

  • Status code indicating success of the function call.

When this function is called prior to the first RAIL_Init() call, the PTI configuration is recorded but activation is deferred to RAIL_Init(). When called subsequent to RAIL_Init(), the radio should be off (idle) and the PTI configuration is recorded and put into effect immediately unless RAIL_EnablePti() had been called just prior to disable PTI, in which case activation is deferred to when RAIL_EnablePti() is subsequently called to enable PTI.

Only one PTI configuration that can be active on a radio, regardless of the number of protocols (unless the application updates the configuration upon a protocol switch – RAIL does not save the configuration in a protocol RAIL instance).

Note

  • On EFR32 platforms GPIO configuration must be unlocked (see GPIO->LOCK register) to configure or use PTI.

Warnings

  • As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.

DeprecatedRAIL 2.x synonym of sl_rail_config_pti().


RAIL_GetPtiConfig#

RAIL_Status_t RAIL_GetPtiConfig (RAIL_Handle_t railHandle, RAIL_PtiConfig_t * ptiConfig)

Get the currently-active PTI configuration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

RAIL_PtiConfig_t *[out]ptiConfig

A non-NULL pointer to the configuration structure to be filled in with the active PTI configuration.

Returns

  • RAIL status indicating success of the function call.

Although most combinations of configurations can be set, it is safest to call this method after configuration to confirm which values were actually set. This function always returns the active PTI configuration on the radio regardless of the active protocol.

DeprecatedRAIL 2.x synonym of sl_rail_get_pti_config().


RAIL_EnablePti#

RAIL_Status_t RAIL_EnablePti (RAIL_Handle_t railHandle, bool enable)

Enable Packet Trace Interface (PTI) output of packet data.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A radio-generic or real RAIL instance handle.

bool[in]enable

PTI is enabled if true; disabled if false.

Returns

  • Status code indicating success of the function call.

Similarly to having only one PTI configuration per radio, PTI can only be enabled or disabled for all protocols. It cannot be individually set to enabled and disabled per protocol (unless the application switches it when the protocol switches – RAIL does not save this state in a protocol RAIL instance).

PTI should be enabled or disabled only when the radio is off (idle).

Note

Warnings

  • On EFR32 platforms GPIO configuration must be unlocked (see GPIO->LOCK register) to configure or use PTI, otherwise a fault or assert might occur. If GPIO configuration locking is desired, PTI must be disabled beforehand either with this function or with RAIL_ConfigPti() using RAIL_PTI_MODE_DISABLED.

  • As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return RAIL_STATUS_INVALID_CALL.

DeprecatedRAIL 2.x synonym of sl_rail_enable_pti().


RAIL_SetPtiProtocol#

RAIL_Status_t RAIL_SetPtiProtocol (RAIL_Handle_t railHandle, RAIL_PtiProtocol_t protocol)

Set a protocol that RAIL outputs on PTI.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

RAIL_PtiProtocol_t[in]protocol

The enumeration representing which protocol the app is using.

Returns

  • Status code indicating success of the function call.

The protocol is output via PTI for each packet. Before any protocol is set, the default value is RAIL_PTI_PROTOCOL_CUSTOM. Use one of the enumeration values so that the Network Analyzer can decode the packet.

Note

  • This function cannot be called unless the radio is currently in the RAIL_RF_STATE_IDLE or RAIL_RF_STATE_INACTIVE states. For this reason, call this function early on before starting radio operations and not changed later.

DeprecatedRAIL 2.x synonym of sl_rail_set_pti_protocol().


RAIL_GetPtiProtocol#

RAIL_PtiProtocol_t RAIL_GetPtiProtocol (RAIL_Handle_t railHandle)

Get the protocol that RAIL outputs on PTI.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • PTI protocol in use.

DeprecatedRAIL 2.x synonym of sl_rail_get_pti_protocol().


sl_rail_config_pti#

sl_rail_status_t sl_rail_config_pti (sl_rail_handle_t rail_handle, const sl_rail_pti_config_t * p_pti_config)

Configure PTI pin locations, serial protocols, and baud rates.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

const sl_rail_pti_config_t *[in]p_pti_config

A non-NULL pointer to the PTI configuration structure to use.

Returns

  • Status code indicating success of the function call.

When this function is called prior to the first sl_rail_init() call, the PTI configuration is recorded but activation is deferred to sl_rail_init(). When called subsequent to sl_rail_init(), the radio should be off (idle) and the PTI configuration is recorded and put into effect immediately unless sl_rail_enable_pti() had been called just prior to disable PTI, in which case activation is deferred to when sl_rail_enable_pti() is subsequently called to enable PTI.

Only one PTI configuration can be active on a radio, regardless of the number of protocols (unless the application updates the configuration upon a protocol switch – RAIL does not save the configuration in a protocol RAIL instance).

Note

  • On EFR32 platforms GPIO configuration must be unlocked (see GPIO->LOCK register) to configure or use PTI.

Warnings

  • As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return SL_RAIL_STATUS_INVALID_CALL.


sl_rail_get_pti_config#

sl_rail_status_t sl_rail_get_pti_config (sl_rail_handle_t rail_handle, sl_rail_pti_config_t * p_pti_config)

Get the currently-active PTI configuration.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

sl_rail_pti_config_t *[out]p_pti_config

A non-NULL pointer to the configuration structure to be filled in with the active PTI configuration on the radio.

Returns

  • Status code indicating success of the function call.

Although most combinations of configurations can be set, it is safest to call this method after configuration to confirm which values were actually set. This function always returns the active PTI configuration on the radio regardless of the active protocol.


sl_rail_enable_pti#

sl_rail_status_t sl_rail_enable_pti (sl_rail_handle_t rail_handle, bool enable)

Enable Packet Trace Interface (PTI) output of packet data.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A radio-generic or real RAIL instance handle.

bool[in]enable

PTI is enabled if true; disabled if false.

Returns

  • Status code indicating success of the function call.

Similarly to having only one PTI configuration per radio, PTI can only be enabled or disabled for all protocols. It cannot be individually set to enabled and disabled per protocol (unless the application switches it when the protocol switches – RAIL does not save this state in a protocol RAIL instance).

PTI should be enabled or disabled only when the radio is off (idle).

Note

Warnings

  • On EFR32 platforms GPIO configuration must be unlocked (see GPIO->LOCK register) to configure or use PTI, otherwise a fault or assert might occur. If GPIO configuration locking is desired, PTI must be disabled beforehand either with this function or with sl_rail_config_pti() using SL_RAIL_PTI_MODE_DISABLED.

  • As this function relies on GPIO access and RAIL is meant to run in TrustZone non-secure world, it is not supported if GPIO is configured as secure peripheral and it will return SL_RAIL_STATUS_INVALID_CALL.


sl_rail_set_pti_protocol#

sl_rail_status_t sl_rail_set_pti_protocol (sl_rail_handle_t rail_handle, sl_rail_pti_protocol_t protocol)

Set a protocol that RAIL outputs on PTI.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

sl_rail_pti_protocol_t[in]protocol

The enumeration representing which protocol the app is using.

Returns

  • Status code indicating success of the function call.

The protocol is output via PTI for each packet. Before any protocol is set, the default value is SL_RAIL_PTI_PROTOCOL_CUSTOM. Use one of the enumeration values so that the Network Analyzer can decode the packet.

Note


sl_rail_get_pti_protocol#

sl_rail_pti_protocol_t sl_rail_get_pti_protocol (sl_rail_handle_t rail_handle)

Get the protocol that RAIL outputs on PTI.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • PTI protocol in use.