Address Filtering#

Configuration APIs for receive packet address filtering.

The address filtering code examines the packet as follows.

Bytes: 0 - 255

0 - 8

0 - 255

0 - 8

Variable

Data_0

Field_0

Data_1

Field_1

Data_2

In the above structure, anything listed as Data_# is an optional section of bytes that RAIL will not process for address filtering. The Field_# segments reference specific sections in the packet that will each be interpreted as an address during address filtering. The application may submit up to four addresses to attempt to match each field segment and each address may have a size of up to 8 bytes. To set up address filtering, first configure the locations and length of the addresses in the packet. Next, configure which combinations of matches in Field_0 and Field_1 should constitute an address match. Last, enter addresses into tables for each field and enable them. The first two of these are part of the RAIL_AddrConfig_t structure while the second part is configured at runtime using the RAIL_SetAddressFilterAddress() API. A brief description of each configuration is listed below.

The offsets and sizes of the fields are assumed fixed for the RAIL address filter. To set them, specify arrays for these values in the sizes and offsets entries in the RAIL_AddrConfig_t structure. A size of zero indicates that a field is disabled. The start offset for a field is relative to the previous start offset and, if you're using frame type decoding, the first start offset is relative to the end of the byte containing the frame type.

Configuring which combinations of Field_0 and Field_1 constitute a match is the most complex portion of the address filter. The easiest way to think about this is with a truth table. If you consider each of the four possible address entries in a field, you can have a match on any one of those or a match for none of them. This is shown in the 5x5 truth table below where Field_0 matches are the rows and Field_1 matches are the columns.

No Match

Address 0

Address 1

Address 2

Address 3

No Match

bit 0

bit 1

bit 2

bit 3

bit 4

Address 0

bit 5

bit 6

bit 7

bit 8

bit 9

Address 1

bit 10

bit 11

bit 12

bit 13

bit 14

Address 2

bit 15

bit 16

bit 17

bit 18

bit 19

Address 3

bit 20

bit 21

bit 22

bit 23

bit 24

Because this is only 25 bits, it can be represented in one 32-bit integer where 1 indicates a filter pass and 0 indicates a filter fail. This is the RAIL_AddrConfig_t::matchTable field and is used during filtering. For common simple configurations, two defines are provided with the truth tables as shown below. The first is ADDRCONFIG_MATCH_TABLE_SINGLE_FIELD, which can be used if only using one address field (either field). If using two fields and want to force in the same address entry in each field, use the second define: ADDRCONFIG_MATCH_TABLE_DOUBLE_FIELD. For more complex systems, create a valid custom table.

Note

  • Address filtering does not function reliably with PHYs that use a data rate greater than 500 kbps. If this is a requirement, filtering must currently be done by the application.

The address filtering code examines the packet as follows.

Bytes: 0 - 255

0 - 8

0 - 255

0 - 8

Variable

Data_0

Field_0

Data_1

Field_1

Data_2

In the above structure, anything listed as Data_# is an optional section of bytes that RAIL will not process for address filtering. The Field_# segments reference specific sections in the packet that will each be interpreted as an address during address filtering. The application may submit up to four addresses to attempt to match each field segment and each address may have a size of up to 8 bytes. To set up address filtering, first configure the locations and length of the addresses in the packet. Next, configure which combinations of matches in Field_0 and Field_1 should constitute an address match. Last, enter addresses into tables for each field and enable them. The first two of these are part of the sl_rail_addr_config_t structure while the second part is configured at runtime using the sl_rail_set_address_filter_address() API. A brief description of each configuration is listed below.

The offsets and sizes of the fields are assumed fixed for the RAIL address filter. To set them, specify arrays for these values in the sizes and offsets entries in the sl_rail_addr_config_t structure. A size of zero indicates that a field is disabled. The start offset for a field is relative to the previous start offset and, if you're using frame type decoding, the first start offset is relative to the end of the byte containing the frame type.

Configuring which combinations of Field_0 and Field_1 constitute a match is the most complex portion of the address filter. The easiest way to think about this is with a truth table. If you consider each of the four possible address entries in a field, you can have a match on any one of those or a match for none of them. This is shown in the 5x5 truth table below where Field_0 matches are the rows and Field_1 matches are the columns.

No Match

Address 0

Address 1

Address 2

Address 3

No Match

bit 0

bit 1

bit 2

bit 3

bit 4

Address 0

bit 5

bit 6

bit 7

bit 8

bit 9

Address 1

bit 10

bit 11

bit 12

bit 13

bit 14

Address 2

bit 15

bit 16

bit 17

bit 18

bit 19

Address 3

bit 20

bit 21

bit 22

bit 23

bit 24

Because this is only 25 bits, it can be represented in one 32-bit integer where 1 indicates a filter pass and 0 indicates a filter fail. This is the sl_rail_addr_config_t::match_table field and is used during filtering. For common simple configurations, two defines are provided with the truth tables as shown below. The first is SL_RAIL_ADDR_CONFIG_MATCH_TABLE_SINGLE_FIELD, which can be used if only using one address field (either field). If using two fields and want to force in the same address entry in each field, use the second define: SL_RAIL_ADDR_CONFIG_MATCH_TABLE_DOUBLE_FIELD. For more complex systems, create a valid custom table.

Note

  • Address filtering does not function reliably with PHYs that use a data rate greater than 500 kbps. If this is a requirement, filtering must currently be done by the application.

Modules#

RAIL_AddrConfig_t

sl_rail_addr_config_t

Typedefs#

typedef uint8_t

A bitmask representation of which 4 filters passed for each ADDRCONFIG_MAX_ADDRESS_FIELDS when filtering has completed successfully.

typedef uint8_t

A bitmask representation of which 4 filters passed for each SL_RAIL_ADDR_CONFIG_MAX_ADDRESS_FIELDS when filtering has completed successfully.

Functions#

RAIL_ConfigAddressFilter(RAIL_Handle_t railHandle, const RAIL_AddrConfig_t *addrConfig)

Configure address filtering.

bool
RAIL_EnableAddressFilter(RAIL_Handle_t railHandle, bool enable)

Enable address filtering.

bool
RAIL_IsAddressFilterEnabled(RAIL_Handle_t railHandle)

Return whether address filtering is currently enabled.

RAIL_ResetAddressFilter(RAIL_Handle_t railHandle)

Reset the address filtering configuration.

RAIL_SetAddressFilterAddress(RAIL_Handle_t railHandle, uint8_t field, uint8_t index, const uint8_t *value, bool enable)

Set an address for filtering in hardware.

RAIL_SetAddressFilterAddressMask(RAIL_Handle_t railHandle, uint8_t field, const uint8_t *bitMask)

Set an address bit mask for filtering in hardware.

RAIL_EnableAddressFilterAddress(RAIL_Handle_t railHandle, bool enable, uint8_t field, uint8_t index)

Enable address filtering for the specified address.

sl_rail_config_address_filter(sl_rail_handle_t rail_handle, const sl_rail_addr_config_t *p_addr_config)

Configure address filtering.

bool
sl_rail_enable_address_filter(sl_rail_handle_t rail_handle, bool enable)

Enable address filtering.

bool
sl_rail_is_address_filter_enabled(sl_rail_handle_t rail_handle)

Return whether address filtering is currently enabled.

sl_rail_reset_address_filter(sl_rail_handle_t rail_handle)

Reset the address filtering configuration.

sl_rail_set_address_filter_address(sl_rail_handle_t rail_handle, uint8_t field, uint8_t index, const uint8_t *p_value, bool enable)

Set an address for filtering in hardware.

sl_rail_set_address_filter_address_mask(sl_rail_handle_t rail_handle, uint8_t field, const uint8_t *p_bitmask)

Set an address bit mask for filtering in hardware.

sl_rail_enable_address_filter_address(sl_rail_handle_t rail_handle, bool enable, uint8_t field, uint8_t index)

Enable address filtering for the specified address.

Macros#

#define
ADDRCONFIG_MATCH_TABLE_SINGLE_FIELD (0x1FFFFFE)

A default address filtering match table for configurations that use only one address field.

#define
ADDRCONFIG_MATCH_TABLE_DOUBLE_FIELD (0x1041040)

A default address filtering match table for configurations that use two address fields and want to match the same index in each.

#define
ADDRCONFIG_MAX_ADDRESS_FIELDS (2)

The maximum number of address fields that can be used by the address filtering logic.

#define
SL_RAIL_ADDR_CONFIG_MATCH_TABLE_SINGLE_FIELD (0x1FFFFFE)

A default address filtering match table for configurations that use only one address field.

#define
SL_RAIL_ADDR_CONFIG_MATCH_TABLE_DOUBLE_FIELD (0x1041040)

A default address filtering match table for configurations that use two address fields and want to match the same index in each.

#define
SL_RAIL_ADDR_CONFIG_MAX_ADDRESS_FIELDS (2)

The maximum number of address fields that can be used by the address filtering logic.

Typedef Documentation#

RAIL_AddrFilterMask_t#

typedef uint8_t RAIL_AddrFilterMask_t

A bitmask representation of which 4 filters passed for each ADDRCONFIG_MAX_ADDRESS_FIELDS when filtering has completed successfully.

It's layout is: | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |-----—+-----—+-----—+-----—+-----—+-----—+-----—+-----—| | Second Address Field Nibble | First Address Field Nibble | | Addr 3 | Addr 2 | Addr 1 | Addr 0 | Addr 3 | Addr 2 | Addr 1 | Addr 0 | | match | match | match | match | match | match | match | match | |-----—+-----—+-----—+-----—+-----—+-----—+-----—+-----—|

Note

DeprecatedRAIL 2.x synonym of sl_rail_addr_filter_mask_t.


sl_rail_addr_filter_mask_t#

typedef uint8_t sl_rail_addr_filter_mask_t

A bitmask representation of which 4 filters passed for each SL_RAIL_ADDR_CONFIG_MAX_ADDRESS_FIELDS when filtering has completed successfully.

It's layout is: | Bit 7 | Bit 6 | Bit 5 | Bit 4 | Bit 3 | Bit 2 | Bit 1 | Bit 0 | |-----—+-----—+-----—+-----—+-----—+-----—+-----—+-----—| | Second Address Field Nibble | First Address Field Nibble | | Addr 3 | Addr 2 | Addr 1 | Addr 0 | Addr 3 | Addr 2 | Addr 1 | Addr 0 | | match | match | match | match | match | match | match | match | |-----—+-----—+-----—+-----—+-----—+-----—+-----—+-----—|

Note


Function Documentation#

RAIL_ConfigAddressFilter#

RAIL_Status_t RAIL_ConfigAddressFilter (RAIL_Handle_t railHandle, const RAIL_AddrConfig_t * addrConfig)

Configure address filtering.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

const RAIL_AddrConfig_t *[in]addrConfig

A pointer to the configuration structure, which defines how addresses are set up in your packets. May be NULL to reset address filtering.

Returns

  • Status code indicating success of the function call.

You must call this function to set up address filtering. You may call it multiple times but all previous information is wiped out each time you call and any configured addresses must be reset.

DeprecatedRAIL 2.x synonym of sl_rail_config_address_filter().


RAIL_EnableAddressFilter#

bool RAIL_EnableAddressFilter (RAIL_Handle_t railHandle, bool enable)

Enable address filtering.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]enable

An argument to indicate whether or not to enable address filtering.

Returns

  • true if address filtering was enabled to start with and false otherwise.

Only allow packets through that pass the current address filtering configuration. This does not reset or change the configuration so you can set that up before turning on this feature.

DeprecatedRAIL 2.x synonym of sl_rail_enable_address_filter().


RAIL_IsAddressFilterEnabled#

bool RAIL_IsAddressFilterEnabled (RAIL_Handle_t railHandle)

Return whether address filtering is currently enabled.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • true if address filtering is enabled and false otherwise.

DeprecatedRAIL 2.x synonym of sl_rail_is_address_filter_enabled().


RAIL_ResetAddressFilter#

RAIL_Status_t RAIL_ResetAddressFilter (RAIL_Handle_t railHandle)

Reset the address filtering configuration.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

Returns

  • Status code indicating success of the function call.

Resets all structures related to address filtering. This does not disable address filtering. It leaves the radio in a state where no packets pass filtering.

DeprecatedRAIL 2.x synonym of sl_rail_reset_address_filter().


RAIL_SetAddressFilterAddress#

RAIL_Status_t RAIL_SetAddressFilterAddress (RAIL_Handle_t railHandle, uint8_t field, uint8_t index, const uint8_t * value, bool enable)

Set an address for filtering in hardware.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t[in]field

Indicates an address field for this address.

uint8_t[in]index

Indicates a match entry for this address for a given field.

const uint8_t *[in]value

A pointer to the address data. This must be at least as long as the size specified in RAIL_ConfigAddressFilter(). The first byte, value[0], will be compared to the first byte received over the air for this address field.

bool[in]enable

A boolean to indicate whether this address should be enabled immediately.

Returns

  • Status code indicating success of the function call.

This function loads the given address into hardware for filtering and starts filtering if you set the enable parameter to true. Otherwise, call RAIL_EnableAddressFilterAddress() to turn it on later.

DeprecatedRAIL 2.x synonym of sl_rail_set_address_filter_address().


RAIL_SetAddressFilterAddressMask#

RAIL_Status_t RAIL_SetAddressFilterAddressMask (RAIL_Handle_t railHandle, uint8_t field, const uint8_t * bitMask)

Set an address bit mask for filtering in hardware.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

uint8_t[in]field

Indicates an address field for this address bit mask.

const uint8_t *[in]bitMask

A pointer to the address bitmask. This must be at least as long as the size specified in RAIL_ConfigAddressFilter(). The first byte, bitMask[0], will be applied to the first byte received over the air for this address field. Bits set to 1 in the bit mask indicate which bit positions in the incoming packet to compare against the stored addresses during address filtering. Bits set to 0 indicate which bit positions to ignore in the incoming packet during address filtering. This bit mask is applied to all address entries.

Returns

  • Status code indicating success of the function call.

This function loads the given address bit mask into hardware for use when address filtering is enabled. All bits in the stored address bit mask are set to 1 during hardware initialization and when either RAIL_ConfigAddressFilter() or RAIL_ResetAddressFilter() are called.

Note

DeprecatedRAIL 2.x synonym of sl_rail_set_address_filter_address_mask().


RAIL_EnableAddressFilterAddress#

RAIL_Status_t RAIL_EnableAddressFilterAddress (RAIL_Handle_t railHandle, bool enable, uint8_t field, uint8_t index)

Enable address filtering for the specified address.

Parameters
TypeDirectionArgument NameDescription
RAIL_Handle_t[in]railHandle

A RAIL instance handle.

bool[in]enable

An argument to indicate whether or not to enable address filtering.

uint8_t[in]field

Indicates an address for the address.

uint8_t[in]index

Indicates a match entry in the given field you want to enable.

Returns

  • Status code indicating success of the function call.

DeprecatedRAIL 2.x synonym of sl_rail_enable_address_filter_address().


sl_rail_config_address_filter#

sl_rail_status_t sl_rail_config_address_filter (sl_rail_handle_t rail_handle, const sl_rail_addr_config_t * p_addr_config)

Configure address filtering.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

const sl_rail_addr_config_t *[in]p_addr_config

A pointer to the configuration structure, which defines how addresses are set up in your packets. May be NULL to reset address filtering.

Returns

  • Status code indicating success of the function call.

You must call this function to set up address filtering. You may call it multiple times but all previous information is wiped out each time you call and any configured addresses must be reset.


sl_rail_enable_address_filter#

bool sl_rail_enable_address_filter (sl_rail_handle_t rail_handle, bool enable)

Enable address filtering.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

bool[in]enable

An argument to indicate whether or not to enable address filtering.

Returns

  • true if address filtering was enabled to start with and false otherwise.

Only allow packets through that pass the current address filtering configuration. This does not reset or change the configuration so you can set that up before turning on this feature.


sl_rail_is_address_filter_enabled#

bool sl_rail_is_address_filter_enabled (sl_rail_handle_t rail_handle)

Return whether address filtering is currently enabled.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • true if address filtering is enabled and false otherwise.


sl_rail_reset_address_filter#

sl_rail_status_t sl_rail_reset_address_filter (sl_rail_handle_t rail_handle)

Reset the address filtering configuration.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

Returns

  • Status code indicating success of the function call.

Resets all structures related to address filtering. This does not disable address filtering. It leaves the radio in a state where no packets pass filtering.


sl_rail_set_address_filter_address#

sl_rail_status_t sl_rail_set_address_filter_address (sl_rail_handle_t rail_handle, uint8_t field, uint8_t index, const uint8_t * p_value, bool enable)

Set an address for filtering in hardware.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint8_t[in]field

Indicates an address field for this address.

uint8_t[in]index

Indicates a match entry for this address for a given field.

const uint8_t *[in]p_value

A pointer to the address data. This must be at least as long as the size specified in sl_rail_config_address_filter(). The first byte, p_value[0], will be compared to the first byte received over the air for this address field.

bool[in]enable

A boolean to indicate whether this address should be enabled immediately.

Returns

  • Status code indicating success of the function call.

This function loads the given address into hardware for filtering and starts filtering if you set the enable parameter to true. Otherwise, call sl_rail_enable_address_filter_address() to turn it on later.


sl_rail_set_address_filter_address_mask#

sl_rail_status_t sl_rail_set_address_filter_address_mask (sl_rail_handle_t rail_handle, uint8_t field, const uint8_t * p_bitmask)

Set an address bit mask for filtering in hardware.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

uint8_t[in]field

Indicates an address field for this address bit mask.

const uint8_t *[in]p_bitmask

A pointer to the address bitmask. This must be at least as long as the size specified in sl_rail_config_address_filter(). The first byte, p_bitmask[0], will be applied to the first byte received over the air for this address field. Bits set to 1 in the bit mask indicate which bit positions in the incoming packet to compare against the stored addresses during address filtering. Bits set to 0 indicate which bit positions to ignore in the incoming packet during address filtering. This bit mask is applied to all address entries.

Returns

  • Status code indicating success of the function call.

This function loads the given address bit mask into hardware for use when address filtering is enabled. All bits in the stored address bit mask are set to 1 during hardware initialization and when either sl_rail_config_address_filter() or sl_rail_reset_address_filter() are called.

Note


sl_rail_enable_address_filter_address#

sl_rail_status_t sl_rail_enable_address_filter_address (sl_rail_handle_t rail_handle, bool enable, uint8_t field, uint8_t index)

Enable address filtering for the specified address.

Parameters
TypeDirectionArgument NameDescription
sl_rail_handle_t[in]rail_handle

A real RAIL instance handle.

bool[in]enable

An argument to indicate whether or not to enable address filtering.

uint8_t[in]field

Indicates an address for the address.

uint8_t[in]index

Indicates a match entry in the given field you want to enable.

Returns

  • Status code indicating success of the function call.