Snippet Examples#
Snippet examples are small projects that demonstrate one particular RS9116 feature or API. The snippet examples are found in the WiSeConnectâ„¢ SDK at the path: <SDK>/examples/snippets and are categorized by the feature that they demonstrate.
Details on the configuration and operation of each snippet example are available in the readme.md file that is found with the example source code and at the following links:
Bluetooth Examples#
bt-power-save
bt-spp-dual-role-with-secure-pairing
BLE Examples#
ble-multiconnection-gatt-test
ble-central
ble-secureconnection
ble-testmodes
ble-datalength
ble-unified-ae-coex-app
ble-throughput-app
ble-power-save
ble-hid-on-gatt
ble-longrange-2mbps
ble-gatt-long-read
ble-privacy
ble-heart-rate-profile
ble-ae-peripheral
ble-accept-list
ble-dual-role
ble-ibeacon
ble-ae-central
Wi-Fi + BLE Examples#
wlan-station-ble-provisioning-select
wlan-station-ble-provisioning
wlan-station-ble-bridge
wlan-station-ble-provisioning-AWS
Wi-Fi Examples#
wlan-tls-client
wlan-http-client-v6
wlan-access-point-v6
wlan-socket-select-app-udp
wlan-sntp-client-v6
wlan-ftp-client
wlan-station-ping
wlan-station-ping-v6
wlan-access-point
wlan-throughput-dual-ip-v4-v6
wlan-socket-select-app
wlan-calibration-app
wlan-mqtt-client-v6
wlan-concurrent-mode
wlan-mqtt-client
wlan-tcp-logging-stats
wlan-embedded-mqtt
wlan-enterprise-client
wlan-http-otaf
wlan-throughput-v6
wlan-concurrent-mode-dual-ip
wlan-power-save-deep-sleep
wlan-device-shadow-logging-stats
wlan-aws-iot-mqtt
wlan-azure-iot
wlan-three-ssl-concurrent-client-sockets
Debug Utility Examples#
Wi-Fi + Dual Mode Bluetooth Examples#
wlan-throughput-bt-spp-ble-dual-role
wlan-https-bt-spp-ble-dual-role