BLE Throughput App#
1. Purpose / Scope#
This application demonstrates how to exchange continuous data to the remote device to measure the On-Air Throughput using a BLE Sniffer.
- In this Application, the GATT server configures with Custom service with write, read, and notification characteristic UUIDs. 
- When connected remote device enables the notification on UUID, Silicon Labs device sends the continuous notifications to the connected device. 
- This is data can be captured with Sniffer to measure the throughputs. 
Sequence of Events
This Application explains to the user how to:
- Create a Simple chat service 
- Make the device advertise / scannable 
- Connect from remote BLE device/ Connect to remote BLE device 
- Initiate the Security 
- Excite the Data length and Phy rate features 
- Sends the notification messages to the connected peer/Smartphone when the notification is enabled 
2. Prerequisites / Setup Requirements#
Before running the application, the user will need the following things to setup.
2.1 Hardware Requirements#
- Windows PC with Host interface(UART/ SPI/ SDIO). - SiWx91x Wi-Fi Evaluation Kit. The SiWx91x supports multiple operating modes. See Operating Modes for details. 
- SoC Mode: - Silicon Labs BRD4325A 
 
- NCP Mode: - Silicon Labs (BRD4180A, BRD4280B); 
- Host MCU Eval Kit. This example has been tested with: - Silicon Labs WSTK + EFR32MG21 
- Silicon Labs WSTK + EFM32GG11 
 
 
 
- BLE peripheral device in case of Silicon Labs module as master. 
- BLE central device in case of Silicon Labs module as slave. 
2.2 Software Requirements#
- Embedded Development Environment - For Silicon Labs EFx32, use the latest version of Simplicity Studio 
 
- Download and install the Silicon Labs EFR Connect App in the android smart phones for testing BLE applications. Users can also use their choice of BLE apps available in Android/iOS smart phones. 
2.3 Setup Diagram:#
   
SoC Mode :


NCP Mode :

3. Application Build Environment#
3.1 Project Setup#
- SoC Mode - Silicon Labs SiWx91x SoC. Follow the Getting Started with SiWx91x SoC to setup the example to work with SiWx91x SoC and Simplicity Studio. 
 
- NCP Mode - Silicon Labs EFx32 Host. Follow the Getting Started with EFx32 to setup the example to work with EFx32 and Simplicity Studio. 
 
3.2 NCP Mode - Host Interface#
By default, the application is configured to use the SPI bus for interfacing between Host platforms(EFR32MG21) and the SiWx91x EVK.
3.3 Bare Metal/RTOS Support#
This application supports bare metal and RTOS environment. By default, the application project files (Keil and Simplicity Studio) are provided with RTOS configuration. To select a bare metal configuration, see Selecting bare metal.
4. Application Configuration Parameters#
The application can be configured to suit your requirements and development environment. Read through the following sections and make any changes needed.
4.1 Open rsi_ble_common_config.h file
4.1.1 User must update the below parameters
- RSI_BLE_NEW_SERVICE_UUID refers to the attribute value of the newly created service. 
    #define RSI_BLE_NEW_SERVICE_UUID                                0xAABB- RSI_BLE_ATTRIBUTE_1_UUID refers to the attribute type of the first attribute under this service (RSI_BLE_NEW_SERVICE_UUID). 
    #define RSI_BLE_ATTRIBUTE_1_UUID                                0x1AA1BLE_THROUGHPUT refers the name of the Silicon Labs device to appear during scanning by remote devices.
    #define RSI_BLE_DEVICE_NAME                                  "BLE_THROUGHPUT"Note: Following are the Non-configurable macros in the application.
- RSI_BLE_CHAR_SERV_UUID refers to the attribute type of the characteristics to be added in a service. 
 #define RSI_BLE_CHAR_SERV_UUID                                    0x2803- RSI_BLE_CLIENT_CHAR_UUID refers to the attribute type of the client characteristics descriptor to be added in a service. 
     #define RSI_BLE_CLIENT_CHAR_UUID                                  0x2902Note: Following are the properties:
- RSI_BLE_ATT_PROPERTY_READ is used to set the READ property to an attribute value. 
#define RSI_BLE_ATT_PROPERTY_READ                                 0x02```
- **RSI_BLE_ATT_PROPERTY_WRITE** is used to set the WRITE property to an attribute value.
```c
 #define RSI_BLE_ATT_PROPERTY_WRITE                                0x08- RSI_BLE_ATT_PROPERTY_NOTIFY is used to set the NOTIFY property to an attribute value. 
     #define RSI_BLE_ATT_PROPERTY_NOTIFY                               0x10BT_GLOBAL_BUFF_LEN refers Number of bytes required by the application and the driver.
	 #define BT_GLOBAL_BUFF_LEN                                        150004.2 Open rsi_ble_config.h file and update/modify following macros,
	 #define RSI_BLE_PWR_INX                                             30
     #define RSI_BLE_PWR_SAVE_OPTIONS                                    0
 
     #define RSI_BLE_REMOTE_DEV_ADDR                                     "00:12:45:AB:1D:32"
     #define RSI_REMOTE_DEVICE_NAME                                      "Note10"
 
     #define CONN_BY_ADDR                                                1
     #define CONN_BY_NAME                                                2
 
     #define CONNECT_OPTION                                              CONN_BY_NAME
 
     #define CENTERAL_ROLE                                               1
     #define PERIPHERAL_ROLE                                             2
     #define CONNECTION_ROLE                                             PERIPHERAL_ROLE
 
     #define CONN_INTERVAL_MIN                                           45
     #define CONN_INTERVAL_MAX                                           45
     #define CONN_LATENCY                                                0
     #define SUPERVISION_TIMEOUT                                         800
 
     #define SMP_ENABLE                                                  1
 
     #define TX_LEN                                                      0xFB
     #define TX_TIME                                                     0x0148
 
     #define TX_PHY_RATE                                                 0x02
     #define RX_PHY_RATE                                                 0x02
     #define CODDED_PHY_RATE                                             0x00
 
     #define NOTIFY_DISABLE                                              0x00
     #define NOTIFY_ENABLE                                               0x01
 
     #define DLE_ON                                                      1
 
     #define DLE_BUFFER_MODE                                             1
     #define DLE_BUFFER_COUNT                                            25
     #define RSI_BLE_MAX_DATA_LEN                                        232Note: rsi_ble_config.h file is already set with the desired configuration in respective example folders user need not change for each example. ```
5. Testing the Application#
- Follow the below steps for the successful execution of the application. 
5.1 Loading the SiWx91x Firmware#
- Refer Getting started with a PC to load the firmware into SiWx91x EVK. The firmware file is located in - <SDK>/connectivity_firmware/
5.2 Creating the Project and builing the Application#
- Refer Getting started with EFX32, for settin-up EFR & EFM host platforms 
5.2.1 Project Creation - SoC Mode :#
- Connect your board. The Si917 compatible SoC board is BRD4325A. 
- Studio should detect your board. Your board will be shown here.   
5.2.2 Project Creation - NCP Mode :#
- Connect your board. The supported NCP boards are: BRD4180A,BRD4280B 
- Studio should detect your board. Your board will be shown here.   
5.2.3 Selecting an example application and generate project#
- Go to the 'EXAMPLE PROJECT & DEMOS' tab and select your desired example application   
- Click 'Create'. The "New Project Wizard" window appears. Click 'Finish'   
5.2.4 Build Project - SoC Mode#
- Once the project is created, right click on project and go to properties → C/C++ Build → Settings → Build Steps 
- Add post_build_script_SimplicityStudio.bat file path (SI917_COMBO_SDK.X.X.X.XX\utilities\isp_scripts_common_flash) in build steps settings as shown in below image.   
- Check for M4 projects macros in preprocessor settings(RSI_M4_INTERFACE=1) 
- Check for 9117 macro in preprocessor settings(CHIP_9117=1). 
- Click on the build icon (hammer) to build the project   
- Successful build output will show as below.   
5.2.5 Build Project - NCP Mode :#
- Check for 9117 macro in preprocessor settings(CHIP_9117=1). 
- Click on the build icon (hammer) to build the project   
- Successful build output will show as below.   
6. Program the device#
- Once the build was successfull, right click on project and click on Debug As->Silicon Labs ARM Program as shown in below image. SoC Mode : 


NCP Mode :#


6.1 Running the SiWx91x Application#
- After the program gets executed, the Silicon Labs module will be in an Advertising state by default. 
- Connect any serial console for prints. 
- Open a EFR Connect App on the Smartphone and do the scan. 
- In the App, the Silicon Labs module device will appear with the name configured in the macro RSI_BLE_DEVICE_NAME (Ex: "BLE_THROUGHPUT")   
- Initiate a connection from the App. 
- After successful connection, EFR connect APP displays the supported services of Silicon Labs module   
- Select the attribute service which is added RSI_BLE_NEW_SERVICE_UUID (Ex: 0xAABB) 
- After Enable notifications for the read attribute RSI_BLE_ATTRIBUTE_2_UUID (Example: 0x1BB1) So that the GATT server notifies when value updated in that particular attribute.   
- Please refer to the given below images for continuous notification received on the mobile.     
7. Observing the output prints on serial terminal#
7.1 SoC Mode:#
- Connect USB to UART connector Tx and GND pins to WSTK radio board. - Connect Tx(Pin-6) to P27 on WSTK 
- Connect GND(Pin 8 or 10) to GND on WSTK   
 
- Prints can see as below in any Console terminal   
- Prints can see as below in any Console terminal   
- Open the project in Simplicity Studio 
- Right click on the project and choose 'Properties' 
- Go to 'C/C++ Build' | 'Settings' | 'GNU ARM C Compiler' | 'Symbols' and remove macro 'RSI_WITH_OS=1' 
- Select 'Apply' and 'OK' to save the settings 




8.2 Bare Metal with Keil#
- Open project in Keil IDE and click on 'Options for Target' 
- Go to 'C/C++' tab and remove 'RSI_WITH_OS' macro present under Preprocessor Symbols 
- Click on 'OK' button to save the settings