Public Attributes#

uint32_t
uint16_t
uint8_t
uint8_t

scan results to host

uint32_t

socket connection request pending

uint32_t

network command request pending

Public Attribute Documentation#

tls_version#

uint32_t tls_version

Definition at line 549 of file include/rsi_wlan_non_rom.h

join_bssid_non_rom#

uint8_t join_bssid_non_rom[6]

Definition at line 550 of file include/rsi_wlan_non_rom.h

socket_bitmap#

uint32_t socket_bitmap

Definition at line 552 of file include/rsi_wlan_non_rom.h

rsi_uart_data_ack_check#

uint8_t rsi_uart_data_ack_check

Definition at line 554 of file include/rsi_wlan_non_rom.h

switch_proto_callback#

void(* switch_proto_callback) (uint16_t mode, uint8_t *bt_disabled_status)

Definition at line 556 of file include/rsi_wlan_non_rom.h

read_data#

uint16_t read_data

Definition at line 558 of file include/rsi_wlan_non_rom.h

callback_list#

rsi_callback_cb_t callback_list

Definition at line 564 of file include/rsi_wlan_non_rom.h

wlan_radio#

uint8_t wlan_radio

Definition at line 566 of file include/rsi_wlan_non_rom.h

ps_listen_interval#

uint16_t ps_listen_interval

Definition at line 567 of file include/rsi_wlan_non_rom.h

emb_mqtt_ssl_enable#

uint8_t emb_mqtt_ssl_enable

Definition at line 569 of file include/rsi_wlan_non_rom.h

scan_results_to_host#

uint8_t scan_results_to_host

scan results to host


Definition at line 572 of file include/rsi_wlan_non_rom.h

socket_cmd_rsp_pending#

uint32_t socket_cmd_rsp_pending

socket connection request pending


Definition at line 575 of file include/rsi_wlan_non_rom.h

nwk_cmd_rsp_pending#

uint32_t nwk_cmd_rsp_pending

network command request pending


Definition at line 577 of file include/rsi_wlan_non_rom.h