Public Attribute Documentation#

min_main_mode_steps#

uint8_t sl_rtl_cs_params::min_main_mode_steps

Minimum number of CS main mode steps to be executed before a sub mode step. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.


max_main_mode_steps#

uint8_t sl_rtl_cs_params::max_main_mode_steps

Maximum number of CS main mode steps to be executed before a sub mode step. Field is ignored if sub mode is set to SL_RTL_CS_MODE_NONE.


main_mode_repetition#

uint32_t sl_rtl_cs_params::main_mode_repetition

Number of main modes repeated from previous subevent (0, 1, 2, 3).


num_calib_steps#

uint8_t sl_rtl_cs_params::num_calib_steps

rtt_type#

sl_rtl_cs_rtt_type sl_rtl_cs_params::rtt_type

cs_sync_phy#

uint8_t sl_rtl_cs_params::cs_sync_phy

channel_map#

uint8_t sl_rtl_cs_params::channel_map[10]

Bluetooth channel bitmap


channel_map_repetition#

uint8_t sl_rtl_cs_params::channel_map_repetition

channel_selection_type#

uint8_t sl_rtl_cs_params::channel_selection_type

ch3c_shape#

uint8_t sl_rtl_cs_params::ch3c_shape

ch3c_jump#

uint8_t sl_rtl_cs_params::ch3c_jump

T_PM_time#

uint8_t sl_rtl_cs_params::T_PM_time

T_IP1_time#

uint8_t sl_rtl_cs_params::T_IP1_time

T_IP2_time#

uint8_t sl_rtl_cs_params::T_IP2_time

T_FCS_time#

uint8_t sl_rtl_cs_params::T_FCS_time

num_antenna_paths#

uint8_t sl_rtl_cs_params::num_antenna_paths

Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.


connection_interval#

uint16_t sl_rtl_cs_params::connection_interval

Connection interval in units of 1.25 ms