Public Attribute Documentation#
procedure_counter#
uint16_t sl_rtl_cs_subevent_data::procedure_counter
CS procedure count since completion of the Channel Sounding Security Start procedure
frequency_compensation#
int16_t sl_rtl_cs_subevent_data::frequency_compensation
Frequency compensation value. Units: 0.01 ppm (15-bit signed integer). - Range: -10000 to 10000. - Value: 0xC000. Frequency compensation value is not available or the role is not initiator. This is reported only in the first subevent in the procedure. For subsequent subevents, this value is set to 0.
reference_power_level#
int8_t sl_rtl_cs_subevent_data::reference_power_level
Reference power level used by the transmission. Units: dBm. - Range: -127 to 20. - Value: 0x07F. The reference power level is not applicable
num_steps#
uint8_t sl_rtl_cs_subevent_data::num_steps
Number of steps in the CS subevent for which results are reported. - Range: 1 to 160.