Public Attributes#

uint8_t *

Public Attribute Documentation#

step_channels#

uint8_t* sl_rtl_ras_additional_info::step_channels

Pointer to the array of the step channels in the measured order


num_steps_reported#

uint8_t sl_rtl_ras_additional_info::num_steps_reported

Number of elements in the step channels array


num_antenna_paths#

uint8_t sl_rtl_ras_additional_info::num_antenna_paths

Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.