Public Attribute Documentation#

start_acl_connection_event#

uint16_t sl_rtl_ras_subevent_header::start_acl_connection_event

frequency_compensation#

int16_t sl_rtl_ras_subevent_header::frequency_compensation

Frequency compensation value. Units: 0.01 ppm (15-bit signed integer). - Range: -10000 to 10000 - Value: 0xC000. Frequency compensation value is not available or the role is not initiator. This is reported only in the first subevent in the procedure. For subsequent subevents, this value is set to 0.


ranging_done_status#

uint8_t sl_rtl_ras_subevent_header::ranging_done_status

subevent_done_status#

uint8_t sl_rtl_ras_subevent_header::subevent_done_status

ranging_abort_reason#

uint8_t sl_rtl_ras_subevent_header::ranging_abort_reason

subevent_abort_reason#

uint8_t sl_rtl_ras_subevent_header::subevent_abort_reason

reference_power_level#

int8_t sl_rtl_ras_subevent_header::reference_power_level

Reference power level used by the transmission. Units: dBm. - Range: -127 to 20 - Value: 0x07F. The reference power level is not applicable


num_steps#

uint8_t sl_rtl_ras_subevent_header::num_steps

Number of steps in the RAS subevent for which results are reported. - Range: 1 to 160