Bluetooth LE Channel Sounding Developer's Guide#
Channel Sounding (CS) is a new feature introduced as part of the Bluetooth core specification 6.0 to enable distance estimation between two Bluetooth Low Energy (LE) devices.
In CS, two devices, known as Initiator and Reflector, exchange information that is measured to provide timing and frequency synchronization, and produce accurate distance estimate between them. It achieves this using Phase Based Ranging (PBR) and Round-Trip Time (RTT) measurement approaches. You can find more information in the Fundamentals section.
Silicon Labs provides modularized software sample projects for the Initiator and Reflector that can be extended to address different use case scenarios. In addition, Silicon Labs offers a reference implementation of a Real-Time Locating (RTL) library, which facilitates distance estimation using CS.
The rest of this Developer's Guide is organized as follows:
Prerequisites: Provides all prerequisites needed to build, program, and use the CS sample projects.
Documentation: Describes where the CS documentations and API reference manual can be found.
Sample Applications: Describes the software architecture, configuration, building and running procedures of the provided sample projects.
Channel Sounding Capabilities & Configurability: Details all supported features, configuration methods, and tuning options for initiator and reflector roles.
Logging & Tools: Describes logging options, debug flows, and available tools for CS development.
Channel Sounding Performance Metrics: Provides detailed benchmarking data (accuracy, latency, energy consumption) for evaluating the channel sounding solution using Silicon Labs development boards.
Simplicity Studio Channel Sounding Analyzer: Describes how to use the Simplicity Studio Channel Sounding Analyzer tool for visualizing and debugging purposes.
Known Issues and Limitations: Lists the issues and limitations known at publication.