Channel Sounding (CS)#

Channel Sounding.

Distances are calculated by following the steps below:

  1. Initialize a sl_rtl_cs_libitem instance.

  2. Set up the algorithm mode and CS parameters.

  3. Create the estimator.

  4. Process the CS procedure data into distance.

  5. Get distance and/or likeliness estimates.

Modules#

sl_rtl_cs_params

sl_rtl_cs_config

sl_rtl_cs_estimator_param_value

sl_rtl_cs_estimator_param

sl_rtl_cs_mode_calib_data

sl_rtl_cs_mode_rtt_data

sl_rtl_cs_pbr_tone

sl_rtl_cs_mode_pbr_data

sl_rtl_cs_step_data

sl_rtl_cs_subevent_data

sl_rtl_cs_procedure

sl_rtl_cs_log_params

sl_rtl_cs_step_data.__unnamed1__

Enumerations#

enum
SL_RTL_CS_ROLE_INITIATOR = 0
SL_RTL_CS_ROLE_REFLECTOR
}
enum
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC = 0
SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY = 1
}
enum
SL_RTL_CS_MODE_CALIBRATION = 0
SL_RTL_CS_MODE_RTT = 1
SL_RTL_CS_MODE_PBR = 2
}
enum
SL_RTL_CS_RTT_TYPE_AAONLY = 0
SL_RTL_CS_RTT_TYPE_SS_32BIT = 1
SL_RTL_CS_RTT_TYPE_SS_96BIT = 2
SL_RTL_CS_RTT_TYPE_RS_32BIT = 3
SL_RTL_CS_RTT_TYPE_RS_64BIT = 4
SL_RTL_CS_RTT_TYPE_RS_96BIT = 5
SL_RTL_CS_RTT_TYPE_RS_128BIT = 6
}
enum
SL_RTL_LAST_KNOWN_DISTANCE = 0
SL_RTL_RANGE_MIN = 1
SL_RTL_RANGE_MAX = 2
SL_RTL_REF_TX_POWER = 3
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED = 0
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RAW
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS = 0
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE
}
enum
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE = 0
}

Typedefs#

typedef void *

CS library item.

Functions#

sl_rtl_cs_init(sl_rtl_cs_libitem *item)
sl_rtl_cs_deinit(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_algo_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_algo_mode mode)
sl_rtl_cs_set_cs_mode(sl_rtl_cs_libitem *item, const sl_rtl_cs_mode cs_mode)
sl_rtl_cs_set_cs_params(sl_rtl_cs_libitem *item, const sl_rtl_cs_params *parameters)
sl_rtl_cs_create_estimator(sl_rtl_cs_libitem *item)
sl_rtl_cs_set_estimator_param(sl_rtl_cs_libitem *item, const sl_rtl_cs_estimator_param *param)
sl_rtl_cs_process(sl_rtl_cs_libitem *item, const uint8_t procedure_count, const sl_rtl_cs_procedure *procedure_data)
sl_rtl_cs_get_distance_estimate(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_type estimate_type, float *distance)
sl_rtl_cs_get_distance_estimate_confidence(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, float *confidence)
sl_rtl_cs_get_distance_estimate_extended_info(sl_rtl_cs_libitem *item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float *extended_info)
sl_rtl_cs_log_enable(sl_rtl_cs_libitem *item, const sl_rtl_cs_log_params *log_params)
sl_rtl_cs_log_disable(sl_rtl_cs_libitem *item)
sl_rtl_cs_log_get_instance_id(sl_rtl_cs_libitem *item, uint8_t *instance_id)

Macros#

#define
SL_RTL_CS_PCT_IQ_BIT_LEN 12
#define
SL_RTL_CS_STEP_MODE_BIT_LEN 8
#define
SL_RTL_CS_CHANNEL_MAP_SIZE 10

Enumeration Documentation#

sl_rtl_cs_role#

sl_rtl_cs_role
Enumerator
SL_RTL_CS_ROLE_INITIATOR

Initiator role.

SL_RTL_CS_ROLE_REFLECTOR

Reflector role.


Definition at line 757 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_algo_mode#

sl_rtl_cs_algo_mode
Enumerator
SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC

Suitable for real-time tracking.

SL_RTL_CS_ALGO_MODE_STATIC_HIGH_ACCURACY

Suitable for ranging between static objects with high-accuracy.


Definition at line 762 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_mode#

sl_rtl_cs_mode
Enumerator
SL_RTL_CS_MODE_CALIBRATION

Calibration mode with no distance estimation enabled.

SL_RTL_CS_MODE_RTT

Round-trip time based estimation (RTT).

SL_RTL_CS_MODE_PBR

Round-trip phase based estimation (PBR).


Definition at line 771 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_rtt_type#

sl_rtl_cs_rtt_type
Enumerator
SL_RTL_CS_RTT_TYPE_AAONLY

RTT AA Only. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_SS_32BIT

RTT with 32-bit sounding sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_SS_96BIT

RTT with 96-bit sounding sequence.

SL_RTL_CS_RTT_TYPE_RS_32BIT

RTT with 32-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_64BIT

RTT with 64-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_96BIT

RTT with 96-bit random sequence. Currently unsupported type.

SL_RTL_CS_RTT_TYPE_RS_128BIT

RTT with 128-bit random sequence. Currently unsupported type.


Definition at line 780 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_estimator_param_type#

sl_rtl_cs_estimator_param_type
Enumerator
SL_RTL_LAST_KNOWN_DISTANCE

Last known distance from the user, if more recent than the last CS measurement.

SL_RTL_RANGE_MIN

Minimum limit for the distance estimation range.

SL_RTL_RANGE_MAX

Maximum limit for the distance estimation range.

SL_RTL_REF_TX_POWER

Reference RSSI value of the TX-device at 1.0 m distance in dBm. Default value is -45.0 dBm.


Definition at line 835 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_distance_estimate_type#

sl_rtl_cs_distance_estimate_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_FILTERED

Distance estimate with built-in post-filtering. Note: The post-filtering would remove any large undesired jumps in the distance reported. However, post-filtering introduces latency in distance reported.

SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RSSI

Distance estimate based on the Packet_RSSI in the calibration (Mode 0) steps

SL_RTL_CS_DISTANCE_ESTIMATE_TYPE_RAW

Distance estimate based solely on the most recent procedure input.


Definition at line 936 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_distance_estimate_confidence_type#

sl_rtl_cs_distance_estimate_confidence_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_LIKELINESS

Likeliness of the distance estimate accuracy, ranging from 0 to 1

SL_RTL_CS_DISTANCE_ESTIMATE_CONFIDENCE_TYPE_BIT_ERROR_RATE

Bit error rate in the RTT random or sounding sequence, ranging from 0 to 1. Only supported for RTT types (see sl_rtl_cs_rtt_type) with random sequence (RS) or sounding sequence (SS).


Definition at line 948 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_distance_estimate_extended_info_type#

sl_rtl_cs_distance_estimate_extended_info_type
Enumerator
SL_RTL_CS_DISTANCE_ESTIMATE_EXTENDED_INFO_TYPE_PROGRESS_PERCENTAGE

Estimation progress in percentage.

  • Range: 0 to 100.


Definition at line 957 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

Typedef Documentation#

sl_rtl_cs_libitem#

typedef void* sl_rtl_cs_libitem

CS library item.


Definition at line 964 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

Function Documentation#

sl_rtl_cs_init#

enum sl_rtl_error_code sl_rtl_cs_init (sl_rtl_cs_libitem * item)
Parameters
[in]item

Pointer to the libitem to be initialized

Initialize the CS libitem instance.

Returns


Definition at line 994 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_deinit#

enum sl_rtl_error_code sl_rtl_cs_deinit (sl_rtl_cs_libitem * item)
Parameters
[in]item

Pointer to the libitem to be deinitialized

Deinitialize a libitem instance of the CS estimator.

Returns


Definition at line 1002 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_set_algo_mode#

enum sl_rtl_error_code sl_rtl_cs_set_algo_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_algo_mode mode)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]mode

Estimator mode as sl_rtl_cs_algo_mode

Set the estimation algorithm mode.

Returns

Set the estimation mode. For example, SL_RTL_CS_ALGO_MODE_REAL_TIME_BASIC sets medium filtering. For further description of the modes, see the documentation of::sl_rtl_cs_algo_mode. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


Definition at line 1020 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_set_cs_mode#

enum sl_rtl_error_code sl_rtl_cs_set_cs_mode (sl_rtl_cs_libitem * item, const sl_rtl_cs_mode cs_mode)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]cs_mode

cs_mode as sl_rtl_cs_mode

Set the estimation CS mode.

Returns

Set the desired cs_mode. For example, SL_RTL_CS_MODE_PBR uses round-trip phase based cs_mode. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


Definition at line 1037 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_set_cs_params#

enum sl_rtl_error_code sl_rtl_cs_set_cs_params (sl_rtl_cs_libitem * item, const sl_rtl_cs_params * parameters)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]parameters

cs_params as sl_rtl_cs_params

Set the estimation CS parameters.

Returns

Set the parameters for the estimator. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


Definition at line 1054 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_create_estimator#

enum sl_rtl_error_code sl_rtl_cs_create_estimator (sl_rtl_cs_libitem * item)
Parameters
[in]item

Pointer to the initialized and configured CS libitem

Create an estimator with the given parameters after initializing the libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called before estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_ALREADY_CREATED.


Definition at line 1069 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_set_estimator_param#

enum sl_rtl_error_code sl_rtl_cs_set_estimator_param (sl_rtl_cs_libitem * item, const sl_rtl_cs_estimator_param * param)
Parameters
[in]item

Pointer to the initialized and configured CS libitem

[in]param

Data structure with the CS algorithm parameter to be set

Set CS algorithm parameters. The function can be called any time before or during the processing calls.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


Definition at line 1086 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_process#

enum sl_rtl_error_code sl_rtl_cs_process (sl_rtl_cs_libitem * item, const uint8_t procedure_count, const sl_rtl_cs_procedure * procedure_data)
Parameters
[in]item

Pointer to the initialized and configured CS libitem

[in]procedure_count

Number of procedures in the procedure_data array

[in]procedure_data

Data structure with the completed CS procedures

Calculate distance estimate based on CS procedures.

Returns

Calculate the distance estimate from the given procedure data. The function can be called with multiple procedures. Use sl_rtl_cs_get_distance to fetch the latest distance estimate. CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


Definition at line 1108 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_get_distance_estimate#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_type estimate_type, float * distance)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]estimate_type

Type of distance estimate

[out]distance

Distance out in meters.

Get distance estimate

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


Definition at line 1127 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_get_distance_estimate_confidence#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_confidence (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_confidence_type confidence_type, float * confidence)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]confidence_type

Type of confidence estimate

[out]confidence

Confidence between 0.0 - 1.0 (unlikely - likely) of the estimated distance

Get distance estimate confidence.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


Definition at line 1147 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_get_distance_estimate_extended_info#

enum sl_rtl_error_code sl_rtl_cs_get_distance_estimate_extended_info (sl_rtl_cs_libitem * item, const sl_rtl_cs_distance_estimate_extended_info_type extended_info_type, float * extended_info)
Parameters
[in]item

Pointer to the initialized CS libitem

[in]extended_info_type

Type of distance estimate extended information

[out]extended_info

Extended info value depending on the extedended_info_type selection

Get distance estimate extended information.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED. This method should be called after estimator is created for CS libitem, or it will fail with error code SL_RTL_ERROR_ESTIMATOR_NOT_CREATED.


Definition at line 1168 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_log_enable#

enum sl_rtl_error_code sl_rtl_cs_log_enable (sl_rtl_cs_libitem * item, const sl_rtl_cs_log_params * log_params)
Parameters
[in]item

Pointer to the CS libitem

[in]log_params

Pointer to the log initialisation parameters

Enable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED.


Definition at line 1184 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_log_disable#

enum sl_rtl_error_code sl_rtl_cs_log_disable (sl_rtl_cs_libitem * item)
Parameters
[in]item

Pointer to the CS libitem

Disable logging for the given CS libitem.

Returns

CS libitem must be initialized before calling this method, or it will fail with return code SL_RTL_ERROR_NOT_INITIALIZED.


Definition at line 1196 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

sl_rtl_cs_log_get_instance_id#

enum sl_rtl_error_code sl_rtl_cs_log_get_instance_id (sl_rtl_cs_libitem * item, uint8_t * instance_id)
Parameters
[in]item

Pointer to the CS libitem

[out]instance_id

Instance ID of the given CS libitem

Get the instance ID of the given CS libitem.

Returns


Definition at line 1205 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h