Public Attribute Documentation#

num_antenna_paths#

uint8_t sl_rtl_cs_config::num_antenna_paths

Number of antenna paths supported by the local controller for the CS tone exchanges. - Range: 1 to 4. The number of antenna paths used during the phase measurement stage of the CS step. - Value: 0. Phase measurement does not occur during the CS step, therefore ignored.


Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

channel_map_repetition#

uint8_t sl_rtl_cs_config::channel_map_repetition

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

main_mode_repetition#

uint32_t sl_rtl_cs_config::main_mode_repetition

Number of main modes repeated from previous subevent (0, 1, 2, 3).


Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

num_calib_steps#

uint8_t sl_rtl_cs_config::num_calib_steps

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

T_PM_time#

uint8_t sl_rtl_cs_config::T_PM_time

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

T_IP1_time#

uint8_t sl_rtl_cs_config::T_IP1_time

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

T_IP2_time#

uint8_t sl_rtl_cs_config::T_IP2_time

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

T_FCS_time#

uint8_t sl_rtl_cs_config::T_FCS_time

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

channel_selection_type#

uint8_t sl_rtl_cs_config::channel_selection_type

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

ch3c_shape#

uint8_t sl_rtl_cs_config::ch3c_shape

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

ch3c_jump#

uint8_t sl_rtl_cs_config::ch3c_jump

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

subevent_len#

uint32_t sl_rtl_cs_config::subevent_len

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

subevents_per_event#

uint8_t sl_rtl_cs_config::subevents_per_event

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

subevent_interval#

uint16_t sl_rtl_cs_config::subevent_interval

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

event_interval#

uint16_t sl_rtl_cs_config::event_interval

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

procedure_interval#

uint16_t sl_rtl_cs_config::procedure_interval

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

procedure_count#

uint16_t sl_rtl_cs_config::procedure_count

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

cs_sync_phy#

uint8_t sl_rtl_cs_config::cs_sync_phy

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

rtt_type#

sl_rtl_cs_rtt_type sl_rtl_cs_config::rtt_type

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h

acl_connection_interval#

uint16_t sl_rtl_cs_config::acl_connection_interval

Definition at line 833 of file /mnt/raid/workspaces/ws.EluogwpbG/overlay/gsdk/util/silicon_labs/rtl/inc/sl_rtl_clib_api.h