Serial Commands 

#


Use the serial commands to get information about and configure the serial configuration.
For more information about the supported serial communication protocols see VCOM and Auxiliary UART.
Commands | Description |
|---|---|
Get information about the serial configuration. | |
Configure the serial configuration. | |
Manually control serial handshake lines. | |
Get serial communication stats. | |
Enable serial communication. | |
Disable serial communication. |
serial vcom#
Gets information about the currently selected serial configuration. Shows the active configuration as well as the configuration stored in persistent memory.
Command Line Syntax
$ serial vcomCommand Line Examples
$ serial vcom
----- Virtual COM port -----
Stored port speed : 115200
Active port speed : 487603
Stored handshake : auto
Actual handshake : disabled
$ serial vcom
----- Aux uart -----
Stored port speed : 115200
Active port speed : 115200
Stored aux uart mode : enabled
Actual aux uart mode : enabled
$ serial vcom
----- Virtual COM port -----
Stored port speed : 115200
Active port speed : 115234
Stored handshake : aux
Actual handshake : rts
RTS Asserted - Ready to Receive.
----- Aux uart -----
Stored port speed : 115200
Active port speed : N/A
Stored aux uart mode : enabled
Actual aux uart mode : disabled
$ serial vcom
----- Virtual COM port -----
Stored port speed : 115200
Active port speed : N/A
Stored handshake : cts
Actual handshake : aux
----- Aux uart -----
Stored port speed : 115200
Active port speed : 115200
Stored aux uart mode : disabled
Actual aux uart mode : enabledserial vcom config#
Configures the serial configuration. You can change the handshake type, the baud rate, or both. By default, the configuration is stored in persistent memory. To skip this, use the --nostore option.
Supported handshake types and baud rates depend on the adapter type. Handshake signals are described from the board controller’s perspective; RTS is an input to the board controller, and CTS is an output from it.
Supported baud rates range from 9600 to 3,686,400. Baud rate configuration for the auxiliary UART is supported only on EKs and DKs.
Handshake type | Description | Supported on |
|---|---|---|
rts | Enable RTS hardware flow control |
|
cts | Enable CTS hardware flow control |
|
rtscts | Enable RTS and CTS hardware flow control |
|
disable | Disable hardware flow control |
|
auto | Automatically set hardware flow control at boot |
|
aux | Enables auxilary UART and disables VCOM |
|
Command Line Syntax
$ serial vcom config [--nostore] [handshake <handshakeType>] [speed <bitrate>]Command Line Examples
$ serial vcom config --nostore handshake rtscts speed 486000
Baudrate set to 486000 bps
Actual baud rate: 487603 Hz
RTS handshake enabled
CTS handshake enabled
Aux uart disabled
$ serial vcom config speed 115200
Baudrate set to 115200 bps
Actual baud rate: 115234 Hz
Serial configuration savedserial vcom ctrl#
Manually controls serial handshake lines. The command supports asserting and deasserting either RTS or CTS or both at the same time.
Command Line Syntax
$ serial vcom ctrl [rts <assert/deassert>] [cts <assert/deassert>]Command Line Examples
$ serial vcom ctrl rts assert
RTS asserted
$ serial vcom ctrl cts assert rts deassert
RTS deasserted
CTS assertedserial vcom stats#
Gets serial communication stats.
Command Line Syntax
$ serial vcom statsCommand Line Example
$ serial vcom stats
### Target to Host ###
From target: 1818 bytes
Discarded: 106 bytes
Forwarded: 1712 bytes
By transport:
CDC: 1712 bytes
Conn: 0 bytes
Appdata: 0 bytes
Last transport: CDC
### Host to Target ###
From host: 21 bytes
Discarded: 0 bytes
Forwarded: 21 bytes
By transport:
CDC: 21 bytes
Conn: 0 bytes
Appdata: 0 bytes
Last transport: CDCserial vcom enable#
Enable serial communication. It is not possible to enable serial communication while the currently selected debug mode is in.
Command Line Syntax
$ serial vcom enableCommand Line Example
$ serial vcom enable
Enabling VCOM.serial vcom disable#
Disable serial communication.
Command Line Syntax
$ serial vcom disableCommand Line Example
$ serial vcom disable
Disabling VCOM.