Troubleshoot Environment Issues#
Objective#
Identify and resolve common development environment issues when using Silicon Labs Tool (SLT) and Silicon Labs Configurator CLI (SLC-CLI).
This section summarizes common environment issues and recommended solutions.
1. SLT Command Not Found#
Issue
The slt command is not recognized after installation.
Solution
Add the SLT installation directory to your system PATH.
Windows: SLT#
Add the directory that contains slt.exe to the Path environment variable.
macOS#
echo 'export PATH=$PATH:/path/to/slt' >> ~/.zshrc source ~/.zshrc
Linux#
echo 'export PATH=$PATH:/path/to/slt' >> ~/.bashrc source ~/.bashrc
2. Java Version Conflict#
Issue
Another Java installation appears earlier in the system PATH, causing conflicts with SLT.
Solution
Ensure that the Java 21 runtime installed by SLT appears before any other Java installation.
Windows#
.silabs\slt\installs\archive\java21-v21.x.x\jre\bin
macOS/Linux: Java#
~/.silabs/slt/installs/archive/java21-v21.x.x/jre/bin
3. SLC-CLI Command Not Found#
Issue
The slc command is not recognized.
Solution
Add the SLC-CLI installation directory to your PATH.
Windows: SLC-CLI#
.silabs\slt\installs\archive\slc-cli-v6.x.x
macOS/Linux: SLC-CLI#
~/.silabs/slt/installs/archive/slc-cli-v6.x.x
4. SDK Not Trusted#
Issue
SLC-CLI does not detect or load an SDK or SDK extension.
Solution
Trust the SDK or extension before you use it.
## Trust an SDK slc signature trust --sdk <sdk_path> ## Trust an extension by path slc signature trust -extpath <extension_path> ## Trust an extension by ID slc signature trust -extid <extension_id>
Note: SLC-CLI ignores untrusted SDKs and extensions without displaying an error.
5. SDK Not Configured#
Issue
SLC commands fail because no default SDK is configured.
Solution
Configure the default SDK.
slc configuration --sdk=<sdk_path> ## Verify configuration slc configuration -e
Without a configured SDK, you must specify --sdk (or an equivalent SDK path option) for every SLC command.
6. GCC Toolchain Not Found#
Issue
The project cannot build because the Arm GCC toolchain is missing or not configured.
Solution
Configure the toolchain:
slc configuration --gcc-toolchain=<gcc_path>
Or set the environment variable:
export ARM_GCC_DIR=<gcc_path>
If the toolchain is not installed:
slt install gcc-arm-none-eabi
Verify the installation:
slt where gcc-arm-none-eabi
7. SDK Installation Blocked#
Issue
Installing a new SDK version fails because installed SDK extensions require updates.
Solution
Allow SLT to update compatible extensions.
slt install simplicity-sdk/<version> --check-updates
8. Network Access Issues (Dev Containers)#
Issue
Development containers cannot access package repositories or extension marketplaces because of proxy restrictions or SSL inspection.
Solution
Configure the corporate SSL certificate:
bash .devcontainer/scripts/configure_cursor_ssl.sh
Alternatively, install the required extensions manually.
9. Project Upgrade Requires Manual Steps#
Issue
slc upgrade stops because manual migration steps are required.
Solution
Force the upgrade and complete the manual steps listed in the output.
slc upgrade \ -p project.slcp \ --sdk-package-path <new_sdk_path> \ --force-upgrade
Quick Diagnostic Checklist#
Verify | Command |
|---|---|
SLT version |
|
SLC configuration |
|
SDK installation |
|
GCC toolchain |
|
Java installation |
|
Installed packages |
|
Best Practices#
Keep SLT and SLC-CLI up to date.
Ensure that SLT uses the bundled Java 21 runtime.
Add the SLT and SLC-CLI installation directories to your system
PATH.Verify SDK and toolchain locations by using
slt where.Trust SDKs and extensions before you generate projects.
Commit project configuration files (
pkg.slt,pkg.lock, anduser.slconf) to source control for reproducible environments.