WiSeConnect - Wi-Fi SDK Version 4.0.2 (May 4, 2026) - Release Notes#
Wi-Fi 6 + BLE (WiSeConnect) SDK Version 4.0.2
Simplicity SDK Version 2025.12.3
The Wi-Fi Software Development Kit (SDK) provides Wi-Fi 6 connectivity in multiple operating modes, including Station and Software Access Point (SoftAP).
Click here for earlier releases.
Release Summary#
Key Features | API Changes | Bug Fixes | Chip Enablement
Key Features#
Added in 4.0.2#
Enhanced background scanning (bgscan) to support extended scan results using a new
advanced_scan_bitmapfield insl_wifi_advanced_scan_configuration_t, including aseen_countper AP and improved Beacon IE parsing with WPA/WPA2 mixed-mode detection.
Added in 4.0.1#
None
Added in 4.0.0#
Added Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) feature support in Station mode
Added Vendor-specific IE support for Station (STA), SoftAP, and Concurrent Modes
API Changes#
Added in 4.0.2#
None
Added in 4.0.1#
None
Added in 4.0.0#
Bug Fixes#
Fixed in 4.0.2#
Fixed an issue where the Wireless Test application became unresponsive when CLI commands (for example,
wifi_ax_transmit_test_start) received more parameters than expected. Added parameter count validation to prevent this issue.Fixed an issue that could cause the Wi-Fi mode set API to return error code -116 when configuring the device in SoftAP mode, ensuring reliable AP initialization across supported environments.
Fixed in 4.0.1#
Fixed a throughput drop in STA mode when 11w is enabled on the STA but disabled on the AP.
Fixed a DHCP handshake failure in Concurrent Mode with NAT+PAT enabled in congested environments.
Fixed in 4.0.0#
Fixed an issue where HTTP server encounters a connection timeout error when the web page is refreshed multiple times.
Added support for configurable PEAP security levels (PEAPSAFE1, PEAPSAFE2) through new encryption enum members to enhance enterprise Wi-Fi authentication security.
Chip Enablement#
Added in 4.0.2#
Added support for BRD2708A board for the Wireless Test example (RF validation).
Added in 4.0.1#
None
Added in 4.0.0#
None
Key Features#
New Features | Enhancements | Removed Features | Deprecated Features
Note: See Feature Matrix for a list of any applicable APIs, examples, software variants, modes, hardware, and host interfaces applicable for each feature.
New Features#
Added in 4.0.2#
Added support for BRD2708A board for the Wireless Test example.
Added in 4.0.1#
None
Added in 4.0.0#
Added Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) feature support in Station mode
Added Vendor-specific IE support for Station (STA), SoftAP, and Concurrent Modes
An additional configurable option for Hidden SSID has been introduced in the
sli_wifi_start_apAPI, complementing the existing opermode configuration. The Hidden SSID can be configured via thesli_wifi_start_apAPI only when SL_WIFI_CUSTOM_FEAT_AP_IN_HIDDEN_MODE is not enabled incustom_feature_bit_map.Added support for reporting Wi-Fi band information for scanned access points in Wi-Fi scan results.
Improved SoftAP scan functionality to return more than 11 results.
Enhancements#
Added in 4.0.2#
The keep-alive timer has been updated to reset only on actual data transmissions and not on Null or QoS-Null frames, thereby preventing indefinite GARP delays and improving interoperability.
The extended scan callback has been enhanced to report the required buffer size through the
data_lengthparameter, enabling applications to dynamically allocate the exact amount of memory needed.
Added in 4.0.1#
None
Added in 4.0.0#
None
Removed Features#
Removed in 4.0.2#
None
Removed in 4.0.1#
None
Removed in 4.0.0#
None
Deprecated Features#
Deprecated in 4.0.2#
None
Deprecated in 4.0.1#
None
Deprecated in 4.0.0#
None
API Changes#
New APIs | Modified APIs | Removed APIs | Deprecated APIs
New APIs#
Added in 4.0.2#
None
Added in 4.0.1#
None
Added in 4.0.0#
New API Signature | Deprecated API replaced by this (if any) |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Modified APIs#
Modified in 4.0.2#
None
Modified in 4.0.1#
None
Modified in 4.0.0#
None
Removed APIs#
Removed in 4.0.2#
None
Removed in 4.0.1#
None
Removed in 4.0.0#
None
Deprecated APIs#
Deprecated in 4.0.2#
None
Deprecated in 4.0.1#
None
Deprecated in 4.0.0#
Deprecated API Name | Planned Removal Date |
|---|---|
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 | |
2027-06 |
Bug Fixes#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
Fixed in 4.0.2#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1605946 | Fixed an issue where the Wireless Test application became unresponsive when CLI commands (for example, wifi_ax_transmit_test_start) received more parameters than expected. Added parameter count validation to prevent this issue. |
None |
|
| 1615670 | Fixed an issue that could cause the Wi-Fi mode set API to return error code -116 when configuring the device in SoftAP mode, ensuring reliable AP initialization across supported environments. | None |
|
Fixed in 4.0.1#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1594590 | Enhanced Wi-Fi extended scan functionality to accurately identify and report WPA3 Transition Mode access points. This addresses cases where extended scan may incorrectly display WPA2 security type instead of WPA3 Transition Mode, ensuring correct security information during provisioning and general scanning. | None |
|
| 1581739 | Enhanced Xmodem firmware upgrade example with improved initialization handling. This addresses cases where sl_net_init() returns SL_STATUS_ALREADY_EXISTS (0x002E) after firmware upgrade, ensuring smooth operation of the wifi_firmware_flashing_from_host_uart_xmodem_bootloader_ncp example. | None |
|
| 1580084 | Improved memory management in sli_si91x_wifi_event_handler.c by optimizing buffer lifecycle handling. This addresses use-after-free scenarios where buffer memory was accessed after being freed, which could lead to heap corruption and unstable RTOS behavior. | None |
|
| 1578195 | Improved buffer handling by initializing local pointer variables (buffer, packet, node, etc.) to NULL. | None |
|
| 1574317 | Added support for BRD2708A board for the Wireless Test example, expanding hardware compatibility for customer applications using this board. | None |
|
| 1569213 | Enhanced at+cal-start command handling in AT commands application. This addresses cases where the command may not execute as expected (error code 4) while maintaining proper M4 power save functionality. | None |
|
| 1569000 | Enhanced AT command parser and BSD socket commands with improved pointer handling and socket setup validation. This addresses TCP socket send API issues (error code 33) in at_commands application, improving reliability for AT command-based applications. | None |
|
| 1559974 | Enhanced sl_net_deinit() functionality with improved cleanup handling for auto-join operations. This addresses cases where sl_net_deinit() may fail with error 0x1 during multiple auto-join iterations, ensuring reliable behavior when switching between network profiles. | None |
|
| 1533583 | Enhanced flash_read_write example with data comparison verification for both TA and M4 regions. The update provides better validation of read/write operations and helps prevent data integrity issues during flash operations. | None |
|
| 1576560 | Updated the keep-alive timer so that it resets only on real data transmissions, but not on Null or QoS-Null frames, preventing indefinite GARP delays and interoperability issues. | None |
|
| 1572862 | Fixed a throughput drop in STA mode when 11w is enabled on the STA but disabled on the AP. | None |
|
| 1557787 | Fixed a DHCP handshake failure in Concurrent Mode with NAT+PAT enabled in congested environments. | None |
|
Fixed in 4.0.0#
| ID | Issue Description | GitHub / Salesforce Reference (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|
| 1465518 | Fixed an issue where HTTP server encounters a connection timeout error when the webpage is refreshed multiple times. | None |
|
| 1502308 | Refactored socket allocation logic to use malloc/memset pattern with intermediate variable for improved error handling. | None |
|
| 1522478 | Improved async event processing and error handling. | None |
|
| 1496506 | The sl_net_init() API now returns an error if an attempt is made to modify the region code on modules where this operation is not permitted. |
None |
|
| 1365272 | Added configurable timeout mechanism with scaling macros for management, internal, and network commands, plus additional wait time for buffer overflow and congestion scenarios. Defaults set to '1'. | None |
|
| 1467697 | Added support for Wi-Fi examples to the OPNs SIWG917Y121MGABA and SIWG917Y110LGABA | None |
|
| 1452673 | Fixed a DTLS data transmission issue where packets could be lost if error 0x100D2 occurred, by implementing an automatic retry mechanism in the DTLS application with a default maximum of 3 retries. | None |
|
| 1451080 | Added the nvm3_lib component in the nvm3 config manager component instead of adding the nvm3_lib component for every application | None |
|
| 1407301 | Azure IoT Hub and Device Provisioning Service (DPS) are migrating their certificate root of trust from the Baltimore CyberTrust Root (expiring in 2025) to the DigiCert Global Root G2. All devices must migrate from azure_baltimore_ca to silabs_digicert_ca for secure TLS connection with Azure IoT Hub and Azure storage services. | None |
|
| 1409946 | Added support for configurable PEAP security levels (PEAPSAFE1, PEAPSAFE2) through new encryption enum members for enhanced enterprise Wi-Fi authentication security. | None |
|
| 1376228 | Resolved firmware corruption during TLS socket cleanup post-IP change during DHCP renewal. | None |
|
| 1371879 | Updated sl_si91x_get_socket_info API to provide host socket info. |
None |
|
| 1268204 | Deinitialize the Wi-Fi client interface when the power save profile is set to DEEP_SLEEP_WITHOUT_RAM_RETENTION. | None |
|
| 1450227 | SLI_MAX_RETRANSMISSION_TIME_VALUE has been updated to 255 (the maximum supported value) and can now be configured as a power of two from 1 to 128. | None |
|
| 1441131 | Replaced all breakpoints with the timeout indication recovery mechanism and with proper status. | None |
|
| 1466129 | Fixed static analysis issue by ensuring listen_interval is cast to uint16_t before assignment in the power save request struct. | None |
|
| 1463798 | Default configurations for Power Save Standby including NCP SoC and PSRAM are available when installing the Configuration Wizard. | None |
|
| 1490559 | The maximum client limit defined in the AP profile configuration will now automatically adjust if it exceeds the value set in the opermode configuration. | None |
|
| 1426767 | Replaced mixed BSD and sl-sockets with SiWx91x async sockets in sli_http_server(). |
None |
|
| 1455876 | Added configurable max retransmission timeout using AWS_IOT_MAX_RETRANSMISSION_TIMEOUT macro to avoid disconnection in case of AWS MQTT. | None |
|
| 1464308 | Resolved extended scan functionality by eliminating global variable dependency and ensuring controlled access. | None |
|
| 1343541 | Refactor the join configuration APIs from sl_si91x_ to sl_wifi_. |
None |
|
| 1467293 | Resolved 'connection reset by peer' errors in RX scenarios for TCP, UDP, and TLS across all applications. | None |
|
| 1464725 | Added a conditional check to prevent setting WLAN_UNCONNECTED_STATE if the DUT is already connected. | None |
|
| 1308081 | For wlan throughput UART NCP applications, the handshake feature bit (SL_SI91X_FEAT_ULP_GPIO_BASED_HANDSHAKE) is enabled by default to ensure reliable socket connections and proper power save operation. You can control this feature using the SL_ENABLE_UART_NCP_BITMAP macro in your preprocessor settings. | None |
|
| 1384564 | Fixed callback status update order to maintain correct status in loop operation | None |
|
| 1478000 | Added sl_string.h header file to provide proper declaration for sl_strnlen() function. Replaced standard strnlen() with SDK-specific sl_strnlen() implementation. Eliminates implicit declaration warnings and compilation failures. |
None |
|
| 1371872 | Resolved the AzureIOT connection issue in the process loop by adding state machine checks. | None |
|
| 1288559 | Added the validation for client idle timeout in AP configuration and mentioned the note of its range and units. | None |
|
| 1478082 | Before each Wi-Fi scan, scan_complete and callback_status are now reset to ensure accurate results. | None |
|
| 1513128 | The default value of client_idle_timeout value is updated from 120000 to 255. | None |
|
| 1385303 | Added support for multiple network interface initialization tracking | None |
|
| 1455151 | Fixed the network manager thread stack overflow during sl_net_deinit() by increasing default stack size to 3072 bytes and making it configurable via NETWORK_MANAGER_THREAD_STACK_SIZE. |
None |
|
| 1402599 | To ensure the TA is also reset during an NCP reset, we are adding a call to sl_wifi_deinit() in the reset handler. | None |
|
| 1467508 | Wi-Fi initialization and deinitialization are managed only by the main application. This change prevents conflicts and ensures reliable operation during firmware updates. No impact to normal operation. | None |
|
| 1321102 | Adding continuous throughput for TCP RX and UDP RX in wifi_station_ble_throughput_app. |
None |
|
| 1407525 | Replaced NVIC_SystemReset() with sl_si91x_soc_nvic_reset() in wireless test example for SoC |
None |
|
| 1499542 | Fix socket shutdown sequence for TCP server socket in the throughput test | None |
|
| 1511479 | Restrict the module from setting the SL_SI91X_EXT_FEAT_FRONT_END_SWITCH_PINS_ULP_GPIO_4_5_0 bit. | None |
|
| 1533724 | Added certificate index for HTTPS GET/POST | None |
|
| 1515226 | Replaced ACX module guard with internal antenna macro in sl_wifi_device.h | None |
|
| 1524218 | Added error handling if any of the configuration is missed in the application. Enhanced MAX PSP is supported when the profile is set to ASSOCIATED_POWER_SAVE_LOW_LATENCY and SL_WIFI_ENABLE_ENHANCED_MAX_PSP bit is enabled in the config feature bitmap. | None |
|
| 1449759 | Added sl_http_server_init |
None |
|
| 1535260 | For open security (SL_WIFI_OPEN), set credential_id to SL_WIFI_NO_CREDENTIAL_ID to avoid unnecessary credential fetch. |
None |
|
| 1456936 | Added sl_net_get_interface_info() and sl_wifi_get_interface_info APIs to retrieve detailed stats for AP and Station interfaces in concurrent Wi-Fi mode. Deprecated sl_wifi_get_wireless_info() due to limited support for multi-interface scenarios. |
None |
|
| 1475983 | Added support to configure the open security type option in examples that use HTTP server feature. | None |
|
| 1425961 | Added a toggle button in the WDT Manager configuration UI to enable or disable the NWP Watchdog Timer (WDT), along with a corresponding value setting for NWP. | None |
|
| 1523410 | Reduced congestion timeout from 400 ms to 30 ms to improve scan efficiency and performance. | None |
|
| 1502519 | Handled a negative scenario where the listen interval aligned with the DTIM beacon. | None |
|
| 1517229 | Fixed a hang in Concurrent Mode where the DUT became unresponsive while attempting to obtain an IPv6 address. | None |
|
| 1532848 | Fixed an issue where DUT incorrectly enabled MFP configuration for AP mode with WPA2 security | None |
|
| 1456765 | Added support to select TKIP cipher suite for WPA connections to access points supporting mixed encryption modes (TKIP+CCMP). | None |
|
| 1462913 | Resolved a stability issue that caused the DUT to hang during continuous DTLS data transfers while operating in WLAN + BLE power save mode on a secure board. | None |
|
| 1435744 | Support added to handle broadcast de-authentication packets in concurrent station mode. | None |
|
| 1405635 | Fixed beacon and broadcast reception issues in congested environments. | None |
|
| 1518842 | Fixed an issue where the module was incorrectly identifying early beacons from the AP, leading to excessive power consumption during long-run tests. | None |
|
Chip Enablement#
Added in 4.0.2#
BRD2708A — supported for the Wireless Test example (see Bug Fixes and Modified Examples).
Added in 4.0.1#
None
Added in 4.0.0#
None
Application Example Changes#
New Examples | Modified Examples | Removed Examples | Deprecated Examples
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
New Examples#
Added in 4.0.2#
None
Added in 4.0.1#
None
Added in 4.0.0#
| Example Name | Description | Supported Software Variants (if applicable) | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Wi-Fi 6 MIMO Throughput See README |
Demonstrates Wi-Fi 6 2x2 MIMO functionality by connecting to a Wi-Fi 6 access point and running throughput tests. | Standard and Lite |
|
|
SPI, UART |
|
WPS Push Button Configuration See README |
Demonstrates using Wi-Fi Protected Setup (WPS) Push Button Configuration (PBC) to connect the device to an access point with minimal user interaction. | Standard and Lite |
|
|
SPI, UART |
|
Access Point V6 See README |
Demonstrates how to set up the device as an IPv6-enabled Wi-Fi Access Point and handle stations joining with IPv6 addresses. | Standard and Lite |
|
|
SPI, UART |
Modified Examples#
Modified in 4.0.2#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Wireless Test
README |
Added support for BRD2708A board for the Wireless Test example. | Standard and Lite |
|
|
SPI, UART |
|
AT Commands
README |
Improved AT command handling and BSD socket setup validation (TCP send path and error handling). | Standard and Lite |
|
|
SPI, UART |
Modified in 4.0.1#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
Flash Read/Write
README |
Updated example to print the data being read and written, improving debug visibility. | Standard and Lite |
|
|
SPI, UART |
|
FW Update Bootloader Xmodem
README |
Improved the firmware upgrade flow by ensuring proper deinitialization of the network before reinitialization after an upgrade. Added error logging for Wi-Fi initialization and deinitialization processes. Ensured cleanup of the network interface before reinitializing following a firmware upgrade. |
Standard and Lite |
|
|
SPI, UART |
Modified in 4.0.0#
| Example Name | Changes | Supported Software Variants if applicable | Supported Modes | Supported OPNs / Boards / OPN Combinations | Supported Host Interfaces |
|---|---|---|---|---|---|
|
AWS Device Shadow See README |
Bug fixes in Wi-Fi connection sequence and error recovery. Improved logging. Minor compatibility improvements. | Standard and Lite |
|
|
SPI, UART |
|
Powersave Standby Associated See README |
Corrected bugs in standby/resume event sequence. Improved standby re-association reliability. | Standard and Lite |
|
|
SPI, UART |
|
Powersave Standby Associated TCP Client See README |
Bug fixes for TCP state handling during and after standby. Enhanced error responses and connection recovery. | Standard and Lite |
|
|
SPI, UART |
|
TWT TCP Client See README |
Addressed issues in Target Wake Time negotiation. Improved fallback handling. Refined power management routines. | Standard and Lite |
|
|
SPI, UART |
|
Wi-Fi Throughput See README |
Resolved packet buffer handling bugs. Fixed callback issues for transmit/receive. Improved throughput reporting stability. Increased the optimization level to O3 for the Wi-Fi Throughput example application to improve the performance with ARM Compiler 6 toolchain. | Standard and Lite |
|
|
SPI |
Removed Examples#
Removed in 4.0.2#
None
Removed in 4.0.1#
None
Removed in 4.0.0#
None
Deprecated Examples#
Deprecated in 4.0.2#
None
Deprecated in 4.0.1#
None
Deprecated in 4.0.0#
None
Known Issues and Limitations#
Note: See the Feature Matrix section for a list of all hardware parts that work with the WiSeConnect SDK.
Added in 4.0.2#
None
Added in 4.0.1#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1607773 | Extended Scan can incorrectly report AP security as WPA2 when the AP is actually configured as WPA/WPA2 Mixed. | None | None |
|
Added in 4.0.0#
| ID | Issue or Limitation Description | GitHub / Salesforce Reference (if any) | Workaround (if any) | Affected Software Variants, Hardware, Modes, Host Interfaces |
|---|---|---|---|---|
| 1451898 | Added validation for SSID, PSK, and PMK lengths in credential and profile management functions to prevent invalid credentials from being set without error. | None | None |
|
| 1494454 | APUT sends deauthentication frames with an unspecified reason to a few stations when 8 stations are connected to it in a congested environment. | None | None |
|
| 1458372 | MCS rates drop in between data transfers causing a reduction in SSL RX throughput. | None | None |
|
| N/A | Command Engine stack overflow can occur if local variables are used in user callback. | None | None |
|
| N/A | When scanning with low-power mode is enabled, a WLAN sensitivity degradation of 3-6 dB is observed, which might prevent access points at longer ranges from appearing in the scan results. | None | None |
|
| 1199044 | Connection issues may be seen with configuring certificate key and programming 4096 bit key and SHA384 / SHA512 certificates in station mode with WPA2 enterprise security. | None | None |
|
| N/A | Less throughput observed in DL-OFDMA with some access points that enabled low-density parity check coding. | None | None |
|
| 1357685 | Extended scan results are not supported with MBSSID feature enabled. | None | None |
|
| 1350997 | Advance Scan is not supported in AP mode. | None | None |
|
| 1454142 | The beacon reception region is elongated before the PS Poll is sent, leading to increased current consumption, under -85 dB RSSI and 70% congestion. | None | None |
|
| 1439592 | SiWx917 power save does not work in station mode when M4 retention is disabled and network processor (NWP) memory is configured at 416 KB or 480 KB. | None | None |
|
| 1443112 | CSA with power save enabled may cause the SiWx917 device to re-join the access point. | None | None |
|
| 1218972 |
When the sl_wifi_enable_target_wake_time API is used, occasional MQTT disconnections may be observed if TWT is configured with longer TWT intervals (>30 seconds) with embedded MQTT + TWT.
|
None |
Use the sl_wifi_target_wake_time_auto_selection API where these dependencies are internally handled.
|
|
| 1569122 | Repeatedly adding and removing two vendor-specific information elements exceeding 40 bytes in length fails. | None | None |
|
| 1569067 | Overriding a vendor-specific IE using a duplicate unique ID in Concurrent Mode causes WLAN connection failure. | None | None |
|
| 1568732 | Vendor-specific IEs are unsupported in BGSCAN probe request frames. | None | None |
|
| 1568490 | Malformed packets are observed when validating vendor-specific information elements in beacons, probe responses, and association responses. | None | None |
|
| 1557787 | Under network congestion, enabling both NAT and PAT features in Concurrent Mode sometimes causes DHCP failures. | None | None |
|
| 1569583 | IPv6 functionality fails in lwip_mqtt_over_tcp application: Global Address and Gateway Address return invalid IPv6 addresses (::), causing MQTT over TCP to fail with error code -1. Link Local Address is correctly assigned, but Global Address remains invalid. | None | None |
|
| 1569213 | AT command at+cal-start fails with error code 4 in at_commands application on SoC with encryption enabled. M4 power save functionality continues to operate correctly despite the command failure. |
None | None |
|
| 1517324 |
Fixed sl_wifi_set_performance_profile() API to prevent data corruption by replacing memcpy between incompatible structures with explicit assignment of listen_interval, monitor_interval, twt_request, and twt_selection fields. Users should migrate to sl_wifi_set_performance_profile_v2() for improved safety and handling.
|
None | None |
|
| 1574418 |
Using slc generate --toolchain gcc or slc generate --with toolchain_gcc may fail with exclusivity errors due to the wiseconnect_toolchain_gcc_standard component incorrectly providing toolchain_gcc, resulting in a conflict with the SiSDK toolchain_gcc component. If using those two command line options results in exclusivity errors, then you can remove them. Note that in a future WiseConnect release, you might have to reintroduce the toolchain option on the command line. Refer to future WiseConnect release notes for updates on possible behavior changes.
| None | None |
|